]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/blackfin/lib/board.c
am33xx/ddr_defs.h: rename DDR2/DDR3 defines to their actual part numbers
[glsdk/glsdk-u-boot.git] / arch / blackfin / lib / board.c
1 /*
2  * U-boot - board.c First C file to be called contains init routines
3  *
4  * Copyright (c) 2005-2008 Analog Devices Inc.
5  *
6  * (C) Copyright 2000-2004
7  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
8  *
9  * Licensed under the GPL-2 or later.
10  */
12 #include <common.h>
13 #include <command.h>
14 #include <stdio_dev.h>
15 #include <serial.h>
16 #include <environment.h>
17 #include <malloc.h>
18 #include <mmc.h>
19 #include <net.h>
20 #include <status_led.h>
21 #include <version.h>
23 #include <asm/cplb.h>
24 #include <asm/mach-common/bits/mpu.h>
25 #include <kgdb.h>
27 #ifdef CONFIG_CMD_NAND
28 #include <nand.h>       /* cannot even include nand.h if it isnt configured */
29 #endif
31 #ifdef CONFIG_BITBANGMII
32 #include <miiphy.h>
33 #endif
35 #if defined(CONFIG_POST)
36 #include <post.h>
37 int post_flag;
38 #endif
40 DECLARE_GLOBAL_DATA_PTR;
42 __attribute__((always_inline))
43 static inline void serial_early_puts(const char *s)
44 {
45 #ifdef CONFIG_DEBUG_EARLY_SERIAL
46         serial_puts("Early: ");
47         serial_puts(s);
48 #endif
49 }
51 static int display_banner(void)
52 {
53         display_options();
54         printf("CPU:   ADSP %s "
55                 "(Detected Rev: 0.%d) "
56                 "(%s boot)\n",
57                 gd->bd->bi_cpu,
58                 bfin_revid(),
59                 get_bfin_boot_mode(CONFIG_BFIN_BOOT_MODE));
60         return 0;
61 }
63 static int init_baudrate(void)
64 {
65         gd->baudrate = getenv_ulong("baudrate", 10, CONFIG_BAUDRATE);
66         return 0;
67 }
69 static void display_global_data(void)
70 {
71         bd_t *bd;
73 #ifndef CONFIG_DEBUG_EARLY_SERIAL
74         return;
75 #endif
77         bd = gd->bd;
78         printf(" gd: %p\n", gd);
79         printf(" |-flags: %lx\n", gd->flags);
80         printf(" |-board_type: %lx\n", gd->board_type);
81         printf(" |-baudrate: %lu\n", gd->baudrate);
82         printf(" |-have_console: %lx\n", gd->have_console);
83         printf(" |-ram_size: %lx\n", gd->ram_size);
84         printf(" |-env_addr: %lx\n", gd->env_addr);
85         printf(" |-env_valid: %lx\n", gd->env_valid);
86         printf(" |-jt(%p): %p\n", gd->jt, *(gd->jt));
87         printf(" \\-bd: %p\n", gd->bd);
88         printf("   |-bi_baudrate: %x\n", bd->bi_baudrate);
89         printf("   |-bi_boot_params: %lx\n", bd->bi_boot_params);
90         printf("   |-bi_memstart: %lx\n", bd->bi_memstart);
91         printf("   |-bi_memsize: %lx\n", bd->bi_memsize);
92         printf("   |-bi_flashstart: %lx\n", bd->bi_flashstart);
93         printf("   |-bi_flashsize: %lx\n", bd->bi_flashsize);
94         printf("   \\-bi_flashoffset: %lx\n", bd->bi_flashoffset);
95 }
97 #define CPLB_PAGE_SIZE (4 * 1024 * 1024)
98 #define CPLB_PAGE_MASK (~(CPLB_PAGE_SIZE - 1))
99 void init_cplbtables(void)
101         volatile uint32_t *ICPLB_ADDR, *ICPLB_DATA;
102         volatile uint32_t *DCPLB_ADDR, *DCPLB_DATA;
103         uint32_t extern_memory;
104         size_t i;
106         void icplb_add(uint32_t addr, uint32_t data)
107         {
108                 *(ICPLB_ADDR + i) = addr;
109                 *(ICPLB_DATA + i) = data;
110         }
111         void dcplb_add(uint32_t addr, uint32_t data)
112         {
113                 *(DCPLB_ADDR + i) = addr;
114                 *(DCPLB_DATA + i) = data;
115         }
117         /* populate a few common entries ... we'll let
118          * the memory map and cplb exception handler do
119          * the rest of the work.
120          */
121         i = 0;
122         ICPLB_ADDR = (uint32_t *)ICPLB_ADDR0;
123         ICPLB_DATA = (uint32_t *)ICPLB_DATA0;
124         DCPLB_ADDR = (uint32_t *)DCPLB_ADDR0;
125         DCPLB_DATA = (uint32_t *)DCPLB_DATA0;
127         icplb_add(0xFFA00000, L1_IMEMORY);
128         dcplb_add(0xFF800000, L1_DMEMORY);
129         ++i;
131         if (CONFIG_MEM_SIZE) {
132                 uint32_t mbase = CONFIG_SYS_MONITOR_BASE;
133                 uint32_t mend  = mbase + CONFIG_SYS_MONITOR_LEN;
134                 mbase &= CPLB_PAGE_MASK;
135                 mend &= CPLB_PAGE_MASK;
137                 icplb_add(mbase, SDRAM_IKERNEL);
138                 dcplb_add(mbase, SDRAM_DKERNEL);
139                 ++i;
141                 /*
142                  * If the monitor crosses a 4 meg boundary, we'll need
143                  * to lock two entries for it.  We assume it doesn't
144                  * cross two 4 meg boundaries ...
145                  */
146                 if (mbase != mend) {
147                         icplb_add(mend, SDRAM_IKERNEL);
148                         dcplb_add(mend, SDRAM_DKERNEL);
149                         ++i;
150                 }
151         }
153         icplb_add(0x20000000, SDRAM_INON_CHBL);
154         dcplb_add(0x20000000, SDRAM_EBIU);
155         ++i;
157         /* Add entries for the rest of external RAM up to the bootrom */
158         extern_memory = 0;
160 #ifdef CONFIG_DEBUG_NULL_PTR
161         icplb_add(extern_memory, (SDRAM_IKERNEL & ~PAGE_SIZE_MASK) | PAGE_SIZE_1KB);
162         dcplb_add(extern_memory, (SDRAM_DKERNEL & ~PAGE_SIZE_MASK) | PAGE_SIZE_1KB);
163         ++i;
164         icplb_add(extern_memory, SDRAM_IKERNEL);
165         dcplb_add(extern_memory, SDRAM_DKERNEL);
166         extern_memory += CPLB_PAGE_SIZE;
167         ++i;
168 #endif
170         while (i < 16 && extern_memory < (CONFIG_SYS_MONITOR_BASE & CPLB_PAGE_MASK)) {
171                 icplb_add(extern_memory, SDRAM_IGENERIC);
172                 dcplb_add(extern_memory, SDRAM_DGENERIC);
173                 extern_memory += CPLB_PAGE_SIZE;
174                 ++i;
175         }
176         while (i < 16) {
177                 icplb_add(0, 0);
178                 dcplb_add(0, 0);
179                 ++i;
180         }
183 static int global_board_data_init(void)
185 #ifndef CONFIG_SYS_GBL_DATA_ADDR
186 # define CONFIG_SYS_GBL_DATA_ADDR 0
187 #endif
188 #ifndef CONFIG_SYS_BD_INFO_ADDR
189 # define CONFIG_SYS_BD_INFO_ADDR 0
190 #endif
192         bd_t *bd;
194         if (CONFIG_SYS_GBL_DATA_ADDR) {
195                 gd = (gd_t *) (CONFIG_SYS_GBL_DATA_ADDR);
196                 memset((void *)gd, 0, GENERATED_GBL_DATA_SIZE);
197         } else {
198                 static gd_t _bfin_gd;
199                 gd = &_bfin_gd;
200         }
202         if (CONFIG_SYS_BD_INFO_ADDR) {
203                 bd = (bd_t *) (CONFIG_SYS_BD_INFO_ADDR);
204                 memset(bd, 0, GENERATED_BD_INFO_SIZE);
205         } else {
206                 static bd_t _bfin_bd;
207                 bd = &_bfin_bd;
208         }
209         gd->bd = bd;
211         bd->bi_r_version = version_string;
212         bd->bi_cpu = __stringify(CONFIG_BFIN_CPU);
213         bd->bi_board_name = BFIN_BOARD_NAME;
214         bd->bi_vco = get_vco();
215         bd->bi_cclk = get_cclk();
216         bd->bi_sclk = get_sclk();
217         bd->bi_memstart = CONFIG_SYS_SDRAM_BASE;
218         bd->bi_memsize = CONFIG_SYS_MAX_RAM_SIZE;
220         return 0;
223 /*
224  * All attempts to come up with a "common" initialization sequence
225  * that works for all boards and architectures failed: some of the
226  * requirements are just _too_ different. To get rid of the resulting
227  * mess of board dependend #ifdef'ed code we now make the whole
228  * initialization sequence configurable to the user.
229  *
230  * The requirements for any new initalization function is simple: it
231  * receives a pointer to the "global data" structure as it's only
232  * argument, and returns an integer return code, where 0 means
233  * "continue" and != 0 means "fatal error, hang the system".
234  */
236 extern int watchdog_init(void);
237 extern int exception_init(void);
238 extern int irq_init(void);
239 extern int timer_init(void);
241 void board_init_f(ulong bootflag)
243         char buf[32];
245 #ifdef CONFIG_BOARD_EARLY_INIT_F
246         serial_early_puts("Board early init flash\n");
247         board_early_init_f();
248 #endif
250         serial_early_puts("Init CPLB tables\n");
251         init_cplbtables();
253         serial_early_puts("Exceptions setup\n");
254         exception_init();
256 #ifndef CONFIG_ICACHE_OFF
257         serial_early_puts("Turn on ICACHE\n");
258         icache_enable();
259 #endif
260 #ifndef CONFIG_DCACHE_OFF
261         serial_early_puts("Turn on DCACHE\n");
262         dcache_enable();
263 #endif
265 #ifdef CONFIG_WATCHDOG
266         serial_early_puts("Setting up external watchdog\n");
267         watchdog_init();
268 #endif
270 #ifdef DEBUG
271         if (GENERATED_GBL_DATA_SIZE < sizeof(*gd))
272                 hang();
273 #endif
274         serial_early_puts("Init global data\n");
276         global_board_data_init();
278         /* Initialize */
279         serial_early_puts("IRQ init\n");
280         irq_init();
281         serial_early_puts("Environment init\n");
282         env_init();
283         serial_early_puts("Baudrate init\n");
284         init_baudrate();
285         serial_early_puts("Serial init\n");
286         serial_init();
287         serial_initialize();
288         serial_early_puts("Console init flash\n");
289         console_init_f();
290         serial_early_puts("End of early debugging\n");
291         display_banner();
293         checkboard();
294         timer_init();
296         printf("Clock: VCO: %s MHz, ", strmhz(buf, get_vco()));
297         printf("Core: %s MHz, ", strmhz(buf, get_cclk()));
298         printf("System: %s MHz\n", strmhz(buf, get_sclk()));
300         if (CONFIG_MEM_SIZE) {
301                 printf("RAM:   ");
302                 print_size(gd->bd->bi_memsize, "\n");
303         }
305 #if defined(CONFIG_POST)
306         post_init_f();
307         post_bootmode_init();
308         post_run(NULL, POST_ROM | post_bootmode_get(0));
309 #endif
311         board_init_r((gd_t *) gd, 0x20000010);
314 static void board_net_init_r(bd_t *bd)
316 #ifdef CONFIG_BITBANGMII
317         bb_miiphy_init();
318 #endif
319 #ifdef CONFIG_CMD_NET
320         printf("Net:   ");
321         eth_initialize(bd);
322 #endif
325 void board_init_r(gd_t * id, ulong dest_addr)
327         bd_t *bd;
328         gd = id;
329         gd->flags |= GD_FLG_RELOC;      /* tell others: relocation done */
330         bd = gd->bd;
332 #if defined(CONFIG_POST)
333         post_output_backlog();
334 #endif
336         /* initialize malloc() area */
337         mem_malloc_init(CONFIG_SYS_MALLOC_BASE, CONFIG_SYS_MALLOC_LEN);
339 #if     !defined(CONFIG_SYS_NO_FLASH)
340         /* Initialize the flash and protect u-boot by default */
341         extern flash_info_t flash_info[];
342         puts("Flash: ");
343         ulong size = flash_init();
344         print_size(size, "\n");
345         flash_protect(FLAG_PROTECT_SET, CONFIG_SYS_FLASH_BASE,
346                 CONFIG_SYS_FLASH_BASE + CONFIG_SYS_MONITOR_LEN - 1,
347                 &flash_info[0]);
348         bd->bi_flashstart = CONFIG_SYS_FLASH_BASE;
349         bd->bi_flashsize = size;
350         bd->bi_flashoffset = 0;
351 #else
352         bd->bi_flashstart = 0;
353         bd->bi_flashsize = 0;
354         bd->bi_flashoffset = 0;
355 #endif
357 #ifdef CONFIG_CMD_NAND
358         puts("NAND:  ");
359         nand_init();            /* go init the NAND */
360 #endif
362 #ifdef CONFIG_GENERIC_MMC
363         puts("MMC:   ");
364         mmc_initialize(bd);
365 #endif
367         /* relocate environment function pointers etc. */
368         env_relocate();
370         /* Initialize stdio devices */
371         stdio_init();
372         jumptable_init();
374         /* Initialize the console (after the relocation and devices init) */
375         console_init_r();
377 #ifdef CONFIG_CMD_KGDB
378         puts("KGDB:  ");
379         kgdb_init();
380 #endif
382 #ifdef CONFIG_STATUS_LED
383         status_led_set(STATUS_LED_BOOT, STATUS_LED_BLINKING);
384         status_led_set(STATUS_LED_CRASH, STATUS_LED_OFF);
385 #endif
387         /* Initialize from environment */
388         load_addr = getenv_ulong("loadaddr", 16, load_addr);
390 #if defined(CONFIG_MISC_INIT_R)
391         /* miscellaneous platform dependent initialisations */
392         misc_init_r();
393 #endif
395         board_net_init_r(bd);
397         display_global_data();
399 #if defined(CONFIG_POST)
400         if (post_flag)
401                 post_run(NULL, POST_RAM | post_bootmode_get(0));
402 #endif
404         if (CONFIG_MEM_SIZE && bfin_os_log_check()) {
405                 puts("\nLog buffer from operating system:\n");
406                 bfin_os_log_dump();
407                 puts("\n");
408         }
410         /* main_loop() can return to retry autoboot, if so just run it again. */
411         for (;;)
412                 main_loop();
415 void hang(void)
417 #ifdef CONFIG_STATUS_LED
418         status_led_set(STATUS_LED_BOOT, STATUS_LED_OFF);
419         status_led_set(STATUS_LED_CRASH, STATUS_LED_BLINKING);
420 #endif
421         puts("### ERROR ### Please RESET the board ###\n");
422         while (1)
423                 /* If a JTAG emulator is hooked up, we'll automatically trigger
424                  * a breakpoint in it.  If one isn't, this is just a NOP.
425                  */
426                 asm("emuexcpt;");