1 /*
2 * (C) Copyright 2002 - 2010
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #ifndef __ASM_GBL_DATA_H
25 #define __ASM_GBL_DATA_H
26 /*
27 * The following data structure is placed in some memory wich is
28 * available very early after boot (like DPRAM on MPC8xx/MPC82xx, or
29 * some locked parts of the data cache) to allow for a minimum set of
30 * global variables during system initialization (until we have set
31 * up the memory controller so that we can use RAM).
32 */
34 typedef struct global_data {
35 bd_t *bd;
36 unsigned long flags;
37 unsigned int baudrate;
38 unsigned long cpu_clk; /* CPU clock in Hz! */
39 unsigned long bus_clk;
40 #ifdef CONFIG_PCI
41 unsigned long pci_clk;
42 #endif
43 #ifdef CONFIG_EXTRA_CLOCK
44 unsigned long inp_clk;
45 unsigned long vco_clk;
46 unsigned long flb_clk;
47 #endif
48 #ifdef CONFIG_FSL_I2C
49 unsigned long i2c1_clk;
50 unsigned long i2c2_clk;
51 #endif
52 phys_size_t ram_size; /* RAM size */
53 unsigned long reloc_off; /* Relocation Offset */
54 unsigned long reset_status; /* reset status register at boot */
55 unsigned long env_addr; /* Address of Environment struct */
56 unsigned long env_valid; /* Checksum of Environment valid? */
57 unsigned long have_console; /* serial_init() was called */
58 #ifdef CONFIG_PRE_CONSOLE_BUFFER
59 unsigned long precon_buf_idx; /* Pre-Console buffer index */
60 #endif
61 #if defined(CONFIG_LCD) || defined(CONFIG_VIDEO)
62 unsigned long fb_base; /* Base addr of framebuffer memory */
63 #endif
64 #ifdef CONFIG_BOARD_TYPES
65 unsigned long board_type;
66 #endif
67 void **jt; /* Standalone app jump table */
68 char env_buf[32]; /* buffer for getenv() before reloc. */
69 } gd_t;
71 #include <asm-generic/global_data_flags.h>
73 #if 0
74 extern gd_t *global_data;
75 #define DECLARE_GLOBAL_DATA_PTR gd_t *gd = global_data
76 #else
77 #define DECLARE_GLOBAL_DATA_PTR register volatile gd_t *gd asm ("d7")
78 #endif
80 #endif /* __ASM_GBL_DATA_H */