1 /*
2 * (C) Copyright 2004 Atmark Techno, Inc.
3 *
4 * Yasushi SHOJI <yashi@atmark-techno.com>
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 *
24 ********************************************************************
25 * NOTE: This header file defines an interface to U-Boot. Including
26 * this (unmodified) header file in another file is considered normal
27 * use of U-Boot, and does *not* fall under the heading of "derived
28 * work".
29 ********************************************************************
30 */
32 #ifndef _U_BOOT_H_
33 #define _U_BOOT_H_
35 typedef struct bd_info {
36 unsigned long bi_memstart; /* start of DRAM memory */
37 phys_size_t bi_memsize; /* size of DRAM memory in bytes */
38 unsigned long bi_flashstart; /* start of FLASH memory */
39 unsigned long bi_flashsize; /* size of FLASH memory */
40 unsigned long bi_flashoffset; /* reserved area for startup monitor */
41 unsigned long bi_sramstart; /* start of SRAM memory */
42 unsigned long bi_sramsize; /* size of SRAM memory */
43 unsigned int bi_baudrate; /* Console Baudrate */
44 } bd_t;
46 /* For image.h:image_check_target_arch() */
47 #define IH_ARCH_DEFAULT IH_ARCH_MICROBLAZE
49 #endif /* _U_BOOT_H_ */