1 /*
2 * Startup Code for MIPS32 XBURST CPU-core
3 *
4 * Copyright (c) 2010 Xiangfu Liu <xiangfu@sharism.cc>
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 */
25 #include <config.h>
26 #include <version.h>
27 #include <asm/regdef.h>
28 #include <asm/mipsregs.h>
29 #include <asm/addrspace.h>
30 #include <asm/cacheops.h>
32 .set noreorder
34 .globl _start
35 .text
36 _start:
37 /* Initialize $gp */
38 bal 1f
39 nop
40 .word _gp
41 1:
42 lw gp, 0(ra)
44 /* Set up temporary stack */
45 li sp, CONFIG_SYS_SDRAM_BASE + CONFIG_SYS_INIT_SP_OFFSET
47 la t9, board_init_f
48 jr t9
49 nop
51 /*
52 * void relocate_code (addr_sp, gd, addr_moni)
53 *
54 * This "function" does not return, instead it continues in RAM
55 * after relocating the monitor code.
56 *
57 * a0 = addr_sp
58 * a1 = gd
59 * a2 = destination address
60 */
61 .globl relocate_code
62 .ent relocate_code
63 relocate_code:
64 move sp, a0 # set new stack pointer
66 li t0, CONFIG_SYS_MONITOR_BASE
67 sub t6, a2, t0 # t6 <-- relocation offset
69 la t3, in_ram
70 lw t2, -12(t3) # t2 <-- __image_copy_end
71 move t1, a2
73 add gp, t6 # adjust gp
75 /*
76 * t0 = source address
77 * t1 = target address
78 * t2 = source end address
79 */
80 1:
81 lw t3, 0(t0)
82 sw t3, 0(t1)
83 addu t0, 4
84 blt t0, t2, 1b
85 addu t1, 4
87 /* If caches were enabled, we would have to flush them here. */
89 /* flush d-cache */
90 li t0, KSEG0
91 addi t1, t0, CONFIG_SYS_DCACHE_SIZE
92 2:
93 cache INDEX_WRITEBACK_INV_D, 0(t0)
94 bne t0, t1, 2b
95 addi t0, CONFIG_SYS_CACHELINE_SIZE
97 sync
99 /* flush i-cache */
100 li t0, KSEG0
101 addi t1, t0, CONFIG_SYS_ICACHE_SIZE
102 3:
103 cache INDEX_INVALIDATE_I, 0(t0)
104 bne t0, t1, 3b
105 addi t0, CONFIG_SYS_CACHELINE_SIZE
107 /* Invalidate BTB */
108 mfc0 t0, CP0_CONFIG, 7
109 nop
110 ori t0, 2
111 mtc0 t0, CP0_CONFIG, 7
112 nop
114 /* Jump to where we've relocated ourselves */
115 addi t0, a2, in_ram - _start
116 jr t0
117 nop
119 .word __rel_dyn_end
120 .word __rel_dyn_start
121 .word __image_copy_end
122 .word _GLOBAL_OFFSET_TABLE_
123 .word num_got_entries
125 in_ram:
126 /*
127 * Now we want to update GOT.
128 *
129 * GOT[0] is reserved. GOT[1] is also reserved for the dynamic object
130 * generated by GNU ld. Skip these reserved entries from relocation.
131 */
132 lw t3, -4(t0) # t3 <-- num_got_entries
133 lw t4, -8(t0) # t4 <-- _GLOBAL_OFFSET_TABLE_
134 add t4, t6 # t4 now holds relocated _G_O_T_
135 addi t4, t4, 8 # skipping first two entries
136 li t2, 2
137 1:
138 lw t1, 0(t4)
139 beqz t1, 2f
140 add t1, t6
141 sw t1, 0(t4)
142 2:
143 addi t2, 1
144 blt t2, t3, 1b
145 addi t4, 4
147 /* Update dynamic relocations */
148 lw t1, -16(t0) # t1 <-- __rel_dyn_start
149 lw t2, -20(t0) # t2 <-- __rel_dyn_end
151 b 2f # skip first reserved entry
152 addi t1, 8
154 1:
155 lw t3, -4(t1) # t3 <-- relocation info
157 sub t3, 3
158 bnez t3, 2f # skip non R_MIPS_REL32 entries
159 nop
161 lw t3, -8(t1) # t3 <-- location to fix up in FLASH
163 lw t4, 0(t3) # t4 <-- original pointer
164 add t4, t6 # t4 <-- adjusted pointer
166 add t3, t6 # t3 <-- location to fix up in RAM
167 sw t4, 0(t3)
169 2:
170 blt t1, t2, 1b
171 addi t1, 8 # each rel.dyn entry is 8 bytes
173 /*
174 * Clear BSS
175 *
176 * GOT is now relocated. Thus __bss_start and __bss_end can be
177 * accessed directly via $gp.
178 */
179 la t1, __bss_start # t1 <-- __bss_start
180 la t2, __bss_end # t2 <-- __bss_end
182 1:
183 sw zero, 0(t1)
184 blt t1, t2, 1b
185 addi t1, 4
187 move a0, a1 # a0 <-- gd
188 la t9, board_init_r
189 jr t9
190 move a1, a2
192 .end relocate_code