1 /*
2 * This file is subject to the terms and conditions of the GNU General Public
3 * License. See the file "COPYING" in the main directory of this archive
4 * for more details.
5 *
6 * Copyright (C) 1995, 1996, 1997, 1999, 2001 by Ralf Baechle
7 * Copyright (C) 1999 by Silicon Graphics, Inc.
8 * Copyright (C) 2001 MIPS Technologies, Inc.
9 * Copyright (C) 2002 Maciej W. Rozycki
10 *
11 * Some useful macros for MIPS assembler code
12 *
13 * Some of the routines below contain useless nops that will be optimized
14 * away by gas in -O mode. These nops are however required to fill delay
15 * slots in noreorder mode.
16 */
17 #ifndef __ASM_ASM_H
18 #define __ASM_ASM_H
20 #include <asm/sgidefs.h>
22 #ifndef CAT
23 #ifdef __STDC__
24 #define __CAT(str1, str2) str1##str2
25 #else
26 #define __CAT(str1, str2) str1/**/str2
27 #endif
28 #define CAT(str1, str2) __CAT(str1, str2)
29 #endif
31 /*
32 * PIC specific declarations
33 * Not used for the kernel but here seems to be the right place.
34 */
35 #ifdef __PIC__
36 #define CPRESTORE(register) \
37 .cprestore register
38 #define CPADD(register) \
39 .cpadd register
40 #define CPLOAD(register) \
41 .cpload register
42 #else
43 #define CPRESTORE(register)
44 #define CPADD(register)
45 #define CPLOAD(register)
46 #endif
48 /*
49 * LEAF - declare leaf routine
50 */
51 #define LEAF(symbol) \
52 .globl symbol; \
53 .align 2; \
54 .type symbol, @function; \
55 .ent symbol, 0; \
56 symbol: .frame sp, 0, ra
58 /*
59 * NESTED - declare nested routine entry point
60 */
61 #define NESTED(symbol, framesize, rpc) \
62 .globl symbol; \
63 .align 2; \
64 .type symbol, @function; \
65 .ent symbol, 0; \
66 symbol: .frame sp, framesize, rpc
68 /*
69 * END - mark end of function
70 */
71 #define END(function) \
72 .end function; \
73 .size function, .-function
75 /*
76 * EXPORT - export definition of symbol
77 */
78 #define EXPORT(symbol) \
79 .globl symbol; \
80 symbol:
82 /*
83 * FEXPORT - export definition of a function symbol
84 */
85 #define FEXPORT(symbol) \
86 .globl symbol; \
87 .type symbol, @function; \
88 symbol:
90 /*
91 * ABS - export absolute symbol
92 */
93 #define ABS(symbol,value) \
94 .globl symbol; \
95 symbol = value
97 #define PANIC(msg) \
98 .set push; \
99 .set reorder; \
100 PTR_LA a0, 8f; \
101 jal panic; \
102 9: b 9b; \
103 .set pop; \
104 TEXT(msg)
106 /*
107 * Print formatted string
108 */
109 #ifdef CONFIG_PRINTK
110 #define PRINT(string) \
111 .set push; \
112 .set reorder; \
113 PTR_LA a0, 8f; \
114 jal printk; \
115 .set pop; \
116 TEXT(string)
117 #else
118 #define PRINT(string)
119 #endif
121 #define TEXT(msg) \
122 .pushsection .data; \
123 8: .asciiz msg; \
124 .popsection;
126 /*
127 * Build text tables
128 */
129 #define TTABLE(string) \
130 .pushsection .text; \
131 .word 1f; \
132 .popsection \
133 .pushsection .data; \
134 1: .asciiz string; \
135 .popsection
137 /*
138 * MIPS IV pref instruction.
139 * Use with .set noreorder only!
140 *
141 * MIPS IV implementations are free to treat this as a nop. The R5000
142 * is one of them. So we should have an option not to use this instruction.
143 */
144 #ifdef CONFIG_CPU_HAS_PREFETCH
146 #define PREF(hint,addr) \
147 .set push; \
148 .set mips4; \
149 pref hint, addr; \
150 .set pop
152 #define PREFX(hint,addr) \
153 .set push; \
154 .set mips4; \
155 prefx hint, addr; \
156 .set pop
158 #else /* !CONFIG_CPU_HAS_PREFETCH */
160 #define PREF(hint, addr)
161 #define PREFX(hint, addr)
163 #endif /* !CONFIG_CPU_HAS_PREFETCH */
165 /*
166 * MIPS ISA IV/V movn/movz instructions and equivalents for older CPUs.
167 */
168 #if (_MIPS_ISA == _MIPS_ISA_MIPS1)
169 #define MOVN(rd, rs, rt) \
170 .set push; \
171 .set reorder; \
172 beqz rt, 9f; \
173 move rd, rs; \
174 .set pop; \
175 9:
176 #define MOVZ(rd, rs, rt) \
177 .set push; \
178 .set reorder; \
179 bnez rt, 9f; \
180 move rd, rs; \
181 .set pop; \
182 9:
183 #endif /* _MIPS_ISA == _MIPS_ISA_MIPS1 */
184 #if (_MIPS_ISA == _MIPS_ISA_MIPS2) || (_MIPS_ISA == _MIPS_ISA_MIPS3)
185 #define MOVN(rd, rs, rt) \
186 .set push; \
187 .set noreorder; \
188 bnezl rt, 9f; \
189 move rd, rs; \
190 .set pop; \
191 9:
192 #define MOVZ(rd, rs, rt) \
193 .set push; \
194 .set noreorder; \
195 beqzl rt, 9f; \
196 move rd, rs; \
197 .set pop; \
198 9:
199 #endif /* (_MIPS_ISA == _MIPS_ISA_MIPS2) || (_MIPS_ISA == _MIPS_ISA_MIPS3) */
200 #if (_MIPS_ISA == _MIPS_ISA_MIPS4 ) || (_MIPS_ISA == _MIPS_ISA_MIPS5) || \
201 (_MIPS_ISA == _MIPS_ISA_MIPS32) || (_MIPS_ISA == _MIPS_ISA_MIPS64)
202 #define MOVN(rd, rs, rt) \
203 movn rd, rs, rt
204 #define MOVZ(rd, rs, rt) \
205 movz rd, rs, rt
206 #endif /* MIPS IV, MIPS V, MIPS32 or MIPS64 */
208 /*
209 * Stack alignment
210 */
211 #if (_MIPS_SIM == _MIPS_SIM_ABI32)
212 #define ALSZ 7
213 #define ALMASK ~7
214 #endif
215 #if (_MIPS_SIM == _MIPS_SIM_NABI32) || (_MIPS_SIM == _MIPS_SIM_ABI64)
216 #define ALSZ 15
217 #define ALMASK ~15
218 #endif
220 /*
221 * Macros to handle different pointer/register sizes for 32/64-bit code
222 */
224 /*
225 * Size of a register
226 */
227 #ifdef __mips64
228 #define SZREG 8
229 #else
230 #define SZREG 4
231 #endif
233 /*
234 * Use the following macros in assemblercode to load/store registers,
235 * pointers etc.
236 */
237 #if (_MIPS_SIM == _MIPS_SIM_ABI32)
238 #define REG_S sw
239 #define REG_L lw
240 #define REG_SUBU subu
241 #define REG_ADDU addu
242 #endif
243 #if (_MIPS_SIM == _MIPS_SIM_NABI32) || (_MIPS_SIM == _MIPS_SIM_ABI64)
244 #define REG_S sd
245 #define REG_L ld
246 #define REG_SUBU dsubu
247 #define REG_ADDU daddu
248 #endif
250 /*
251 * How to add/sub/load/store/shift C int variables.
252 */
253 #if (_MIPS_SZINT == 32)
254 #define INT_ADD add
255 #define INT_ADDU addu
256 #define INT_ADDI addi
257 #define INT_ADDIU addiu
258 #define INT_SUB sub
259 #define INT_SUBU subu
260 #define INT_L lw
261 #define INT_S sw
262 #define INT_SLL sll
263 #define INT_SLLV sllv
264 #define INT_SRL srl
265 #define INT_SRLV srlv
266 #define INT_SRA sra
267 #define INT_SRAV srav
268 #endif
270 #if (_MIPS_SZINT == 64)
271 #define INT_ADD dadd
272 #define INT_ADDU daddu
273 #define INT_ADDI daddi
274 #define INT_ADDIU daddiu
275 #define INT_SUB dsub
276 #define INT_SUBU dsubu
277 #define INT_L ld
278 #define INT_S sd
279 #define INT_SLL dsll
280 #define INT_SLLV dsllv
281 #define INT_SRL dsrl
282 #define INT_SRLV dsrlv
283 #define INT_SRA dsra
284 #define INT_SRAV dsrav
285 #endif
287 /*
288 * How to add/sub/load/store/shift C long variables.
289 */
290 #if (_MIPS_SZLONG == 32)
291 #define LONG_ADD add
292 #define LONG_ADDU addu
293 #define LONG_ADDI addi
294 #define LONG_ADDIU addiu
295 #define LONG_SUB sub
296 #define LONG_SUBU subu
297 #define LONG_L lw
298 #define LONG_S sw
299 #define LONG_SLL sll
300 #define LONG_SLLV sllv
301 #define LONG_SRL srl
302 #define LONG_SRLV srlv
303 #define LONG_SRA sra
304 #define LONG_SRAV srav
306 #define LONG .word
307 #define LONGSIZE 4
308 #define LONGMASK 3
309 #define LONGLOG 2
310 #endif
312 #if (_MIPS_SZLONG == 64)
313 #define LONG_ADD dadd
314 #define LONG_ADDU daddu
315 #define LONG_ADDI daddi
316 #define LONG_ADDIU daddiu
317 #define LONG_SUB dsub
318 #define LONG_SUBU dsubu
319 #define LONG_L ld
320 #define LONG_S sd
321 #define LONG_SLL dsll
322 #define LONG_SLLV dsllv
323 #define LONG_SRL dsrl
324 #define LONG_SRLV dsrlv
325 #define LONG_SRA dsra
326 #define LONG_SRAV dsrav
328 #define LONG .dword
329 #define LONGSIZE 8
330 #define LONGMASK 7
331 #define LONGLOG 3
332 #endif
334 /*
335 * How to add/sub/load/store/shift pointers.
336 */
337 #if (_MIPS_SZPTR == 32)
338 #define PTR_ADD add
339 #define PTR_ADDU addu
340 #define PTR_ADDI addi
341 #define PTR_ADDIU addiu
342 #define PTR_SUB sub
343 #define PTR_SUBU subu
344 #define PTR_L lw
345 #define PTR_S sw
346 #define PTR_LA la
347 #define PTR_LI li
348 #define PTR_SLL sll
349 #define PTR_SLLV sllv
350 #define PTR_SRL srl
351 #define PTR_SRLV srlv
352 #define PTR_SRA sra
353 #define PTR_SRAV srav
355 #define PTR_SCALESHIFT 2
357 #define PTR .word
358 #define PTRSIZE 4
359 #define PTRLOG 2
360 #endif
362 #if (_MIPS_SZPTR == 64)
363 #define PTR_ADD dadd
364 #define PTR_ADDU daddu
365 #define PTR_ADDI daddi
366 #define PTR_ADDIU daddiu
367 #define PTR_SUB dsub
368 #define PTR_SUBU dsubu
369 #define PTR_L ld
370 #define PTR_S sd
371 #define PTR_LA dla
372 #define PTR_LI dli
373 #define PTR_SLL dsll
374 #define PTR_SLLV dsllv
375 #define PTR_SRL dsrl
376 #define PTR_SRLV dsrlv
377 #define PTR_SRA dsra
378 #define PTR_SRAV dsrav
380 #define PTR_SCALESHIFT 3
382 #define PTR .dword
383 #define PTRSIZE 8
384 #define PTRLOG 3
385 #endif
387 /*
388 * Some cp0 registers were extended to 64bit for MIPS III.
389 */
390 #if (_MIPS_SIM == _MIPS_SIM_ABI32)
391 #define MFC0 mfc0
392 #define MTC0 mtc0
393 #endif
394 #if (_MIPS_SIM == _MIPS_SIM_NABI32) || (_MIPS_SIM == _MIPS_SIM_ABI64)
395 #define MFC0 dmfc0
396 #define MTC0 dmtc0
397 #endif
399 #define SSNOP sll zero, zero, 1
401 #ifdef CONFIG_SGI_IP28
402 /* Inhibit speculative stores to volatile (e.g.DMA) or invalid addresses. */
403 #include <asm/cacheops.h>
404 #define R10KCBARRIER(addr) cache Cache_Barrier, addr;
405 #else
406 #define R10KCBARRIER(addr)
407 #endif
409 #endif /* __ASM_ASM_H */