1 /*
2 * (C) Copyright 2003
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #include <common.h>
25 #include <command.h>
26 #include <malloc.h>
27 #include <stdio_dev.h>
28 #include <version.h>
29 #include <net.h>
30 #include <environment.h>
31 #include <nand.h>
32 #include <onenand_uboot.h>
33 #include <spi.h>
35 #ifdef CONFIG_BITBANGMII
36 #include <miiphy.h>
37 #endif
39 DECLARE_GLOBAL_DATA_PTR;
41 ulong monitor_flash_len;
43 static char *failed = "*** failed ***\n";
45 /*
46 * mips_io_port_base is the begin of the address space to which x86 style
47 * I/O ports are mapped.
48 */
49 unsigned long mips_io_port_base = -1;
51 int __board_early_init_f(void)
52 {
53 /*
54 * Nothing to do in this dummy implementation
55 */
56 return 0;
57 }
58 int board_early_init_f(void)
59 __attribute__((weak, alias("__board_early_init_f")));
61 static int init_func_ram(void)
62 {
63 #ifdef CONFIG_BOARD_TYPES
64 int board_type = gd->board_type;
65 #else
66 int board_type = 0; /* use dummy arg */
67 #endif
68 puts("DRAM: ");
70 gd->ram_size = initdram(board_type);
71 if (gd->ram_size > 0) {
72 print_size(gd->ram_size, "\n");
73 return 0;
74 }
75 puts(failed);
76 return 1;
77 }
79 static int display_banner(void)
80 {
82 printf("\n\n%s\n\n", version_string);
83 return 0;
84 }
86 #ifndef CONFIG_SYS_NO_FLASH
87 static void display_flash_config(ulong size)
88 {
89 puts("Flash: ");
90 print_size(size, "\n");
91 }
92 #endif
94 static int init_baudrate(void)
95 {
96 gd->baudrate = getenv_ulong("baudrate", 10, CONFIG_BAUDRATE);
97 return 0;
98 }
101 /*
102 * Breath some life into the board...
103 *
104 * The first part of initialization is running from Flash memory;
105 * its main purpose is to initialize the RAM so that we
106 * can relocate the monitor code to RAM.
107 */
109 /*
110 * All attempts to come up with a "common" initialization sequence
111 * that works for all boards and architectures failed: some of the
112 * requirements are just _too_ different. To get rid of the resulting
113 * mess of board dependend #ifdef'ed code we now make the whole
114 * initialization sequence configurable to the user.
115 *
116 * The requirements for any new initalization function is simple: it
117 * receives a pointer to the "global data" structure as it's only
118 * argument, and returns an integer return code, where 0 means
119 * "continue" and != 0 means "fatal error, hang the system".
120 */
121 typedef int (init_fnc_t)(void);
123 init_fnc_t *init_sequence[] = {
124 board_early_init_f,
125 timer_init,
126 env_init, /* initialize environment */
127 #ifdef CONFIG_INCA_IP
128 incaip_set_cpuclk, /* set cpu clock according to env. variable */
129 #endif
130 init_baudrate, /* initialize baudrate settings */
131 serial_init, /* serial communications setup */
132 console_init_f,
133 display_banner, /* say that we are here */
134 checkboard,
135 init_func_ram,
136 NULL,
137 };
140 void board_init_f(ulong bootflag)
141 {
142 gd_t gd_data, *id;
143 bd_t *bd;
144 init_fnc_t **init_fnc_ptr;
145 ulong addr, addr_sp, len = (ulong)&uboot_end - CONFIG_SYS_MONITOR_BASE;
146 ulong *s;
148 /* Pointer is writable since we allocated a register for it.
149 */
150 gd = &gd_data;
151 /* compiler optimization barrier needed for GCC >= 3.4 */
152 __asm__ __volatile__("" : : : "memory");
154 memset((void *)gd, 0, sizeof(gd_t));
156 for (init_fnc_ptr = init_sequence; *init_fnc_ptr; ++init_fnc_ptr) {
157 if ((*init_fnc_ptr)() != 0)
158 hang();
159 }
161 /*
162 * Now that we have DRAM mapped and working, we can
163 * relocate the code and continue running from DRAM.
164 */
165 addr = CONFIG_SYS_SDRAM_BASE + gd->ram_size;
167 /* We can reserve some RAM "on top" here.
168 */
170 /* round down to next 4 kB limit.
171 */
172 addr &= ~(4096 - 1);
173 debug("Top of RAM usable for U-Boot at: %08lx\n", addr);
175 /* Reserve memory for U-Boot code, data & bss
176 * round down to next 16 kB limit
177 */
178 addr -= len;
179 addr &= ~(16 * 1024 - 1);
181 debug("Reserving %ldk for U-Boot at: %08lx\n", len >> 10, addr);
183 /* Reserve memory for malloc() arena.
184 */
185 addr_sp = addr - TOTAL_MALLOC_LEN;
186 debug("Reserving %dk for malloc() at: %08lx\n",
187 TOTAL_MALLOC_LEN >> 10, addr_sp);
189 /*
190 * (permanently) allocate a Board Info struct
191 * and a permanent copy of the "global" data
192 */
193 addr_sp -= sizeof(bd_t);
194 bd = (bd_t *)addr_sp;
195 gd->bd = bd;
196 debug("Reserving %zu Bytes for Board Info at: %08lx\n",
197 sizeof(bd_t), addr_sp);
199 addr_sp -= sizeof(gd_t);
200 id = (gd_t *)addr_sp;
201 debug("Reserving %zu Bytes for Global Data at: %08lx\n",
202 sizeof(gd_t), addr_sp);
204 /* Reserve memory for boot params.
205 */
206 addr_sp -= CONFIG_SYS_BOOTPARAMS_LEN;
207 bd->bi_boot_params = addr_sp;
208 debug("Reserving %dk for boot params() at: %08lx\n",
209 CONFIG_SYS_BOOTPARAMS_LEN >> 10, addr_sp);
211 /*
212 * Finally, we set up a new (bigger) stack.
213 *
214 * Leave some safety gap for SP, force alignment on 16 byte boundary
215 * Clear initial stack frame
216 */
217 addr_sp -= 16;
218 addr_sp &= ~0xF;
219 s = (ulong *)addr_sp;
220 *s-- = 0;
221 *s-- = 0;
222 addr_sp = (ulong)s;
223 debug("Stack Pointer at: %08lx\n", addr_sp);
225 /*
226 * Save local variables to board info struct
227 */
228 bd->bi_memstart = CONFIG_SYS_SDRAM_BASE; /* start of DRAM */
229 bd->bi_memsize = gd->ram_size; /* size of DRAM in bytes */
230 bd->bi_baudrate = gd->baudrate; /* Console Baudrate */
232 memcpy(id, (void *)gd, sizeof(gd_t));
234 relocate_code(addr_sp, id, addr);
236 /* NOTREACHED - relocate_code() does not return */
237 }
239 /*
240 * This is the next part if the initialization sequence: we are now
241 * running from RAM and have a "normal" C environment, i. e. global
242 * data can be written, BSS has been cleared, the stack size in not
243 * that critical any more, etc.
244 */
246 void board_init_r(gd_t *id, ulong dest_addr)
247 {
248 #ifndef CONFIG_SYS_NO_FLASH
249 ulong size;
250 #endif
251 #ifndef CONFIG_ENV_IS_NOWHERE
252 extern char *env_name_spec;
253 #endif
254 bd_t *bd;
256 gd = id;
257 gd->flags |= GD_FLG_RELOC; /* tell others: relocation done */
259 debug("Now running in RAM - U-Boot at: %08lx\n", dest_addr);
261 gd->reloc_off = dest_addr - CONFIG_SYS_MONITOR_BASE;
263 monitor_flash_len = (ulong)&uboot_end_data - dest_addr;
265 #if defined(CONFIG_NEEDS_MANUAL_RELOC)
266 /*
267 * We have to relocate the command table manually
268 */
269 fixup_cmdtable(ll_entry_start(cmd_tbl_t, cmd),
270 ll_entry_count(cmd_tbl_t, cmd));
271 #endif /* defined(CONFIG_NEEDS_MANUAL_RELOC) */
273 /* there are some other pointer constants we must deal with */
274 #ifndef CONFIG_ENV_IS_NOWHERE
275 env_name_spec += gd->reloc_off;
276 #endif
278 bd = gd->bd;
280 /* The Malloc area is immediately below the monitor copy in DRAM */
281 mem_malloc_init(CONFIG_SYS_MONITOR_BASE + gd->reloc_off -
282 TOTAL_MALLOC_LEN, TOTAL_MALLOC_LEN);
283 malloc_bin_reloc();
285 #ifndef CONFIG_SYS_NO_FLASH
286 /* configure available FLASH banks */
287 size = flash_init();
288 display_flash_config(size);
289 bd->bi_flashstart = CONFIG_SYS_FLASH_BASE;
290 bd->bi_flashsize = size;
292 #if CONFIG_SYS_MONITOR_BASE == CONFIG_SYS_FLASH_BASE
293 bd->bi_flashoffset = monitor_flash_len; /* reserved area for U-Boot */
294 #else
295 bd->bi_flashoffset = 0;
296 #endif
297 #else
298 bd->bi_flashstart = 0;
299 bd->bi_flashsize = 0;
300 bd->bi_flashoffset = 0;
301 #endif
303 #ifdef CONFIG_CMD_NAND
304 puts("NAND: ");
305 nand_init(); /* go init the NAND */
306 #endif
308 #if defined(CONFIG_CMD_ONENAND)
309 onenand_init();
310 #endif
312 /* relocate environment function pointers etc. */
313 env_relocate();
315 #if defined(CONFIG_PCI)
316 /*
317 * Do pci configuration
318 */
319 pci_init();
320 #endif
322 /** leave this here (after malloc(), environment and PCI are working) **/
323 /* Initialize stdio devices */
324 stdio_init();
326 jumptable_init();
328 /* Initialize the console (after the relocation and devices init) */
329 console_init_r();
330 /** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** ** **/
332 /* Initialize from environment */
333 load_addr = getenv_ulong("loadaddr", 16, load_addr);
335 #ifdef CONFIG_CMD_SPI
336 puts("SPI: ");
337 spi_init(); /* go init the SPI */
338 puts("ready\n");
339 #endif
341 #if defined(CONFIG_MISC_INIT_R)
342 /* miscellaneous platform dependent initialisations */
343 misc_init_r();
344 #endif
346 #ifdef CONFIG_BITBANGMII
347 bb_miiphy_init();
348 #endif
349 #if defined(CONFIG_CMD_NET)
350 puts("Net: ");
351 eth_initialize(gd->bd);
352 #endif
354 /* main_loop() can return to retry autoboot, if so just run it again. */
355 for (;;)
356 main_loop();
358 /* NOTREACHED - no way out of command loop except booting */
359 }
361 void hang(void)
362 {
363 puts("### ERROR ### Please RESET the board ###\n");
364 for (;;)
365 ;
366 }