]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/openrisc/include/asm/u-boot.h
Merge remote-tracking branch 'u-boot-ti/master'
[glsdk/glsdk-u-boot.git] / arch / openrisc / include / asm / u-boot.h
1 /*
2  * (C) Copyright 2003
3  * Wolfgang Denk, DENX Software Engineering, <wd@denx.de>
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  *
23  ********************************************************************
24  * NOTE: This header file defines an interface to U-Boot. Including
25  * this (unmodified) header file in another file is considered normal
26  * use of U-Boot, and does *not* fall under the heading of "derived
27  * work".
28  ********************************************************************
29  */
31 #ifndef _U_BOOT_H_
32 #define _U_BOOT_H_
34 typedef struct bd_info {
35         unsigned int    bi_baudrate;    /* serial console baudrate */
36         unsigned long   bi_arch_number; /* unique id for this board */
37         unsigned long   bi_boot_params; /* where this board expects params */
38         unsigned long   bi_memstart;    /* start of DRAM memory */
39         phys_size_t     bi_memsize;     /* size of DRAM memory in bytes */
40         unsigned long   bi_flashstart;  /* start of FLASH memory */
41         unsigned long   bi_flashsize;   /* size  of FLASH memory */
42         unsigned long   bi_flashoffset; /* reserved area for startup monitor */
43 } bd_t;
45 #define IH_ARCH_DEFAULT IH_ARCH_OPENRISC
47 #endif  /* _U_BOOT_H_ */