Merge branch 'master' of git://git.denx.de/u-boot-ppc4xx
[glsdk/glsdk-u-boot.git] / arch / powerpc / config.mk
1 #
2 # (C) Copyright 2000-2002
3 # Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 #
5 # See file CREDITS for list of people who contributed to this
6 # project.
7 #
8 # This program is free software; you can redistribute it and/or
9 # modify it under the terms of the GNU General Public License as
10 # published by the Free Software Foundation; either version 2 of
11 # the License, or (at your option) any later version.
12 #
13 # This program is distributed in the hope that it will be useful,
14 # but WITHOUT ANY WARRANTY; without even the implied warranty of
15 # MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16 # GNU General Public License for more details.
17 #
18 # You should have received a copy of the GNU General Public License
19 # along with this program; if not, write to the Free Software
20 # Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 # MA 02111-1307 USA
22 #
24 CROSS_COMPILE ?= ppc_8xx-
26 STANDALONE_LOAD_ADDR = 0x40000
28 PLATFORM_RELFLAGS += -mrelocatable
29 PLATFORM_CPPFLAGS += -DCONFIG_PPC -D__powerpc__
30 PLATFORM_LDFLAGS  += -n
32 #
33 # When cross-compiling on NetBSD, we have to define __PPC__ or else we
34 # will pick up a va_list declaration that is incompatible with the
35 # actual argument lists emitted by the compiler.
36 #
37 # [Tested on NetBSD/i386 1.5 + cross-powerpc-netbsd-1.3]
39 ifeq ($(CROSS_COMPILE),powerpc-netbsd-)
40 PLATFORM_CPPFLAGS+= -D__PPC__
41 endif
42 ifeq ($(CROSS_COMPILE),powerpc-openbsd-)
43 PLATFORM_CPPFLAGS+= -D__PPC__
44 endif