1 /*
2 * Copyright (c) 2001 Navin Boppuri / Prashant Patel
3 * <nboppuri@trinetcommunication.com>,
4 * <pmpatel@trinetcommunication.com>
5 * Copyright (c) 2001 Gerd Mennchen <Gerd.Mennchen@icn.siemens.de>
6 * Copyright (c) 2001 Wolfgang Denk, DENX Software Engineering, <wd@denx.de>.
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 /*
28 * MPC5xx CPM SPI interface.
29 *
30 * Parts of this code are probably not portable and/or specific to
31 * the board which I used for the tests. Please send fixes/complaints
32 * to wd@denx.de
33 *
34 * Ported to MPC5xx
35 * Copyright (c) 2003 Denis Peter, MPL AG Switzerland, d.petr@mpl.ch.
36 */
38 #include <common.h>
39 #include <mpc5xx.h>
40 #include <asm/5xx_immap.h>
41 #include <linux/ctype.h>
42 #include <malloc.h>
43 #include <post.h>
44 #include <net.h>
46 #if defined(CONFIG_SPI)
48 #undef DEBUG
50 #define SPI_EEPROM_WREN 0x06
51 #define SPI_EEPROM_RDSR 0x05
52 #define SPI_EEPROM_READ 0x03
53 #define SPI_EEPROM_WRITE 0x02
56 #ifdef DEBUG
58 #define DPRINT(a) printf a;
59 /* -----------------------------------------------
60 * Helper functions to peek into tx and rx buffers
61 * ----------------------------------------------- */
62 static const char * const hex_digit = "0123456789ABCDEF";
64 static char quickhex (int i)
65 {
66 return hex_digit[i];
67 }
69 static void memdump (void *pv, int num)
70 {
71 int i;
72 unsigned char *pc = (unsigned char *) pv;
74 for (i = 0; i < num; i++)
75 printf ("%c%c ", quickhex (pc[i] >> 4), quickhex (pc[i] & 0x0f));
76 printf ("\t");
77 for (i = 0; i < num; i++)
78 printf ("%c", isprint (pc[i]) ? pc[i] : '.');
79 printf ("\n");
80 }
81 #else /* !DEBUG */
83 #define DPRINT(a)
85 #endif /* DEBUG */
87 /* -------------------
88 * Function prototypes
89 * ------------------- */
90 void spi_init (void);
92 ssize_t spi_read (uchar *, int, uchar *, int);
93 ssize_t spi_write (uchar *, int, uchar *, int);
94 ssize_t spi_xfer (size_t);
97 /* **************************************************************************
98 *
99 * Function: spi_init_f
100 *
101 * Description: Init SPI-Controller (ROM part)
102 *
103 * return: ---
104 *
105 * *********************************************************************** */
107 void spi_init_f (void)
108 {
109 int i;
111 volatile immap_t *immr;
112 volatile qsmcm5xx_t *qsmcm;
114 immr = (immap_t *) CONFIG_SYS_IMMR;
115 qsmcm = (qsmcm5xx_t *)&immr->im_qsmcm;
117 qsmcm->qsmcm_qsmcr = 0; /* all accesses enabled */
118 qsmcm->qsmcm_qspi_il = 0; /* lowest IRQ */
120 /* --------------------------------------------
121 * GPIO or per. Function
122 * PQSPAR[00] = 0 reserved
123 * PQSPAR[01] = 1 [0x4000] -> PERI: (SPICS3)
124 * PQSPAR[02] = 0 [0x0000] -> GPIO
125 * PQSPAR[03] = 0 [0x0000] -> GPIO
126 * PQSPAR[04] = 1 [0x0800] -> PERI: (SPICS0)
127 * PQSPAR[05] = 0 reseved
128 * PQSPAR[06] = 1 [0x0200] -> PERI: (SPIMOSI)
129 * PQSPAR[07] = 1 [0x0100] -> PERI: (SPIMISO)
130 * -------------------------------------------- */
131 qsmcm->qsmcm_pqspar = 0x3 | (CONFIG_SYS_SPI_CS_USED << 3);
133 /* --------------------------------------------
134 * DDRQS[00] = 0 reserved
135 * DDRQS[01] = 1 [0x0040] -> SPICS3 Output
136 * DDRQS[02] = 0 [0x0000] -> GPIO Output
137 * DDRQS[03] = 0 [0x0000] -> GPIO Output
138 * DDRQS[04] = 1 [0x0008] -> SPICS0 Output
139 * DDRQS[05] = 1 [0x0004] -> SPICLK Output
140 * DDRQS[06] = 1 [0x0002] -> SPIMOSI Output
141 * DDRQS[07] = 0 [0x0001] -> SPIMISO Input
142 * -------------------------------------------- */
143 qsmcm->qsmcm_ddrqs = 0x7E;
144 /* --------------------------------------------
145 * Base state for used SPI CS pins, if base = 0 active must be 1
146 * PORTQS[00] = 0 reserved
147 * PORTQS[01] = 0 reserved
148 * PORTQS[02] = 0 reserved
149 * PORTQS[03] = 0 reserved
150 * PORTQS[04] = 0 [0x0000] RxD2
151 * PORTQS[05] = 1 [0x0400] TxD2
152 * PORTQS[06] = 0 [0x0000] RxD1
153 * PORTQS[07] = 1 [0x0100] TxD1
154 * PORTQS[08] = 0 reserved
155 * PORTQS[09] = 0 [0x0000] -> SPICS3 Base Output
156 * PORTQS[10] = 0 [0x0000] -> SPICS2 Base Output
157 * PORTQS[11] = 0 [0x0000] -> SPICS1 Base Output
158 * PORTQS[12] = 0 [0x0000] -> SPICS0 Base Output
159 * PORTQS[13] = 0 [0x0004] -> SPICLK Output
160 * PORTQS[14] = 0 [0x0002] -> SPIMOSI Output
161 * PORTQS[15] = 0 [0x0001] -> SPIMISO Input
162 * -------------------------------------------- */
163 qsmcm->qsmcm_portqs |= (CONFIG_SYS_SPI_CS_BASE << 3);
164 /* --------------------------------------------
165 * Controll Register 0
166 * SPCR0[00] = 1 (0x8000) Master
167 * SPCR0[01] = 0 (0x0000) Wired-Or
168 * SPCR0[2..5] = (0x2000) Bits per transfer (default 8)
169 * SPCR0[06] = 0 (0x0000) Normal polarity
170 * SPCR0[07] = 0 (0x0000) Normal Clock Phase
171 * SPCR0[08..15] = 14 1.4MHz
172 */
173 qsmcm->qsmcm_spcr0=0xA00E;
174 /* --------------------------------------------
175 * Controll Register 1
176 * SPCR1[00] = 0 (0x0000) QSPI enabled
177 * SPCR1[1..7] = (0x7F00) Delay before Transfer
178 * SPCR1[8..15] = (0x0000) Delay After transfer (204.8usec@40MHz)
179 */
180 qsmcm->qsmcm_spcr1=0x7F00;
181 /* --------------------------------------------
182 * Controll Register 2
183 * SPCR2[00] = 0 (0x0000) SPI IRQs Disabeld
184 * SPCR2[01] = 0 (0x0000) No Wrap around
185 * SPCR2[02] = 0 (0x0000) Wrap to 0
186 * SPCR2[3..7] = (0x0000) End Queue pointer = 0
187 * SPCR2[8..10] = 0 (0x0000) reserved
188 * SPCR2[11..15] = 0 (0x0000) NewQueue Address = 0
189 */
190 qsmcm->qsmcm_spcr2=0x0000;
191 /* --------------------------------------------
192 * Controll Register 3
193 * SPCR3[00..04] = 0 (0x0000) reserved
194 * SPCR3[05] = 0 (0x0000) Feedback disabled
195 * SPCR3[06] = 0 (0x0000) IRQ on HALTA & MODF disabled
196 * SPCR3[07] = 0 (0x0000) Not halted
197 */
198 qsmcm->qsmcm_spcr3=0x00;
199 /* --------------------------------------------
200 * SPSR (Controll Register 3) Read only/ reset Flags 08,09,10
201 * SPCR3[08] = 1 (0x80) QSPI finished
202 * SPCR3[09] = 1 (0x40) Mode Fault Flag
203 * SPCR3[10] = 1 (0x20) HALTA
204 * SPCR3[11..15] = 0 (0x0000) Last executed command
205 */
206 qsmcm->qsmcm_spsr=0xE0;
207 /*-------------------------------------------
208 * Setup RAM
209 */
210 for(i=0;i<32;i++) {
211 qsmcm->qsmcm_recram[i]=0x0000;
212 qsmcm->qsmcm_tranram[i]=0x0000;
213 qsmcm->qsmcm_comdram[i]=0x00;
214 }
215 return;
216 }
218 /* **************************************************************************
219 *
220 * Function: spi_init_r
221 * Dummy, all initializations have been done in spi_init_r
222 * *********************************************************************** */
223 void spi_init_r (void)
224 {
225 return;
227 }
229 /****************************************************************************
230 * Function: spi_write
231 **************************************************************************** */
232 ssize_t short_spi_write (uchar *addr, int alen, uchar *buffer, int len)
233 {
234 int i,dlen;
235 volatile immap_t *immr;
236 volatile qsmcm5xx_t *qsmcm;
238 immr = (immap_t *) CONFIG_SYS_IMMR;
239 qsmcm = (qsmcm5xx_t *)&immr->im_qsmcm;
240 for(i=0;i<32;i++) {
241 qsmcm->qsmcm_recram[i]=0x0000;
242 qsmcm->qsmcm_tranram[i]=0x0000;
243 qsmcm->qsmcm_comdram[i]=0x00;
244 }
245 qsmcm->qsmcm_tranram[0] = SPI_EEPROM_WREN; /* write enable */
246 spi_xfer(1);
247 i=0;
248 qsmcm->qsmcm_tranram[i++] = SPI_EEPROM_WRITE; /* WRITE memory array */
249 qsmcm->qsmcm_tranram[i++] = addr[0];
250 qsmcm->qsmcm_tranram[i++] = addr[1];
252 for(dlen=0;dlen<len;dlen++) {
253 qsmcm->qsmcm_tranram[i+dlen] = buffer[dlen]; /* WRITE memory array */
254 }
255 /* transmit it */
256 spi_xfer(i+dlen);
257 /* ignore received data */
258 for (i = 0; i < 1000; i++) {
259 qsmcm->qsmcm_tranram[0] = SPI_EEPROM_RDSR; /* read status */
260 qsmcm->qsmcm_tranram[1] = 0;
261 spi_xfer(2);
262 if (!(qsmcm->qsmcm_recram[1] & 1)) {
263 break;
264 }
265 udelay(1000);
266 }
267 if (i >= 1000) {
268 printf ("*** spi_write: Time out while writing!\n");
269 }
270 return len;
271 }
273 #define TRANSFER_LEN 16
275 ssize_t spi_write (uchar *addr, int alen, uchar *buffer, int len)
276 {
277 int index,i,newlen;
278 uchar newaddr[2];
279 int curraddr;
281 curraddr=(addr[alen-2]<<8)+addr[alen-1];
282 i=len;
283 index=0;
284 do {
285 newaddr[1]=(curraddr & 0xff);
286 newaddr[0]=((curraddr>>8) & 0xff);
287 if(i>TRANSFER_LEN) {
288 newlen=TRANSFER_LEN;
289 i-=TRANSFER_LEN;
290 }
291 else {
292 newlen=i;
293 i=0;
294 }
295 short_spi_write (newaddr, 2, &buffer[index], newlen);
296 index+=newlen;
297 curraddr+=newlen;
298 }while(i);
299 return (len);
300 }
302 /****************************************************************************
303 * Function: spi_read
304 **************************************************************************** */
305 ssize_t short_spi_read (uchar *addr, int alen, uchar *buffer, int len)
306 {
307 int i;
308 volatile immap_t *immr;
309 volatile qsmcm5xx_t *qsmcm;
311 immr = (immap_t *) CONFIG_SYS_IMMR;
312 qsmcm = (qsmcm5xx_t *)&immr->im_qsmcm;
314 for(i=0;i<32;i++) {
315 qsmcm->qsmcm_recram[i]=0x0000;
316 qsmcm->qsmcm_tranram[i]=0x0000;
317 qsmcm->qsmcm_comdram[i]=0x00;
318 }
319 i=0;
320 qsmcm->qsmcm_tranram[i++] = (SPI_EEPROM_READ); /* READ memory array */
321 qsmcm->qsmcm_tranram[i++] = addr[0] & 0xff;
322 qsmcm->qsmcm_tranram[i++] = addr[1] & 0xff;
323 spi_xfer(3 + len);
324 for(i=0;i<len;i++) {
325 *buffer++=(char)qsmcm->qsmcm_recram[i+3];
326 }
327 return len;
328 }
330 ssize_t spi_read (uchar *addr, int alen, uchar *buffer, int len)
331 {
332 int index,i,newlen;
333 uchar newaddr[2];
334 int curraddr;
336 curraddr=(addr[alen-2]<<8)+addr[alen-1];
337 i=len;
338 index=0;
339 do {
340 newaddr[1]=(curraddr & 0xff);
341 newaddr[0]=((curraddr>>8) & 0xff);
342 if(i>TRANSFER_LEN) {
343 newlen=TRANSFER_LEN;
344 i-=TRANSFER_LEN;
345 }
346 else {
347 newlen=i;
348 i=0;
349 }
350 short_spi_read (newaddr, 2, &buffer[index], newlen);
351 index+=newlen;
352 curraddr+=newlen;
353 }while(i);
354 return (len);
355 }
357 /****************************************************************************
358 * Function: spi_xfer
359 **************************************************************************** */
360 ssize_t spi_xfer (size_t count)
361 {
362 volatile immap_t *immr;
363 volatile qsmcm5xx_t *qsmcm;
364 int i;
365 int tm;
366 ushort status;
367 immr = (immap_t *) CONFIG_SYS_IMMR;
368 qsmcm = (qsmcm5xx_t *)&immr->im_qsmcm;
369 DPRINT (("*** spi_xfer entered count %d***\n",count));
371 /* Set CS for device */
372 for(i=0;i<(count-1);i++)
373 qsmcm->qsmcm_comdram[i] = 0x80 | CONFIG_SYS_SPI_CS_ACT; /* CS3 is connected to the SPI EEPROM */
375 qsmcm->qsmcm_comdram[i] = CONFIG_SYS_SPI_CS_ACT; /* CS3 is connected to the SPI EEPROM */
376 qsmcm->qsmcm_spcr2=((count-1)&0x1F)<<8;
378 DPRINT (("*** spi_xfer: Bytes to be xferred: %d ***\n", count));
380 qsmcm->qsmcm_spsr=0xE0; /* clear all flags */
382 /* start spi transfer */
383 DPRINT (("*** spi_xfer: Performing transfer ...\n"));
384 qsmcm->qsmcm_spcr1 |= 0x8000; /* Start transmit */
386 /* --------------------------------
387 * Wait for SPI transmit to get out
388 * or time out (1 second = 1000 ms)
389 * -------------------------------- */
390 for (tm=0; tm<1000; ++tm) {
391 status=qsmcm->qsmcm_spcr1;
392 if((status & 0x8000)==0)
393 break;
394 udelay (1000);
395 }
396 if (tm >= 1000) {
397 printf ("*** spi_xfer: Time out while xferring to/from SPI!\n");
398 }
399 #ifdef DEBUG
400 printf ("\nspi_xfer: txbuf after xfer\n");
401 memdump ((void *) qsmcm->qsmcm_tranram, 32); /* dump of txbuf before transmit */
402 printf ("spi_xfer: rxbuf after xfer\n");
403 memdump ((void *) qsmcm->qsmcm_recram, 32); /* dump of rxbuf after transmit */
404 printf ("\nspi_xfer: commbuf after xfer\n");
405 memdump ((void *) qsmcm->qsmcm_comdram, 32); /* dump of txbuf before transmit */
406 printf ("\n");
407 #endif
409 return count;
410 }
412 #endif /* CONFIG_SPI */