]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/powerpc/cpu/mpc5xxx/usb_ohci.h
Move arch/ppc to arch/powerpc
[glsdk/glsdk-u-boot.git] / arch / powerpc / cpu / mpc5xxx / usb_ohci.h
1 /*
2  * URB OHCI HCD (Host Controller Driver) for USB.
3  *
4  * (C) Copyright 1999 Roman Weissgaerber <weissg@vienna.at>
5  * (C) Copyright 2000-2001 David Brownell <dbrownell@users.sourceforge.net>
6  *
7  * usb-ohci.h
8  */
11 static int cc_to_error[16] = {
13 /* mapping of the OHCI CC status to error codes */
14         /* No  Error  */               0,
15         /* CRC Error  */               USB_ST_CRC_ERR,
16         /* Bit Stuff  */               USB_ST_BIT_ERR,
17         /* Data Togg  */               USB_ST_CRC_ERR,
18         /* Stall      */               USB_ST_STALLED,
19         /* DevNotResp */               -1,
20         /* PIDCheck   */               USB_ST_BIT_ERR,
21         /* UnExpPID   */               USB_ST_BIT_ERR,
22         /* DataOver   */               USB_ST_BUF_ERR,
23         /* DataUnder  */               USB_ST_BUF_ERR,
24         /* reservd    */               -1,
25         /* reservd    */               -1,
26         /* BufferOver */               USB_ST_BUF_ERR,
27         /* BuffUnder  */               USB_ST_BUF_ERR,
28         /* Not Access */               -1,
29         /* Not Access */               -1
30 };
32 /* ED States */
34 #define ED_NEW          0x00
35 #define ED_UNLINK       0x01
36 #define ED_OPER         0x02
37 #define ED_DEL          0x04
38 #define ED_URB_DEL      0x08
40 /* usb_ohci_ed */
41 struct ed {
42         __u32 hwINFO;
43         __u32 hwTailP;
44         __u32 hwHeadP;
45         __u32 hwNextED;
47         struct ed *ed_prev;
48         __u8 int_period;
49         __u8 int_branch;
50         __u8 int_load;
51         __u8 int_interval;
52         __u8 state;
53         __u8 type;
54         __u16 last_iso;
55         struct ed *ed_rm_list;
57         struct usb_device *usb_dev;
58         __u32 unused[3];
59 } __attribute__((aligned(16)));
60 typedef struct ed ed_t;
63 /* TD info field */
64 #define TD_CC       0xf0000000
65 #define TD_CC_GET(td_p) ((td_p >>28) & 0x0f)
66 #define TD_CC_SET(td_p, cc) (td_p) = ((td_p) & 0x0fffffff) | (((cc) & 0x0f) << 28)
67 #define TD_EC       0x0C000000
68 #define TD_T        0x03000000
69 #define TD_T_DATA0  0x02000000
70 #define TD_T_DATA1  0x03000000
71 #define TD_T_TOGGLE 0x00000000
72 #define TD_R        0x00040000
73 #define TD_DI       0x00E00000
74 #define TD_DI_SET(X) (((X) & 0x07)<< 21)
75 #define TD_DP       0x00180000
76 #define TD_DP_SETUP 0x00000000
77 #define TD_DP_IN    0x00100000
78 #define TD_DP_OUT   0x00080000
80 #define TD_ISO      0x00010000
81 #define TD_DEL      0x00020000
83 /* CC Codes */
84 #define TD_CC_NOERROR      0x00
85 #define TD_CC_CRC          0x01
86 #define TD_CC_BITSTUFFING  0x02
87 #define TD_CC_DATATOGGLEM  0x03
88 #define TD_CC_STALL        0x04
89 #define TD_DEVNOTRESP      0x05
90 #define TD_PIDCHECKFAIL    0x06
91 #define TD_UNEXPECTEDPID   0x07
92 #define TD_DATAOVERRUN     0x08
93 #define TD_DATAUNDERRUN    0x09
94 #define TD_BUFFEROVERRUN   0x0C
95 #define TD_BUFFERUNDERRUN  0x0D
96 #define TD_NOTACCESSED     0x0F
99 #define MAXPSW 1
101 struct td {
102         __u32 hwINFO;
103         __u32 hwCBP;            /* Current Buffer Pointer */
104         __u32 hwNextTD;         /* Next TD Pointer */
105         __u32 hwBE;             /* Memory Buffer End Pointer */
107         __u8 unused;
108         __u8 index;
109         struct ed *ed;
110         struct td *next_dl_td;
111         struct usb_device *usb_dev;
112         int transfer_len;
113         __u32 data;
115         __u32 unused2[2];
116 } __attribute__((aligned(32)));
117 typedef struct td td_t;
119 #define OHCI_ED_SKIP    (1 << 14)
121 /*
122  * The HCCA (Host Controller Communications Area) is a 256 byte
123  * structure defined in the OHCI spec. that the host controller is
124  * told the base address of.  It must be 256-byte aligned.
125  */
127 #define NUM_INTS 32     /* part of the OHCI standard */
128 struct ohci_hcca {
129         __u32   int_table[NUM_INTS];    /* Interrupt ED table */
130         __u16   pad1;                   /* set to 0 on each frame_no change */
131         __u16   frame_no;               /* current frame number */
132         __u32   done_head;              /* info returned for an interrupt */
133         u8              reserved_for_hc[116];
134 } __attribute__((aligned(256)));
137 /*
138  * Maximum number of root hub ports.
139  */
140 #define MAX_ROOT_PORTS  15      /* maximum OHCI root hub ports */
142 /*
143  * This is the structure of the OHCI controller's memory mapped I/O
144  * region.  This is Memory Mapped I/O.  You must use the readl() and
145  * writel() macros defined in asm/io.h to access these!!
146  */
147 struct ohci_regs {
148         /* control and status registers */
149         __u32   revision;
150         __u32   control;
151         __u32   cmdstatus;
152         __u32   intrstatus;
153         __u32   intrenable;
154         __u32   intrdisable;
155         /* memory pointers */
156         __u32   hcca;
157         __u32   ed_periodcurrent;
158         __u32   ed_controlhead;
159         __u32   ed_controlcurrent;
160         __u32   ed_bulkhead;
161         __u32   ed_bulkcurrent;
162         __u32   donehead;
163         /* frame counters */
164         __u32   fminterval;
165         __u32   fmremaining;
166         __u32   fmnumber;
167         __u32   periodicstart;
168         __u32   lsthresh;
169         /* Root hub ports */
170         struct  ohci_roothub_regs {
171                 __u32   a;
172                 __u32   b;
173                 __u32   status;
174                 __u32   portstatus[MAX_ROOT_PORTS];
175         } roothub;
176 } __attribute__((aligned(32)));
179 /* OHCI CONTROL AND STATUS REGISTER MASKS */
181 /*
182  * HcControl (control) register masks
183  */
184 #define OHCI_CTRL_CBSR  (3 << 0)        /* control/bulk service ratio */
185 #define OHCI_CTRL_PLE   (1 << 2)        /* periodic list enable */
186 #define OHCI_CTRL_IE    (1 << 3)        /* isochronous enable */
187 #define OHCI_CTRL_CLE   (1 << 4)        /* control list enable */
188 #define OHCI_CTRL_BLE   (1 << 5)        /* bulk list enable */
189 #define OHCI_CTRL_HCFS  (3 << 6)        /* host controller functional state */
190 #define OHCI_CTRL_IR    (1 << 8)        /* interrupt routing */
191 #define OHCI_CTRL_RWC   (1 << 9)        /* remote wakeup connected */
192 #define OHCI_CTRL_RWE   (1 << 10)       /* remote wakeup enable */
194 /* pre-shifted values for HCFS */
195 #       define OHCI_USB_RESET   (0 << 6)
196 #       define OHCI_USB_RESUME  (1 << 6)
197 #       define OHCI_USB_OPER    (2 << 6)
198 #       define OHCI_USB_SUSPEND (3 << 6)
200 /*
201  * HcCommandStatus (cmdstatus) register masks
202  */
203 #define OHCI_HCR        (1 << 0)        /* host controller reset */
204 #define OHCI_CLF        (1 << 1)        /* control list filled */
205 #define OHCI_BLF        (1 << 2)        /* bulk list filled */
206 #define OHCI_OCR        (1 << 3)        /* ownership change request */
207 #define OHCI_SOC        (3 << 16)       /* scheduling overrun count */
209 /*
210  * masks used with interrupt registers:
211  * HcInterruptStatus (intrstatus)
212  * HcInterruptEnable (intrenable)
213  * HcInterruptDisable (intrdisable)
214  */
215 #define OHCI_INTR_SO    (1 << 0)        /* scheduling overrun */
216 #define OHCI_INTR_WDH   (1 << 1)        /* writeback of done_head */
217 #define OHCI_INTR_SF    (1 << 2)        /* start frame */
218 #define OHCI_INTR_RD    (1 << 3)        /* resume detect */
219 #define OHCI_INTR_UE    (1 << 4)        /* unrecoverable error */
220 #define OHCI_INTR_FNO   (1 << 5)        /* frame number overflow */
221 #define OHCI_INTR_RHSC  (1 << 6)        /* root hub status change */
222 #define OHCI_INTR_OC    (1 << 30)       /* ownership change */
223 #define OHCI_INTR_MIE   (1 << 31)       /* master interrupt enable */
226 /* Virtual Root HUB */
227 struct virt_root_hub {
228         int devnum; /* Address of Root Hub endpoint */
229         void *dev;  /* was urb */
230         void *int_addr;
231         int send;
232         int interval;
233 };
235 /* USB HUB CONSTANTS (not OHCI-specific; see hub.h) */
237 /* destination of request */
238 #define RH_INTERFACE               0x01
239 #define RH_ENDPOINT                0x02
240 #define RH_OTHER                   0x03
242 #define RH_CLASS                   0x20
243 #define RH_VENDOR                  0x40
245 /* Requests: bRequest << 8 | bmRequestType */
246 #define RH_GET_STATUS           0x0080
247 #define RH_CLEAR_FEATURE        0x0100
248 #define RH_SET_FEATURE          0x0300
249 #define RH_SET_ADDRESS          0x0500
250 #define RH_GET_DESCRIPTOR       0x0680
251 #define RH_SET_DESCRIPTOR       0x0700
252 #define RH_GET_CONFIGURATION    0x0880
253 #define RH_SET_CONFIGURATION    0x0900
254 #define RH_GET_STATE            0x0280
255 #define RH_GET_INTERFACE        0x0A80
256 #define RH_SET_INTERFACE        0x0B00
257 #define RH_SYNC_FRAME           0x0C80
258 /* Our Vendor Specific Request */
259 #define RH_SET_EP               0x2000
262 /* Hub port features */
263 #define RH_PORT_CONNECTION         0x00
264 #define RH_PORT_ENABLE             0x01
265 #define RH_PORT_SUSPEND            0x02
266 #define RH_PORT_OVER_CURRENT       0x03
267 #define RH_PORT_RESET              0x04
268 #define RH_PORT_POWER              0x08
269 #define RH_PORT_LOW_SPEED          0x09
271 #define RH_C_PORT_CONNECTION       0x10
272 #define RH_C_PORT_ENABLE           0x11
273 #define RH_C_PORT_SUSPEND          0x12
274 #define RH_C_PORT_OVER_CURRENT     0x13
275 #define RH_C_PORT_RESET            0x14
277 /* Hub features */
278 #define RH_C_HUB_LOCAL_POWER       0x00
279 #define RH_C_HUB_OVER_CURRENT      0x01
281 #define RH_DEVICE_REMOTE_WAKEUP    0x00
282 #define RH_ENDPOINT_STALL          0x01
284 #define RH_ACK                     0x01
285 #define RH_REQ_ERR                 -1
286 #define RH_NACK                    0x00
289 /* OHCI ROOT HUB REGISTER MASKS */
291 /* roothub.portstatus [i] bits */
292 #define RH_PS_CCS            0x00000001         /* current connect status */
293 #define RH_PS_PES            0x00000002         /* port enable status*/
294 #define RH_PS_PSS            0x00000004         /* port suspend status */
295 #define RH_PS_POCI           0x00000008         /* port over current indicator */
296 #define RH_PS_PRS            0x00000010         /* port reset status */
297 #define RH_PS_PPS            0x00000100         /* port power status */
298 #define RH_PS_LSDA           0x00000200         /* low speed device attached */
299 #define RH_PS_CSC            0x00010000         /* connect status change */
300 #define RH_PS_PESC           0x00020000         /* port enable status change */
301 #define RH_PS_PSSC           0x00040000         /* port suspend status change */
302 #define RH_PS_OCIC           0x00080000         /* over current indicator change */
303 #define RH_PS_PRSC           0x00100000         /* port reset status change */
305 /* roothub.status bits */
306 #define RH_HS_LPS            0x00000001         /* local power status */
307 #define RH_HS_OCI            0x00000002         /* over current indicator */
308 #define RH_HS_DRWE           0x00008000         /* device remote wakeup enable */
309 #define RH_HS_LPSC           0x00010000         /* local power status change */
310 #define RH_HS_OCIC           0x00020000         /* over current indicator change */
311 #define RH_HS_CRWE           0x80000000         /* clear remote wakeup enable */
313 /* roothub.b masks */
314 #define RH_B_DR         0x0000ffff              /* device removable flags */
315 #define RH_B_PPCM       0xffff0000              /* port power control mask */
317 /* roothub.a masks */
318 #define RH_A_NDP        (0xff << 0)             /* number of downstream ports */
319 #define RH_A_PSM        (1 << 8)                /* power switching mode */
320 #define RH_A_NPS        (1 << 9)                /* no power switching */
321 #define RH_A_DT         (1 << 10)               /* device type (mbz) */
322 #define RH_A_OCPM       (1 << 11)               /* over current protection mode */
323 #define RH_A_NOCP       (1 << 12)               /* no over current protection */
324 #define RH_A_POTPGT     (0xff << 24)            /* power on to power good time */
326 /* urb */
327 #define N_URB_TD 48
328 typedef struct
330         ed_t *ed;
331         __u16 length;   /* number of tds associated with this request */
332         __u16 td_cnt;   /* number of tds already serviced */
333         int   state;
334         unsigned long pipe;
335         int actual_length;
336         td_t *td[N_URB_TD];     /* list pointer to all corresponding TDs associated with this request */
337 } urb_priv_t;
338 #define URB_DEL 1
340 /*
341  * This is the full ohci controller description
342  *
343  * Note how the "proper" USB information is just
344  * a subset of what the full implementation needs. (Linus)
345  */
348 typedef struct ohci {
349         struct ohci_hcca *hcca;         /* hcca */
350         /*dma_addr_t hcca_dma;*/
352         int irq;
353         int disabled;                   /* e.g. got a UE, we're hung */
354         int sleeping;
355         unsigned long flags;            /* for HC bugs */
357         struct ohci_regs *regs; /* OHCI controller's memory */
359         ed_t *ed_rm_list[2];     /* lists of all endpoints to be removed */
360         ed_t *ed_bulktail;       /* last endpoint of bulk list */
361         ed_t *ed_controltail;    /* last endpoint of control list */
362         int intrstatus;
363         __u32 hc_control;               /* copy of the hc control reg */
364         struct usb_device *dev[32];
365         struct virt_root_hub rh;
367         const char      *slot_name;
368 } ohci_t;
370 #define NUM_EDS 8               /* num of preallocated endpoint descriptors */
372 struct ohci_device {
373         ed_t    ed[NUM_EDS];
374         int ed_cnt;
375 };
377 /* hcd */
378 /* endpoint */
379 static int ep_link(ohci_t * ohci, ed_t * ed);
380 static int ep_unlink(ohci_t * ohci, ed_t * ed);
381 static ed_t * ep_add_ed(struct usb_device * usb_dev, unsigned long pipe);
383 /*-------------------------------------------------------------------------*/
385 /* we need more TDs than EDs */
386 #define NUM_TD 64
388 /* +1 so we can align the storage */
389 td_t gtd[NUM_TD+1];
390 /* pointers to aligned storage */
391 td_t *ptd;
393 /* TDs ... */
394 static inline struct td *
395 td_alloc (struct usb_device *usb_dev)
397         int i;
398         struct td       *td;
400         td = NULL;
401         for (i = 0; i < NUM_TD; i++)
402         {
403                 if (ptd[i].usb_dev == NULL)
404                 {
405                         td = &ptd[i];
406                         td->usb_dev = usb_dev;
407                         break;
408                 }
409         }
411         return td;
414 static inline void
415 ed_free (struct ed *ed)
417         ed->usb_dev = NULL;