1 /*
2 * (C) Copyright 2004, Freescale, Inc
3 * TsiChung Liew, Tsi-Chung.Liew@freescale.com.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #include <common.h>
25 #include <mpc8220.h>
26 #include <asm/processor.h>
28 DECLARE_GLOBAL_DATA_PTR;
30 typedef struct pllmultiplier {
31 u8 hid1;
32 int multi;
33 int vco_div;
34 } pllcfg_t;
36 /* ------------------------------------------------------------------------- */
38 /*
39 *
40 */
42 int get_clocks (void)
43 {
44 pllcfg_t bus2core[] = {
45 {0x02, 2, 8}, /* 1 */
46 {0x01, 2, 4},
47 {0x0C, 3, 8}, /* 1.5 */
48 {0x00, 3, 4},
49 {0x18, 3, 2},
50 {0x05, 4, 4}, /* 2 */
51 {0x04, 4, 2},
52 {0x11, 5, 4}, /* 2.5 */
53 {0x06, 5, 2},
54 {0x10, 6, 4}, /* 3 */
55 {0x08, 6, 2},
56 {0x0E, 7, 2}, /* 3.5 */
57 {0x0A, 8, 2}, /* 4 */
58 {0x07, 9, 2}, /* 4.5 */
59 {0x0B, 10, 2}, /* 5 */
60 {0x09, 11, 2}, /* 5.5 */
61 {0x0D, 12, 2}, /* 6 */
62 {0x12, 13, 2}, /* 6.5 */
63 {0x14, 14, 2}, /* 7 */
64 {0x16, 15, 2}, /* 7.5 */
65 {0x1C, 16, 2} /* 8 */
66 };
67 u32 hid1;
68 int i, size, pci2bus;
70 #if !defined(CONFIG_SYS_MPC8220_CLKIN)
71 #error clock measuring not implemented yet - define CONFIG_SYS_MPC8220_CLKIN
72 #endif
74 gd->inp_clk = CONFIG_SYS_MPC8220_CLKIN;
76 /* Read XLB to PCI(INP) clock multiplier */
77 pci2bus = (*((volatile u32 *)PCI_REG_PCIGSCR) &
78 PCI_REG_PCIGSCR_PCI2XLB_CLK_MASK)>>PCI_REG_PCIGSCR_PCI2XLB_CLK_BIT;
80 /* XLB bus clock */
81 gd->bus_clk = CONFIG_SYS_MPC8220_CLKIN * pci2bus;
83 /* PCI clock is same as input clock */
84 gd->pci_clk = CONFIG_SYS_MPC8220_CLKIN;
86 /* FlexBus is temporary set as the same as input clock */
87 /* will do dynamic in the future */
88 gd->flb_clk = CONFIG_SYS_MPC8220_CLKIN;
90 /* CPU Clock - Read HID1 */
91 asm volatile ("mfspr %0, 1009":"=r" (hid1):);
93 size = sizeof (bus2core) / sizeof (pllcfg_t);
95 hid1 >>= 27;
97 for (i = 0; i < size; i++)
98 if (hid1 == bus2core[i].hid1) {
99 gd->cpu_clk = (bus2core[i].multi * gd->bus_clk) >> 1;
100 gd->vco_clk = CONFIG_SYS_MPC8220_SYSPLL_VCO_MULTIPLIER * (gd->pci_clk * bus2core[i].vco_div)/2;
101 break;
102 }
104 /* hardcoded 81MHz for now */
105 gd->pev_clk = 81000000;
107 return (0);
108 }
110 int prt_mpc8220_clks (void)
111 {
112 char buf1[32], buf2[32], buf3[32], buf4[32];
114 printf (" Bus %s MHz, CPU %s MHz, PCI %s MHz, VCO %s MHz\n",
115 strmhz(buf1, gd->bus_clk),
116 strmhz(buf2, gd->cpu_clk),
117 strmhz(buf3, gd->pci_clk),
118 strmhz(buf4, gd->vco_clk)
119 );
120 return (0);
121 }
123 /* ------------------------------------------------------------------------- */