1 /*
2 * Copyright (C) 1998 Dan Malek <dmalek@jlc.net>
3 * Copyright (C) 1999 Magnus Damm <kieraypc01.p.y.kie.era.ericsson.se>
4 * Copyright (C) 2000,2001,2002 Wolfgang Denk <wd@denx.de>
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 */
25 /* U-Boot - Startup Code for PowerPC based Embedded Boards
26 *
27 *
28 * The processor starts at 0x00000100 and the code is executed
29 * from flash. The code is organized to be at an other address
30 * in memory, but as long we don't jump around before relocating.
31 * board_init lies at a quite high address and when the cpu has
32 * jumped there, everything is ok.
33 * This works because the cpu gives the FLASH (CS0) the whole
34 * address space at startup, and board_init lies as a echo of
35 * the flash somewhere up there in the memorymap.
36 *
37 * board_init will change CS0 to be positioned at the correct
38 * address and (s)dram will be positioned at address 0
39 */
40 #include <config.h>
41 #include <mpc824x.h>
42 #include <timestamp.h>
43 #include <version.h>
45 #define _LINUX_CONFIG_H 1 /* avoid reading Linux autoconf.h file */
47 #include <ppc_asm.tmpl>
48 #include <ppc_defs.h>
50 #include <asm/cache.h>
51 #include <asm/mmu.h>
53 #ifndef CONFIG_IDENT_STRING
54 #define CONFIG_IDENT_STRING ""
55 #endif
57 /* We don't want the MMU yet.
58 */
59 #undef MSR_KERNEL
60 /* FP, Machine Check and Recoverable Interr. */
61 #define MSR_KERNEL ( MSR_FP | MSR_ME | MSR_RI )
63 /*
64 * Set up GOT: Global Offset Table
65 *
66 * Use r12 to access the GOT
67 */
68 START_GOT
69 GOT_ENTRY(_GOT2_TABLE_)
70 GOT_ENTRY(_FIXUP_TABLE_)
72 GOT_ENTRY(_start)
73 GOT_ENTRY(_start_of_vectors)
74 GOT_ENTRY(_end_of_vectors)
75 GOT_ENTRY(transfer_to_handler)
77 GOT_ENTRY(__init_end)
78 GOT_ENTRY(_end)
79 GOT_ENTRY(__bss_start)
80 #if defined(CONFIG_FADS)
81 GOT_ENTRY(environment)
82 #endif
83 END_GOT
85 /*
86 * r3 - 1st arg to board_init(): IMMP pointer
87 * r4 - 2nd arg to board_init(): boot flag
88 */
89 .text
90 .long 0x27051956 /* U-Boot Magic Number */
91 .globl version_string
92 version_string:
93 .ascii U_BOOT_VERSION
94 .ascii " (", U_BOOT_DATE, " - ", U_BOOT_TIME, ")"
95 .ascii CONFIG_IDENT_STRING, "\0"
97 . = EXC_OFF_SYS_RESET
98 .globl _start
99 _start:
100 li r21, BOOTFLAG_COLD /* Normal Power-On: Boot from FLASH */
101 b boot_cold
103 . = EXC_OFF_SYS_RESET + 0x10
105 .globl _start_warm
106 _start_warm:
107 li r21, BOOTFLAG_WARM /* Software reboot */
108 b boot_warm
110 boot_cold:
111 boot_warm:
113 /* Initialize machine status; enable machine check interrupt */
114 /*----------------------------------------------------------------------*/
115 li r3, MSR_KERNEL /* Set FP, ME, RI flags */
116 mtmsr r3
117 mtspr SRR1, r3 /* Make SRR1 match MSR */
119 addis r0,0,0x0000 /* lets make sure that r0 is really 0 */
120 mtspr HID0, r0 /* disable I and D caches */
122 mfspr r3, ICR /* clear Interrupt Cause Register */
124 mfmsr r3 /* turn off address translation */
125 addis r4,0,0xffff
126 ori r4,r4,0xffcf
127 and r3,r3,r4
128 mtmsr r3
129 isync
130 sync /* the MMU should be off... */
133 in_flash:
134 #if defined(CONFIG_BMW)
135 bl early_init_f /* Must be ASM: no stack yet! */
136 #endif
137 /*
138 * Setup BATs - cannot be done in C since we don't have a stack yet
139 */
140 bl setup_bats
142 /* Enable MMU.
143 */
144 mfmsr r3
145 ori r3, r3, (MSR_IR | MSR_DR)
146 mtmsr r3
147 #if !defined(CONFIG_BMW)
148 /* Enable and invalidate data cache.
149 */
150 mfspr r3, HID0
151 mr r2, r3
152 ori r3, r3, HID0_DCE | HID0_DCI
153 ori r2, r2, HID0_DCE
154 sync
155 mtspr HID0, r3
156 mtspr HID0, r2
157 sync
159 /* Allocate Initial RAM in data cache.
160 */
161 lis r3, CONFIG_SYS_INIT_RAM_ADDR@h
162 ori r3, r3, CONFIG_SYS_INIT_RAM_ADDR@l
163 li r2, 128
164 mtctr r2
165 1:
166 dcbz r0, r3
167 addi r3, r3, 32
168 bdnz 1b
170 /* Lock way0 in data cache.
171 */
172 mfspr r3, 1011
173 lis r2, 0xffff
174 ori r2, r2, 0xff1f
175 and r3, r3, r2
176 ori r3, r3, 0x0080
177 sync
178 mtspr 1011, r3
179 #endif /* !CONFIG_BMW */
180 /*
181 * Thisk the stack pointer *somewhere* sensible. Doesnt
182 * matter much where as we'll move it when we relocate
183 */
184 lis r1, (CONFIG_SYS_INIT_RAM_ADDR + CONFIG_SYS_GBL_DATA_OFFSET)@h
185 ori r1, r1, (CONFIG_SYS_INIT_RAM_ADDR + CONFIG_SYS_GBL_DATA_OFFSET)@l
187 li r0, 0 /* Make room for stack frame header and */
188 stwu r0, -4(r1) /* clear final stack frame so that */
189 stwu r0, -4(r1) /* stack backtraces terminate cleanly */
191 /* let the C-code set up the rest */
192 /* */
193 /* Be careful to keep code relocatable ! */
194 /*----------------------------------------------------------------------*/
196 GET_GOT /* initialize GOT access */
198 /* r3: IMMR */
199 bl cpu_init_f /* run low-level CPU init code (from Flash) */
201 mr r3, r21
202 /* r3: BOOTFLAG */
203 bl board_init_f /* run 1st part of board init code (from Flash) */
206 .globl _start_of_vectors
207 _start_of_vectors:
209 /* Machine check */
210 STD_EXCEPTION(EXC_OFF_MACH_CHCK, MachineCheck, MachineCheckException)
212 /* Data Storage exception. "Never" generated on the 860. */
213 STD_EXCEPTION(EXC_OFF_DATA_STOR, DataStorage, UnknownException)
215 /* Instruction Storage exception. "Never" generated on the 860. */
216 STD_EXCEPTION(EXC_OFF_INS_STOR, InstStorage, UnknownException)
218 /* External Interrupt exception. */
219 STD_EXCEPTION(EXC_OFF_EXTERNAL, ExtInterrupt, external_interrupt)
221 /* Alignment exception. */
222 . = EXC_OFF_ALIGN
223 Alignment:
224 EXCEPTION_PROLOG(SRR0, SRR1)
225 mfspr r4,DAR
226 stw r4,_DAR(r21)
227 mfspr r5,DSISR
228 stw r5,_DSISR(r21)
229 addi r3,r1,STACK_FRAME_OVERHEAD
230 EXC_XFER_TEMPLATE(Alignment, AlignmentException, MSR_KERNEL, COPY_EE)
232 /* Program check exception */
233 . = EXC_OFF_PROGRAM
234 ProgramCheck:
235 EXCEPTION_PROLOG(SRR0, SRR1)
236 addi r3,r1,STACK_FRAME_OVERHEAD
237 EXC_XFER_TEMPLATE(ProgramCheck, ProgramCheckException,
238 MSR_KERNEL, COPY_EE)
240 /* No FPU on MPC8xx. This exception is not supposed to happen.
241 */
242 STD_EXCEPTION(EXC_OFF_FPUNAVAIL, FPUnavailable, UnknownException)
244 /* I guess we could implement decrementer, and may have
245 * to someday for timekeeping.
246 */
247 STD_EXCEPTION(EXC_OFF_DECR, Decrementer, timer_interrupt)
248 STD_EXCEPTION(0xa00, Trap_0a, UnknownException)
249 STD_EXCEPTION(0xb00, Trap_0b, UnknownException)
250 STD_EXCEPTION(0xc00, SystemCall, UnknownException)
252 STD_EXCEPTION(EXC_OFF_TRACE, SingleStep, UnknownException)
254 STD_EXCEPTION(EXC_OFF_FPUNASSIST, Trap_0e, UnknownException)
255 STD_EXCEPTION(EXC_OFF_PMI, Trap_0f, UnknownException)
257 STD_EXCEPTION(EXC_OFF_ITME, InstructionTransMiss, UnknownException)
258 STD_EXCEPTION(EXC_OFF_DLTME, DataLoadTransMiss, UnknownException)
259 STD_EXCEPTION(EXC_OFF_DSTME, DataStoreTransMiss, UnknownException)
260 STD_EXCEPTION(EXC_OFF_IABE, InstructionBreakpoint, DebugException)
261 STD_EXCEPTION(EXC_OFF_SMIE, SysManageInt, UnknownException)
262 STD_EXCEPTION(0x1500, Reserved5, UnknownException)
263 STD_EXCEPTION(0x1600, Reserved6, UnknownException)
264 STD_EXCEPTION(0x1700, Reserved7, UnknownException)
265 STD_EXCEPTION(0x1800, Reserved8, UnknownException)
266 STD_EXCEPTION(0x1900, Reserved9, UnknownException)
267 STD_EXCEPTION(0x1a00, ReservedA, UnknownException)
268 STD_EXCEPTION(0x1b00, ReservedB, UnknownException)
269 STD_EXCEPTION(0x1c00, ReservedC, UnknownException)
270 STD_EXCEPTION(0x1d00, ReservedD, UnknownException)
271 STD_EXCEPTION(0x1e00, ReservedE, UnknownException)
272 STD_EXCEPTION(0x1f00, ReservedF, UnknownException)
274 STD_EXCEPTION(EXC_OFF_RMTE, RunModeTrace, UnknownException)
276 .globl _end_of_vectors
277 _end_of_vectors:
280 . = 0x3000
282 /*
283 * This code finishes saving the registers to the exception frame
284 * and jumps to the appropriate handler for the exception.
285 * Register r21 is pointer into trap frame, r1 has new stack pointer.
286 */
287 .globl transfer_to_handler
288 transfer_to_handler:
289 stw r22,_NIP(r21)
290 lis r22,MSR_POW@h
291 andc r23,r23,r22
292 stw r23,_MSR(r21)
293 SAVE_GPR(7, r21)
294 SAVE_4GPRS(8, r21)
295 SAVE_8GPRS(12, r21)
296 SAVE_8GPRS(24, r21)
297 #if 0
298 andi. r23,r23,MSR_PR
299 mfspr r23,SPRG3 /* if from user, fix up tss.regs */
300 beq 2f
301 addi r24,r1,STACK_FRAME_OVERHEAD
302 stw r24,PT_REGS(r23)
303 2: addi r2,r23,-TSS /* set r2 to current */
304 tovirt(r2,r2,r23)
305 #endif
306 mflr r23
307 andi. r24,r23,0x3f00 /* get vector offset */
308 stw r24,TRAP(r21)
309 li r22,0
310 stw r22,RESULT(r21)
311 mtspr SPRG2,r22 /* r1 is now kernel sp */
312 #if 0
313 addi r24,r2,TASK_STRUCT_SIZE /* check for kernel stack overflow */
314 cmplw 0,r1,r2
315 cmplw 1,r1,r24
316 crand 1,1,4
317 bgt stack_ovf /* if r2 < r1 < r2+TASK_STRUCT_SIZE */
318 #endif
319 lwz r24,0(r23) /* virtual address of handler */
320 lwz r23,4(r23) /* where to go when done */
321 mtspr SRR0,r24
322 ori r20,r20,0x30 /* enable IR, DR */
323 mtspr SRR1,r20
324 mtlr r23
325 SYNC
326 rfi /* jump to handler, enable MMU */
328 int_return:
329 mfmsr r28 /* Disable interrupts */
330 li r4,0
331 ori r4,r4,MSR_EE
332 andc r28,r28,r4
333 SYNC /* Some chip revs need this... */
334 mtmsr r28
335 SYNC
336 lwz r2,_CTR(r1)
337 lwz r0,_LINK(r1)
338 mtctr r2
339 mtlr r0
340 lwz r2,_XER(r1)
341 lwz r0,_CCR(r1)
342 mtspr XER,r2
343 mtcrf 0xFF,r0
344 REST_10GPRS(3, r1)
345 REST_10GPRS(13, r1)
346 REST_8GPRS(23, r1)
347 REST_GPR(31, r1)
348 lwz r2,_NIP(r1) /* Restore environment */
349 lwz r0,_MSR(r1)
350 mtspr SRR0,r2
351 mtspr SRR1,r0
352 lwz r0,GPR0(r1)
353 lwz r2,GPR2(r1)
354 lwz r1,GPR1(r1)
355 SYNC
356 rfi
358 /* Cache functions.
359 */
360 .globl icache_enable
361 icache_enable:
362 mfspr r5,HID0 /* turn on the I cache. */
363 ori r5,r5,0x8800 /* Instruction cache only! */
364 addis r6,0,0xFFFF
365 ori r6,r6,0xF7FF
366 and r6,r5,r6 /* clear the invalidate bit */
367 sync
368 mtspr HID0,r5
369 mtspr HID0,r6
370 isync
371 sync
372 blr
374 .globl icache_disable
375 icache_disable:
376 mfspr r5,HID0
377 addis r6,0,0xFFFF
378 ori r6,r6,0x7FFF
379 and r5,r5,r6
380 sync
381 mtspr HID0,r5
382 isync
383 sync
384 blr
386 .globl icache_status
387 icache_status:
388 mfspr r3, HID0
389 srwi r3, r3, 15 /* >>15 & 1=> select bit 16 */
390 andi. r3, r3, 1
391 blr
393 .globl dcache_enable
394 dcache_enable:
395 mfspr r5,HID0 /* turn on the D cache. */
396 ori r5,r5,0x4400 /* Data cache only! */
397 mfspr r4, PVR /* read PVR */
398 srawi r3, r4, 16 /* shift off the least 16 bits */
399 cmpi 0, 0, r3, 0xC /* Check for Max pvr */
400 bne NotMax
401 ori r5,r5,0x0040 /* setting the DCFA bit, for Max rev 1 errata */
402 NotMax:
403 addis r6,0,0xFFFF
404 ori r6,r6,0xFBFF
405 and r6,r5,r6 /* clear the invalidate bit */
406 sync
407 mtspr HID0,r5
408 mtspr HID0,r6
409 isync
410 sync
411 blr
413 .globl dcache_disable
414 dcache_disable:
415 mfspr r5,HID0
416 addis r6,0,0xFFFF
417 ori r6,r6,0xBFFF
418 and r5,r5,r6
419 sync
420 mtspr HID0,r5
421 isync
422 sync
423 blr
425 .globl dcache_status
426 dcache_status:
427 mfspr r3, HID0
428 srwi r3, r3, 14 /* >>14 & 1=> select bit 17 */
429 andi. r3, r3, 1
430 blr
432 .globl dc_read
433 dc_read:
434 /*TODO : who uses this, what should it do?
435 */
436 blr
439 .globl get_pvr
440 get_pvr:
441 mfspr r3, PVR
442 blr
445 /*------------------------------------------------------------------------------*/
447 /*
448 * void relocate_code (addr_sp, gd, addr_moni)
449 *
450 * This "function" does not return, instead it continues in RAM
451 * after relocating the monitor code.
452 *
453 * r3 = dest
454 * r4 = src
455 * r5 = length in bytes
456 * r6 = cachelinesize
457 */
458 .globl relocate_code
459 relocate_code:
461 mr r1, r3 /* Set new stack pointer */
462 mr r9, r4 /* Save copy of Global Data pointer */
463 mr r10, r5 /* Save copy of Destination Address */
465 GET_GOT
466 mr r3, r5 /* Destination Address */
467 #ifdef CONFIG_SYS_RAMBOOT
468 lis r4, CONFIG_SYS_SDRAM_BASE@h /* Source Address */
469 ori r4, r4, CONFIG_SYS_SDRAM_BASE@l
470 #else
471 lis r4, CONFIG_SYS_MONITOR_BASE@h /* Source Address */
472 ori r4, r4, CONFIG_SYS_MONITOR_BASE@l
473 #endif
474 lwz r5, GOT(__init_end)
475 sub r5, r5, r4
476 li r6, CONFIG_SYS_CACHELINE_SIZE /* Cache Line Size */
478 /*
479 * Fix GOT pointer:
480 *
481 * New GOT-PTR = (old GOT-PTR - CONFIG_SYS_MONITOR_BASE) + Destination Address
482 *
483 * Offset:
484 */
485 sub r15, r10, r4
487 /* First our own GOT */
488 add r12, r12, r15
489 /* the the one used by the C code */
490 add r30, r30, r15
492 /*
493 * Now relocate code
494 */
496 cmplw cr1,r3,r4
497 addi r0,r5,3
498 srwi. r0,r0,2
499 beq cr1,4f /* In place copy is not necessary */
500 beq 7f /* Protect against 0 count */
501 mtctr r0
502 bge cr1,2f
504 la r8,-4(r4)
505 la r7,-4(r3)
506 1: lwzu r0,4(r8)
507 stwu r0,4(r7)
508 bdnz 1b
509 b 4f
511 2: slwi r0,r0,2
512 add r8,r4,r0
513 add r7,r3,r0
514 3: lwzu r0,-4(r8)
515 stwu r0,-4(r7)
516 bdnz 3b
518 4:
519 #if !defined(CONFIG_BMW)
520 /* Unlock the data cache and invalidate locked area */
521 xor r0, r0, r0
522 mtspr 1011, r0
523 lis r4, CONFIG_SYS_INIT_RAM_ADDR@h
524 ori r4, r4, CONFIG_SYS_INIT_RAM_ADDR@l
525 li r0, 128
526 mtctr r0
527 41:
528 dcbi r0, r4
529 addi r4, r4, 32
530 bdnz 41b
531 #endif
533 /*
534 * Now flush the cache: note that we must start from a cache aligned
535 * address. Otherwise we might miss one cache line.
536 */
537 cmpwi r6,0
538 add r5,r3,r5
539 beq 7f /* Always flush prefetch queue in any case */
540 subi r0,r6,1
541 andc r3,r3,r0
542 mr r4,r3
543 5: dcbst 0,r4
544 add r4,r4,r6
545 cmplw r4,r5
546 blt 5b
547 sync /* Wait for all dcbst to complete on bus */
548 mr r4,r3
549 6: icbi 0,r4
550 add r4,r4,r6
551 cmplw r4,r5
552 blt 6b
553 7: sync /* Wait for all icbi to complete on bus */
554 isync
556 /*
557 * We are done. Do not return, instead branch to second part of board
558 * initialization, now running from RAM.
559 */
561 addi r0, r10, in_ram - _start + EXC_OFF_SYS_RESET
562 mtlr r0
563 blr
565 in_ram:
567 /*
568 * Relocation Function, r12 point to got2+0x8000
569 *
570 * Adjust got2 pointers, no need to check for 0, this code
571 * already puts a few entries in the table.
572 */
573 li r0,__got2_entries@sectoff@l
574 la r3,GOT(_GOT2_TABLE_)
575 lwz r11,GOT(_GOT2_TABLE_)
576 mtctr r0
577 sub r11,r3,r11
578 addi r3,r3,-4
579 1: lwzu r0,4(r3)
580 cmpwi r0,0
581 beq- 2f
582 add r0,r0,r11
583 stw r0,0(r3)
584 2: bdnz 1b
586 /*
587 * Now adjust the fixups and the pointers to the fixups
588 * in case we need to move ourselves again.
589 */
590 li r0,__fixup_entries@sectoff@l
591 lwz r3,GOT(_FIXUP_TABLE_)
592 cmpwi r0,0
593 mtctr r0
594 addi r3,r3,-4
595 beq 4f
596 3: lwzu r4,4(r3)
597 lwzux r0,r4,r11
598 add r0,r0,r11
599 stw r10,0(r3)
600 stw r0,0(r4)
601 bdnz 3b
602 4:
603 clear_bss:
604 /*
605 * Now clear BSS segment
606 */
607 lwz r3,GOT(__bss_start)
608 lwz r4,GOT(_end)
610 cmplw 0, r3, r4
611 beq 6f
613 li r0, 0
614 5:
615 stw r0, 0(r3)
616 addi r3, r3, 4
617 cmplw 0, r3, r4
618 blt 5b
619 6:
621 mr r3, r9 /* Global Data pointer */
622 mr r4, r10 /* Destination Address */
623 bl board_init_r
625 /*
626 * Copy exception vector code to low memory
627 *
628 * r3: dest_addr
629 * r7: source address, r8: end address, r9: target address
630 */
631 .globl trap_init
632 trap_init:
633 mflr r4 /* save link register */
634 GET_GOT
635 lwz r7, GOT(_start)
636 lwz r8, GOT(_end_of_vectors)
638 li r9, 0x100 /* reset vector always at 0x100 */
640 cmplw 0, r7, r8
641 bgelr /* return if r7>=r8 - just in case */
642 1:
643 lwz r0, 0(r7)
644 stw r0, 0(r9)
645 addi r7, r7, 4
646 addi r9, r9, 4
647 cmplw 0, r7, r8
648 bne 1b
650 /*
651 * relocate `hdlr' and `int_return' entries
652 */
653 li r7, .L_MachineCheck - _start + EXC_OFF_SYS_RESET
654 li r8, Alignment - _start + EXC_OFF_SYS_RESET
655 2:
656 bl trap_reloc
657 addi r7, r7, 0x100 /* next exception vector */
658 cmplw 0, r7, r8
659 blt 2b
661 li r7, .L_Alignment - _start + EXC_OFF_SYS_RESET
662 bl trap_reloc
664 li r7, .L_ProgramCheck - _start + EXC_OFF_SYS_RESET
665 bl trap_reloc
667 li r7, .L_FPUnavailable - _start + EXC_OFF_SYS_RESET
668 li r8, SystemCall - _start + EXC_OFF_SYS_RESET
669 3:
670 bl trap_reloc
671 addi r7, r7, 0x100 /* next exception vector */
672 cmplw 0, r7, r8
673 blt 3b
675 li r7, .L_SingleStep - _start + EXC_OFF_SYS_RESET
676 li r8, _end_of_vectors - _start + EXC_OFF_SYS_RESET
677 4:
678 bl trap_reloc
679 addi r7, r7, 0x100 /* next exception vector */
680 cmplw 0, r7, r8
681 blt 4b
683 mtlr r4 /* restore link register */
684 blr
686 /* Setup the BAT registers.
687 */
688 setup_bats:
689 lis r4, CONFIG_SYS_IBAT0L@h
690 ori r4, r4, CONFIG_SYS_IBAT0L@l
691 lis r3, CONFIG_SYS_IBAT0U@h
692 ori r3, r3, CONFIG_SYS_IBAT0U@l
693 mtspr IBAT0L, r4
694 mtspr IBAT0U, r3
695 isync
697 lis r4, CONFIG_SYS_DBAT0L@h
698 ori r4, r4, CONFIG_SYS_DBAT0L@l
699 lis r3, CONFIG_SYS_DBAT0U@h
700 ori r3, r3, CONFIG_SYS_DBAT0U@l
701 mtspr DBAT0L, r4
702 mtspr DBAT0U, r3
703 isync
705 lis r4, CONFIG_SYS_IBAT1L@h
706 ori r4, r4, CONFIG_SYS_IBAT1L@l
707 lis r3, CONFIG_SYS_IBAT1U@h
708 ori r3, r3, CONFIG_SYS_IBAT1U@l
709 mtspr IBAT1L, r4
710 mtspr IBAT1U, r3
711 isync
713 lis r4, CONFIG_SYS_DBAT1L@h
714 ori r4, r4, CONFIG_SYS_DBAT1L@l
715 lis r3, CONFIG_SYS_DBAT1U@h
716 ori r3, r3, CONFIG_SYS_DBAT1U@l
717 mtspr DBAT1L, r4
718 mtspr DBAT1U, r3
719 isync
721 lis r4, CONFIG_SYS_IBAT2L@h
722 ori r4, r4, CONFIG_SYS_IBAT2L@l
723 lis r3, CONFIG_SYS_IBAT2U@h
724 ori r3, r3, CONFIG_SYS_IBAT2U@l
725 mtspr IBAT2L, r4
726 mtspr IBAT2U, r3
727 isync
729 lis r4, CONFIG_SYS_DBAT2L@h
730 ori r4, r4, CONFIG_SYS_DBAT2L@l
731 lis r3, CONFIG_SYS_DBAT2U@h
732 ori r3, r3, CONFIG_SYS_DBAT2U@l
733 mtspr DBAT2L, r4
734 mtspr DBAT2U, r3
735 isync
737 lis r4, CONFIG_SYS_IBAT3L@h
738 ori r4, r4, CONFIG_SYS_IBAT3L@l
739 lis r3, CONFIG_SYS_IBAT3U@h
740 ori r3, r3, CONFIG_SYS_IBAT3U@l
741 mtspr IBAT3L, r4
742 mtspr IBAT3U, r3
743 isync
745 lis r4, CONFIG_SYS_DBAT3L@h
746 ori r4, r4, CONFIG_SYS_DBAT3L@l
747 lis r3, CONFIG_SYS_DBAT3U@h
748 ori r3, r3, CONFIG_SYS_DBAT3U@l
749 mtspr DBAT3L, r4
750 mtspr DBAT3U, r3
751 isync
753 /* Invalidate TLBs.
754 * -> for (val = 0; val < 0x20000; val+=0x1000)
755 * -> tlbie(val);
756 */
757 lis r3, 0
758 lis r5, 2
760 1:
761 tlbie r3
762 addi r3, r3, 0x1000
763 cmp 0, 0, r3, r5
764 blt 1b
766 blr