1 /*
2 * (C) Copyright 2000, 2001, 2002
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 *
23 * Hacked for MPC8260 by Murray.Jensen@cmst.csiro.au, 19-Oct-00, with
24 * changes based on the file arch/powerpc/mbxboot/m8260_tty.c from the
25 * Linux/PPC sources (m8260_tty.c had no copyright info in it).
26 */
28 /*
29 * Minimal serial functions needed to use one of the SMC ports
30 * as serial console interface.
31 */
33 #include <common.h>
34 #include <mpc8260.h>
35 #include <asm/cpm_8260.h>
36 #include <serial.h>
37 #include <linux/compiler.h>
39 DECLARE_GLOBAL_DATA_PTR;
41 #if defined(CONFIG_CONS_ON_SMC)
43 #if CONFIG_CONS_INDEX == 1 /* Console on SMC1 */
45 #define SMC_INDEX 0
46 #define PROFF_SMC_BASE PROFF_SMC1_BASE
47 #define PROFF_SMC PROFF_SMC1
48 #define CPM_CR_SMC_PAGE CPM_CR_SMC1_PAGE
49 #define CPM_CR_SMC_SBLOCK CPM_CR_SMC1_SBLOCK
50 #define CMXSMR_MASK (CMXSMR_SMC1|CMXSMR_SMC1CS_MSK)
51 #define CMXSMR_VALUE CMXSMR_SMC1CS_BRG7
53 #elif CONFIG_CONS_INDEX == 2 /* Console on SMC2 */
55 #define SMC_INDEX 1
56 #define PROFF_SMC_BASE PROFF_SMC2_BASE
57 #define PROFF_SMC PROFF_SMC2
58 #define CPM_CR_SMC_PAGE CPM_CR_SMC2_PAGE
59 #define CPM_CR_SMC_SBLOCK CPM_CR_SMC2_SBLOCK
60 #define CMXSMR_MASK (CMXSMR_SMC2|CMXSMR_SMC2CS_MSK)
61 #define CMXSMR_VALUE CMXSMR_SMC2CS_BRG8
63 #else
65 #error "console not correctly defined"
67 #endif
69 #if !defined(CONFIG_SYS_SMC_RXBUFLEN)
70 #define CONFIG_SYS_SMC_RXBUFLEN 1
71 #define CONFIG_SYS_MAXIDLE 0
72 #else
73 #if !defined(CONFIG_SYS_MAXIDLE)
74 #error "you must define CONFIG_SYS_MAXIDLE"
75 #endif
76 #endif
78 typedef volatile struct serialbuffer {
79 cbd_t rxbd; /* Rx BD */
80 cbd_t txbd; /* Tx BD */
81 uint rxindex; /* index for next character to read */
82 volatile uchar rxbuf[CONFIG_SYS_SMC_RXBUFLEN];/* rx buffers */
83 volatile uchar txbuf; /* tx buffers */
84 } serialbuffer_t;
86 /* map rs_table index to baud rate generator index */
87 static unsigned char brg_map[] = {
88 6, /* BRG7 for SMC1 */
89 7, /* BRG8 for SMC2 */
90 0, /* BRG1 for SCC1 */
91 1, /* BRG1 for SCC2 */
92 2, /* BRG1 for SCC3 */
93 3, /* BRG1 for SCC4 */
94 };
96 static int mpc8260_smc_serial_init(void)
97 {
98 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
99 volatile smc_t *sp;
100 volatile smc_uart_t *up;
101 volatile cpm8260_t *cp = &(im->im_cpm);
102 uint dpaddr;
103 volatile serialbuffer_t *rtx;
105 /* initialize pointers to SMC */
107 sp = (smc_t *) &(im->im_smc[SMC_INDEX]);
108 *(ushort *)(&im->im_dprambase[PROFF_SMC_BASE]) = PROFF_SMC;
109 up = (smc_uart_t *)&im->im_dprambase[PROFF_SMC];
111 /* Disable transmitter/receiver. */
112 sp->smc_smcmr &= ~(SMCMR_REN | SMCMR_TEN);
114 /* NOTE: I/O port pins are set up via the iop_conf_tab[] table */
116 /* Allocate space for two buffer descriptors in the DP ram.
117 * damm: allocating space after the two buffers for rx/tx data
118 */
120 /* allocate size of struct serialbuffer with bd rx/tx,
121 * buffer rx/tx and rx index
122 */
123 dpaddr = m8260_cpm_dpalloc((sizeof(serialbuffer_t)), 16);
125 rtx = (serialbuffer_t *)&im->im_dprambase[dpaddr];
127 /* Set the physical address of the host memory buffers in
128 * the buffer descriptors.
129 */
130 rtx->rxbd.cbd_bufaddr = (uint) &rtx->rxbuf;
131 rtx->rxbd.cbd_sc = 0;
133 rtx->txbd.cbd_bufaddr = (uint) &rtx->txbuf;
134 rtx->txbd.cbd_sc = 0;
136 /* Set up the uart parameters in the parameter ram. */
137 up->smc_rbase = dpaddr;
138 up->smc_tbase = dpaddr+sizeof(cbd_t);
139 up->smc_rfcr = CPMFCR_EB;
140 up->smc_tfcr = CPMFCR_EB;
141 up->smc_brklen = 0;
142 up->smc_brkec = 0;
143 up->smc_brkcr = 0;
145 /* Set UART mode, 8 bit, no parity, one stop.
146 * Enable receive and transmit.
147 */
148 sp->smc_smcmr = smcr_mk_clen(9) | SMCMR_SM_UART;
150 /* Mask all interrupts and remove anything pending. */
151 sp->smc_smcm = 0;
152 sp->smc_smce = 0xff;
154 /* put the SMC channel into NMSI (non multiplexd serial interface)
155 * mode and wire either BRG7 to SMC1 or BRG8 to SMC2 (15-17).
156 */
157 im->im_cpmux.cmx_smr = (im->im_cpmux.cmx_smr&~CMXSMR_MASK)|CMXSMR_VALUE;
159 /* Set up the baud rate generator. */
160 serial_setbrg ();
162 /* Make the first buffer the only buffer. */
163 rtx->txbd.cbd_sc |= BD_SC_WRAP;
164 rtx->rxbd.cbd_sc |= BD_SC_EMPTY | BD_SC_WRAP;
166 /* single/multi character receive. */
167 up->smc_mrblr = CONFIG_SYS_SMC_RXBUFLEN;
168 up->smc_maxidl = CONFIG_SYS_MAXIDLE;
169 rtx->rxindex = 0;
171 /* Initialize Tx/Rx parameters. */
173 while (cp->cp_cpcr & CPM_CR_FLG) /* wait if cp is busy */
174 ;
176 cp->cp_cpcr = mk_cr_cmd(CPM_CR_SMC_PAGE, CPM_CR_SMC_SBLOCK,
177 0, CPM_CR_INIT_TRX) | CPM_CR_FLG;
179 while (cp->cp_cpcr & CPM_CR_FLG) /* wait if cp is busy */
180 ;
182 /* Enable transmitter/receiver. */
183 sp->smc_smcmr |= SMCMR_REN | SMCMR_TEN;
185 return (0);
186 }
188 static void mpc8260_smc_serial_setbrg(void)
189 {
190 #if defined(CONFIG_CONS_USE_EXTC)
191 m8260_cpm_extcbrg(brg_map[SMC_INDEX], gd->baudrate,
192 CONFIG_CONS_EXTC_RATE, CONFIG_CONS_EXTC_PINSEL);
193 #else
194 m8260_cpm_setbrg(brg_map[SMC_INDEX], gd->baudrate);
195 #endif
196 }
198 static void mpc8260_smc_serial_putc(const char c)
199 {
200 volatile smc_uart_t *up;
201 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
202 volatile serialbuffer_t *rtx;
204 if (c == '\n')
205 serial_putc ('\r');
207 up = (smc_uart_t *)&(im->im_dprambase[PROFF_SMC]);
209 rtx = (serialbuffer_t *)&im->im_dprambase[up->smc_rbase];
211 /* Wait for last character to go. */
212 while (rtx->txbd.cbd_sc & BD_SC_READY & BD_SC_READY)
213 ;
214 rtx->txbuf = c;
215 rtx->txbd.cbd_datlen = 1;
216 rtx->txbd.cbd_sc |= BD_SC_READY;
217 }
219 static int mpc8260_smc_serial_getc(void)
220 {
221 volatile smc_uart_t *up;
222 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
223 volatile serialbuffer_t *rtx;
224 unsigned char c;
226 up = (smc_uart_t *)&(im->im_dprambase[PROFF_SMC]);
228 rtx = (serialbuffer_t *)&im->im_dprambase[up->smc_rbase];
230 /* Wait for character to show up. */
231 while (rtx->rxbd.cbd_sc & BD_SC_EMPTY)
232 ;
234 /* the characters are read one by one,
235 * use the rxindex to know the next char to deliver
236 */
237 c = *(unsigned char *) (rtx->rxbd.cbd_bufaddr + rtx->rxindex);
238 rtx->rxindex++;
240 /* check if all char are readout, then make prepare for next receive */
241 if (rtx->rxindex >= rtx->rxbd.cbd_datlen) {
242 rtx->rxindex = 0;
243 rtx->rxbd.cbd_sc |= BD_SC_EMPTY;
244 }
245 return(c);
246 }
248 static int mpc8260_smc_serial_tstc(void)
249 {
250 volatile smc_uart_t *up;
251 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
252 volatile serialbuffer_t *rtx;
254 up = (smc_uart_t *)&(im->im_dprambase[PROFF_SMC]);
255 rtx = (serialbuffer_t *)&im->im_dprambase[up->smc_rbase];
257 return !(rtx->rxbd.cbd_sc & BD_SC_EMPTY);
258 }
260 static struct serial_device mpc8260_smc_serial_drv = {
261 .name = "mpc8260_smc_uart",
262 .start = mpc8260_smc_serial_init,
263 .stop = NULL,
264 .setbrg = mpc8260_smc_serial_setbrg,
265 .putc = mpc8260_smc_serial_putc,
266 .puts = default_serial_puts,
267 .getc = mpc8260_smc_serial_getc,
268 .tstc = mpc8260_smc_serial_tstc,
269 };
271 void mpc8260_smc_serial_initialize(void)
272 {
273 serial_register(&mpc8260_smc_serial_drv);
274 }
276 __weak struct serial_device *default_serial_console(void)
277 {
278 return &mpc8260_smc_serial_drv;
279 }
280 #endif /* CONFIG_CONS_ON_SMC */
282 #if defined(CONFIG_KGDB_ON_SMC)
284 #if defined(CONFIG_CONS_ON_SMC) && CONFIG_KGDB_INDEX == CONFIG_CONS_INDEX
285 #error Whoops! serial console and kgdb are on the same smc serial port
286 #endif
288 #if CONFIG_KGDB_INDEX == 1 /* KGDB Port on SMC1 */
290 #define KGDB_SMC_INDEX 0
291 #define KGDB_PROFF_SMC_BASE PROFF_SMC1_BASE
292 #define KGDB_PROFF_SMC PROFF_SMC1
293 #define KGDB_CPM_CR_SMC_PAGE CPM_CR_SMC1_PAGE
294 #define KGDB_CPM_CR_SMC_SBLOCK CPM_CR_SMC1_SBLOCK
295 #define KGDB_CMXSMR_MASK (CMXSMR_SMC1|CMXSMR_SMC1CS_MSK)
296 #define KGDB_CMXSMR_VALUE CMXSMR_SMC1CS_BRG7
298 #elif CONFIG_KGDB_INDEX == 2 /* KGDB Port on SMC2 */
300 #define KGDB_SMC_INDEX 1
301 #define KGDB_PROFF_SMC_BASE PROFF_SMC2_BASE
302 #define KGDB_PROFF_SMC PROFF_SMC2
303 #define KGDB_CPM_CR_SMC_PAGE CPM_CR_SMC2_PAGE
304 #define KGDB_CPM_CR_SMC_SBLOCK CPM_CR_SMC2_SBLOCK
305 #define KGDB_CMXSMR_MASK (CMXSMR_SMC2|CMXSMR_SMC2CS_MSK)
306 #define KGDB_CMXSMR_VALUE CMXSMR_SMC2CS_BRG8
308 #else
310 #error "console not correctly defined"
312 #endif
314 void
315 kgdb_serial_init (void)
316 {
317 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
318 volatile smc_t *sp;
319 volatile smc_uart_t *up;
320 volatile cbd_t *tbdf, *rbdf;
321 volatile cpm8260_t *cp = &(im->im_cpm);
322 uint dpaddr, speed = CONFIG_KGDB_BAUDRATE;
323 char *s, *e;
325 if ((s = getenv("kgdbrate")) != NULL && *s != '\0') {
326 ulong rate = simple_strtoul(s, &e, 10);
327 if (e > s && *e == '\0')
328 speed = rate;
329 }
331 /* initialize pointers to SMC */
333 sp = (smc_t *) &(im->im_smc[KGDB_SMC_INDEX]);
334 *(ushort *)(&im->im_dprambase[KGDB_PROFF_SMC_BASE]) = KGDB_PROFF_SMC;
335 up = (smc_uart_t *)&im->im_dprambase[KGDB_PROFF_SMC];
337 /* Disable transmitter/receiver. */
338 sp->smc_smcmr &= ~(SMCMR_REN | SMCMR_TEN);
340 /* NOTE: I/O port pins are set up via the iop_conf_tab[] table */
342 /* Allocate space for two buffer descriptors in the DP ram.
343 * damm: allocating space after the two buffers for rx/tx data
344 */
346 dpaddr = m8260_cpm_dpalloc((2 * sizeof (cbd_t)) + 2, 16);
348 /* Set the physical address of the host memory buffers in
349 * the buffer descriptors.
350 */
351 rbdf = (cbd_t *)&im->im_dprambase[dpaddr];
352 rbdf->cbd_bufaddr = (uint) (rbdf+2);
353 rbdf->cbd_sc = 0;
354 tbdf = rbdf + 1;
355 tbdf->cbd_bufaddr = ((uint) (rbdf+2)) + 1;
356 tbdf->cbd_sc = 0;
358 /* Set up the uart parameters in the parameter ram. */
359 up->smc_rbase = dpaddr;
360 up->smc_tbase = dpaddr+sizeof(cbd_t);
361 up->smc_rfcr = CPMFCR_EB;
362 up->smc_tfcr = CPMFCR_EB;
363 up->smc_brklen = 0;
364 up->smc_brkec = 0;
365 up->smc_brkcr = 0;
367 /* Set UART mode, 8 bit, no parity, one stop.
368 * Enable receive and transmit.
369 */
370 sp->smc_smcmr = smcr_mk_clen(9) | SMCMR_SM_UART;
372 /* Mask all interrupts and remove anything pending. */
373 sp->smc_smcm = 0;
374 sp->smc_smce = 0xff;
376 /* put the SMC channel into NMSI (non multiplexd serial interface)
377 * mode and wire either BRG7 to SMC1 or BRG8 to SMC2 (15-17).
378 */
379 im->im_cpmux.cmx_smr =
380 (im->im_cpmux.cmx_smr & ~KGDB_CMXSMR_MASK) | KGDB_CMXSMR_VALUE;
382 /* Set up the baud rate generator. */
383 #if defined(CONFIG_KGDB_USE_EXTC)
384 m8260_cpm_extcbrg(brg_map[KGDB_SMC_INDEX], speed,
385 CONFIG_KGDB_EXTC_RATE, CONFIG_KGDB_EXTC_PINSEL);
386 #else
387 m8260_cpm_setbrg(brg_map[KGDB_SMC_INDEX], speed);
388 #endif
390 /* Make the first buffer the only buffer. */
391 tbdf->cbd_sc |= BD_SC_WRAP;
392 rbdf->cbd_sc |= BD_SC_EMPTY | BD_SC_WRAP;
394 /* Single character receive. */
395 up->smc_mrblr = 1;
396 up->smc_maxidl = 0;
398 /* Initialize Tx/Rx parameters. */
400 while (cp->cp_cpcr & CPM_CR_FLG) /* wait if cp is busy */
401 ;
403 cp->cp_cpcr = mk_cr_cmd(KGDB_CPM_CR_SMC_PAGE, KGDB_CPM_CR_SMC_SBLOCK,
404 0, CPM_CR_INIT_TRX) | CPM_CR_FLG;
406 while (cp->cp_cpcr & CPM_CR_FLG) /* wait if cp is busy */
407 ;
409 /* Enable transmitter/receiver. */
410 sp->smc_smcmr |= SMCMR_REN | SMCMR_TEN;
412 printf("SMC%d at %dbps ", CONFIG_KGDB_INDEX, speed);
413 }
415 void
416 putDebugChar(const char c)
417 {
418 volatile cbd_t *tbdf;
419 volatile char *buf;
420 volatile smc_uart_t *up;
421 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
423 if (c == '\n')
424 putDebugChar ('\r');
426 up = (smc_uart_t *)&(im->im_dprambase[KGDB_PROFF_SMC]);
428 tbdf = (cbd_t *)&im->im_dprambase[up->smc_tbase];
430 /* Wait for last character to go. */
431 buf = (char *)tbdf->cbd_bufaddr;
432 while (tbdf->cbd_sc & BD_SC_READY)
433 ;
435 *buf = c;
436 tbdf->cbd_datlen = 1;
437 tbdf->cbd_sc |= BD_SC_READY;
438 }
440 void
441 putDebugStr (const char *s)
442 {
443 while (*s) {
444 putDebugChar (*s++);
445 }
446 }
448 int
449 getDebugChar(void)
450 {
451 volatile cbd_t *rbdf;
452 volatile unsigned char *buf;
453 volatile smc_uart_t *up;
454 volatile immap_t *im = (immap_t *)CONFIG_SYS_IMMR;
455 unsigned char c;
457 up = (smc_uart_t *)&(im->im_dprambase[KGDB_PROFF_SMC]);
459 rbdf = (cbd_t *)&im->im_dprambase[up->smc_rbase];
461 /* Wait for character to show up. */
462 buf = (unsigned char *)rbdf->cbd_bufaddr;
463 while (rbdf->cbd_sc & BD_SC_EMPTY)
464 ;
465 c = *buf;
466 rbdf->cbd_sc |= BD_SC_EMPTY;
468 return(c);
469 }
471 void
472 kgdb_interruptible(int yes)
473 {
474 return;
475 }
477 #endif /* CONFIG_KGDB_ON_SMC */