1 /*
2 * Copyright (c) 2001 Navin Boppuri / Prashant Patel
3 * <nboppuri@trinetcommunication.com>,
4 * <pmpatel@trinetcommunication.com>
5 * Copyright (c) 2001 Gerd Mennchen <Gerd.Mennchen@icn.siemens.de>
6 * Copyright (c) 2001-2003 Wolfgang Denk, DENX Software Engineering, <wd@denx.de>.
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 /*
28 * MPC8260 CPM SPI interface.
29 *
30 * Parts of this code are probably not portable and/or specific to
31 * the board which I used for the tests. Please send fixes/complaints
32 * to wd@denx.de
33 *
34 */
36 #include <common.h>
37 #include <asm/cpm_8260.h>
38 #include <linux/ctype.h>
39 #include <malloc.h>
40 #include <post.h>
41 #include <net.h>
43 #if defined(CONFIG_SPI)
45 /* Warning:
46 * You cannot enable DEBUG for early system initalization, i. e. when
47 * this driver is used to read environment parameters like "baudrate"
48 * from EEPROM which are used to initialize the serial port which is
49 * needed to print the debug messages...
50 */
51 #undef DEBUG
53 #define SPI_EEPROM_WREN 0x06
54 #define SPI_EEPROM_RDSR 0x05
55 #define SPI_EEPROM_READ 0x03
56 #define SPI_EEPROM_WRITE 0x02
58 /* ---------------------------------------------------------------
59 * Offset for initial SPI buffers in DPRAM:
60 * We need a 520 byte scratch DPRAM area to use at an early stage.
61 * It is used between the two initialization calls (spi_init_f()
62 * and spi_init_r()).
63 * The value 0x2000 makes it far enough from the start of the data
64 * area (as well as from the stack pointer).
65 * --------------------------------------------------------------- */
66 #ifndef CONFIG_SYS_SPI_INIT_OFFSET
67 #define CONFIG_SYS_SPI_INIT_OFFSET 0x2000
68 #endif
70 #define CPM_SPI_BASE 0x100
72 #ifdef DEBUG
74 #define DPRINT(a) printf a;
75 /* -----------------------------------------------
76 * Helper functions to peek into tx and rx buffers
77 * ----------------------------------------------- */
78 static const char * const hex_digit = "0123456789ABCDEF";
80 static char quickhex (int i)
81 {
82 return hex_digit[i];
83 }
85 static void memdump (void *pv, int num)
86 {
87 int i;
88 unsigned char *pc = (unsigned char *) pv;
90 for (i = 0; i < num; i++)
91 printf ("%c%c ", quickhex (pc[i] >> 4), quickhex (pc[i] & 0x0f));
92 printf ("\t");
93 for (i = 0; i < num; i++)
94 printf ("%c", isprint (pc[i]) ? pc[i] : '.');
95 printf ("\n");
96 }
97 #else /* !DEBUG */
99 #define DPRINT(a)
101 #endif /* DEBUG */
103 /* -------------------
104 * Function prototypes
105 * ------------------- */
106 void spi_init (void);
108 ssize_t spi_read (uchar *, int, uchar *, int);
109 ssize_t spi_write (uchar *, int, uchar *, int);
110 ssize_t spi_xfer (size_t);
112 /* -------------------
113 * Variables
114 * ------------------- */
116 #define MAX_BUFFER 0x104
118 /* ----------------------------------------------------------------------
119 * Initially we place the RX and TX buffers at a fixed location in DPRAM!
120 * ---------------------------------------------------------------------- */
121 static uchar *rxbuf =
122 (uchar *)&((immap_t *)CONFIG_SYS_IMMR)->im_dprambase
123 [CONFIG_SYS_SPI_INIT_OFFSET];
124 static uchar *txbuf =
125 (uchar *)&((immap_t *)CONFIG_SYS_IMMR)->im_dprambase
126 [CONFIG_SYS_SPI_INIT_OFFSET+MAX_BUFFER];
128 /* **************************************************************************
129 *
130 * Function: spi_init_f
131 *
132 * Description: Init SPI-Controller (ROM part)
133 *
134 * return: ---
135 *
136 * *********************************************************************** */
137 void spi_init_f (void)
138 {
139 unsigned int dpaddr;
141 volatile spi_t *spi;
142 volatile immap_t *immr;
143 volatile cpm8260_t *cp;
144 volatile cbd_t *tbdf, *rbdf;
146 immr = (immap_t *) CONFIG_SYS_IMMR;
147 cp = (cpm8260_t *) &immr->im_cpm;
149 *(ushort *)(&immr->im_dprambase[PROFF_SPI_BASE]) = PROFF_SPI;
150 spi = (spi_t *)&immr->im_dprambase[PROFF_SPI];
152 /* 1 */
153 /* ------------------------------------------------
154 * Initialize Port D SPI pins
155 * (we are only in Master Mode !)
156 * ------------------------------------------------ */
158 /* --------------------------------------------
159 * GPIO or per. Function
160 * PPARD[16] = 1 [0x00008000] (SPIMISO)
161 * PPARD[17] = 1 [0x00004000] (SPIMOSI)
162 * PPARD[18] = 1 [0x00002000] (SPICLK)
163 * PPARD[12] = 0 [0x00080000] -> GPIO: (CS for ATC EEPROM)
164 * -------------------------------------------- */
165 immr->im_ioport.iop_ppard |= 0x0000E000; /* set bits */
166 immr->im_ioport.iop_ppard &= ~0x00080000; /* reset bit */
168 /* ----------------------------------------------
169 * In/Out or per. Function 0/1
170 * PDIRD[16] = 0 [0x00008000] -> PERI1: SPIMISO
171 * PDIRD[17] = 0 [0x00004000] -> PERI1: SPIMOSI
172 * PDIRD[18] = 0 [0x00002000] -> PERI1: SPICLK
173 * PDIRD[12] = 1 [0x00080000] -> GPIO OUT: CS for ATC EEPROM
174 * ---------------------------------------------- */
175 immr->im_ioport.iop_pdird &= ~0x0000E000;
176 immr->im_ioport.iop_pdird |= 0x00080000;
178 /* ----------------------------------------------
179 * special option reg.
180 * PSORD[16] = 1 [0x00008000] -> SPIMISO
181 * PSORD[17] = 1 [0x00004000] -> SPIMOSI
182 * PSORD[18] = 1 [0x00002000] -> SPICLK
183 * ---------------------------------------------- */
184 immr->im_ioport.iop_psord |= 0x0000E000;
186 /* Initialize the parameter ram.
187 * We need to make sure many things are initialized to zero
188 */
189 spi->spi_rstate = 0;
190 spi->spi_rdp = 0;
191 spi->spi_rbptr = 0;
192 spi->spi_rbc = 0;
193 spi->spi_rxtmp = 0;
194 spi->spi_tstate = 0;
195 spi->spi_tdp = 0;
196 spi->spi_tbptr = 0;
197 spi->spi_tbc = 0;
198 spi->spi_txtmp = 0;
200 /* Allocate space for one transmit and one receive buffer
201 * descriptor in the DP ram
202 */
203 #ifdef CONFIG_SYS_ALLOC_DPRAM
204 dpaddr = m8260_cpm_dpalloc (sizeof(cbd_t)*2, 8);
205 #else
206 dpaddr = CPM_SPI_BASE;
207 #endif
209 /* 3 */
210 /* Set up the SPI parameters in the parameter ram */
211 spi->spi_rbase = dpaddr;
212 spi->spi_tbase = dpaddr + sizeof (cbd_t);
214 /***********IMPORTANT******************/
216 /*
217 * Setting transmit and receive buffer descriptor pointers
218 * initially to rbase and tbase. Only the microcode patches
219 * documentation talks about initializing this pointer. This
220 * is missing from the sample I2C driver. If you dont
221 * initialize these pointers, the kernel hangs.
222 */
223 spi->spi_rbptr = spi->spi_rbase;
224 spi->spi_tbptr = spi->spi_tbase;
226 /* 4 */
227 /* Init SPI Tx + Rx Parameters */
228 while (cp->cp_cpcr & CPM_CR_FLG)
229 ;
230 cp->cp_cpcr = mk_cr_cmd(CPM_CR_SPI_PAGE, CPM_CR_SPI_SBLOCK,
231 0, CPM_CR_INIT_TRX) | CPM_CR_FLG;
232 while (cp->cp_cpcr & CPM_CR_FLG)
233 ;
235 /* 6 */
236 /* Set to big endian. */
237 spi->spi_tfcr = CPMFCR_EB;
238 spi->spi_rfcr = CPMFCR_EB;
240 /* 7 */
241 /* Set maximum receive size. */
242 spi->spi_mrblr = MAX_BUFFER;
244 /* 8 + 9 */
245 /* tx and rx buffer descriptors */
246 tbdf = (cbd_t *) & immr->im_dprambase[spi->spi_tbase];
247 rbdf = (cbd_t *) & immr->im_dprambase[spi->spi_rbase];
249 tbdf->cbd_sc &= ~BD_SC_READY;
250 rbdf->cbd_sc &= ~BD_SC_EMPTY;
252 /* Set the bd's rx and tx buffer address pointers */
253 rbdf->cbd_bufaddr = (ulong) rxbuf;
254 tbdf->cbd_bufaddr = (ulong) txbuf;
256 /* 10 + 11 */
257 immr->im_spi.spi_spie = SPI_EMASK; /* Clear all SPI events */
258 immr->im_spi.spi_spim = 0x00; /* Mask all SPI events */
261 return;
262 }
264 /* **************************************************************************
265 *
266 * Function: spi_init_r
267 *
268 * Description: Init SPI-Controller (RAM part) -
269 * The malloc engine is ready and we can move our buffers to
270 * normal RAM
271 *
272 * return: ---
273 *
274 * *********************************************************************** */
275 void spi_init_r (void)
276 {
277 volatile spi_t *spi;
278 volatile immap_t *immr;
279 volatile cpm8260_t *cp;
280 volatile cbd_t *tbdf, *rbdf;
282 immr = (immap_t *) CONFIG_SYS_IMMR;
283 cp = (cpm8260_t *) &immr->im_cpm;
285 spi = (spi_t *)&immr->im_dprambase[PROFF_SPI];
287 /* tx and rx buffer descriptors */
288 tbdf = (cbd_t *) & immr->im_dprambase[spi->spi_tbase];
289 rbdf = (cbd_t *) & immr->im_dprambase[spi->spi_rbase];
291 /* Allocate memory for RX and TX buffers */
292 rxbuf = (uchar *) malloc (MAX_BUFFER);
293 txbuf = (uchar *) malloc (MAX_BUFFER);
295 rbdf->cbd_bufaddr = (ulong) rxbuf;
296 tbdf->cbd_bufaddr = (ulong) txbuf;
298 return;
299 }
301 /****************************************************************************
302 * Function: spi_write
303 **************************************************************************** */
304 ssize_t spi_write (uchar *addr, int alen, uchar *buffer, int len)
305 {
306 int i;
308 memset(rxbuf, 0, MAX_BUFFER);
309 memset(txbuf, 0, MAX_BUFFER);
310 *txbuf = SPI_EEPROM_WREN; /* write enable */
311 spi_xfer(1);
312 memcpy(txbuf, addr, alen);
313 *txbuf = SPI_EEPROM_WRITE; /* WRITE memory array */
314 memcpy(alen + txbuf, buffer, len);
315 spi_xfer(alen + len);
316 /* ignore received data */
317 for (i = 0; i < 1000; i++) {
318 *txbuf = SPI_EEPROM_RDSR; /* read status */
319 txbuf[1] = 0;
320 spi_xfer(2);
321 if (!(rxbuf[1] & 1)) {
322 break;
323 }
324 udelay(1000);
325 }
326 if (i >= 1000) {
327 printf ("*** spi_write: Time out while writing!\n");
328 }
330 return len;
331 }
333 /****************************************************************************
334 * Function: spi_read
335 **************************************************************************** */
336 ssize_t spi_read (uchar *addr, int alen, uchar *buffer, int len)
337 {
338 memset(rxbuf, 0, MAX_BUFFER);
339 memset(txbuf, 0, MAX_BUFFER);
340 memcpy(txbuf, addr, alen);
341 *txbuf = SPI_EEPROM_READ; /* READ memory array */
343 /*
344 * There is a bug in 860T (?) that cuts the last byte of input
345 * if we're reading into DPRAM. The solution we choose here is
346 * to always read len+1 bytes (we have one extra byte at the
347 * end of the buffer).
348 */
349 spi_xfer(alen + len + 1);
350 memcpy(buffer, alen + rxbuf, len);
352 return len;
353 }
355 /****************************************************************************
356 * Function: spi_xfer
357 **************************************************************************** */
358 ssize_t spi_xfer (size_t count)
359 {
360 volatile immap_t *immr;
361 volatile cpm8260_t *cp;
362 volatile spi_t *spi;
363 cbd_t *tbdf, *rbdf;
364 int tm;
366 DPRINT (("*** spi_xfer entered ***\n"));
368 immr = (immap_t *) CONFIG_SYS_IMMR;
369 cp = (cpm8260_t *) &immr->im_cpm;
371 spi = (spi_t *)&immr->im_dprambase[PROFF_SPI];
373 tbdf = (cbd_t *) & immr->im_dprambase[spi->spi_tbase];
374 rbdf = (cbd_t *) & immr->im_dprambase[spi->spi_rbase];
376 /* Board-specific: Set CS for device (ATC EEPROM) */
377 immr->im_ioport.iop_pdatd &= ~0x00080000;
379 /* Setting tx bd status and data length */
380 tbdf->cbd_sc = BD_SC_READY | BD_SC_LAST | BD_SC_WRAP;
381 tbdf->cbd_datlen = count;
383 DPRINT (("*** spi_xfer: Bytes to be xferred: %d ***\n",
384 tbdf->cbd_datlen));
386 /* Setting rx bd status and data length */
387 rbdf->cbd_sc = BD_SC_EMPTY | BD_SC_WRAP;
388 rbdf->cbd_datlen = 0; /* rx length has no significance */
390 immr->im_spi.spi_spmode = SPMODE_REV |
391 SPMODE_MSTR |
392 SPMODE_EN |
393 SPMODE_LEN(8) | /* 8 Bits per char */
394 SPMODE_PM(0x8) ; /* medium speed */
395 immr->im_spi.spi_spie = SPI_EMASK; /* Clear all SPI events */
396 immr->im_spi.spi_spim = 0x00; /* Mask all SPI events */
398 /* start spi transfer */
399 DPRINT (("*** spi_xfer: Performing transfer ...\n"));
400 immr->im_spi.spi_spcom |= SPI_STR; /* Start transmit */
402 /* --------------------------------
403 * Wait for SPI transmit to get out
404 * or time out (1 second = 1000 ms)
405 * -------------------------------- */
406 for (tm=0; tm<1000; ++tm) {
407 if (immr->im_spi.spi_spie & SPI_TXB) { /* Tx Buffer Empty */
408 DPRINT (("*** spi_xfer: Tx buffer empty\n"));
409 break;
410 }
411 if ((tbdf->cbd_sc & BD_SC_READY) == 0) {
412 DPRINT (("*** spi_xfer: Tx BD done\n"));
413 break;
414 }
415 udelay (1000);
416 }
417 if (tm >= 1000) {
418 printf ("*** spi_xfer: Time out while xferring to/from SPI!\n");
419 }
420 DPRINT (("*** spi_xfer: ... transfer ended\n"));
422 #ifdef DEBUG
423 printf ("\nspi_xfer: txbuf after xfer\n");
424 memdump ((void *) txbuf, 16); /* dump of txbuf before transmit */
425 printf ("spi_xfer: rxbuf after xfer\n");
426 memdump ((void *) rxbuf, 16); /* dump of rxbuf after transmit */
427 printf ("\n");
428 #endif
430 /* Clear CS for device */
431 immr->im_ioport.iop_pdatd |= 0x00080000;
433 return count;
434 }
435 #endif /* CONFIG_SPI */