1 /*
2 * Copyright 2008-2011 Freescale Semiconductor, Inc.
3 *
4 * See file CREDITS for list of people who contributed to this
5 * project.
6 *
7 * This program is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU General Public License as
9 * published by the Free Software Foundation; either version 2 of
10 * the License, or (at your option) any later version.
11 *
12 * This program is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15 * GNU General Public License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with this program; if not, write to the Free Software
19 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20 * MA 02111-1307 USA
21 */
23 #include <common.h>
24 #include <asm/processor.h>
25 #include <ioports.h>
26 #include <lmb.h>
27 #include <asm/io.h>
28 #include <asm/mmu.h>
29 #include <asm/fsl_law.h>
30 #include "mp.h"
32 DECLARE_GLOBAL_DATA_PTR;
34 u32 get_my_id()
35 {
36 return mfspr(SPRN_PIR);
37 }
39 /*
40 * Determine if U-Boot should keep secondary cores in reset, or let them out
41 * of reset and hold them in a spinloop
42 */
43 int hold_cores_in_reset(int verbose)
44 {
45 const char *s = getenv("mp_holdoff");
47 /* Default to no, overriden by 'y', 'yes', 'Y', 'Yes', or '1' */
48 if (s && (*s == 'y' || *s == 'Y' || *s == '1')) {
49 if (verbose) {
50 puts("Secondary cores are being held in reset.\n");
51 puts("See 'mp_holdoff' environment variable\n");
52 }
54 return 1;
55 }
57 return 0;
58 }
60 int cpu_reset(int nr)
61 {
62 volatile ccsr_pic_t *pic = (void *)(CONFIG_SYS_MPC8xxx_PIC_ADDR);
63 out_be32(&pic->pir, 1 << nr);
64 /* the dummy read works around an errata on early 85xx MP PICs */
65 (void)in_be32(&pic->pir);
66 out_be32(&pic->pir, 0x0);
68 return 0;
69 }
71 int cpu_status(int nr)
72 {
73 u32 *table, id = get_my_id();
75 if (hold_cores_in_reset(1))
76 return 0;
78 if (nr == id) {
79 table = (u32 *)get_spin_virt_addr();
80 printf("table base @ 0x%p\n", table);
81 } else {
82 table = (u32 *)get_spin_virt_addr() + nr * NUM_BOOT_ENTRY;
83 printf("Running on cpu %d\n", id);
84 printf("\n");
85 printf("table @ 0x%p\n", table);
86 printf(" addr - 0x%08x\n", table[BOOT_ENTRY_ADDR_LOWER]);
87 printf(" pir - 0x%08x\n", table[BOOT_ENTRY_PIR]);
88 printf(" r3 - 0x%08x\n", table[BOOT_ENTRY_R3_LOWER]);
89 printf(" r6 - 0x%08x\n", table[BOOT_ENTRY_R6_LOWER]);
90 }
92 return 0;
93 }
95 #ifdef CONFIG_FSL_CORENET
96 int cpu_disable(int nr)
97 {
98 volatile ccsr_gur_t *gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
100 setbits_be32(&gur->coredisrl, 1 << nr);
102 return 0;
103 }
105 int is_core_disabled(int nr) {
106 ccsr_gur_t *gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
107 u32 coredisrl = in_be32(&gur->coredisrl);
109 return (coredisrl & (1 << nr));
110 }
111 #else
112 int cpu_disable(int nr)
113 {
114 volatile ccsr_gur_t *gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
116 switch (nr) {
117 case 0:
118 setbits_be32(&gur->devdisr, MPC85xx_DEVDISR_CPU0);
119 break;
120 case 1:
121 setbits_be32(&gur->devdisr, MPC85xx_DEVDISR_CPU1);
122 break;
123 default:
124 printf("Invalid cpu number for disable %d\n", nr);
125 return 1;
126 }
128 return 0;
129 }
131 int is_core_disabled(int nr) {
132 ccsr_gur_t *gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
133 u32 devdisr = in_be32(&gur->devdisr);
135 switch (nr) {
136 case 0:
137 return (devdisr & MPC85xx_DEVDISR_CPU0);
138 case 1:
139 return (devdisr & MPC85xx_DEVDISR_CPU1);
140 default:
141 printf("Invalid cpu number for disable %d\n", nr);
142 }
144 return 0;
145 }
146 #endif
148 static u8 boot_entry_map[4] = {
149 0,
150 BOOT_ENTRY_PIR,
151 BOOT_ENTRY_R3_LOWER,
152 BOOT_ENTRY_R6_LOWER,
153 };
155 int cpu_release(int nr, int argc, char * const argv[])
156 {
157 u32 i, val, *table = (u32 *)get_spin_virt_addr() + nr * NUM_BOOT_ENTRY;
158 u64 boot_addr;
160 if (hold_cores_in_reset(1))
161 return 0;
163 if (nr == get_my_id()) {
164 printf("Invalid to release the boot core.\n\n");
165 return 1;
166 }
168 if (argc != 4) {
169 printf("Invalid number of arguments to release.\n\n");
170 return 1;
171 }
173 boot_addr = simple_strtoull(argv[0], NULL, 16);
175 /* handle pir, r3, r6 */
176 for (i = 1; i < 4; i++) {
177 if (argv[i][0] != '-') {
178 u8 entry = boot_entry_map[i];
179 val = simple_strtoul(argv[i], NULL, 16);
180 table[entry] = val;
181 }
182 }
184 table[BOOT_ENTRY_ADDR_UPPER] = (u32)(boot_addr >> 32);
186 /* ensure all table updates complete before final address write */
187 eieio();
189 table[BOOT_ENTRY_ADDR_LOWER] = (u32)(boot_addr & 0xffffffff);
191 return 0;
192 }
194 u32 determine_mp_bootpg(void)
195 {
196 /* if we have 4G or more of memory, put the boot page at 4Gb-4k */
197 if ((u64)gd->ram_size > 0xfffff000)
198 return (0xfffff000);
200 return (gd->ram_size - 4096);
201 }
203 ulong get_spin_phys_addr(void)
204 {
205 extern ulong __secondary_start_page;
206 extern ulong __spin_table;
208 return (determine_mp_bootpg() +
209 (ulong)&__spin_table - (ulong)&__secondary_start_page);
210 }
212 ulong get_spin_virt_addr(void)
213 {
214 extern ulong __secondary_start_page;
215 extern ulong __spin_table;
217 return (CONFIG_BPTR_VIRT_ADDR +
218 (ulong)&__spin_table - (ulong)&__secondary_start_page);
219 }
221 #ifdef CONFIG_FSL_CORENET
222 static void plat_mp_up(unsigned long bootpg)
223 {
224 u32 cpu_up_mask, whoami;
225 u32 *table = (u32 *)get_spin_virt_addr();
226 volatile ccsr_gur_t *gur;
227 volatile ccsr_local_t *ccm;
228 volatile ccsr_rcpm_t *rcpm;
229 volatile ccsr_pic_t *pic;
230 int timeout = 10;
231 u32 mask = cpu_mask();
232 struct law_entry e;
234 gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
235 ccm = (void *)(CONFIG_SYS_FSL_CORENET_CCM_ADDR);
236 rcpm = (void *)(CONFIG_SYS_FSL_CORENET_RCPM_ADDR);
237 pic = (void *)(CONFIG_SYS_MPC8xxx_PIC_ADDR);
239 whoami = in_be32(&pic->whoami);
240 cpu_up_mask = 1 << whoami;
241 out_be32(&ccm->bstrl, bootpg);
243 e = find_law(bootpg);
244 out_be32(&ccm->bstrar, LAW_EN | e.trgt_id << 20 | LAW_SIZE_4K);
246 /* readback to sync write */
247 in_be32(&ccm->bstrar);
249 /* disable time base at the platform */
250 out_be32(&rcpm->ctbenrl, cpu_up_mask);
252 out_be32(&gur->brrl, mask);
254 /* wait for everyone */
255 while (timeout) {
256 unsigned int i, cpu, nr_cpus = cpu_numcores();
258 for_each_cpu(i, cpu, nr_cpus, mask) {
259 if (table[cpu * NUM_BOOT_ENTRY + BOOT_ENTRY_ADDR_LOWER])
260 cpu_up_mask |= (1 << cpu);
261 }
263 if ((cpu_up_mask & mask) == mask)
264 break;
266 udelay(100);
267 timeout--;
268 }
270 if (timeout == 0)
271 printf("CPU up timeout. CPU up mask is %x should be %x\n",
272 cpu_up_mask, mask);
274 /* enable time base at the platform */
275 out_be32(&rcpm->ctbenrl, 0);
277 /* readback to sync write */
278 in_be32(&rcpm->ctbenrl);
280 mtspr(SPRN_TBWU, 0);
281 mtspr(SPRN_TBWL, 0);
283 out_be32(&rcpm->ctbenrl, mask);
285 #ifdef CONFIG_MPC8xxx_DISABLE_BPTR
286 /*
287 * Disabling Boot Page Translation allows the memory region 0xfffff000
288 * to 0xffffffff to be used normally. Leaving Boot Page Translation
289 * enabled remaps 0xfffff000 to SDRAM which makes that memory region
290 * unusable for normal operation but it does allow OSes to easily
291 * reset a processor core to put it back into U-Boot's spinloop.
292 */
293 clrbits_be32(&ccm->bstrar, LAW_EN);
294 #endif
295 }
296 #else
297 static void plat_mp_up(unsigned long bootpg)
298 {
299 u32 up, cpu_up_mask, whoami;
300 u32 *table = (u32 *)get_spin_virt_addr();
301 volatile u32 bpcr;
302 volatile ccsr_local_ecm_t *ecm = (void *)(CONFIG_SYS_MPC85xx_ECM_ADDR);
303 volatile ccsr_gur_t *gur = (void *)(CONFIG_SYS_MPC85xx_GUTS_ADDR);
304 volatile ccsr_pic_t *pic = (void *)(CONFIG_SYS_MPC8xxx_PIC_ADDR);
305 u32 devdisr;
306 int timeout = 10;
308 whoami = in_be32(&pic->whoami);
309 out_be32(&ecm->bptr, 0x80000000 | (bootpg >> 12));
311 /* disable time base at the platform */
312 devdisr = in_be32(&gur->devdisr);
313 if (whoami)
314 devdisr |= MPC85xx_DEVDISR_TB0;
315 else
316 devdisr |= MPC85xx_DEVDISR_TB1;
317 out_be32(&gur->devdisr, devdisr);
319 /* release the hounds */
320 up = ((1 << cpu_numcores()) - 1);
321 bpcr = in_be32(&ecm->eebpcr);
322 bpcr |= (up << 24);
323 out_be32(&ecm->eebpcr, bpcr);
324 asm("sync; isync; msync");
326 cpu_up_mask = 1 << whoami;
327 /* wait for everyone */
328 while (timeout) {
329 int i;
330 for (i = 0; i < cpu_numcores(); i++) {
331 if (table[i * NUM_BOOT_ENTRY + BOOT_ENTRY_ADDR_LOWER])
332 cpu_up_mask |= (1 << i);
333 };
335 if ((cpu_up_mask & up) == up)
336 break;
338 udelay(100);
339 timeout--;
340 }
342 if (timeout == 0)
343 printf("CPU up timeout. CPU up mask is %x should be %x\n",
344 cpu_up_mask, up);
346 /* enable time base at the platform */
347 if (whoami)
348 devdisr |= MPC85xx_DEVDISR_TB1;
349 else
350 devdisr |= MPC85xx_DEVDISR_TB0;
351 out_be32(&gur->devdisr, devdisr);
353 /* readback to sync write */
354 in_be32(&gur->devdisr);
356 mtspr(SPRN_TBWU, 0);
357 mtspr(SPRN_TBWL, 0);
359 devdisr &= ~(MPC85xx_DEVDISR_TB0 | MPC85xx_DEVDISR_TB1);
360 out_be32(&gur->devdisr, devdisr);
362 #ifdef CONFIG_MPC8xxx_DISABLE_BPTR
363 /*
364 * Disabling Boot Page Translation allows the memory region 0xfffff000
365 * to 0xffffffff to be used normally. Leaving Boot Page Translation
366 * enabled remaps 0xfffff000 to SDRAM which makes that memory region
367 * unusable for normal operation but it does allow OSes to easily
368 * reset a processor core to put it back into U-Boot's spinloop.
369 */
370 clrbits_be32(&ecm->bptr, 0x80000000);
371 #endif
372 }
373 #endif
375 void cpu_mp_lmb_reserve(struct lmb *lmb)
376 {
377 u32 bootpg = determine_mp_bootpg();
379 lmb_reserve(lmb, bootpg, 4096);
380 }
382 void setup_mp(void)
383 {
384 extern ulong __secondary_start_page;
385 extern ulong __bootpg_addr;
386 ulong fixup = (ulong)&__secondary_start_page;
387 u32 bootpg = determine_mp_bootpg();
389 /* Some OSes expect secondary cores to be held in reset */
390 if (hold_cores_in_reset(0))
391 return;
393 /* Store the bootpg's SDRAM address for use by secondary CPU cores */
394 __bootpg_addr = bootpg;
396 /* look for the tlb covering the reset page, there better be one */
397 int i = find_tlb_idx((void *)CONFIG_BPTR_VIRT_ADDR, 1);
399 /* we found a match */
400 if (i != -1) {
401 /* map reset page to bootpg so we can copy code there */
402 disable_tlb(i);
404 set_tlb(1, CONFIG_BPTR_VIRT_ADDR, bootpg, /* tlb, epn, rpn */
405 MAS3_SX|MAS3_SW|MAS3_SR, MAS2_I|MAS2_G, /* perms, wimge */
406 0, i, BOOKE_PAGESZ_4K, 1); /* ts, esel, tsize, iprot */
408 memcpy((void *)CONFIG_BPTR_VIRT_ADDR, (void *)fixup, 4096);
410 plat_mp_up(bootpg);
411 } else {
412 puts("WARNING: No reset page TLB. "
413 "Skipping secondary core setup\n");
414 }
415 }