]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/powerpc/cpu/mpc85xx/tlb.c
Merge remote-tracking branch 'u-boot-ti/master'
[glsdk/glsdk-u-boot.git] / arch / powerpc / cpu / mpc85xx / tlb.c
1 /*
2  * Copyright 2008-2011 Freescale Semiconductor, Inc.
3  *
4  * (C) Copyright 2000
5  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
6  *
7  * See file CREDITS for list of people who contributed to this
8  * project.
9  *
10  * This program is free software; you can redistribute it and/or
11  * modify it under the terms of the GNU General Public License as
12  * published by the Free Software Foundation; either version 2 of
13  * the License, or (at your option) any later version.
14  *
15  * This program is distributed in the hope that it will be useful,
16  * but WITHOUT ANY WARRANTY; without even the implied warranty of
17  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
18  * GNU General Public License for more details.
19  *
20  * You should have received a copy of the GNU General Public License
21  * along with this program; if not, write to the Free Software
22  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23  * MA 02111-1307 USA
24  */
26 #include <common.h>
27 #include <asm/processor.h>
28 #include <asm/mmu.h>
29 #ifdef CONFIG_ADDR_MAP
30 #include <addr_map.h>
31 #endif
33 DECLARE_GLOBAL_DATA_PTR;
35 void invalidate_tlb(u8 tlb)
36 {
37         if (tlb == 0)
38                 mtspr(MMUCSR0, 0x4);
39         if (tlb == 1)
40                 mtspr(MMUCSR0, 0x2);
41 }
43 void init_tlbs(void)
44 {
45         int i;
47         for (i = 0; i < num_tlb_entries; i++) {
48                 write_tlb(tlb_table[i].mas0,
49                           tlb_table[i].mas1,
50                           tlb_table[i].mas2,
51                           tlb_table[i].mas3,
52                           tlb_table[i].mas7);
53         }
55         return ;
56 }
58 #ifndef CONFIG_NAND_SPL
59 void read_tlbcam_entry(int idx, u32 *valid, u32 *tsize, unsigned long *epn,
60                        phys_addr_t *rpn)
61 {
62         u32 _mas1;
64         mtspr(MAS0, FSL_BOOKE_MAS0(1, idx, 0));
65         asm volatile("tlbre;isync");
66         _mas1 = mfspr(MAS1);
68         *valid = (_mas1 & MAS1_VALID);
69         *tsize = (_mas1 >> 8) & 0xf;
70         *epn = mfspr(MAS2) & MAS2_EPN;
71         *rpn = mfspr(MAS3) & MAS3_RPN;
72 #ifdef CONFIG_ENABLE_36BIT_PHYS
73         *rpn |= ((u64)mfspr(MAS7)) << 32;
74 #endif
75 }
77 void print_tlbcam(void)
78 {
79         int i;
80         unsigned int num_cam = mfspr(SPRN_TLB1CFG) & 0xfff;
82         /* walk all the entries */
83         printf("TLBCAM entries\n");
84         for (i = 0; i < num_cam; i++) {
85                 unsigned long epn;
86                 u32 tsize, valid;
87                 phys_addr_t rpn;
89                 read_tlbcam_entry(i, &valid, &tsize, &epn, &rpn);
90                 printf("entry %02d: V: %d EPN 0x%08x RPN 0x%08llx size:",
91                         i, (valid == 0) ? 0 : 1, (unsigned int)epn,
92                         (unsigned long long)rpn);
93                 print_size(TSIZE_TO_BYTES(tsize), "\n");
94         }
95 }
97 static inline void use_tlb_cam(u8 idx)
98 {
99         int i = idx / 32;
100         int bit = idx % 32;
102         gd->used_tlb_cams[i] |= (1 << bit);
105 static inline void free_tlb_cam(u8 idx)
107         int i = idx / 32;
108         int bit = idx % 32;
110         gd->used_tlb_cams[i] &= ~(1 << bit);
113 void init_used_tlb_cams(void)
115         int i;
116         unsigned int num_cam = mfspr(SPRN_TLB1CFG) & 0xfff;
118         for (i = 0; i < ((CONFIG_SYS_NUM_TLBCAMS+31)/32); i++)
119                 gd->used_tlb_cams[i] = 0;
121         /* walk all the entries */
122         for (i = 0; i < num_cam; i++) {
123                 mtspr(MAS0, FSL_BOOKE_MAS0(1, i, 0));
124                 asm volatile("tlbre;isync");
125                 if (mfspr(MAS1) & MAS1_VALID)
126                         use_tlb_cam(i);
127         }
130 int find_free_tlbcam(void)
132         int i;
133         u32 idx;
135         for (i = 0; i < ((CONFIG_SYS_NUM_TLBCAMS+31)/32); i++) {
136                 idx = ffz(gd->used_tlb_cams[i]);
138                 if (idx != 32)
139                         break;
140         }
142         idx += i * 32;
144         if (idx >= CONFIG_SYS_NUM_TLBCAMS)
145                 return -1;
147         return idx;
150 void set_tlb(u8 tlb, u32 epn, u64 rpn,
151              u8 perms, u8 wimge,
152              u8 ts, u8 esel, u8 tsize, u8 iprot)
154         u32 _mas0, _mas1, _mas2, _mas3, _mas7;
156         if (tlb == 1)
157                 use_tlb_cam(esel);
159         _mas0 = FSL_BOOKE_MAS0(tlb, esel, 0);
160         _mas1 = FSL_BOOKE_MAS1(1, iprot, 0, ts, tsize);
161         _mas2 = FSL_BOOKE_MAS2(epn, wimge);
162         _mas3 = FSL_BOOKE_MAS3(rpn, 0, perms);
163         _mas7 = FSL_BOOKE_MAS7(rpn);
165         write_tlb(_mas0, _mas1, _mas2, _mas3, _mas7);
167 #ifdef CONFIG_ADDR_MAP
168         if ((tlb == 1) && (gd->flags & GD_FLG_RELOC))
169                 addrmap_set_entry(epn, rpn, TSIZE_TO_BYTES(tsize), esel);
170 #endif
173 void disable_tlb(u8 esel)
175         u32 _mas0, _mas1, _mas2, _mas3;
177         free_tlb_cam(esel);
179         _mas0 = FSL_BOOKE_MAS0(1, esel, 0);
180         _mas1 = 0;
181         _mas2 = 0;
182         _mas3 = 0;
184         mtspr(MAS0, _mas0);
185         mtspr(MAS1, _mas1);
186         mtspr(MAS2, _mas2);
187         mtspr(MAS3, _mas3);
188 #ifdef CONFIG_ENABLE_36BIT_PHYS
189         mtspr(MAS7, 0);
190 #endif
191         asm volatile("isync;msync;tlbwe;isync");
193 #ifdef CONFIG_ADDR_MAP
194         if (gd->flags & GD_FLG_RELOC)
195                 addrmap_set_entry(0, 0, 0, esel);
196 #endif
199 static void tlbsx (const volatile unsigned *addr)
201         __asm__ __volatile__ ("tlbsx 0,%0" : : "r" (addr), "m" (*addr));
204 /* return -1 if we didn't find anything */
205 int find_tlb_idx(void *addr, u8 tlbsel)
207         u32 _mas0, _mas1;
209         /* zero out Search PID, AS */
210         mtspr(MAS6, 0);
212         tlbsx(addr);
214         _mas0 = mfspr(MAS0);
215         _mas1 = mfspr(MAS1);
217         /* we found something, and its in the TLB we expect */
218         if ((MAS1_VALID & _mas1) &&
219                 (MAS0_TLBSEL(tlbsel) == (_mas0 & MAS0_TLBSEL_MSK))) {
220                 return ((_mas0 & MAS0_ESEL_MSK) >> 16);
221         }
223         return -1;
226 #ifdef CONFIG_ADDR_MAP
227 void init_addr_map(void)
229         int i;
230         unsigned int num_cam = mfspr(SPRN_TLB1CFG) & 0xfff;
232         /* walk all the entries */
233         for (i = 0; i < num_cam; i++) {
234                 unsigned long epn;
235                 u32 tsize, valid;
236                 phys_addr_t rpn;
238                 read_tlbcam_entry(i, &valid, &tsize, &epn, &rpn);
239                 if (valid & MAS1_VALID)
240                         addrmap_set_entry(epn, rpn, TSIZE_TO_BYTES(tsize), i);
241         }
243         return ;
245 #endif
247 unsigned int
248 setup_ddr_tlbs_phys(phys_addr_t p_addr, unsigned int memsize_in_meg)
250         int i;
251         unsigned int tlb_size;
252         unsigned int wimge = MAS2_M;
253         unsigned int ram_tlb_address = (unsigned int)CONFIG_SYS_DDR_SDRAM_BASE;
254         unsigned int max_cam;
255         u64 size, memsize = (u64)memsize_in_meg << 20;
257 #ifdef CONFIG_SYS_PPC_DDR_WIMGE
258         wimge = CONFIG_SYS_PPC_DDR_WIMGE;
259 #endif
260         size = min(memsize, CONFIG_MAX_MEM_MAPPED);
261         if ((mfspr(SPRN_MMUCFG) & MMUCFG_MAVN) == MMUCFG_MAVN_V1) {
262                 /* Convert (4^max) kB to (2^max) bytes */
263                 max_cam = ((mfspr(SPRN_TLB1CFG) >> 16) & 0xf) * 2 + 10;
264         } else {
265                 /* Convert (2^max) kB to (2^max) bytes */
266                 max_cam = __ilog2(mfspr(SPRN_TLB1PS)) + 10;
267         }
269         for (i = 0; size && i < 8; i++) {
270                 int ram_tlb_index = find_free_tlbcam();
271                 u32 camsize = __ilog2_u64(size) & ~1U;
272                 u32 align = __ilog2(ram_tlb_address) & ~1U;
274                 if (ram_tlb_index == -1)
275                         break;
277                 if (align == -2) align = max_cam;
278                 if (camsize > align)
279                         camsize = align;
281                 if (camsize > max_cam)
282                         camsize = max_cam;
284                 tlb_size = (camsize - 10) / 2;
286                 set_tlb(1, ram_tlb_address, p_addr,
287                         MAS3_SX|MAS3_SW|MAS3_SR, wimge,
288                         0, ram_tlb_index, tlb_size, 1);
290                 size -= 1ULL << camsize;
291                 memsize -= 1ULL << camsize;
292                 ram_tlb_address += 1UL << camsize;
293                 p_addr += 1UL << camsize;
294         }
296         if (memsize)
297                 print_size(memsize, " left unmapped\n");
298         return memsize_in_meg;
301 unsigned int setup_ddr_tlbs(unsigned int memsize_in_meg)
303         return
304                 setup_ddr_tlbs_phys(CONFIG_SYS_DDR_SDRAM_BASE, memsize_in_meg);
307 /* Invalidate the DDR TLBs for the requested size */
308 void clear_ddr_tlbs_phys(phys_addr_t p_addr, unsigned int memsize_in_meg)
310         u32 vstart = CONFIG_SYS_DDR_SDRAM_BASE;
311         unsigned long epn;
312         u32 tsize, valid, ptr;
313         phys_addr_t rpn = 0;
314         int ddr_esel;
315         u64 memsize = (u64)memsize_in_meg << 20;
317         ptr = vstart;
319         while (ptr < (vstart + memsize)) {
320                 ddr_esel = find_tlb_idx((void *)ptr, 1);
321                 if (ddr_esel != -1) {
322                         read_tlbcam_entry(ddr_esel, &valid, &tsize, &epn, &rpn);
323                         disable_tlb(ddr_esel);
324                 }
325                 ptr += TSIZE_TO_BYTES(tsize);
326         }
329 void clear_ddr_tlbs(unsigned int memsize_in_meg)
331         clear_ddr_tlbs_phys(CONFIG_SYS_DDR_SDRAM_BASE, memsize_in_meg);
335 #endif /* !CONFIG_NAND_SPL */