]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/powerpc/cpu/mpc86xx/release.S
fsl_i2c: Added a callpoint for i2c_board_late_init
[glsdk/glsdk-u-boot.git] / arch / powerpc / cpu / mpc86xx / release.S
1 /*
2  * Copyright 2004, 2007, 2008 Freescale Semiconductor.
3  * Srikanth Srinivasan <srikanth.srinivaan@freescale.com>
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
23 #include <config.h>
24 #include <mpc86xx.h>
25 #include <version.h>
27 #include <ppc_asm.tmpl>
28 #include <ppc_defs.h>
30 #include <asm/cache.h>
31 #include <asm/mmu.h>
33 /* If this is a multi-cpu system then we need to handle the
34  * 2nd cpu.  The assumption is that the 2nd cpu is being
35  * held in boot holdoff mode until the 1st cpu unlocks it
36  * from Linux.  We'll do some basic cpu init and then pass
37  * it to the Linux Reset Vector.
38  * Sri:  Much of this initialization is not required. Linux
39  * rewrites the bats, and the sprs and also enables the L1 cache.
40  *
41  * Core 0 must copy this to a 1M aligned region and set BPTR
42  * to point to it.
43  */
44         .align 12
45 .globl __secondary_start_page
46 __secondary_start_page:
47         .space 0x100    /* space over to reset vector loc */
48         mfspr   r0, MSSCR0
49         andi.   r0, r0, 0x0020
50         rlwinm  r0,r0,27,31,31
51         mtspr   PIR, r0
53         /* Invalidate BATs */
54         li      r0, 0
55         mtspr   IBAT0U, r0
56         mtspr   IBAT1U, r0
57         mtspr   IBAT2U, r0
58         mtspr   IBAT3U, r0
59         mtspr   IBAT4U, r0
60         mtspr   IBAT5U, r0
61         mtspr   IBAT6U, r0
62         mtspr   IBAT7U, r0
63         isync
64         mtspr   DBAT0U, r0
65         mtspr   DBAT1U, r0
66         mtspr   DBAT2U, r0
67         mtspr   DBAT3U, r0
68         mtspr   DBAT4U, r0
69         mtspr   DBAT5U, r0
70         mtspr   DBAT6U, r0
71         mtspr   DBAT7U, r0
72         isync
73         sync
75         /* enable extended addressing */
76         mfspr   r0, HID0
77         lis     r0, (HID0_HIGH_BAT_EN | HID0_XBSEN | HID0_XAEN)@h
78         ori     r0, r0, (HID0_HIGH_BAT_EN | HID0_XBSEN | HID0_XAEN)@l
79         mtspr   HID0, r0
80         sync
81         isync
83 #ifdef CONFIG_SYS_L2
84         /* init the L2 cache */
85         addis   r3, r0, L2_INIT@h
86         ori     r3, r3, L2_INIT@l
87         sync
88         mtspr   l2cr, r3
89 #ifdef CONFIG_ALTIVEC
90         dssall
91 #endif
92         /* invalidate the L2 cache */
93         mfspr   r3, l2cr
94         rlwinm. r3, r3, 0, 0, 0
95         beq     1f
97         mfspr   r3, l2cr
98         rlwinm  r3, r3, 0, 1, 31
100 #ifdef  CONFIG_ALTIVEC
101         dssall
102 #endif
103         sync
104         mtspr   l2cr, r3
105         sync
106 1:      mfspr   r3, l2cr
107         oris    r3, r3, L2CR_L2I@h
108         mtspr   l2cr, r3
110 invl2:
111         mfspr   r3, l2cr
112         andis.  r3, r3, L2CR_L2I@h
113         bne     invl2
114         sync
115 #endif
117         /* enable and invalidate the data cache */
118         mfspr   r3, HID0
119         li      r5, HID0_DCFI|HID0_DLOCK
120         andc    r3, r3, r5
121         mtspr   HID0, r3                /* no invalidate, unlock */
122         ori     r3, r3, HID0_DCE
123         ori     r5, r3, HID0_DCFI
124         mtspr   HID0, r5                /* enable + invalidate */
125         mtspr   HID0, r3                /* enable */
126         sync
127 #ifdef CONFIG_SYS_L2
128         sync
129         lis     r3, L2_ENABLE@h
130         ori     r3, r3, L2_ENABLE@l
131         mtspr   l2cr, r3
132         isync
133         sync
134 #endif
136         /* enable and invalidate the instruction cache*/
137         mfspr   r3, HID0
138         li      r5, HID0_ICFI|HID0_ILOCK
139         andc    r3, r3, r5
140         ori     r3, r3, HID0_ICE
141         ori     r5, r3, HID0_ICFI
142         mtspr   HID0, r5
143         mtspr   HID0, r3
144         isync
145         sync
147         /* TBEN in HID0 */
148         mfspr   r4, HID0
149         oris    r4, r4, 0x0400
150         mtspr   HID0, r4
151         sync
152         isync
154         /* MCP|SYNCBE|ABE in HID1 */
155         mfspr   r4, HID1
156         oris    r4, r4, 0x8000
157         ori     r4, r4, 0x0C00
158         mtspr   HID1, r4
159         sync
160         isync
162         lis     r3, CONFIG_LINUX_RESET_VEC@h
163         ori     r3, r3, CONFIG_LINUX_RESET_VEC@l
164         mtlr    r3
165         blr
167         /* Never Returns, Running in Linux Now */