1 /*
2 * (C) Copyright 2000
3 * Paolo Scaffardi, AIRVENT SAM s.p.a - RIMINI(ITALY), arsenio@tin.it
4 *
5 * (C) Copyright 2000 Sysgo Real-Time Solutions, GmbH <www.elinos.com>
6 * Marius Groeger <mgroeger@sysgo.de>
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 *
26 * Back ported to the 8xx platform (from the 8260 platform) by
27 * Murray.Jensen@cmst.csiro.au, 27-Jan-01.
28 */
30 #include <common.h>
32 #ifdef CONFIG_HARD_I2C
34 #include <commproc.h>
35 #include <i2c.h>
36 #ifdef CONFIG_LWMON
37 #include <watchdog.h>
38 #endif
40 DECLARE_GLOBAL_DATA_PTR;
42 /* define to enable debug messages */
43 #undef DEBUG_I2C
45 /* tx/rx timeout (we need the i2c early, so we don't use get_timer()) */
46 #define TOUT_LOOP 1000000
48 #define NUM_RX_BDS 4
49 #define NUM_TX_BDS 4
50 #define MAX_TX_SPACE 256
51 #define I2C_RXTX_LEN 128 /* maximum tx/rx buffer length */
53 typedef struct I2C_BD
54 {
55 unsigned short status;
56 unsigned short length;
57 unsigned char *addr;
58 } I2C_BD;
59 #define BD_I2C_TX_START 0x0400 /* special status for i2c: Start condition */
61 #define BD_I2C_TX_CL 0x0001 /* collision error */
62 #define BD_I2C_TX_UN 0x0002 /* underflow error */
63 #define BD_I2C_TX_NAK 0x0004 /* no acknowledge error */
64 #define BD_I2C_TX_ERR (BD_I2C_TX_NAK|BD_I2C_TX_UN|BD_I2C_TX_CL)
66 #define BD_I2C_RX_ERR BD_SC_OV
68 typedef void (*i2c_ecb_t)(int, int); /* error callback function */
70 /* This structure keeps track of the bd and buffer space usage. */
71 typedef struct i2c_state {
72 int rx_idx; /* index to next free Rx BD */
73 int tx_idx; /* index to next free Tx BD */
74 void *rxbd; /* pointer to next free Rx BD */
75 void *txbd; /* pointer to next free Tx BD */
76 int tx_space; /* number of Tx bytes left */
77 unsigned char *tx_buf; /* pointer to free Tx area */
78 i2c_ecb_t err_cb; /* error callback function */
79 } i2c_state_t;
82 /* flags for i2c_send() and i2c_receive() */
83 #define I2CF_ENABLE_SECONDARY 0x01 /* secondary_address is valid */
84 #define I2CF_START_COND 0x02 /* tx: generate start condition */
85 #define I2CF_STOP_COND 0x04 /* tx: generate stop condition */
87 /* return codes */
88 #define I2CERR_NO_BUFFERS 0x01 /* no more BDs or buffer space */
89 #define I2CERR_MSG_TOO_LONG 0x02 /* tried to send/receive to much data */
90 #define I2CERR_TIMEOUT 0x03 /* timeout in i2c_doio() */
91 #define I2CERR_QUEUE_EMPTY 0x04 /* i2c_doio called without send/receive */
93 /* error callback flags */
94 #define I2CECB_RX_ERR 0x10 /* this is a receive error */
95 #define I2CECB_RX_ERR_OV 0x02 /* receive overrun error */
96 #define I2CECB_RX_MASK 0x0f /* mask for error bits */
97 #define I2CECB_TX_ERR 0x20 /* this is a transmit error */
98 #define I2CECB_TX_CL 0x01 /* transmit collision error */
99 #define I2CECB_TX_UN 0x02 /* transmit underflow error */
100 #define I2CECB_TX_NAK 0x04 /* transmit no ack error */
101 #define I2CECB_TX_MASK 0x0f /* mask for error bits */
102 #define I2CECB_TIMEOUT 0x40 /* this is a timeout error */
104 #ifdef DEBUG_I2C
105 #define PRINTD(x) printf x
106 #else
107 #define PRINTD(x)
108 #endif
110 /*
111 * Returns the best value of I2BRG to meet desired clock speed of I2C with
112 * input parameters (clock speed, filter, and predivider value).
113 * It returns computer speed value and the difference between it and desired
114 * speed.
115 */
116 static inline int
117 i2c_roundrate(int hz, int speed, int filter, int modval,
118 int *brgval, int *totspeed)
119 {
120 int moddiv = 1 << (5-(modval & 3)), brgdiv, div;
122 PRINTD(("\t[I2C] trying hz=%d, speed=%d, filter=%d, modval=%d\n",
123 hz, speed, filter, modval));
125 div = moddiv * speed;
126 brgdiv = (hz + div - 1) / div;
128 PRINTD(("\t\tmoddiv=%d, brgdiv=%d\n", moddiv, brgdiv));
130 *brgval = ((brgdiv + 1) / 2) - 3 - (2*filter);
132 if ((*brgval < 0) || (*brgval > 255)) {
133 PRINTD(("\t\trejected brgval=%d\n", *brgval));
134 return -1;
135 }
137 brgdiv = 2 * (*brgval + 3 + (2 * filter));
138 div = moddiv * brgdiv ;
139 *totspeed = hz / div;
141 PRINTD(("\t\taccepted brgval=%d, totspeed=%d\n", *brgval, *totspeed));
143 return 0;
144 }
146 /*
147 * Sets the I2C clock predivider and divider to meet required clock speed.
148 */
149 static int
150 i2c_setrate (int hz, int speed)
151 {
152 immap_t *immap = (immap_t *) CONFIG_SYS_IMMR;
153 volatile i2c8xx_t *i2c = (i2c8xx_t *) & immap->im_i2c;
154 int brgval,
155 modval, /* 0-3 */
156 bestspeed_diff = speed,
157 bestspeed_brgval = 0,
158 bestspeed_modval = 0,
159 bestspeed_filter = 0,
160 totspeed,
161 filter = 0; /* Use this fixed value */
163 for (modval = 0; modval < 4; modval++) {
164 if (i2c_roundrate(hz,speed,filter,modval,&brgval,&totspeed) == 0) {
165 int diff = speed - totspeed;
167 if ((diff >= 0) && (diff < bestspeed_diff)) {
168 bestspeed_diff = diff;
169 bestspeed_modval = modval;
170 bestspeed_brgval = brgval;
171 bestspeed_filter = filter;
172 }
173 }
174 }
176 PRINTD (("[I2C] Best is:\n"));
177 PRINTD (("[I2C] CPU=%dhz RATE=%d F=%d I2MOD=%08x I2BRG=%08x DIFF=%dhz\n",
178 hz,
179 speed,
180 bestspeed_filter,
181 bestspeed_modval,
182 bestspeed_brgval,
183 bestspeed_diff));
185 i2c->i2c_i2mod |= ((bestspeed_modval & 3) << 1) | (bestspeed_filter << 3);
186 i2c->i2c_i2brg = bestspeed_brgval & 0xff;
188 PRINTD (("[I2C] i2mod=%08x i2brg=%08x\n", i2c->i2c_i2mod,
189 i2c->i2c_i2brg));
191 return 1;
192 }
194 void
195 i2c_init(int speed, int slaveaddr)
196 {
197 volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
198 volatile cpm8xx_t *cp = (cpm8xx_t *)&immap->im_cpm;
199 volatile i2c8xx_t *i2c = (i2c8xx_t *)&immap->im_i2c;
200 volatile iic_t *iip = (iic_t *)&cp->cp_dparam[PROFF_IIC];
201 ulong rbase, tbase;
202 volatile I2C_BD *rxbd, *txbd;
203 uint dpaddr;
205 #ifdef CONFIG_SYS_I2C_INIT_BOARD
206 /* call board specific i2c bus reset routine before accessing the */
207 /* environment, which might be in a chip on that bus. For details */
208 /* about this problem see doc/I2C_Edge_Conditions. */
209 i2c_init_board();
210 #endif
212 #ifdef CONFIG_SYS_I2C_UCODE_PATCH
213 iip = (iic_t *)&cp->cp_dpmem[iip->iic_rpbase];
214 #else
215 /* Disable relocation */
216 iip->iic_rpbase = 0;
217 #endif
219 #ifdef CONFIG_SYS_ALLOC_DPRAM
220 dpaddr = iip->iic_rbase;
221 if (dpaddr == 0) {
222 /* need to allocate dual port ram */
223 dpaddr = dpram_alloc_align(
224 (NUM_RX_BDS * sizeof(I2C_BD)) + (NUM_TX_BDS * sizeof(I2C_BD)) +
225 MAX_TX_SPACE, 8);
226 }
227 #else
228 dpaddr = CPM_I2C_BASE;
229 #endif
231 /*
232 * initialise data in dual port ram:
233 *
234 * dpaddr->rbase -> rx BD (NUM_RX_BDS * sizeof(I2C_BD) bytes)
235 * tbase -> tx BD (NUM_TX_BDS * sizeof(I2C_BD) bytes)
236 * tx buffer (MAX_TX_SPACE bytes)
237 */
239 rbase = dpaddr;
240 tbase = rbase + NUM_RX_BDS * sizeof(I2C_BD);
242 /* Initialize Port B I2C pins. */
243 cp->cp_pbpar |= 0x00000030;
244 cp->cp_pbdir |= 0x00000030;
245 cp->cp_pbodr |= 0x00000030;
247 /* Disable interrupts */
248 i2c->i2c_i2mod = 0x00;
249 i2c->i2c_i2cmr = 0x00;
250 i2c->i2c_i2cer = 0xff;
251 i2c->i2c_i2add = slaveaddr;
253 /*
254 * Set the I2C BRG Clock division factor from desired i2c rate
255 * and current CPU rate (we assume sccr dfbgr field is 0;
256 * divide BRGCLK by 1)
257 */
258 PRINTD(("[I2C] Setting rate...\n"));
259 i2c_setrate (gd->cpu_clk, CONFIG_SYS_I2C_SPEED) ;
261 /* Set I2C controller in master mode */
262 i2c->i2c_i2com = 0x01;
264 /* Set SDMA bus arbitration level to 5 (SDCR) */
265 immap->im_siu_conf.sc_sdcr = 0x0001 ;
267 /* Initialize Tx/Rx parameters */
268 iip->iic_rbase = rbase;
269 iip->iic_tbase = tbase;
270 rxbd = (I2C_BD *)((unsigned char *)&cp->cp_dpmem[iip->iic_rbase]);
271 txbd = (I2C_BD *)((unsigned char *)&cp->cp_dpmem[iip->iic_tbase]);
273 PRINTD(("[I2C] rbase = %04x\n", iip->iic_rbase));
274 PRINTD(("[I2C] tbase = %04x\n", iip->iic_tbase));
275 PRINTD(("[I2C] rxbd = %08x\n", (int)rxbd));
276 PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
278 /* Set big endian byte order */
279 iip->iic_tfcr = 0x10;
280 iip->iic_rfcr = 0x10;
282 /* Set maximum receive size. */
283 iip->iic_mrblr = I2C_RXTX_LEN;
285 #ifdef CONFIG_SYS_I2C_UCODE_PATCH
286 /*
287 * Initialize required parameters if using microcode patch.
288 */
289 iip->iic_rbptr = iip->iic_rbase;
290 iip->iic_tbptr = iip->iic_tbase;
291 iip->iic_rstate = 0;
292 iip->iic_tstate = 0;
293 #else
294 cp->cp_cpcr = mk_cr_cmd(CPM_CR_CH_I2C, CPM_CR_INIT_TRX) | CPM_CR_FLG;
295 do {
296 __asm__ __volatile__ ("eieio");
297 } while (cp->cp_cpcr & CPM_CR_FLG);
298 #endif
300 /* Clear events and interrupts */
301 i2c->i2c_i2cer = 0xff;
302 i2c->i2c_i2cmr = 0x00;
303 }
305 static void
306 i2c_newio(i2c_state_t *state)
307 {
308 volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
309 volatile cpm8xx_t *cp = (cpm8xx_t *)&immap->im_cpm;
310 volatile iic_t *iip = (iic_t *)&cp->cp_dparam[PROFF_IIC];
312 PRINTD(("[I2C] i2c_newio\n"));
314 #ifdef CONFIG_SYS_I2C_UCODE_PATCH
315 iip = (iic_t *)&cp->cp_dpmem[iip->iic_rpbase];
316 #endif
317 state->rx_idx = 0;
318 state->tx_idx = 0;
319 state->rxbd = (void*)&cp->cp_dpmem[iip->iic_rbase];
320 state->txbd = (void*)&cp->cp_dpmem[iip->iic_tbase];
321 state->tx_space = MAX_TX_SPACE;
322 state->tx_buf = (uchar*)state->txbd + NUM_TX_BDS * sizeof(I2C_BD);
323 state->err_cb = NULL;
325 PRINTD(("[I2C] rxbd = %08x\n", (int)state->rxbd));
326 PRINTD(("[I2C] txbd = %08x\n", (int)state->txbd));
327 PRINTD(("[I2C] tx_buf = %08x\n", (int)state->tx_buf));
329 /* clear the buffer memory */
330 memset((char *)state->tx_buf, 0, MAX_TX_SPACE);
331 }
333 static int
334 i2c_send(i2c_state_t *state,
335 unsigned char address,
336 unsigned char secondary_address,
337 unsigned int flags,
338 unsigned short size,
339 unsigned char *dataout)
340 {
341 volatile I2C_BD *txbd;
342 int i,j;
344 PRINTD(("[I2C] i2c_send add=%02d sec=%02d flag=%02d size=%d\n",
345 address, secondary_address, flags, size));
347 /* trying to send message larger than BD */
348 if (size > I2C_RXTX_LEN)
349 return I2CERR_MSG_TOO_LONG;
351 /* no more free bds */
352 if (state->tx_idx >= NUM_TX_BDS || state->tx_space < (2 + size))
353 return I2CERR_NO_BUFFERS;
355 txbd = (I2C_BD *)state->txbd;
356 txbd->addr = state->tx_buf;
358 PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
360 if (flags & I2CF_START_COND) {
361 PRINTD(("[I2C] Formatting addresses...\n"));
362 if (flags & I2CF_ENABLE_SECONDARY) {
363 txbd->length = size + 2; /* Length of msg + dest addr */
364 txbd->addr[0] = address << 1;
365 txbd->addr[1] = secondary_address;
366 i = 2;
367 } else {
368 txbd->length = size + 1; /* Length of msg + dest addr */
369 txbd->addr[0] = address << 1; /* Write dest addr to BD */
370 i = 1;
371 }
372 } else {
373 txbd->length = size; /* Length of message */
374 i = 0;
375 }
377 /* set up txbd */
378 txbd->status = BD_SC_READY;
379 if (flags & I2CF_START_COND)
380 txbd->status |= BD_I2C_TX_START;
381 if (flags & I2CF_STOP_COND)
382 txbd->status |= BD_SC_LAST | BD_SC_WRAP;
384 /* Copy data to send into buffer */
385 PRINTD(("[I2C] copy data...\n"));
386 for(j = 0; j < size; i++, j++)
387 txbd->addr[i] = dataout[j];
389 PRINTD(("[I2C] txbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
390 txbd->length,
391 txbd->status,
392 txbd->addr[0],
393 txbd->addr[1]));
395 /* advance state */
396 state->tx_buf += txbd->length;
397 state->tx_space -= txbd->length;
398 state->tx_idx++;
399 state->txbd = (void*)(txbd + 1);
401 return 0;
402 }
404 static int
405 i2c_receive(i2c_state_t *state,
406 unsigned char address,
407 unsigned char secondary_address,
408 unsigned int flags,
409 unsigned short size_to_expect,
410 unsigned char *datain)
411 {
412 volatile I2C_BD *rxbd, *txbd;
414 PRINTD(("[I2C] i2c_receive %02d %02d %02d\n", address, secondary_address, flags));
416 /* Expected to receive too much */
417 if (size_to_expect > I2C_RXTX_LEN)
418 return I2CERR_MSG_TOO_LONG;
420 /* no more free bds */
421 if (state->tx_idx >= NUM_TX_BDS || state->rx_idx >= NUM_RX_BDS
422 || state->tx_space < 2)
423 return I2CERR_NO_BUFFERS;
425 rxbd = (I2C_BD *)state->rxbd;
426 txbd = (I2C_BD *)state->txbd;
428 PRINTD(("[I2C] rxbd = %08x\n", (int)rxbd));
429 PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
431 txbd->addr = state->tx_buf;
433 /* set up TXBD for destination address */
434 if (flags & I2CF_ENABLE_SECONDARY) {
435 txbd->length = 2;
436 txbd->addr[0] = address << 1; /* Write data */
437 txbd->addr[1] = secondary_address; /* Internal address */
438 txbd->status = BD_SC_READY;
439 } else {
440 txbd->length = 1 + size_to_expect;
441 txbd->addr[0] = (address << 1) | 0x01;
442 txbd->status = BD_SC_READY;
443 memset(&txbd->addr[1], 0, txbd->length);
444 }
446 /* set up rxbd for reception */
447 rxbd->status = BD_SC_EMPTY;
448 rxbd->length = size_to_expect;
449 rxbd->addr = datain;
451 txbd->status |= BD_I2C_TX_START;
452 if (flags & I2CF_STOP_COND) {
453 txbd->status |= BD_SC_LAST | BD_SC_WRAP;
454 rxbd->status |= BD_SC_WRAP;
455 }
457 PRINTD(("[I2C] txbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
458 txbd->length,
459 txbd->status,
460 txbd->addr[0],
461 txbd->addr[1]));
462 PRINTD(("[I2C] rxbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
463 rxbd->length,
464 rxbd->status,
465 rxbd->addr[0],
466 rxbd->addr[1]));
468 /* advance state */
469 state->tx_buf += txbd->length;
470 state->tx_space -= txbd->length;
471 state->tx_idx++;
472 state->txbd = (void*)(txbd + 1);
473 state->rx_idx++;
474 state->rxbd = (void*)(rxbd + 1);
476 return 0;
477 }
480 static int i2c_doio(i2c_state_t *state)
481 {
482 volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
483 volatile cpm8xx_t *cp = (cpm8xx_t *)&immap->im_cpm;
484 volatile i2c8xx_t *i2c = (i2c8xx_t *)&immap->im_i2c;
485 volatile iic_t *iip = (iic_t *)&cp->cp_dparam[PROFF_IIC];
486 volatile I2C_BD *txbd, *rxbd;
487 volatile int j = 0;
489 PRINTD(("[I2C] i2c_doio\n"));
491 #ifdef CONFIG_SYS_I2C_UCODE_PATCH
492 iip = (iic_t *)&cp->cp_dpmem[iip->iic_rpbase];
493 #endif
495 if (state->tx_idx <= 0 && state->rx_idx <= 0) {
496 PRINTD(("[I2C] No I/O is queued\n"));
497 return I2CERR_QUEUE_EMPTY;
498 }
500 iip->iic_rbptr = iip->iic_rbase;
501 iip->iic_tbptr = iip->iic_tbase;
503 /* Enable I2C */
504 PRINTD(("[I2C] Enabling I2C...\n"));
505 i2c->i2c_i2mod |= 0x01;
507 /* Begin transmission */
508 i2c->i2c_i2com |= 0x80;
510 /* Loop until transmit & receive completed */
512 if (state->tx_idx > 0) {
513 txbd = ((I2C_BD*)state->txbd) - 1;
514 PRINTD(("[I2C] Transmitting...(txbd=0x%08lx)\n", (ulong)txbd));
515 while((txbd->status & BD_SC_READY) && (j++ < TOUT_LOOP)) {
516 if (ctrlc()) {
517 return (-1);
518 }
519 __asm__ __volatile__ ("eieio");
520 }
521 }
523 if ((state->rx_idx > 0) && (j < TOUT_LOOP)) {
524 rxbd = ((I2C_BD*)state->rxbd) - 1;
525 PRINTD(("[I2C] Receiving...(rxbd=0x%08lx)\n", (ulong)rxbd));
526 while((rxbd->status & BD_SC_EMPTY) && (j++ < TOUT_LOOP)) {
527 if (ctrlc()) {
528 return (-1);
529 }
530 __asm__ __volatile__ ("eieio");
531 }
532 }
534 /* Turn off I2C */
535 i2c->i2c_i2mod &= ~0x01;
537 if (state->err_cb != NULL) {
538 int n, i, b;
540 /*
541 * if we have an error callback function, look at the
542 * error bits in the bd status and pass them back
543 */
545 if ((n = state->tx_idx) > 0) {
546 for (i = 0; i < n; i++) {
547 txbd = ((I2C_BD*)state->txbd) - (n - i);
548 if ((b = txbd->status & BD_I2C_TX_ERR) != 0)
549 (*state->err_cb)(I2CECB_TX_ERR|b, i);
550 }
551 }
553 if ((n = state->rx_idx) > 0) {
554 for (i = 0; i < n; i++) {
555 rxbd = ((I2C_BD*)state->rxbd) - (n - i);
556 if ((b = rxbd->status & BD_I2C_RX_ERR) != 0)
557 (*state->err_cb)(I2CECB_RX_ERR|b, i);
558 }
559 }
561 if (j >= TOUT_LOOP)
562 (*state->err_cb)(I2CECB_TIMEOUT, 0);
563 }
565 return (j >= TOUT_LOOP) ? I2CERR_TIMEOUT : 0;
566 }
568 static int had_tx_nak;
570 static void
571 i2c_test_callback(int flags, int xnum)
572 {
573 if ((flags & I2CECB_TX_ERR) && (flags & I2CECB_TX_NAK))
574 had_tx_nak = 1;
575 }
577 int i2c_probe(uchar chip)
578 {
579 i2c_state_t state;
580 int rc;
581 uchar buf[1];
583 i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
585 i2c_newio(&state);
587 state.err_cb = i2c_test_callback;
588 had_tx_nak = 0;
590 rc = i2c_receive(&state, chip, 0, I2CF_START_COND|I2CF_STOP_COND, 1, buf);
592 if (rc != 0)
593 return (rc);
595 rc = i2c_doio(&state);
597 if ((rc != 0) && (rc != I2CERR_TIMEOUT))
598 return (rc);
600 return (had_tx_nak);
601 }
603 int i2c_read(uchar chip, uint addr, int alen, uchar *buffer, int len)
604 {
605 i2c_state_t state;
606 uchar xaddr[4];
607 int rc;
609 #ifdef CONFIG_LWMON
610 WATCHDOG_RESET();
611 #endif
613 xaddr[0] = (addr >> 24) & 0xFF;
614 xaddr[1] = (addr >> 16) & 0xFF;
615 xaddr[2] = (addr >> 8) & 0xFF;
616 xaddr[3] = addr & 0xFF;
618 #ifdef CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW
619 /*
620 * EEPROM chips that implement "address overflow" are ones like
621 * Catalyst 24WC04/08/16 which has 9/10/11 bits of address and the
622 * extra bits end up in the "chip address" bit slots. This makes
623 * a 24WC08 (1Kbyte) chip look like four 256 byte chips.
624 *
625 * Note that we consider the length of the address field to still
626 * be one byte because the extra address bits are hidden in the
627 * chip address.
628 */
629 chip |= ((addr >> (alen * 8)) & CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW);
630 #endif
632 i2c_newio(&state);
634 rc = i2c_send(&state, chip, 0, I2CF_START_COND, alen, &xaddr[4-alen]);
635 if (rc != 0) {
636 if (gd->have_console)
637 printf("i2c_read: i2c_send failed (%d)\n", rc);
638 return 1;
639 }
641 rc = i2c_receive(&state, chip, 0, I2CF_STOP_COND, len, buffer);
642 if (rc != 0) {
643 if (gd->have_console)
644 printf("i2c_read: i2c_receive failed (%d)\n", rc);
645 return 1;
646 }
648 rc = i2c_doio(&state);
649 if (rc != 0) {
650 if (gd->have_console)
651 printf("i2c_read: i2c_doio failed (%d)\n", rc);
652 return 1;
653 }
654 return 0;
655 }
657 int i2c_write(uchar chip, uint addr, int alen, uchar *buffer, int len)
658 {
659 i2c_state_t state;
660 uchar xaddr[4];
661 int rc;
663 xaddr[0] = (addr >> 24) & 0xFF;
664 xaddr[1] = (addr >> 16) & 0xFF;
665 xaddr[2] = (addr >> 8) & 0xFF;
666 xaddr[3] = addr & 0xFF;
668 #ifdef CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW
669 /*
670 * EEPROM chips that implement "address overflow" are ones like
671 * Catalyst 24WC04/08/16 which has 9/10/11 bits of address and the
672 * extra bits end up in the "chip address" bit slots. This makes
673 * a 24WC08 (1Kbyte) chip look like four 256 byte chips.
674 *
675 * Note that we consider the length of the address field to still
676 * be one byte because the extra address bits are hidden in the
677 * chip address.
678 */
679 chip |= ((addr >> (alen * 8)) & CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW);
680 #endif
682 i2c_newio(&state);
684 rc = i2c_send(&state, chip, 0, I2CF_START_COND, alen, &xaddr[4-alen]);
685 if (rc != 0) {
686 if (gd->have_console)
687 printf("i2c_write: first i2c_send failed (%d)\n", rc);
688 return 1;
689 }
691 rc = i2c_send(&state, 0, 0, I2CF_STOP_COND, len, buffer);
692 if (rc != 0) {
693 if (gd->have_console)
694 printf("i2c_write: second i2c_send failed (%d)\n", rc);
695 return 1;
696 }
698 rc = i2c_doio(&state);
699 if (rc != 0) {
700 if (gd->have_console)
701 printf("i2c_write: i2c_doio failed (%d)\n", rc);
702 return 1;
703 }
704 return 0;
705 }
707 #endif /* CONFIG_HARD_I2C */