1 /*
2 * Copyright 2008 Freescale Semiconductor, Inc.
3 *
4 * This program is free software; you can redistribute it and/or
5 * modify it under the terms of the GNU General Public License
6 * Version 2 as published by the Free Software Foundation.
7 */
9 /*
10 * Generic driver for Freescale DDR/DDR2/DDR3 memory controller.
11 * Based on code from spd_sdram.c
12 * Author: James Yang [at freescale.com]
13 */
15 #include <common.h>
16 #include <asm/fsl_ddr_sdram.h>
18 #include "ddr.h"
20 extern void fsl_ddr_set_lawbar(
21 const common_timing_params_t *memctl_common_params,
22 unsigned int memctl_interleaved,
23 unsigned int ctrl_num);
25 /* processor specific function */
26 extern void fsl_ddr_set_memctl_regs(const fsl_ddr_cfg_regs_t *regs,
27 unsigned int ctrl_num);
29 /* Board-specific functions defined in each board's ddr.c */
30 extern void fsl_ddr_get_spd(generic_spd_eeprom_t *ctrl_dimms_spd,
31 unsigned int ctrl_num);
33 /*
34 * ASSUMPTIONS:
35 * - Same number of CONFIG_DIMM_SLOTS_PER_CTLR on each controller
36 * - Same memory data bus width on all controllers
37 *
38 * NOTES:
39 *
40 * The memory controller and associated documentation use confusing
41 * terminology when referring to the orgranization of DRAM.
42 *
43 * Here is a terminology translation table:
44 *
45 * memory controller/documention |industry |this code |signals
46 * -------------------------------|-----------|-----------|-----------------
47 * physical bank/bank |rank |rank |chip select (CS)
48 * logical bank/sub-bank |bank |bank |bank address (BA)
49 * page/row |row |page |row address
50 * ??? |column |column |column address
51 *
52 * The naming confusion is further exacerbated by the descriptions of the
53 * memory controller interleaving feature, where accesses are interleaved
54 * _BETWEEN_ two seperate memory controllers. This is configured only in
55 * CS0_CONFIG[INTLV_CTL] of each memory controller.
56 *
57 * memory controller documentation | number of chip selects
58 * | per memory controller supported
59 * --------------------------------|-----------------------------------------
60 * cache line interleaving | 1 (CS0 only)
61 * page interleaving | 1 (CS0 only)
62 * bank interleaving | 1 (CS0 only)
63 * superbank interleraving | depends on bank (chip select)
64 * | interleraving [rank interleaving]
65 * | mode used on every memory controller
66 *
67 * Even further confusing is the existence of the interleaving feature
68 * _WITHIN_ each memory controller. The feature is referred to in
69 * documentation as chip select interleaving or bank interleaving,
70 * although it is configured in the DDR_SDRAM_CFG field.
71 *
72 * Name of field | documentation name | this code
73 * -----------------------------|-----------------------|------------------
74 * DDR_SDRAM_CFG[BA_INTLV_CTL] | Bank (chip select) | rank interleaving
75 * | interleaving
76 */
78 #ifdef DEBUG
79 const char *step_string_tbl[] = {
80 "STEP_GET_SPD",
81 "STEP_COMPUTE_DIMM_PARMS",
82 "STEP_COMPUTE_COMMON_PARMS",
83 "STEP_GATHER_OPTS",
84 "STEP_ASSIGN_ADDRESSES",
85 "STEP_COMPUTE_REGS",
86 "STEP_PROGRAM_REGS",
87 "STEP_ALL"
88 };
90 const char * step_to_string(unsigned int step) {
92 unsigned int s = __ilog2(step);
94 if ((1 << s) != step)
95 return step_string_tbl[7];
97 return step_string_tbl[s];
98 }
99 #endif
101 int step_assign_addresses(fsl_ddr_info_t *pinfo,
102 unsigned int dbw_cap_adj[],
103 unsigned int *memctl_interleaving,
104 unsigned int *rank_interleaving)
105 {
106 int i, j;
108 /*
109 * If a reduced data width is requested, but the SPD
110 * specifies a physically wider device, adjust the
111 * computed dimm capacities accordingly before
112 * assigning addresses.
113 */
114 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
115 unsigned int found = 0;
117 switch (pinfo->memctl_opts[i].data_bus_width) {
118 case 2:
119 /* 16-bit */
120 printf("can't handle 16-bit mode yet\n");
121 break;
123 case 1:
124 /* 32-bit */
125 for (j = 0; j < CONFIG_DIMM_SLOTS_PER_CTLR; j++) {
126 unsigned int dw;
127 dw = pinfo->dimm_params[i][j].data_width;
128 if (pinfo->dimm_params[i][j].n_ranks
129 && (dw == 72 || dw == 64)) {
130 /*
131 * FIXME: can't really do it
132 * like this because this just
133 * further reduces the memory
134 */
135 found = 1;
136 break;
137 }
138 }
139 if (found) {
140 dbw_cap_adj[i] = 1;
141 }
142 break;
144 case 0:
145 /* 64-bit */
146 break;
148 default:
149 printf("unexpected data bus width "
150 "specified controller %u\n", i);
151 return 1;
152 }
153 }
155 /*
156 * Check if all controllers are configured for memory
157 * controller interleaving.
158 */
159 j = 0;
160 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
161 if (pinfo->memctl_opts[i].memctl_interleaving) {
162 j++;
163 }
164 }
165 if (j == 2)
166 *memctl_interleaving = 1;
168 /* Check that all controllers are rank interleaving. */
169 j = 0;
170 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
171 if (pinfo->memctl_opts[i].ba_intlv_ctl) {
172 j++;
173 }
174 }
175 if (j == 2)
176 *rank_interleaving = 1;
178 if (*memctl_interleaving) {
179 unsigned long long addr, total_mem_per_ctlr = 0;
180 /*
181 * If interleaving between memory controllers,
182 * make each controller start at a base address
183 * of 0.
184 *
185 * Also, if bank interleaving (chip select
186 * interleaving) is enabled on each memory
187 * controller, CS0 needs to be programmed to
188 * cover the entire memory range on that memory
189 * controller
190 *
191 * Bank interleaving also implies that each
192 * addressed chip select is identical in size.
193 */
195 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
196 addr = 0;
197 pinfo->common_timing_params[i].base_address = 0ull;
198 for (j = 0; j < CONFIG_DIMM_SLOTS_PER_CTLR; j++) {
199 unsigned long long cap
200 = pinfo->dimm_params[i][j].capacity;
202 pinfo->dimm_params[i][j].base_address = addr;
203 addr += cap >> dbw_cap_adj[i];
204 total_mem_per_ctlr += cap >> dbw_cap_adj[i];
205 }
206 }
207 pinfo->common_timing_params[0].total_mem = total_mem_per_ctlr;
208 } else {
209 /*
210 * Simple linear assignment if memory
211 * controllers are not interleaved.
212 */
213 unsigned long long cur_memsize = 0;
214 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
215 u64 total_mem_per_ctlr = 0;
216 pinfo->common_timing_params[i].base_address =
217 cur_memsize;
218 for (j = 0; j < CONFIG_DIMM_SLOTS_PER_CTLR; j++) {
219 /* Compute DIMM base addresses. */
220 unsigned long long cap =
221 pinfo->dimm_params[i][j].capacity;
222 pinfo->dimm_params[i][j].base_address =
223 cur_memsize;
224 cur_memsize += cap >> dbw_cap_adj[i];
225 total_mem_per_ctlr += cap >> dbw_cap_adj[i];
226 }
227 pinfo->common_timing_params[i].total_mem =
228 total_mem_per_ctlr;
229 }
230 }
232 return 0;
233 }
235 unsigned long long
236 fsl_ddr_compute(fsl_ddr_info_t *pinfo, unsigned int start_step)
237 {
238 unsigned int i, j;
239 unsigned int all_controllers_memctl_interleaving = 0;
240 unsigned int all_controllers_rank_interleaving = 0;
241 unsigned long long total_mem = 0;
243 fsl_ddr_cfg_regs_t *ddr_reg = pinfo->fsl_ddr_config_reg;
244 common_timing_params_t *timing_params = pinfo->common_timing_params;
246 /* data bus width capacity adjust shift amount */
247 unsigned int dbw_capacity_adjust[CONFIG_NUM_DDR_CONTROLLERS];
249 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
250 dbw_capacity_adjust[i] = 0;
251 }
253 debug("starting at step %u (%s)\n",
254 start_step, step_to_string(start_step));
256 switch (start_step) {
257 case STEP_GET_SPD:
258 /* STEP 1: Gather all DIMM SPD data */
259 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
260 fsl_ddr_get_spd(pinfo->spd_installed_dimms[i], i);
261 }
263 case STEP_COMPUTE_DIMM_PARMS:
264 /* STEP 2: Compute DIMM parameters from SPD data */
266 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
267 for (j = 0; j < CONFIG_DIMM_SLOTS_PER_CTLR; j++) {
268 unsigned int retval;
269 generic_spd_eeprom_t *spd =
270 &(pinfo->spd_installed_dimms[i][j]);
271 dimm_params_t *pdimm =
272 &(pinfo->dimm_params[i][j]);
274 retval = compute_dimm_parameters(spd, pdimm, i);
275 if (retval == 2) {
276 printf("Error: compute_dimm_parameters"
277 " non-zero returned FATAL value "
278 "for memctl=%u dimm=%u\n", i, j);
279 return 0;
280 }
281 if (retval) {
282 debug("Warning: compute_dimm_parameters"
283 " non-zero return value for memctl=%u "
284 "dimm=%u\n", i, j);
285 }
286 }
287 }
289 case STEP_COMPUTE_COMMON_PARMS:
290 /*
291 * STEP 3: Compute a common set of timing parameters
292 * suitable for all of the DIMMs on each memory controller
293 */
294 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
295 debug("Computing lowest common DIMM"
296 " parameters for memctl=%u\n", i);
297 compute_lowest_common_dimm_parameters(
298 pinfo->dimm_params[i],
299 &timing_params[i],
300 CONFIG_DIMM_SLOTS_PER_CTLR);
301 }
303 case STEP_GATHER_OPTS:
304 /* STEP 4: Gather configuration requirements from user */
305 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
306 debug("Reloading memory controller "
307 "configuration options for memctl=%u\n", i);
308 /*
309 * This "reloads" the memory controller options
310 * to defaults. If the user "edits" an option,
311 * next_step points to the step after this,
312 * which is currently STEP_ASSIGN_ADDRESSES.
313 */
314 populate_memctl_options(
315 timing_params[i].all_DIMMs_registered,
316 &pinfo->memctl_opts[i],
317 pinfo->dimm_params[i], i);
318 }
320 case STEP_ASSIGN_ADDRESSES:
321 /* STEP 5: Assign addresses to chip selects */
322 step_assign_addresses(pinfo,
323 dbw_capacity_adjust,
324 &all_controllers_memctl_interleaving,
325 &all_controllers_rank_interleaving);
327 case STEP_COMPUTE_REGS:
328 /* STEP 6: compute controller register values */
329 debug("FSL Memory ctrl cg register computation\n");
330 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
331 if (timing_params[i].ndimms_present == 0) {
332 memset(&ddr_reg[i], 0,
333 sizeof(fsl_ddr_cfg_regs_t));
334 continue;
335 }
337 compute_fsl_memctl_config_regs(
338 &pinfo->memctl_opts[i],
339 &ddr_reg[i], &timing_params[i],
340 pinfo->dimm_params[i],
341 dbw_capacity_adjust[i]);
342 }
344 default:
345 break;
346 }
348 /* Compute the total amount of memory. */
350 /*
351 * If bank interleaving but NOT memory controller interleaving
352 * CS_BNDS describe the quantity of memory on each memory
353 * controller, so the total is the sum across.
354 */
355 if (!all_controllers_memctl_interleaving
356 && all_controllers_rank_interleaving) {
357 total_mem = 0;
358 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
359 total_mem += timing_params[i].total_mem;
360 }
362 } else {
363 /*
364 * Compute the amount of memory available just by
365 * looking for the highest valid CSn_BNDS value.
366 * This allows us to also experiment with using
367 * only CS0 when using dual-rank DIMMs.
368 */
369 unsigned int max_end = 0;
371 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
372 for (j = 0; j < CONFIG_CHIP_SELECTS_PER_CTRL; j++) {
373 fsl_ddr_cfg_regs_t *reg = &ddr_reg[i];
374 if (reg->cs[j].config & 0x80000000) {
375 unsigned int end;
376 end = reg->cs[j].bnds & 0xFFF;
377 if (end > max_end) {
378 max_end = end;
379 }
380 }
381 }
382 }
384 total_mem = 1 + (((unsigned long long)max_end << 24ULL)
385 | 0xFFFFFFULL);
386 }
388 return total_mem;
389 }
391 /*
392 * fsl_ddr_sdram() -- this is the main function to be called by
393 * initdram() in the board file.
394 *
395 * It returns amount of memory configured in bytes.
396 */
397 phys_size_t fsl_ddr_sdram(void)
398 {
399 unsigned int i;
400 unsigned int memctl_interleaved;
401 unsigned long long total_memory;
402 fsl_ddr_info_t info;
404 /* Reset info structure. */
405 memset(&info, 0, sizeof(fsl_ddr_info_t));
407 /* Compute it once normally. */
408 total_memory = fsl_ddr_compute(&info, STEP_GET_SPD);
410 /* Check for memory controller interleaving. */
411 memctl_interleaved = 0;
412 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
413 memctl_interleaved +=
414 info.memctl_opts[i].memctl_interleaving;
415 }
417 if (memctl_interleaved) {
418 if (memctl_interleaved == CONFIG_NUM_DDR_CONTROLLERS) {
419 debug("memctl interleaving\n");
420 /*
421 * Change the meaning of memctl_interleaved
422 * to be "boolean".
423 */
424 memctl_interleaved = 1;
425 } else {
426 printf("Warning: memctl interleaving not "
427 "properly configured on all controllers\n");
428 memctl_interleaved = 0;
429 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++)
430 info.memctl_opts[i].memctl_interleaving = 0;
431 debug("Recomputing with memctl_interleaving off.\n");
432 total_memory = fsl_ddr_compute(&info,
433 STEP_ASSIGN_ADDRESSES);
434 }
435 }
437 /* Program configuration registers. */
438 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
439 debug("Programming controller %u\n", i);
440 if (info.common_timing_params[i].ndimms_present == 0) {
441 debug("No dimms present on controller %u; "
442 "skipping programming\n", i);
443 continue;
444 }
446 fsl_ddr_set_memctl_regs(&(info.fsl_ddr_config_reg[i]), i);
447 }
449 if (memctl_interleaved) {
450 const unsigned int ctrl_num = 0;
452 /* Only set LAWBAR1 if memory controller interleaving is on. */
453 fsl_ddr_set_lawbar(&info.common_timing_params[0],
454 memctl_interleaved, ctrl_num);
455 } else {
456 /*
457 * Memory controller interleaving is NOT on;
458 * set each lawbar individually.
459 */
460 for (i = 0; i < CONFIG_NUM_DDR_CONTROLLERS; i++) {
461 fsl_ddr_set_lawbar(&info.common_timing_params[i],
462 0, i);
463 }
464 }
466 debug("total_memory = %llu\n", total_memory);
468 #if !defined(CONFIG_PHYS_64BIT)
469 /* Check for 4G or more. Bad. */
470 if (total_memory >= (1ull << 32)) {
471 printf("Detected %lld MB of memory\n", total_memory >> 20);
472 printf("This U-Boot only supports < 4G of DDR\n");
473 printf("You could rebuild it with CONFIG_PHYS_64BIT\n");
474 total_memory = CONFIG_MAX_MEM_MAPPED;
475 }
476 #endif
478 return total_memory;
479 }