1 /*
2 * Copyright 2009-2010 Freescale Semiconductor, Inc.
3 *
4 * See file CREDITS for list of people who contributed to this
5 * project.
6 *
7 * This program is free software; you can redistribute it and/or
8 * modify it under the terms of the GNU General Public License as
9 * published by the Free Software Foundation; either version 2 of
10 * the License, or (at your option) any later version.
11 *
12 * This program is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15 * GNU General Public License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with this program; if not, write to the Free Software
19 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
20 * MA 02111-1307 USA
21 */
23 #include <common.h>
24 #include <asm/fsl_law.h>
25 #include <pci.h>
27 struct pci_info {
28 u32 cfg;
29 };
31 /* The cfg field is a bit mask in which each bit represents the value of
32 * cfg_IO_ports[] signal and the bit is set if the interface would be
33 * enabled based on the value of cfg_IO_ports[] signal
34 *
35 * On MPC86xx/PQ3 based systems:
36 * we extract cfg_IO_ports from GUTS register PORDEVSR
37 *
38 * cfg_IO_ports only exist on systems w/PCIe (we set cfg 0 for systems
39 * without PCIe)
40 */
42 #if defined(CONFIG_MPC8540) || defined(CONFIG_MPC8560)
43 static struct pci_info pci_config_info[] =
44 {
45 [LAW_TRGT_IF_PCI] = {
46 .cfg = 0,
47 },
48 };
49 #elif defined(CONFIG_MPC8541) || defined(CONFIG_MPC8555)
50 static struct pci_info pci_config_info[] =
51 {
52 [LAW_TRGT_IF_PCI] = {
53 .cfg = 0,
54 },
55 };
56 #elif defined(CONFIG_MPC8536)
57 static struct pci_info pci_config_info[] =
58 {
59 [LAW_TRGT_IF_PCI] = {
60 .cfg = 0,
61 },
62 [LAW_TRGT_IF_PCIE_1] = {
63 .cfg = (1 << 2) | (1 << 3) | (1 << 5) | (1 << 7),
64 },
65 [LAW_TRGT_IF_PCIE_2] = {
66 .cfg = (1 << 5) | (1 << 7),
67 },
68 [LAW_TRGT_IF_PCIE_3] = {
69 .cfg = (1 << 7),
70 },
71 };
72 #elif defined(CONFIG_MPC8544)
73 static struct pci_info pci_config_info[] =
74 {
75 [LAW_TRGT_IF_PCI] = {
76 .cfg = 0,
77 },
78 [LAW_TRGT_IF_PCIE_1] = {
79 .cfg = (1 << 2) | (1 << 3) | (1 << 4) | (1 << 5) |
80 (1 << 6) | (1 << 7),
81 },
82 [LAW_TRGT_IF_PCIE_2] = {
83 .cfg = (1 << 4) | (1 << 5) | (1 << 6) | (1 << 7),
84 },
85 [LAW_TRGT_IF_PCIE_3] = {
86 .cfg = (1 << 6) | (1 << 7),
87 },
88 };
89 #elif defined(CONFIG_MPC8548)
90 static struct pci_info pci_config_info[] =
91 {
92 [LAW_TRGT_IF_PCI_1] = {
93 .cfg = 0,
94 },
95 [LAW_TRGT_IF_PCI_2] = {
96 .cfg = 0,
97 },
98 /* PCI_2 is always host and we dont use iosel to determine enable/disable */
99 [LAW_TRGT_IF_PCIE_1] = {
100 .cfg = (1 << 3) | (1 << 4) | (1 << 7),
101 },
102 };
103 #elif defined(CONFIG_MPC8568)
104 static struct pci_info pci_config_info[] =
105 {
106 [LAW_TRGT_IF_PCI] = {
107 .cfg = 0,
108 },
109 [LAW_TRGT_IF_PCIE_1] = {
110 .cfg = (1 << 3) | (1 << 4) | (1 << 7),
111 },
112 };
113 #elif defined(CONFIG_MPC8569)
114 static struct pci_info pci_config_info[] =
115 {
116 [LAW_TRGT_IF_PCIE_1] = {
117 .cfg = (1 << 0) | (1 << 4) | (1 << 5) | (1 << 6) | (1 << 7) |
118 (1 << 8) | (1 << 0xc) | (1 << 0xf),
119 },
120 };
121 #elif defined(CONFIG_MPC8572)
122 static struct pci_info pci_config_info[] =
123 {
124 [LAW_TRGT_IF_PCIE_1] = {
125 .cfg = (1 << 2) | (1 << 3) | (1 << 7) |
126 (1 << 0xb) | (1 << 0xc) | (1 << 0xf),
127 },
128 [LAW_TRGT_IF_PCIE_2] = {
129 .cfg = (1 << 3) | (1 << 7),
130 },
131 [LAW_TRGT_IF_PCIE_3] = {
132 .cfg = (1 << 7),
133 },
134 };
135 #elif defined(CONFIG_MPC8610)
136 static struct pci_info pci_config_info[] =
137 {
138 [LAW_TRGT_IF_PCI_1] = {
139 .cfg = 0,
140 },
141 [LAW_TRGT_IF_PCIE_1] = {
142 .cfg = (1 << 1) | (1 << 4),
143 },
144 [LAW_TRGT_IF_PCIE_2] = {
145 .cfg = (1 << 0) | (1 << 4),
146 },
147 };
148 #elif defined(CONFIG_MPC8641)
149 static struct pci_info pci_config_info[] =
150 {
151 [LAW_TRGT_IF_PCIE_1] = {
152 .cfg = (1 << 2) | (1 << 3) | (1 << 5) | (1 << 6) |
153 (1 << 7) | (1 << 0xe) | (1 << 0xf),
154 },
155 };
156 #elif defined(CONFIG_P1011) || defined(CONFIG_P1020) || \
157 defined(CONFIG_P1012) || defined(CONFIG_P1021)
158 static struct pci_info pci_config_info[] =
159 {
160 [LAW_TRGT_IF_PCIE_1] = {
161 .cfg = (1 << 0) | (1 << 6) | (1 << 0xe) | (1 << 0xf),
162 },
163 [LAW_TRGT_IF_PCIE_2] = {
164 .cfg = (1 << 0xe),
165 },
166 };
167 #elif defined(CONFIG_P1013) || defined(CONFIG_P1022)
168 static struct pci_info pci_config_info[] =
169 {
170 [LAW_TRGT_IF_PCIE_1] = {
171 .cfg = (1 << 6) | (1 << 7) | (1 << 9) | (1 << 0xa) |
172 (1 << 0xb) | (1 << 0xd) | (1 << 0xe) |
173 (1 << 0xf) | (1 << 0x15) | (1 << 0x16) |
174 (1 << 0x17) | (1 << 0x18) | (1 << 0x19) |
175 (1 << 0x1a) | (1 << 0x1b) | (1 << 0x1c) |
176 (1 << 0x1d) | (1 << 0x1e) | (1 << 0x1f),
177 },
178 [LAW_TRGT_IF_PCIE_2] = {
179 .cfg = (1 << 0) | (1 << 1) | (1 << 6) | (1 << 7) |
180 (1 << 9) | (1 << 0xa) | (1 << 0xb) | (1 << 0xd) |
181 (1 << 0x15) | (1 << 0x16) | (1 << 0x17) |
182 (1 << 0x18) | (1 << 0x1c),
183 },
184 [LAW_TRGT_IF_PCIE_3] = {
185 .cfg = (1 << 6) | (1 << 7) | (1 << 9) | (1 << 0xd) |
186 (1 << 0x15) | (1 << 0x16) | (1 << 0x17) | (1 << 0x18) |
187 (1 << 0x19) | (1 << 0x1a) | (1 << 0x1b),
188 },
189 };
190 #elif defined(CONFIG_P2010) || defined(CONFIG_P2020)
191 static struct pci_info pci_config_info[] =
192 {
193 [LAW_TRGT_IF_PCIE_1] = {
194 .cfg = (1 << 0) | (1 << 2) | (1 << 4) | (1 << 6) |
195 (1 << 0xd) | (1 << 0xe) | (1 << 0xf),
196 },
197 [LAW_TRGT_IF_PCIE_2] = {
198 .cfg = (1 << 2) | (1 << 0xe),
199 },
200 [LAW_TRGT_IF_PCIE_3] = {
201 .cfg = (1 << 2) | (1 << 4),
202 },
203 };
204 #elif defined(CONFIG_FSL_CORENET)
205 #else
206 #error Need to define pci_config_info for processor
207 #endif
209 #ifndef CONFIG_FSL_CORENET
210 int is_fsl_pci_cfg(enum law_trgt_if trgt, u32 io_sel)
211 {
212 return ((1 << io_sel) & pci_config_info[trgt].cfg);
213 }
214 #endif