]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/powerpc/include/asm/global_data.h
Merge remote-tracking branch 'u-boot-ti/master'
[glsdk/glsdk-u-boot.git] / arch / powerpc / include / asm / global_data.h
1 /*
2  * (C) Copyright 2002-2010
3  * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #ifndef __ASM_GBL_DATA_H
25 #define __ASM_GBL_DATA_H
27 #include "config.h"
28 #include "asm/types.h"
30 /*
31  * The following data structure is placed in some memory wich is
32  * available very early after boot (like DPRAM on MPC8xx/MPC82xx, or
33  * some locked parts of the data cache) to allow for a minimum set of
34  * global variables during system initialization (until we have set
35  * up the memory controller so that we can use RAM).
36  */
38 typedef struct  global_data {
39         bd_t            *bd;
40         unsigned long   flags;
41         unsigned int    baudrate;
42         unsigned long   cpu_clk;        /* CPU clock in Hz! */
43         unsigned long   bus_clk;
44 #if defined(CONFIG_8xx)
45         unsigned long   brg_clk;
46 #endif
47 #if defined(CONFIG_CPM2)
48         /* There are many clocks on the MPC8260 - see page 9-5 */
49         unsigned long   vco_out;
50         unsigned long   cpm_clk;
51         unsigned long   scc_clk;
52         unsigned long   brg_clk;
53 #ifdef CONFIG_PCI
54         unsigned long   pci_clk;
55 #endif
56 #endif
57         unsigned long   mem_clk;
58 #if defined(CONFIG_MPC83xx)
59         /* There are other clocks in the MPC83XX */
60         u32 csb_clk;
61 #if defined(CONFIG_MPC8308) || defined(CONFIG_MPC831x) || \
62         defined(CONFIG_MPC834x) || defined(CONFIG_MPC837x)
63         u32 tsec1_clk;
64         u32 tsec2_clk;
65         u32 usbdr_clk;
66 #elif defined(CONFIG_MPC8309)
67         u32 usbdr_clk;
68 #endif
69 #if defined (CONFIG_MPC834x)
70         u32 usbmph_clk;
71 #endif /* CONFIG_MPC834x */
72 #if defined(CONFIG_MPC8315)
73         u32 tdm_clk;
74 #endif
75         u32 core_clk;
76         u32 enc_clk;
77         u32 lbiu_clk;
78         u32 lclk_clk;
79         u32 pci_clk;
80 #if defined(CONFIG_MPC8308) || defined(CONFIG_MPC831x) || \
81         defined(CONFIG_MPC837x)
82         u32 pciexp1_clk;
83         u32 pciexp2_clk;
84 #endif
85 #if defined(CONFIG_MPC837x) || defined(CONFIG_MPC8315)
86         u32 sata_clk;
87 #endif
88 #if defined(CONFIG_MPC8360)
89         u32  mem_sec_clk;
90 #endif /* CONFIG_MPC8360 */
91 #endif
92 #if defined(CONFIG_FSL_ESDHC)
93         u32 sdhc_clk;
94 #endif
95 #if defined(CONFIG_MPC85xx) || defined(CONFIG_MPC86xx)
96         u32 lbc_clk;
97         void *cpu;
98 #endif /* CONFIG_MPC85xx || CONFIG_MPC86xx */
99 #if defined(CONFIG_MPC83xx) || defined(CONFIG_MPC85xx) || defined(CONFIG_MPC86xx)
100         u32 i2c1_clk;
101         u32 i2c2_clk;
102 #endif
103 #if defined(CONFIG_QE)
104         u32 qe_clk;
105         u32 brg_clk;
106         uint mp_alloc_base;
107         uint mp_alloc_top;
108 #endif /* CONFIG_QE */
109 #if defined(CONFIG_FSL_LAW)
110         u32 used_laws;
111 #endif
112 #if defined(CONFIG_E500)
113         u32 used_tlb_cams[(CONFIG_SYS_NUM_TLBCAMS+31)/32];
114 #endif
115 #if defined(CONFIG_MPC5xxx)
116         unsigned long   ipb_clk;
117         unsigned long   pci_clk;
118 #endif
119 #if defined(CONFIG_MPC512X)
120         u32 ips_clk;
121         u32 csb_clk;
122         u32 pci_clk;
123 #endif /* CONFIG_MPC512X */
124 #if defined(CONFIG_MPC8220)
125         unsigned long   bExtUart;
126         unsigned long   inp_clk;
127         unsigned long   pci_clk;
128         unsigned long   vco_clk;
129         unsigned long   pev_clk;
130         unsigned long   flb_clk;
131 #endif
132         phys_size_t     ram_size;       /* RAM size */
133         unsigned long   reset_status;   /* reset status register at boot        */
134 #if defined(CONFIG_MPC83xx)
135         unsigned long   arbiter_event_attributes;
136         unsigned long   arbiter_event_address;
137 #endif
138         unsigned long   env_addr;       /* Address  of Environment struct       */
139         unsigned long   env_valid;      /* Checksum of Environment valid?       */
140         unsigned long   have_console;   /* serial_init() was called             */
141 #ifdef CONFIG_PRE_CONSOLE_BUFFER
142         unsigned long   precon_buf_idx; /* Pre-Console buffer index */
143 #endif
144 #if defined(CONFIG_SYS_ALLOC_DPRAM) || defined(CONFIG_CPM2)
145         unsigned int    dp_alloc_base;
146         unsigned int    dp_alloc_top;
147 #endif
148 #if defined(CONFIG_4xx)
149         u32  uart_clk;
150 #endif /* CONFIG_4xx */
151 #if defined(CONFIG_SYS_GT_6426x)
152         unsigned int    mirror_hack[16];
153 #endif
154 #if defined(CONFIG_A3000)       || \
155     defined(CONFIG_HIDDEN_DRAGON)  || \
156     defined(CONFIG_MUSENKI)     ||  \
157     defined(CONFIG_SANDPOINT)
158         void *          console_addr;
159 #endif
160         unsigned long   relocaddr;      /* Start address of U-Boot in RAM */
161 #if defined(CONFIG_LCD) || defined(CONFIG_VIDEO)
162         unsigned long   fb_base;        /* Base address of framebuffer memory   */
163 #endif
164 #if defined(CONFIG_POST) || defined(CONFIG_LOGBUFFER)
165         unsigned long   post_log_word;  /* Record POST activities */
166         unsigned long   post_log_res; /* success of POST test */
167         unsigned long   post_init_f_time;  /* When post_init_f started */
168 #endif
169 #ifdef CONFIG_BOARD_TYPES
170         unsigned long   board_type;
171 #endif
172 #ifdef CONFIG_MODEM_SUPPORT
173         unsigned long do_mdm_init;
174         unsigned long be_quiet;
175 #endif
176 #if defined(CONFIG_LWMON) || defined(CONFIG_LWMON5)
177         unsigned long kbd_status;
178 #endif
179 #ifdef CONFIG_SYS_FPGA_COUNT
180         unsigned fpga_state[CONFIG_SYS_FPGA_COUNT];
181 #endif
182 #if defined(CONFIG_WD_MAX_RATE)
183         unsigned long long wdt_last;    /* trace watch-dog triggering rate */
184 #endif
185         void            **jt;           /* jump table */
186         char            env_buf[32];    /* buffer for getenv() before reloc. */
187 } gd_t;
189 #include <asm-generic/global_data_flags.h>
191 #if 1
192 #define DECLARE_GLOBAL_DATA_PTR     register volatile gd_t *gd asm ("r2")
193 #else /* We could use plain global data, but the resulting code is bigger */
194 #define XTRN_DECLARE_GLOBAL_DATA_PTR    extern
195 #define DECLARE_GLOBAL_DATA_PTR     XTRN_DECLARE_GLOBAL_DATA_PTR \
196                                     gd_t *gd
197 #endif
199 #endif /* __ASM_GBL_DATA_H */