1 /*
2 * (C) Copyright 2002
3 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #ifndef __ASM_GBL_DATA_H
25 #define __ASM_GBL_DATA_H
27 #include "config.h"
28 #include "asm/types.h"
30 /*
31 * The following data structure is placed in some memory wich is
32 * available very early after boot (like DPRAM on MPC8xx/MPC82xx, or
33 * some locked parts of the data cache) to allow for a minimum set of
34 * global variables during system initialization (until we have set
35 * up the memory controller so that we can use RAM).
36 *
37 * Keep it *SMALL* and remember to set CONFIG_SYS_GBL_DATA_SIZE > sizeof(gd_t)
38 */
40 typedef struct global_data {
41 bd_t *bd;
42 unsigned long flags;
43 unsigned long baudrate;
44 unsigned long cpu_clk; /* CPU clock in Hz! */
45 unsigned long bus_clk;
46 #if defined(CONFIG_8xx)
47 unsigned long brg_clk;
48 #endif
49 #if defined(CONFIG_CPM2)
50 /* There are many clocks on the MPC8260 - see page 9-5 */
51 unsigned long vco_out;
52 unsigned long cpm_clk;
53 unsigned long scc_clk;
54 unsigned long brg_clk;
55 #ifdef CONFIG_PCI
56 unsigned long pci_clk;
57 #endif
58 #endif
59 unsigned long mem_clk;
60 #if defined(CONFIG_MPC83xx)
61 /* There are other clocks in the MPC83XX */
62 u32 csb_clk;
63 #if defined(CONFIG_MPC834x) || defined(CONFIG_MPC831x) || defined(CONFIG_MPC837x)
64 u32 tsec1_clk;
65 u32 tsec2_clk;
66 u32 usbdr_clk;
67 #endif
68 #if defined (CONFIG_MPC834x)
69 u32 usbmph_clk;
70 #endif /* CONFIG_MPC834x */
71 #if defined(CONFIG_MPC8315)
72 u32 tdm_clk;
73 #endif
74 u32 core_clk;
75 u32 enc_clk;
76 u32 lbiu_clk;
77 u32 lclk_clk;
78 u32 pci_clk;
79 #if defined(CONFIG_MPC837x) || defined(CONFIG_MPC831x)
80 u32 pciexp1_clk;
81 u32 pciexp2_clk;
82 #endif
83 #if defined(CONFIG_MPC837x) || defined(CONFIG_MPC8315)
84 u32 sata_clk;
85 #endif
86 #if defined(CONFIG_MPC8360)
87 u32 mem_sec_clk;
88 #endif /* CONFIG_MPC8360 */
89 #endif
90 #if defined(CONFIG_FSL_ESDHC)
91 u32 sdhc_clk;
92 #endif
93 #if defined(CONFIG_MPC85xx) || defined(CONFIG_MPC86xx)
94 u32 lbc_clk;
95 void *cpu;
96 #endif /* CONFIG_MPC85xx || CONFIG_MPC86xx */
97 #if defined(CONFIG_MPC83xx) || defined(CONFIG_MPC85xx) || defined(CONFIG_MPC86xx)
98 u32 i2c1_clk;
99 u32 i2c2_clk;
100 #endif
101 #if defined(CONFIG_QE)
102 u32 qe_clk;
103 u32 brg_clk;
104 uint mp_alloc_base;
105 uint mp_alloc_top;
106 #endif /* CONFIG_QE */
107 #if defined(CONFIG_FSL_LAW)
108 u32 used_laws;
109 #endif
110 #if defined(CONFIG_E500)
111 u32 used_tlb_cams[(CONFIG_SYS_NUM_TLBCAMS+31)/32];
112 #endif
113 #if defined(CONFIG_MPC5xxx)
114 unsigned long ipb_clk;
115 unsigned long pci_clk;
116 #endif
117 #if defined(CONFIG_MPC512X)
118 u32 ips_clk;
119 u32 csb_clk;
120 u32 pci_clk;
121 #endif /* CONFIG_MPC512X */
122 #if defined(CONFIG_MPC8220)
123 unsigned long bExtUart;
124 unsigned long inp_clk;
125 unsigned long pci_clk;
126 unsigned long vco_clk;
127 unsigned long pev_clk;
128 unsigned long flb_clk;
129 #endif
130 phys_size_t ram_size; /* RAM size */
131 unsigned long reset_status; /* reset status register at boot */
132 #if defined(CONFIG_MPC83xx)
133 unsigned long arbiter_event_attributes;
134 unsigned long arbiter_event_address;
135 #endif
136 unsigned long env_addr; /* Address of Environment struct */
137 unsigned long env_valid; /* Checksum of Environment valid? */
138 unsigned long have_console; /* serial_init() was called */
139 #if defined(CONFIG_SYS_ALLOC_DPRAM) || defined(CONFIG_CPM2)
140 unsigned int dp_alloc_base;
141 unsigned int dp_alloc_top;
142 #endif
143 #if defined(CONFIG_4xx)
144 u32 uart_clk;
145 #endif /* CONFIG_4xx */
146 #if defined(CONFIG_SYS_GT_6426x)
147 unsigned int mirror_hack[16];
148 #endif
149 #if defined(CONFIG_A3000) || \
150 defined(CONFIG_HIDDEN_DRAGON) || \
151 defined(CONFIG_MUSENKI) || \
152 defined(CONFIG_SANDPOINT)
153 void * console_addr;
154 #endif
155 unsigned long relocaddr; /* Start address of U-Boot in RAM */
156 #if defined(CONFIG_LCD) || defined(CONFIG_VIDEO)
157 unsigned long fb_base; /* Base address of framebuffer memory */
158 #endif
159 #if defined(CONFIG_POST) || defined(CONFIG_LOGBUFFER)
160 unsigned long post_log_word; /* Record POST activities */
161 unsigned long post_init_f_time; /* When post_init_f started */
162 #endif
163 #ifdef CONFIG_BOARD_TYPES
164 unsigned long board_type;
165 #endif
166 #ifdef CONFIG_MODEM_SUPPORT
167 unsigned long do_mdm_init;
168 unsigned long be_quiet;
169 #endif
170 #if defined(CONFIG_LWMON) || defined(CONFIG_LWMON5)
171 unsigned long kbd_status;
172 #endif
173 #if defined(CONFIG_WD_MAX_RATE)
174 unsigned long long wdt_last; /* trace watch-dog triggering rate */
175 #endif
176 void **jt; /* jump table */
177 } gd_t;
179 /*
180 * Global Data Flags
181 */
182 #define GD_FLG_RELOC 0x00001 /* Code was relocated to RAM */
183 #define GD_FLG_DEVINIT 0x00002 /* Devices have been initialized */
184 #define GD_FLG_SILENT 0x00004 /* Silent mode */
185 #define GD_FLG_POSTFAIL 0x00008 /* Critical POST test failed */
186 #define GD_FLG_POSTSTOP 0x00010 /* POST seqeunce aborted */
187 #define GD_FLG_LOGINIT 0x00020 /* Log Buffer has been initialized */
188 #define GD_FLG_DISABLE_CONSOLE 0x00040 /* Disable console (in & out) */
190 #if 1
191 #define DECLARE_GLOBAL_DATA_PTR register volatile gd_t *gd asm ("r2")
192 #else /* We could use plain global data, but the resulting code is bigger */
193 #define XTRN_DECLARE_GLOBAL_DATA_PTR extern
194 #define DECLARE_GLOBAL_DATA_PTR XTRN_DECLARE_GLOBAL_DATA_PTR \
195 gd_t *gd
196 #endif
198 #endif /* __ASM_GBL_DATA_H */