1 /*
2 * (C) Copyright 2008
3 * Ricado Ribalda-Universidad Autonoma de Madrid-ricardo.ribalda@uam.es
4 * This work has been supported by: QTechnology http://qtec.com/
5 * Based on interrupts.c Wolfgang Denk-DENX Software Engineering-wd@denx.de
6 *
7 * This program is free software: you can redistribute it and/or modify
8 * it under the terms of the GNU General Public License as published by
9 * the Free Software Foundation, either version 2 of the License, or
10 * (at your option) any later version.
11 *
12 * This program is distributed in the hope that it will be useful,
13 * but WITHOUT ANY WARRANTY; without even the implied warranty of
14 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
15 * GNU General Public License for more details.
16 *
17 * You should have received a copy of the GNU General Public License
18 * along with this program. If not, see <http://www.gnu.org/licenses/>.
19 */
20 #ifndef INTERRUPT_H
21 #define INTERRUPT_H
23 #if defined(CONFIG_XILINX_440)
24 #include <asm/xilinx_irq.h>
25 #else
26 #include <asm/ppc4xx-uic.h>
27 #endif
29 void pic_enable(void);
30 void pic_irq_enable(unsigned int irq);
31 void pic_irq_disable(unsigned int irq);
32 void pic_irq_ack(unsigned int irq);
33 void external_interrupt(struct pt_regs *regs);
34 void interrupt_run_handler(int vec);
36 #endif