]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/ppc/cpu/mpc8260/commproc.c
fsl_i2c: Added a callpoint for i2c_board_late_init
[glsdk/glsdk-u-boot.git] / arch / ppc / cpu / mpc8260 / commproc.c
1 /*
2  * This file is based on "arch/ppc/8260_io/commproc.c" - here is it's
3  * copyright notice:
4  *
5  * General Purpose functions for the global management of the
6  * 8260 Communication Processor Module.
7  * Copyright (c) 1999 Dan Malek (dmalek@jlc.net)
8  * Copyright (c) 2000 MontaVista Software, Inc (source@mvista.com)
9  *      2.3.99 Updates
10  *
11  * In addition to the individual control of the communication
12  * channels, there are a few functions that globally affect the
13  * communication processor.
14  *
15  * Buffer descriptors must be allocated from the dual ported memory
16  * space.  The allocator for that is here.  When the communication
17  * process is reset, we reclaim the memory available.  There is
18  * currently no deallocator for this memory.
19  */
20 #include <common.h>
21 #include <asm/cpm_8260.h>
23 DECLARE_GLOBAL_DATA_PTR;
25 void
26 m8260_cpm_reset(void)
27 {
28         volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
29         volatile ulong count;
31         /* Reclaim the DP memory for our use.
32         */
33         gd->dp_alloc_base = CPM_DATAONLY_BASE;
34         gd->dp_alloc_top = gd->dp_alloc_base + CPM_DATAONLY_SIZE;
36         /*
37          * Reset CPM
38          */
39         immr->im_cpm.cp_cpcr = CPM_CR_RST;
40         count = 0;
41         do {                    /* Spin until command processed         */
42                 __asm__ __volatile__ ("eieio");
43         } while ((immr->im_cpm.cp_cpcr & CPM_CR_FLG) && ++count < 1000000);
45 #ifdef CONFIG_HARD_I2C
46         *((unsigned short*)(&immr->im_dprambase[PROFF_I2C_BASE])) = 0;
47 #endif
48 }
50 /* Allocate some memory from the dual ported ram.
51  * To help protocols with object alignment restrictions, we do that
52  * if they ask.
53  */
54 uint
55 m8260_cpm_dpalloc(uint size, uint align)
56 {
57         volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
58         uint    retloc;
59         uint    align_mask, off;
60         uint    savebase;
62         align_mask = align - 1;
63         savebase = gd->dp_alloc_base;
65         if ((off = (gd->dp_alloc_base & align_mask)) != 0)
66                 gd->dp_alloc_base += (align - off);
68         if ((off = size & align_mask) != 0)
69                 size += align - off;
71         if ((gd->dp_alloc_base + size) >= gd->dp_alloc_top) {
72                 gd->dp_alloc_base = savebase;
73                 panic("m8260_cpm_dpalloc: ran out of dual port ram!");
74         }
76         retloc = gd->dp_alloc_base;
77         gd->dp_alloc_base += size;
79         memset((void *)&immr->im_dprambase[retloc], 0, size);
81         return(retloc);
82 }
84 /* We also own one page of host buffer space for the allocation of
85  * UART "fifos" and the like.
86  */
87 uint
88 m8260_cpm_hostalloc(uint size, uint align)
89 {
90         /* the host might not even have RAM yet - just use dual port RAM */
91         return (m8260_cpm_dpalloc(size, align));
92 }
94 /* Set a baud rate generator.  This needs lots of work.  There are
95  * eight BRGs, which can be connected to the CPM channels or output
96  * as clocks.  The BRGs are in two different block of internal
97  * memory mapped space.
98  * The baud rate clock is the system clock divided by something.
99  * It was set up long ago during the initial boot phase and is
100  * is given to us.
101  * Baud rate clocks are zero-based in the driver code (as that maps
102  * to port numbers).  Documentation uses 1-based numbering.
103  */
104 #define BRG_INT_CLK     gd->brg_clk
105 #define BRG_UART_CLK    (BRG_INT_CLK / 16)
107 /* This function is used by UARTs, or anything else that uses a 16x
108  * oversampled clock.
109  */
110 void
111 m8260_cpm_setbrg(uint brg, uint rate)
113         volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
114         volatile uint   *bp;
115         uint cd = BRG_UART_CLK / rate;
117         if ((BRG_UART_CLK % rate) < (rate / 2))
118                 cd--;
119         if (brg < 4) {
120                 bp = (uint *)&immr->im_brgc1;
121         }
122         else {
123                 bp = (uint *)&immr->im_brgc5;
124                 brg -= 4;
125         }
126         bp += brg;
127         *bp = (cd << 1) | CPM_BRG_EN;
130 /* This function is used to set high speed synchronous baud rate
131  * clocks.
132  */
133 void
134 m8260_cpm_fastbrg(uint brg, uint rate, int div16)
136         volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
137         volatile uint   *bp;
139         /* This is good enough to get SMCs running.....
140         */
141         if (brg < 4) {
142                 bp = (uint *)&immr->im_brgc1;
143         }
144         else {
145                 bp = (uint *)&immr->im_brgc5;
146                 brg -= 4;
147         }
148         bp += brg;
149         *bp = (((((BRG_INT_CLK+rate-1)/rate)-1)&0xfff)<<1)|CPM_BRG_EN;
150         if (div16)
151                 *bp |= CPM_BRG_DIV16;
154 /* This function is used to set baud rate generators using an external
155  * clock source and 16x oversampling.
156  */
158 void
159 m8260_cpm_extcbrg(uint brg, uint rate, uint extclk, int pinsel)
161         volatile immap_t *immr = (immap_t *)CONFIG_SYS_IMMR;
162         volatile uint   *bp;
164         if (brg < 4) {
165                 bp = (uint *)&immr->im_brgc1;
166         }
167         else {
168                 bp = (uint *)&immr->im_brgc5;
169                 brg -= 4;
170         }
171         bp += brg;
172         *bp = ((((((extclk/16)+rate-1)/rate)-1)&0xfff)<<1)|CPM_BRG_EN;
173         if (pinsel == 0)
174                 *bp |= CPM_BRG_EXTC_CLK3_9;
175         else
176                 *bp |= CPM_BRG_EXTC_CLK5_15;
179 #if defined(CONFIG_POST) || defined(CONFIG_LOGBUFFER)
181 void post_word_store (ulong a)
183         volatile ulong *save_addr =
184                 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_POST_WORD_ADDR);
186         *save_addr = a;
189 ulong post_word_load (void)
191         volatile ulong *save_addr =
192                 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_POST_WORD_ADDR);
194         return *save_addr;
197 #endif  /* CONFIG_POST || CONFIG_LOGBUFFER*/
199 #ifdef CONFIG_BOOTCOUNT_LIMIT
201 void bootcount_store (ulong a)
203         volatile ulong *save_addr =
204                 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_BOOTCOUNT_ADDR);
206         save_addr[0] = a;
207         save_addr[1] = BOOTCOUNT_MAGIC;
210 ulong bootcount_load (void)
212         volatile ulong *save_addr =
213                 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_BOOTCOUNT_ADDR);
215         if (save_addr[1] != BOOTCOUNT_MAGIC)
216                 return 0;
217         else
218                 return save_addr[0];
221 #endif /* CONFIG_BOOTCOUNT_LIMIT */