]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/ppc/cpu/mpc8260/i2c.c
fsl_i2c: Added a callpoint for i2c_board_late_init
[glsdk/glsdk-u-boot.git] / arch / ppc / cpu / mpc8260 / i2c.c
1 /*
2  * (C) Copyright 2000
3  * Paolo Scaffardi, AIRVENT SAM s.p.a - RIMINI(ITALY), arsenio@tin.it
4  *
5  * (C) Copyright 2000 Sysgo Real-Time Solutions, GmbH <www.elinos.com>
6  * Marius Groeger <mgroeger@sysgo.de>
7  *
8  * See file CREDITS for list of people who contributed to this
9  * project.
10  *
11  * This program is free software; you can redistribute it and/or
12  * modify it under the terms of the GNU General Public License as
13  * published by the Free Software Foundation; either version 2 of
14  * the License, or (at your option) any later version.
15  *
16  * This program is distributed in the hope that it will be useful,
17  * but WITHOUT ANY WARRANTY; without even the implied warranty of
18  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
19  * GNU General Public License for more details.
20  *
21  * You should have received a copy of the GNU General Public License
22  * along with this program; if not, write to the Free Software
23  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24  * MA 02111-1307 USA
25  */
27 #include <common.h>
29 #if defined(CONFIG_HARD_I2C)
31 #include <asm/cpm_8260.h>
32 #include <i2c.h>
34 /* define to enable debug messages */
35 #undef  DEBUG_I2C
37 DECLARE_GLOBAL_DATA_PTR;
39 #if defined(CONFIG_I2C_MULTI_BUS)
40 static unsigned int i2c_bus_num __attribute__ ((section (".data"))) = 0;
41 #endif /* CONFIG_I2C_MULTI_BUS */
43 /* uSec to wait between polls of the i2c */
44 #define DELAY_US        100
45 /* uSec to wait for the CPM to start processing the buffer */
46 #define START_DELAY_US  1000
48 /*
49  * tx/rx per-byte timeout: we delay DELAY_US uSec between polls so the
50  * timeout will be (tx_length + rx_length) * DELAY_US * TOUT_LOOP
51  */
52 #define TOUT_LOOP 5
54 /*-----------------------------------------------------------------------
55  * Set default values
56  */
57 #ifndef CONFIG_SYS_I2C_SPEED
58 #define CONFIG_SYS_I2C_SPEED    50000
59 #endif
61 /*-----------------------------------------------------------------------
62  */
64 typedef void (*i2c_ecb_t)(int, int, void *);    /* error callback function */
66 /* This structure keeps track of the bd and buffer space usage. */
67 typedef struct i2c_state {
68         int             rx_idx;         /* index   to next free Rx BD */
69         int             tx_idx;         /* index   to next free Tx BD */
70         void            *rxbd;          /* pointer to next free Rx BD */
71         void            *txbd;          /* pointer to next free Tx BD */
72         int             tx_space;       /* number  of Tx bytes left   */
73         unsigned char   *tx_buf;        /* pointer to free Tx area    */
74         i2c_ecb_t       err_cb;         /* error callback function    */
75         void            *cb_data;       /* private data to be passed  */
76 } i2c_state_t;
78 /* flags for i2c_send() and i2c_receive() */
79 #define I2CF_ENABLE_SECONDARY   0x01    /* secondary_address is valid   */
80 #define I2CF_START_COND         0x02    /* tx: generate start condition */
81 #define I2CF_STOP_COND          0x04    /* tx: generate stop  condition */
83 /* return codes */
84 #define I2CERR_NO_BUFFERS       1       /* no more BDs or buffer space  */
85 #define I2CERR_MSG_TOO_LONG     2       /* tried to send/receive to much data   */
86 #define I2CERR_TIMEOUT          3       /* timeout in i2c_doio()        */
87 #define I2CERR_QUEUE_EMPTY      4       /* i2c_doio called without send/receive */
88 #define I2CERR_IO_ERROR         5       /* had an error during comms    */
90 /* error callback flags */
91 #define I2CECB_RX_ERR           0x10    /* this is a receive error      */
92 #define     I2CECB_RX_OV        0x02    /* receive overrun error        */
93 #define     I2CECB_RX_MASK      0x0f    /* mask for error bits          */
94 #define I2CECB_TX_ERR           0x20    /* this is a transmit error     */
95 #define     I2CECB_TX_CL        0x01    /* transmit collision error     */
96 #define     I2CECB_TX_UN        0x02    /* transmit underflow error     */
97 #define     I2CECB_TX_NAK       0x04    /* transmit no ack error        */
98 #define     I2CECB_TX_MASK      0x0f    /* mask for error bits          */
99 #define I2CECB_TIMEOUT          0x40    /* this is a timeout error      */
101 #define ERROR_I2C_NONE          0
102 #define ERROR_I2C_LENGTH        1
104 #define I2C_WRITE_BIT           0x00
105 #define I2C_READ_BIT            0x01
107 #define I2C_RXTX_LEN    128     /* maximum tx/rx buffer length */
110 #define NUM_RX_BDS 4
111 #define NUM_TX_BDS 4
112 #define MAX_TX_SPACE 256
114 typedef struct I2C_BD
116   unsigned short status;
117   unsigned short length;
118   unsigned char *addr;
119 } I2C_BD;
120 #define BD_I2C_TX_START 0x0400  /* special status for i2c: Start condition */
122 #define BD_I2C_TX_CL    0x0001  /* collision error */
123 #define BD_I2C_TX_UN    0x0002  /* underflow error */
124 #define BD_I2C_TX_NAK   0x0004  /* no acknowledge error */
125 #define BD_I2C_TX_ERR   (BD_I2C_TX_NAK|BD_I2C_TX_UN|BD_I2C_TX_CL)
127 #define BD_I2C_RX_ERR   BD_SC_OV
129 #ifdef DEBUG_I2C
130 #define PRINTD(x) printf x
131 #else
132 #define PRINTD(x)
133 #endif
135 /*
136  * Returns the best value of I2BRG to meet desired clock speed of I2C with
137  * input parameters (clock speed, filter, and predivider value).
138  * It returns computer speed value and the difference between it and desired
139  * speed.
140  */
141 static inline int
142 i2c_roundrate(int hz, int speed, int filter, int modval,
143                 int *brgval, int *totspeed)
145     int moddiv = 1 << (5-(modval & 3)), brgdiv, div;
147     PRINTD(("\t[I2C] trying hz=%d, speed=%d, filter=%d, modval=%d\n",
148         hz, speed, filter, modval));
150     div = moddiv * speed;
151     brgdiv = (hz + div - 1) / div;
153     PRINTD(("\t\tmoddiv=%d, brgdiv=%d\n", moddiv, brgdiv));
155     *brgval = ((brgdiv + 1) / 2) - 3 - (2*filter);
157     if ((*brgval < 0) || (*brgval > 255)) {
158           PRINTD(("\t\trejected brgval=%d\n", *brgval));
159           return -1;
160     }
162     brgdiv = 2 * (*brgval + 3 + (2 * filter));
163     div = moddiv * brgdiv ;
164     *totspeed = hz / div;
166     PRINTD(("\t\taccepted brgval=%d, totspeed=%d\n", *brgval, *totspeed));
168     return  0;
171 /*
172  * Sets the I2C clock predivider and divider to meet required clock speed.
173  */
174 static int i2c_setrate(int hz, int speed)
176     immap_t     *immap = (immap_t *)CONFIG_SYS_IMMR ;
177     volatile i2c8260_t *i2c = (i2c8260_t *)&immap->im_i2c;
178     int brgval,
179           modval,       /* 0-3 */
180           bestspeed_diff = speed,
181           bestspeed_brgval=0,
182           bestspeed_modval=0,
183           bestspeed_filter=0,
184           totspeed,
185           filter = 0; /* Use this fixed value */
187         for (modval = 0; modval < 4; modval++)
188         {
189                 if (i2c_roundrate (hz, speed, filter, modval, &brgval, &totspeed) == 0)
190                 {
191                         int diff = speed - totspeed ;
193                         if ((diff >= 0) && (diff < bestspeed_diff))
194                         {
195                                 bestspeed_diff  = diff ;
196                                 bestspeed_modval        = modval;
197                                 bestspeed_brgval        = brgval;
198                                 bestspeed_filter        = filter;
199                         }
200                 }
201         }
203     PRINTD(("[I2C] Best is:\n"));
204     PRINTD(("[I2C] CPU=%dhz RATE=%d F=%d I2MOD=%08x I2BRG=%08x DIFF=%dhz\n",
205                    hz, speed,
206                    bestspeed_filter, bestspeed_modval, bestspeed_brgval,
207                    bestspeed_diff));
209     i2c->i2c_i2mod |= ((bestspeed_modval & 3) << 1) | (bestspeed_filter << 3);
210     i2c->i2c_i2brg = bestspeed_brgval & 0xff;
212     PRINTD(("[I2C] i2mod=%08x i2brg=%08x\n", i2c->i2c_i2mod, i2c->i2c_i2brg));
214     return 1 ;
217 void i2c_init(int speed, int slaveadd)
219         volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
220         volatile cpm8260_t *cp = (cpm8260_t *)&immap->im_cpm;
221         volatile i2c8260_t *i2c = (i2c8260_t *)&immap->im_i2c;
222         volatile iic_t *iip;
223         ulong rbase, tbase;
224         volatile I2C_BD *rxbd, *txbd;
225         uint dpaddr;
227 #ifdef CONFIG_SYS_I2C_INIT_BOARD
228         /* call board specific i2c bus reset routine before accessing the   */
229         /* environment, which might be in a chip on that bus. For details   */
230         /* about this problem see doc/I2C_Edge_Conditions.                  */
231         i2c_init_board();
232 #endif
234         dpaddr = *((unsigned short*)(&immap->im_dprambase[PROFF_I2C_BASE]));
235         if (dpaddr == 0) {
236             /* need to allocate dual port ram */
237             dpaddr = m8260_cpm_dpalloc(64 +
238                 (NUM_RX_BDS * sizeof(I2C_BD)) + (NUM_TX_BDS * sizeof(I2C_BD)) +
239                 MAX_TX_SPACE, 64);
240             *((unsigned short*)(&immap->im_dprambase[PROFF_I2C_BASE])) = dpaddr;
241         }
243         /*
244          * initialise data in dual port ram:
245          *
246          *        dpaddr -> parameter ram (64 bytes)
247          *         rbase -> rx BD         (NUM_RX_BDS * sizeof(I2C_BD) bytes)
248          *         tbase -> tx BD         (NUM_TX_BDS * sizeof(I2C_BD) bytes)
249          *                  tx buffer     (MAX_TX_SPACE bytes)
250          */
252         iip = (iic_t *)&immap->im_dprambase[dpaddr];
253         memset((void*)iip, 0, sizeof(iic_t));
255         rbase = dpaddr + 64;
256         tbase = rbase + NUM_RX_BDS * sizeof(I2C_BD);
258         /* Disable interrupts */
259         i2c->i2c_i2mod = 0x00;
260         i2c->i2c_i2cmr = 0x00;
261         i2c->i2c_i2cer = 0xff;
262         i2c->i2c_i2add = slaveadd;
264         /*
265          * Set the I2C BRG Clock division factor from desired i2c rate
266          * and current CPU rate (we assume sccr dfbgr field is 0;
267          * divide BRGCLK by 1)
268          */
269         PRINTD(("[I2C] Setting rate...\n"));
270         i2c_setrate (gd->brg_clk, CONFIG_SYS_I2C_SPEED) ;
272         /* Set I2C controller in master mode */
273         i2c->i2c_i2com = 0x01;
275         /* Initialize Tx/Rx parameters */
276         iip->iic_rbase = rbase;
277         iip->iic_tbase = tbase;
278         rxbd = (I2C_BD *)((unsigned char *)&immap->im_dprambase[iip->iic_rbase]);
279         txbd = (I2C_BD *)((unsigned char *)&immap->im_dprambase[iip->iic_tbase]);
281         PRINTD(("[I2C] rbase = %04x\n", iip->iic_rbase));
282         PRINTD(("[I2C] tbase = %04x\n", iip->iic_tbase));
283         PRINTD(("[I2C] rxbd = %08x\n", (int)rxbd));
284         PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
286         /* Set big endian byte order */
287         iip->iic_tfcr = 0x10;
288         iip->iic_rfcr = 0x10;
290         /* Set maximum receive size. */
291         iip->iic_mrblr = I2C_RXTX_LEN;
293     cp->cp_cpcr = mk_cr_cmd(CPM_CR_I2C_PAGE,
294                                                         CPM_CR_I2C_SBLOCK,
295                                                         0x00,
296                                                         CPM_CR_INIT_TRX) | CPM_CR_FLG;
297     do {
298                 __asm__ __volatile__ ("eieio");
299     } while (cp->cp_cpcr & CPM_CR_FLG);
301         /* Clear events and interrupts */
302         i2c->i2c_i2cer = 0xff;
303         i2c->i2c_i2cmr = 0x00;
306 static
307 void i2c_newio(i2c_state_t *state)
309         volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
310         volatile iic_t *iip;
311         uint dpaddr;
313         PRINTD(("[I2C] i2c_newio\n"));
315         dpaddr = *((unsigned short*)(&immap->im_dprambase[PROFF_I2C_BASE]));
316         iip = (iic_t *)&immap->im_dprambase[dpaddr];
317         state->rx_idx = 0;
318         state->tx_idx = 0;
319         state->rxbd = (void*)&immap->im_dprambase[iip->iic_rbase];
320         state->txbd = (void*)&immap->im_dprambase[iip->iic_tbase];
321         state->tx_space = MAX_TX_SPACE;
322         state->tx_buf = (uchar*)state->txbd + NUM_TX_BDS * sizeof(I2C_BD);
323         state->err_cb = NULL;
324         state->cb_data = NULL;
326         PRINTD(("[I2C] rxbd = %08x\n", (int)state->rxbd));
327         PRINTD(("[I2C] txbd = %08x\n", (int)state->txbd));
328         PRINTD(("[I2C] tx_buf = %08x\n", (int)state->tx_buf));
330         /* clear the buffer memory */
331         memset((char *)state->tx_buf, 0, MAX_TX_SPACE);
334 static
335 int i2c_send(i2c_state_t *state,
336                          unsigned char address,
337                          unsigned char secondary_address,
338                          unsigned int flags,
339                          unsigned short size,
340                          unsigned char *dataout)
342         volatile I2C_BD *txbd;
343         int i,j;
345         PRINTD(("[I2C] i2c_send add=%02d sec=%02d flag=%02d size=%d\n",
346                         address, secondary_address, flags, size));
348         /* trying to send message larger than BD */
349         if (size > I2C_RXTX_LEN)
350           return I2CERR_MSG_TOO_LONG;
352         /* no more free bds */
353         if (state->tx_idx >= NUM_TX_BDS || state->tx_space < (2 + size))
354           return I2CERR_NO_BUFFERS;
356         txbd = (I2C_BD *)state->txbd;
357         txbd->addr = state->tx_buf;
359         PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
361     if (flags & I2CF_START_COND)
362     {
363         PRINTD(("[I2C] Formatting addresses...\n"));
364         if (flags & I2CF_ENABLE_SECONDARY)
365         {
366                 txbd->length = size + 2;  /* Length of message plus dest addresses */
367                 txbd->addr[0] = address << 1;
368                 txbd->addr[1] = secondary_address;
369                 i = 2;
370         }
371         else
372         {
373                 txbd->length = size + 1;  /* Length of message plus dest address */
374                 txbd->addr[0] = address << 1;  /* Write destination address to BD */
375                 i = 1;
376         }
377     }
378     else
379     {
380         txbd->length = size;  /* Length of message */
381         i = 0;
382     }
384         /* set up txbd */
385         txbd->status = BD_SC_READY;
386         if (flags & I2CF_START_COND)
387           txbd->status |= BD_I2C_TX_START;
388         if (flags & I2CF_STOP_COND)
389           txbd->status |= BD_SC_LAST | BD_SC_WRAP;
391         /* Copy data to send into buffer */
392         PRINTD(("[I2C] copy data...\n"));
393         for(j = 0; j < size; i++, j++)
394           txbd->addr[i] = dataout[j];
396         PRINTD(("[I2C] txbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
397                    txbd->length,
398                    txbd->status,
399                    txbd->addr[0],
400                    txbd->addr[1]));
402         /* advance state */
403         state->tx_buf += txbd->length;
404         state->tx_space -= txbd->length;
405         state->tx_idx++;
406         state->txbd = (void*)(txbd + 1);
408         return 0;
411 static
412 int i2c_receive(i2c_state_t *state,
413                                 unsigned char address,
414                                 unsigned char secondary_address,
415                                 unsigned int flags,
416                                 unsigned short size_to_expect,
417                                 unsigned char *datain)
419         volatile I2C_BD *rxbd, *txbd;
421         PRINTD(("[I2C] i2c_receive %02d %02d %02d\n", address, secondary_address, flags));
423         /* Expected to receive too much */
424         if (size_to_expect > I2C_RXTX_LEN)
425           return I2CERR_MSG_TOO_LONG;
427         /* no more free bds */
428         if (state->tx_idx >= NUM_TX_BDS || state->rx_idx >= NUM_RX_BDS
429                  || state->tx_space < 2)
430           return I2CERR_NO_BUFFERS;
432         rxbd = (I2C_BD *)state->rxbd;
433         txbd = (I2C_BD *)state->txbd;
435         PRINTD(("[I2C] rxbd = %08x\n", (int)rxbd));
436         PRINTD(("[I2C] txbd = %08x\n", (int)txbd));
438         txbd->addr = state->tx_buf;
440         /* set up TXBD for destination address */
441         if (flags & I2CF_ENABLE_SECONDARY)
442         {
443                 txbd->length = 2;
444                 txbd->addr[0] = address << 1;   /* Write data */
445                 txbd->addr[1] = secondary_address;  /* Internal address */
446                 txbd->status = BD_SC_READY;
447         }
448         else
449         {
450                 txbd->length = 1 + size_to_expect;
451                 txbd->addr[0] = (address << 1) | 0x01;
452                 txbd->status = BD_SC_READY;
453                 memset(&txbd->addr[1], 0, txbd->length);
454         }
456         /* set up rxbd for reception */
457         rxbd->status = BD_SC_EMPTY;
458         rxbd->length = size_to_expect;
459         rxbd->addr = datain;
461         txbd->status |= BD_I2C_TX_START;
462         if (flags & I2CF_STOP_COND)
463         {
464                 txbd->status |= BD_SC_LAST | BD_SC_WRAP;
465                 rxbd->status |= BD_SC_WRAP;
466         }
468         PRINTD(("[I2C] txbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
469                    txbd->length,
470                    txbd->status,
471                    txbd->addr[0],
472                    txbd->addr[1]));
473         PRINTD(("[I2C] rxbd: length=0x%04x status=0x%04x addr[0]=0x%02x addr[1]=0x%02x\n",
474                    rxbd->length,
475                    rxbd->status,
476                    rxbd->addr[0],
477                    rxbd->addr[1]));
479         /* advance state */
480         state->tx_buf += txbd->length;
481         state->tx_space -= txbd->length;
482         state->tx_idx++;
483         state->txbd = (void*)(txbd + 1);
484         state->rx_idx++;
485         state->rxbd = (void*)(rxbd + 1);
487         return 0;
491 static
492 int i2c_doio(i2c_state_t *state)
494         volatile immap_t *immap = (immap_t *)CONFIG_SYS_IMMR ;
495         volatile iic_t *iip;
496         volatile i2c8260_t *i2c = (i2c8260_t *)&immap->im_i2c;
497         volatile I2C_BD *txbd, *rxbd;
498         int  n, i, b, rxcnt = 0, rxtimeo = 0, txcnt = 0, txtimeo = 0, rc = 0;
499         uint dpaddr;
501         PRINTD(("[I2C] i2c_doio\n"));
503         if (state->tx_idx <= 0 && state->rx_idx <= 0) {
504                 PRINTD(("[I2C] No I/O is queued\n"));
505                 return I2CERR_QUEUE_EMPTY;
506         }
508         dpaddr = *((unsigned short*)(&immap->im_dprambase[PROFF_I2C_BASE]));
509         iip = (iic_t *)&immap->im_dprambase[dpaddr];
510         iip->iic_rbptr = iip->iic_rbase;
511         iip->iic_tbptr = iip->iic_tbase;
513         /* Enable I2C */
514         PRINTD(("[I2C] Enabling I2C...\n"));
515         i2c->i2c_i2mod |= 0x01;
517         /* Begin transmission */
518         i2c->i2c_i2com |= 0x80;
520         /* Loop until transmit & receive completed */
522         if ((n = state->tx_idx) > 0) {
524                 txbd = ((I2C_BD*)state->txbd) - n;
525                 for (i = 0; i < n; i++) {
526                         txtimeo += TOUT_LOOP * txbd->length;
527                         txbd++;
528                 }
530                 txbd--; /* wait until last in list is done */
532                 PRINTD(("[I2C] Transmitting...(txbd=0x%08lx)\n", (ulong)txbd));
534                 udelay(START_DELAY_US); /* give it time to start */
535                 while((txbd->status & BD_SC_READY) && (++txcnt < txtimeo)) {
536                         udelay(DELAY_US);
537                         if (ctrlc())
538                                 return (-1);
539                         __asm__ __volatile__ ("eieio");
540                 }
541         }
543         if (txcnt < txtimeo && (n = state->rx_idx) > 0) {
545                 rxbd = ((I2C_BD*)state->rxbd) - n;
546                 for (i = 0; i < n; i++) {
547                         rxtimeo += TOUT_LOOP * rxbd->length;
548                         rxbd++;
549                 }
551                 rxbd--; /* wait until last in list is done */
553                 PRINTD(("[I2C] Receiving...(rxbd=0x%08lx)\n", (ulong)rxbd));
555                 udelay(START_DELAY_US); /* give it time to start */
556                 while((rxbd->status & BD_SC_EMPTY) && (++rxcnt < rxtimeo)) {
557                         udelay(DELAY_US);
558                         if (ctrlc())
559                                 return (-1);
560                         __asm__ __volatile__ ("eieio");
561                 }
562         }
564         /* Turn off I2C */
565         i2c->i2c_i2mod &= ~0x01;
567         if ((n = state->tx_idx) > 0) {
568                 for (i = 0; i < n; i++) {
569                         txbd = ((I2C_BD*)state->txbd) - (n - i);
570                         if ((b = txbd->status & BD_I2C_TX_ERR) != 0) {
571                                 if (state->err_cb != NULL)
572                                         (*state->err_cb)(I2CECB_TX_ERR|b, i,
573                                                 state->cb_data);
574                                 if (rc == 0)
575                                         rc = I2CERR_IO_ERROR;
576                         }
577                 }
578         }
580         if ((n = state->rx_idx) > 0) {
581                 for (i = 0; i < n; i++) {
582                         rxbd = ((I2C_BD*)state->rxbd) - (n - i);
583                         if ((b = rxbd->status & BD_I2C_RX_ERR) != 0) {
584                                 if (state->err_cb != NULL)
585                                         (*state->err_cb)(I2CECB_RX_ERR|b, i,
586                                                 state->cb_data);
587                                 if (rc == 0)
588                                         rc = I2CERR_IO_ERROR;
589                         }
590                 }
591         }
593         if ((txtimeo > 0 && txcnt >= txtimeo) || \
594             (rxtimeo > 0 && rxcnt >= rxtimeo)) {
595                 if (state->err_cb != NULL)
596                         (*state->err_cb)(I2CECB_TIMEOUT, -1, state->cb_data);
597                 if (rc == 0)
598                         rc = I2CERR_TIMEOUT;
599         }
601         return (rc);
604 static void
605 i2c_probe_callback(int flags, int xnum, void *data)
607         /*
608          * the only acceptable errors are a transmit NAK or a receive
609          * overrun - tx NAK means the device does not exist, rx OV
610          * means the device must have responded to the slave address
611          * even though the transfer failed
612          */
613         if (flags == (I2CECB_TX_ERR|I2CECB_TX_NAK))
614                 *(int *)data |= 1;
615         if (flags == (I2CECB_RX_ERR|I2CECB_RX_OV))
616                 *(int *)data |= 2;
619 int
620 i2c_probe(uchar chip)
622         i2c_state_t state;
623         int rc, err_flag;
624         uchar buf[1];
626         i2c_newio(&state);
628         state.err_cb = i2c_probe_callback;
629         state.cb_data = (void *) &err_flag;
630         err_flag = 0;
632         rc = i2c_receive(&state, chip, 0, I2CF_START_COND|I2CF_STOP_COND, 1, buf);
634         if (rc != 0)
635                 return (rc);    /* probe failed */
637         rc = i2c_doio(&state);
639         if (rc == 0)
640                 return (0);     /* device exists - read succeeded */
642         if (rc == I2CERR_TIMEOUT)
643                 return (-1);    /* device does not exist - timeout */
645         if (rc != I2CERR_IO_ERROR || err_flag == 0)
646                 return (rc);    /* probe failed */
648         if (err_flag & 1)
649                 return (-1);    /* device does not exist - had transmit NAK */
651         return (0);     /* device exists - had receive overrun */
655 int
656 i2c_read(uchar chip, uint addr, int alen, uchar *buffer, int len)
658         i2c_state_t state;
659         uchar xaddr[4];
660         int rc;
662         xaddr[0] = (addr >> 24) & 0xFF;
663         xaddr[1] = (addr >> 16) & 0xFF;
664         xaddr[2] = (addr >>  8) & 0xFF;
665         xaddr[3] =  addr        & 0xFF;
667 #ifdef CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW
668          /*
669           * EEPROM chips that implement "address overflow" are ones
670           * like Catalyst 24WC04/08/16 which has 9/10/11 bits of address
671           * and the extra bits end up in the "chip address" bit slots.
672           * This makes a 24WC08 (1Kbyte) chip look like four 256 byte
673           * chips.
674           *
675           * Note that we consider the length of the address field to still
676           * be one byte because the extra address bits are hidden in the
677           * chip address.
678           */
679         chip |= ((addr >> (alen * 8)) & CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW);
680 #endif
682         i2c_newio(&state);
684         rc = i2c_send(&state, chip, 0, I2CF_START_COND, alen, &xaddr[4-alen]);
685         if (rc != 0) {
686                 printf("i2c_read: i2c_send failed (%d)\n", rc);
687                 return 1;
688         }
690         rc = i2c_receive(&state, chip, 0, I2CF_STOP_COND, len, buffer);
691         if (rc != 0) {
692                 printf("i2c_read: i2c_receive failed (%d)\n", rc);
693                 return 1;
694         }
696         rc = i2c_doio(&state);
697         if (rc != 0) {
698                 printf("i2c_read: i2c_doio failed (%d)\n", rc);
699                 return 1;
700         }
701         return 0;
704 int
705 i2c_write(uchar chip, uint addr, int alen, uchar *buffer, int len)
707         i2c_state_t state;
708         uchar xaddr[4];
709         int rc;
711         xaddr[0] = (addr >> 24) & 0xFF;
712         xaddr[1] = (addr >> 16) & 0xFF;
713         xaddr[2] = (addr >>  8) & 0xFF;
714         xaddr[3] =  addr        & 0xFF;
716 #ifdef CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW
717          /*
718           * EEPROM chips that implement "address overflow" are ones
719           * like Catalyst 24WC04/08/16 which has 9/10/11 bits of address
720           * and the extra bits end up in the "chip address" bit slots.
721           * This makes a 24WC08 (1Kbyte) chip look like four 256 byte
722           * chips.
723           *
724           * Note that we consider the length of the address field to still
725           * be one byte because the extra address bits are hidden in the
726           * chip address.
727           */
728         chip |= ((addr >> (alen * 8)) & CONFIG_SYS_I2C_EEPROM_ADDR_OVERFLOW);
729 #endif
731         i2c_newio(&state);
733         rc = i2c_send(&state, chip, 0, I2CF_START_COND, alen, &xaddr[4-alen]);
734         if (rc != 0) {
735                 printf("i2c_write: first i2c_send failed (%d)\n", rc);
736                 return 1;
737         }
739         rc = i2c_send(&state, 0, 0, I2CF_STOP_COND, len, buffer);
740         if (rc != 0) {
741                 printf("i2c_write: second i2c_send failed (%d)\n", rc);
742                 return 1;
743         }
745         rc = i2c_doio(&state);
746         if (rc != 0) {
747                 printf("i2c_write: i2c_doio failed (%d)\n", rc);
748                 return 1;
749         }
750         return 0;
753 #if defined(CONFIG_I2C_MULTI_BUS)
754 /*
755  * Functions for multiple I2C bus handling
756  */
757 unsigned int i2c_get_bus_num(void)
759         return i2c_bus_num;
762 int i2c_set_bus_num(unsigned int bus)
764 #if defined(CONFIG_I2C_MUX)
765         if (bus < CONFIG_SYS_MAX_I2C_BUS) {
766                 i2c_bus_num = bus;
767         } else {
768                 int     ret;
770                 ret = i2x_mux_select_mux(bus);
771                 if (ret == 0)
772                         i2c_bus_num = bus;
773                 else
774                         return ret;
775         }
776 #else
777         if (bus >= CONFIG_SYS_MAX_I2C_BUS)
778                 return -1;
779         i2c_bus_num = bus;
780 #endif
781         return 0;
784 #endif  /* CONFIG_I2C_MULTI_BUS */
785 #endif  /* CONFIG_HARD_I2C */