a42b230ff35e62db43727e437a6f97bd7f30771c
1 /*
2 * Copyright (C) Freescale Semiconductor, Inc. 2007
3 *
4 * Author: Scott Wood <scottwood@freescale.com>,
5 * with some bits from older board-specific PCI initialization.
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
26 #include <common.h>
27 #include <pci.h>
29 #if defined(CONFIG_OF_LIBFDT)
30 #include <libfdt.h>
31 #include <fdt_support.h>
32 #endif
34 #include <asm/mpc8349_pci.h>
36 #define MAX_BUSES 2
38 DECLARE_GLOBAL_DATA_PTR;
40 static struct pci_controller pci_hose[MAX_BUSES];
41 static int pci_num_buses;
43 static void pci_init_bus(int bus, struct pci_region *reg)
44 {
45 volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
46 volatile pot83xx_t *pot = immr->ios.pot;
47 volatile pcictrl83xx_t *pci_ctrl = &immr->pci_ctrl[bus];
48 struct pci_controller *hose = &pci_hose[bus];
49 u32 dev;
50 u16 reg16;
51 int i;
53 if (bus == 1)
54 pot += 3;
56 /* Setup outbound translation windows */
57 for (i = 0; i < 3; i++, reg++, pot++) {
58 if (reg->size == 0)
59 break;
61 hose->regions[i] = *reg;
62 hose->region_count++;
64 pot->potar = reg->bus_start >> 12;
65 pot->pobar = reg->phys_start >> 12;
66 pot->pocmr = ~(reg->size - 1) >> 12;
68 if (reg->flags & PCI_REGION_IO)
69 pot->pocmr |= POCMR_IO;
70 #ifdef CONFIG_83XX_PCI_STREAMING
71 else if (reg->flags & PCI_REGION_PREFETCH)
72 pot->pocmr |= POCMR_SE;
73 #endif
75 if (bus == 1)
76 pot->pocmr |= POCMR_DST;
78 pot->pocmr |= POCMR_EN;
79 }
81 /* Point inbound translation at RAM */
82 pci_ctrl->pitar1 = 0;
83 pci_ctrl->pibar1 = 0;
84 pci_ctrl->piebar1 = 0;
85 pci_ctrl->piwar1 = PIWAR_EN | PIWAR_PF | PIWAR_RTT_SNOOP |
86 PIWAR_WTT_SNOOP | (__ilog2(gd->ram_size - 1));
88 i = hose->region_count++;
89 hose->regions[i].bus_start = 0;
90 hose->regions[i].phys_start = 0;
91 hose->regions[i].size = gd->ram_size;
92 hose->regions[i].flags = PCI_REGION_MEM | PCI_REGION_SYS_MEMORY;
94 hose->first_busno = pci_last_busno() + 1;
95 hose->last_busno = 0xff;
97 pci_setup_indirect(hose, CONFIG_SYS_IMMR + 0x8300 + bus * 0x80,
98 CONFIG_SYS_IMMR + 0x8304 + bus * 0x80);
100 pci_register_hose(hose);
102 /*
103 * Write to Command register
104 */
105 reg16 = 0xff;
106 dev = PCI_BDF(hose->first_busno, 0, 0);
107 pci_hose_read_config_word(hose, dev, PCI_COMMAND, ®16);
108 reg16 |= PCI_COMMAND_SERR | PCI_COMMAND_MASTER | PCI_COMMAND_MEMORY;
109 pci_hose_write_config_word(hose, dev, PCI_COMMAND, reg16);
111 /*
112 * Clear non-reserved bits in status register.
113 */
114 pci_hose_write_config_word(hose, dev, PCI_STATUS, 0xffff);
115 pci_hose_write_config_byte(hose, dev, PCI_LATENCY_TIMER, 0x80);
116 pci_hose_write_config_byte(hose, dev, PCI_CACHE_LINE_SIZE, 0x08);
118 #ifdef CONFIG_PCI_SCAN_SHOW
119 printf("PCI: Bus Dev VenId DevId Class Int\n");
120 #endif
121 #ifndef CONFIG_PCISLAVE
122 /*
123 * Hose scan.
124 */
125 hose->last_busno = pci_hose_scan(hose);
126 #endif
127 }
129 /*
130 * The caller must have already set OCCR, and the PCI_LAW BARs
131 * must have been set to cover all of the requested regions.
132 *
133 * If fewer than three regions are requested, then the region
134 * list is terminated with a region of size 0.
135 */
136 void mpc83xx_pci_init(int num_buses, struct pci_region **reg, int warmboot)
137 {
138 volatile immap_t *immr = (volatile immap_t *)CONFIG_SYS_IMMR;
139 int i;
141 if (num_buses > MAX_BUSES) {
142 printf("%d PCI buses requsted, %d supported\n",
143 num_buses, MAX_BUSES);
145 num_buses = MAX_BUSES;
146 }
148 pci_num_buses = num_buses;
150 /*
151 * Release PCI RST Output signal.
152 * Power on to RST high must be at least 100 ms as per PCI spec.
153 * On warm boots only 1 ms is required.
154 */
155 udelay(warmboot ? 1000 : 100000);
157 for (i = 0; i < num_buses; i++)
158 immr->pci_ctrl[i].gcr = 1;
160 /*
161 * RST high to first config access must be at least 2^25 cycles
162 * as per PCI spec. This could be cut in half if we know we're
163 * running at 66MHz. This could be insufficiently long if we're
164 * running the PCI bus at significantly less than 33MHz.
165 */
166 udelay(1020000);
168 for (i = 0; i < num_buses; i++)
169 pci_init_bus(i, reg[i]);
170 }
172 #ifdef CONFIG_PCISLAVE
174 #define PCI_FUNCTION_CONFIG 0x44
175 #define PCI_FUNCTION_CFG_LOCK 0x20
177 /*
178 * Unlock the configuration bit so that the host system can begin booting
179 *
180 * This should be used after you have:
181 * 1) Called mpc83xx_pci_init()
182 * 2) Set up your inbound translation windows to the appropriate size
183 */
184 void mpc83xx_pcislave_unlock(int bus)
185 {
186 struct pci_controller *hose = &pci_hose[bus];
187 u32 dev;
188 u16 reg16;
190 /* Unlock configuration lock in PCI function configuration register */
191 dev = PCI_BDF(hose->first_busno, 0, 0);
192 pci_hose_read_config_word (hose, dev, PCI_FUNCTION_CONFIG, ®16);
193 reg16 &= ~(PCI_FUNCTION_CFG_LOCK);
194 pci_hose_write_config_word (hose, dev, PCI_FUNCTION_CONFIG, reg16);
196 /* The configuration bit is now unlocked, so we can scan the bus */
197 hose->last_busno = pci_hose_scan(hose);
198 }
199 #endif
201 #if defined(CONFIG_OF_LIBFDT)
202 void ft_pci_setup(void *blob, bd_t *bd)
203 {
204 int nodeoffset;
205 int tmp[2];
206 const char *path;
208 if (pci_num_buses < 1)
209 return;
211 nodeoffset = fdt_path_offset(blob, "/aliases");
212 if (nodeoffset >= 0) {
213 path = fdt_getprop(blob, nodeoffset, "pci0", NULL);
214 if (path) {
215 tmp[0] = cpu_to_be32(pci_hose[0].first_busno);
216 tmp[1] = cpu_to_be32(pci_hose[0].last_busno);
217 do_fixup_by_path(blob, path, "bus-range",
218 &tmp, sizeof(tmp), 1);
220 tmp[0] = cpu_to_be32(gd->pci_clk);
221 do_fixup_by_path(blob, path, "clock-frequency",
222 &tmp, sizeof(tmp[0]), 1);
223 }
225 if (pci_num_buses < 2)
226 return;
228 path = fdt_getprop(blob, nodeoffset, "pci1", NULL);
229 if (path) {
230 tmp[0] = cpu_to_be32(pci_hose[1].first_busno);
231 tmp[1] = cpu_to_be32(pci_hose[1].last_busno);
232 do_fixup_by_path(blob, path, "bus-range",
233 &tmp, sizeof(tmp), 1);
235 tmp[0] = cpu_to_be32(gd->pci_clk);
236 do_fixup_by_path(blob, path, "clock-frequency",
237 &tmp, sizeof(tmp[0]), 1);
238 }
239 }
240 }
241 #endif /* CONFIG_OF_LIBFDT */