594aace4b12553bf4e7253feef89f648ae505a58
1 /*
2 * Adapted for Motorola MPC8560 chips
3 * Xianghua Xiao <x.xiao@motorola.com>
4 *
5 * This file is based on "arch/ppc/8260_io/commproc.c" - here is it's
6 * copyright notice:
7 *
8 * General Purpose functions for the global management of the
9 * 8220 Communication Processor Module.
10 * Copyright (c) 1999 Dan Malek (dmalek@jlc.net)
11 * Copyright (c) 2000 MontaVista Software, Inc (source@mvista.com)
12 * 2.3.99 Updates
13 * Copyright (c) 2003 Motorola,Inc.
14 *
15 * In addition to the individual control of the communication
16 * channels, there are a few functions that globally affect the
17 * communication processor.
18 *
19 * Buffer descriptors must be allocated from the dual ported memory
20 * space. The allocator for that is here. When the communication
21 * process is reset, we reclaim the memory available. There is
22 * currently no deallocator for this memory.
23 */
24 #include <common.h>
25 #include <asm/cpm_85xx.h>
27 DECLARE_GLOBAL_DATA_PTR;
29 /*
30 * because we have stack and init data in dual port ram
31 * we must reduce the size
32 */
33 #undef CPM_DATAONLY_SIZE
34 #define CPM_DATAONLY_SIZE ((uint)(8 * 1024) - CPM_DATAONLY_BASE)
36 void
37 m8560_cpm_reset(void)
38 {
39 volatile ccsr_cpm_t *cpm = (ccsr_cpm_t *)CONFIG_SYS_MPC85xx_CPM_ADDR;
40 volatile ulong count;
42 gd = (gd_t *) (CONFIG_SYS_INIT_RAM_ADDR + CONFIG_SYS_GBL_DATA_OFFSET);
44 /* Reclaim the DP memory for our use.
45 */
46 gd->dp_alloc_base = CPM_DATAONLY_BASE;
47 gd->dp_alloc_top = gd->dp_alloc_base + CPM_DATAONLY_SIZE;
49 /*
50 * Reset CPM
51 */
52 cpm->im_cpm_cp.cpcr = CPM_CR_RST;
53 count = 0;
54 do { /* Spin until command processed */
55 __asm__ __volatile__ ("eieio");
56 } while ((cpm->im_cpm_cp.cpcr & CPM_CR_FLG) && ++count < 1000000);
57 }
59 /* Allocate some memory from the dual ported ram.
60 * To help protocols with object alignment restrictions, we do that
61 * if they ask.
62 */
63 uint
64 m8560_cpm_dpalloc(uint size, uint align)
65 {
66 volatile ccsr_cpm_t *cpm = (ccsr_cpm_t *)CONFIG_SYS_MPC85xx_CPM_ADDR;
67 uint retloc;
68 uint align_mask, off;
69 uint savebase;
71 align_mask = align - 1;
72 savebase = gd->dp_alloc_base;
74 if ((off = (gd->dp_alloc_base & align_mask)) != 0)
75 gd->dp_alloc_base += (align - off);
77 if ((off = size & align_mask) != 0)
78 size += align - off;
80 if ((gd->dp_alloc_base + size) >= gd->dp_alloc_top) {
81 gd->dp_alloc_base = savebase;
82 panic("m8560_cpm_dpalloc: ran out of dual port ram!");
83 }
85 retloc = gd->dp_alloc_base;
86 gd->dp_alloc_base += size;
88 memset((void *)&(cpm->im_dprambase[retloc]), 0, size);
90 return(retloc);
91 }
93 /* We also own one page of host buffer space for the allocation of
94 * UART "fifos" and the like.
95 */
96 uint
97 m8560_cpm_hostalloc(uint size, uint align)
98 {
99 /* the host might not even have RAM yet - just use dual port RAM */
100 return (m8560_cpm_dpalloc(size, align));
101 }
103 /* Set a baud rate generator. This needs lots of work. There are
104 * eight BRGs, which can be connected to the CPM channels or output
105 * as clocks. The BRGs are in two different block of internal
106 * memory mapped space.
107 * The baud rate clock is the system clock divided by something.
108 * It was set up long ago during the initial boot phase and is
109 * is given to us.
110 * Baud rate clocks are zero-based in the driver code (as that maps
111 * to port numbers). Documentation uses 1-based numbering.
112 */
113 #define BRG_INT_CLK gd->brg_clk
114 #define BRG_UART_CLK ((BRG_INT_CLK + 15) / 16)
116 /* This function is used by UARTS, or anything else that uses a 16x
117 * oversampled clock.
118 */
119 void
120 m8560_cpm_setbrg(uint brg, uint rate)
121 {
122 volatile ccsr_cpm_t *cpm = (ccsr_cpm_t *)CONFIG_SYS_MPC85xx_CPM_ADDR;
123 volatile uint *bp;
125 /* This is good enough to get SMCs running.....
126 */
127 if (brg < 4) {
128 bp = (uint *)&(cpm->im_cpm_brg1.brgc1);
129 }
130 else {
131 bp = (uint *)&(cpm->im_cpm_brg2.brgc5);
132 brg -= 4;
133 }
134 bp += brg;
135 *bp = (((((BRG_UART_CLK+rate-1)/rate)-1)&0xfff)<<1)|CPM_BRG_EN;
136 }
138 /* This function is used to set high speed synchronous baud rate
139 * clocks.
140 */
141 void
142 m8560_cpm_fastbrg(uint brg, uint rate, int div16)
143 {
144 volatile ccsr_cpm_t *cpm = (ccsr_cpm_t *)CONFIG_SYS_MPC85xx_CPM_ADDR;
145 volatile uint *bp;
147 /* This is good enough to get SMCs running.....
148 */
149 if (brg < 4) {
150 bp = (uint *)&(cpm->im_cpm_brg1.brgc1);
151 }
152 else {
153 bp = (uint *)&(cpm->im_cpm_brg2.brgc5);
154 brg -= 4;
155 }
156 bp += brg;
157 *bp = (((((BRG_INT_CLK+rate-1)/rate)-1)&0xfff)<<1)|CPM_BRG_EN;
158 if (div16)
159 *bp |= CPM_BRG_DIV16;
160 }
162 /* This function is used to set baud rate generators using an external
163 * clock source and 16x oversampling.
164 */
166 void
167 m8560_cpm_extcbrg(uint brg, uint rate, uint extclk, int pinsel)
168 {
169 volatile ccsr_cpm_t *cpm = (ccsr_cpm_t *)CONFIG_SYS_MPC85xx_CPM_ADDR;
170 volatile uint *bp;
172 if (brg < 4) {
173 bp = (uint *)&(cpm->im_cpm_brg1.brgc1);
174 }
175 else {
176 bp = (uint *)&(cpm->im_cpm_brg2.brgc5);
177 brg -= 4;
178 }
179 bp += brg;
180 *bp = ((((((extclk/16)+rate-1)/rate)-1)&0xfff)<<1)|CPM_BRG_EN;
181 if (pinsel == 0)
182 *bp |= CPM_BRG_EXTC_CLK3_9;
183 else
184 *bp |= CPM_BRG_EXTC_CLK5_15;
185 }
187 #ifdef CONFIG_POST
189 void post_word_store (ulong a)
190 {
191 volatile ulong *save_addr =
192 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_POST_WORD_ADDR);
194 *save_addr = a;
195 }
197 ulong post_word_load (void)
198 {
199 volatile ulong *save_addr =
200 (volatile ulong *)(CONFIG_SYS_IMMR + CPM_POST_WORD_ADDR);
202 return *save_addr;
203 }
205 #endif /* CONFIG_POST */