1 /*
2 * U-boot - x86 Startup Code
3 *
4 * (C) Copyright 2008-2011
5 * Graeme Russ, <graeme.russ@gmail.com>
6 *
7 * (C) Copyright 2002
8 * Daniel Engström, Omicron Ceti AB, <daniel@omicron.se>
9 *
10 * See file CREDITS for list of people who contributed to this
11 * project.
12 *
13 * This program is free software; you can redistribute it and/or
14 * modify it under the terms of the GNU General Public License as
15 * published by the Free Software Foundation; either version 2 of
16 * the License, or (at your option) any later version.
17 *
18 * This program is distributed in the hope that it will be useful,
19 * but WITHOUT ANY WARRANTY; without even the implied warranty of
20 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
21 * GNU General Public License for more details.
22 *
23 * You should have received a copy of the GNU General Public License
24 * along with this program; if not, write to the Free Software
25 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
26 * MA 02111-1307 USA
27 */
29 #include <config.h>
30 #include <version.h>
31 #include <asm/global_data.h>
32 #include <asm/processor.h>
33 #include <asm/processor-flags.h>
34 #include <generated/generic-asm-offsets.h>
36 .section .text
37 .code32
38 .globl _start
39 .type _start, @function
40 .globl _x86boot_start
41 _x86boot_start:
42 /*
43 * This is the fail safe 32-bit bootstrap entry point. The
44 * following code is not executed from a cold-reset (actually, a
45 * lot of it is, but from real-mode after cold reset. It is
46 * repeated here to put the board into a state as close to cold
47 * reset as necessary)
48 */
49 cli
50 cld
52 /* Turn off cache (this might require a 486-class CPU) */
53 movl %cr0, %eax
54 orl $(X86_CR0_NW | X86_CR0_CD), %eax
55 movl %eax, %cr0
56 wbinvd
58 /* Tell 32-bit code it is being entered from an in-RAM copy */
59 movw $GD_FLG_WARM_BOOT, %bx
60 jmp 1f
61 _start:
62 /*
63 * This is the 32-bit cold-reset entry point. Initialize %bx to 0
64 * in case we're preceeded by some sort of boot stub.
65 */
66 movw $GD_FLG_COLD_BOOT, %bx
67 1:
69 /* Load the segement registes to match the gdt loaded in start16.S */
70 movl $(X86_GDT_ENTRY_32BIT_DS * X86_GDT_ENTRY_SIZE), %eax
71 movw %ax, %fs
72 movw %ax, %ds
73 movw %ax, %gs
74 movw %ax, %es
75 movw %ax, %ss
77 /* Clear the interrupt vectors */
78 lidt blank_idt_ptr
80 /* Early platform init (setup gpio, etc ) */
81 jmp early_board_init
82 .globl early_board_init_ret
83 early_board_init_ret:
85 /* Initialise Cache-As-RAM */
86 jmp car_init
87 .globl car_init_ret
88 car_init_ret:
89 /*
90 * We now have CONFIG_SYS_CAR_SIZE bytes of Cache-As-RAM (or SRAM,
91 * or fully initialised SDRAM - we really don't care which)
92 * starting at CONFIG_SYS_CAR_ADDR to be used as a temporary stack
93 */
95 /* Stack grows down from top of CAR */
96 movl $(CONFIG_SYS_CAR_ADDR + CONFIG_SYS_CAR_SIZE), %esp
98 /* Reserve space on stack for global data */
99 subl $GENERATED_GBL_DATA_SIZE, %esp
101 /* Align global data to 16-byte boundary */
102 andl $0xfffffff0, %esp
104 /* Setup first parameter to setup_gdt */
105 movl %esp, %eax
107 /* Reserve space for global descriptor table */
108 subl $X86_GDT_SIZE, %esp
110 /* Align temporary global descriptor table to 16-byte boundary */
111 andl $0xfffffff0, %esp
113 /* Set second parameter to setup_gdt */
114 movl %esp, %edx
116 /* gd->gd_addr = gd (Required to allow gd->xyz to work) */
117 movl %eax, (%eax)
119 /* Setup global descriptor table so gd->xyz works */
120 call setup_gdt
122 /* Set parameter to board_init_f() to boot flags */
123 xorl %eax, %eax
124 movw %bx, %ax
126 /* Enter, U-boot! */
127 call board_init_f
129 /* indicate (lack of) progress */
130 movw $0x85, %ax
131 jmp die
133 .globl board_init_f_r_trampoline
134 .type board_init_f_r_trampoline, @function
135 board_init_f_r_trampoline:
136 /*
137 * SDRAM has been initialised, U-Boot code has been copied into
138 * RAM, BSS has been cleared and relocation adjustments have been
139 * made. It is now time to jump into the in-RAM copy of U-Boot
140 *
141 * %eax = Address of top of new stack
142 */
144 /* Stack grows down from top of SDRAM */
145 movl %eax, %esp
147 /* Reserve space on stack for global data */
148 subl $GENERATED_GBL_DATA_SIZE, %esp
150 /* Align global data to 16-byte boundary */
151 andl $0xfffffff0, %esp
153 /* Setup first parameter to memcpy (and setup_gdt) */
154 movl %esp, %eax
156 /* Setup second parameter to memcpy */
157 fs movl 0, %edx
159 /* Set third parameter to memcpy */
160 movl $GENERATED_GBL_DATA_SIZE, %ecx
162 /* Copy global data from CAR to SDRAM stack */
163 call memcpy
165 /* Reserve space for global descriptor table */
166 subl $X86_GDT_SIZE, %esp
168 /* Align global descriptor table to 16-byte boundary */
169 andl $0xfffffff0, %esp
171 /* Set second parameter to setup_gdt */
172 movl %esp, %edx
174 /* gd->gd_addr = gd (Required to allow gd->xyz to work) */
175 movl %eax, (%eax)
177 /* Setup global descriptor table so gd->xyz works */
178 call setup_gdt
180 /* Re-enter U-Boot by calling board_init_f_r */
181 call board_init_f_r
183 die:
184 hlt
185 jmp die
186 hlt
188 blank_idt_ptr:
189 .word 0 /* limit */
190 .long 0 /* base */
192 .p2align 2 /* force 4-byte alignment */
194 multiboot_header:
195 /* magic */
196 .long 0x1BADB002
197 /* flags */
198 .long (1 << 16)
199 /* checksum */
200 .long -0x1BADB002 - (1 << 16)
201 /* header addr */
202 .long multiboot_header - _x86boot_start + CONFIG_SYS_TEXT_BASE
203 /* load addr */
204 .long CONFIG_SYS_TEXT_BASE
205 /* load end addr */
206 .long 0
207 /* bss end addr */
208 .long 0
209 /* entry addr */
210 .long CONFIG_SYS_TEXT_BASE