]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - arch/x86/include/asm/cache.h
fs:ext4:write: Initialize cache aligned filename buffer
[glsdk/glsdk-u-boot.git] / arch / x86 / include / asm / cache.h
1 /*
2  * Copyright (c) 2011 The Chromium OS Authors.
3  * See file CREDITS for list of people who contributed to this
4  * project.
5  *
6  * This program is free software; you can redistribute it and/or
7  * modify it under the terms of the GNU General Public License as
8  * published by the Free Software Foundation; either version 2 of
9  * the License, or (at your option) any later version.
10  *
11  * This program is distributed in the hope that it will be useful,
12  * but WITHOUT ANY WARRANTY; without even the implied warranty of
13  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14  * GNU General Public License for more details.
15  *
16  * You should have received a copy of the GNU General Public License
17  * along with this program; if not, write to the Free Software
18  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19  * MA 02111-1307 USA
20  */
22 #ifndef __X86_CACHE_H__
23 #define __X86_CACHE_H__
25 /*
26  * If CONFIG_SYS_CACHELINE_SIZE is defined use it for DMA alignment.  Otherwise
27  * use 64-bytes, a safe default for x86.
28  */
29 #ifdef CONFIG_SYS_CACHELINE_SIZE
30 #define ARCH_DMA_MINALIGN       CONFIG_SYS_CACHELINE_SIZE
31 #else
32 #define ARCH_DMA_MINALIGN       64
33 #endif
35 #endif /* __X86_CACHE_H__ */