1 #ifndef _ASM_IO_H
2 #define _ASM_IO_H
4 #include <compiler.h>
6 /*
7 * This file contains the definitions for the x86 IO instructions
8 * inb/inw/inl/outb/outw/outl and the "string versions" of the same
9 * (insb/insw/insl/outsb/outsw/outsl). You can also use "pausing"
10 * versions of the single-IO instructions (inb_p/inw_p/..).
11 *
12 * This file is not meant to be obfuscating: it's just complicated
13 * to (a) handle it all in a way that makes gcc able to optimize it
14 * as well as possible and (b) trying to avoid writing the same thing
15 * over and over again with slight variations and possibly making a
16 * mistake somewhere.
17 */
19 /*
20 * Thanks to James van Artsdalen for a better timing-fix than
21 * the two short jumps: using outb's to a nonexistent port seems
22 * to guarantee better timings even on fast machines.
23 *
24 * On the other hand, I'd like to be sure of a non-existent port:
25 * I feel a bit unsafe about using 0x80 (should be safe, though)
26 *
27 * Linus
28 */
30 /*
31 * Bit simplified and optimized by Jan Hubicka
32 * Support of BIGMEM added by Gerhard Wichert, Siemens AG, July 1999.
33 *
34 * isa_memset_io, isa_memcpy_fromio, isa_memcpy_toio added,
35 * isa_read[wl] and isa_write[wl] fixed
36 * - Arnaldo Carvalho de Melo <acme@conectiva.com.br>
37 */
39 #define IO_SPACE_LIMIT 0xffff
41 #include <asm/types.h>
44 #ifdef __KERNEL__
47 /*
48 * readX/writeX() are used to access memory mapped devices. On some
49 * architectures the memory mapped IO stuff needs to be accessed
50 * differently. On the x86 architecture, we just read/write the
51 * memory location directly.
52 */
54 #define readb(addr) (*(volatile unsigned char *) (addr))
55 #define readw(addr) (*(volatile unsigned short *) (addr))
56 #define readl(addr) (*(volatile unsigned int *) (addr))
57 #define __raw_readb readb
58 #define __raw_readw readw
59 #define __raw_readl readl
61 #define writeb(b,addr) (*(volatile unsigned char *) (addr) = (b))
62 #define writew(b,addr) (*(volatile unsigned short *) (addr) = (b))
63 #define writel(b,addr) (*(volatile unsigned int *) (addr) = (b))
64 #define __raw_writeb writeb
65 #define __raw_writew writew
66 #define __raw_writel writel
68 #define memset_io(a,b,c) memset((a),(b),(c))
69 #define memcpy_fromio(a,b,c) memcpy((a),(b),(c))
70 #define memcpy_toio(a,b,c) memcpy((a),(b),(c))
72 /*
73 * ISA space is 'always mapped' on a typical x86 system, no need to
74 * explicitly ioremap() it. The fact that the ISA IO space is mapped
75 * to PAGE_OFFSET is pure coincidence - it does not mean ISA values
76 * are physical addresses. The following constant pointer can be
77 * used as the IO-area pointer (it can be iounmapped as well, so the
78 * analogy with PCI is quite large):
79 */
80 #define isa_readb(a) readb((a))
81 #define isa_readw(a) readw((a))
82 #define isa_readl(a) readl((a))
83 #define isa_writeb(b,a) writeb(b,(a))
84 #define isa_writew(w,a) writew(w,(a))
85 #define isa_writel(l,a) writel(l,(a))
86 #define isa_memset_io(a,b,c) memset_io((a),(b),(c))
87 #define isa_memcpy_fromio(a,b,c) memcpy_fromio((a),(b),(c))
88 #define isa_memcpy_toio(a,b,c) memcpy_toio((a),(b),(c))
91 static inline int check_signature(unsigned long io_addr,
92 const unsigned char *signature, int length)
93 {
94 int retval = 0;
95 do {
96 if (readb(io_addr) != *signature)
97 goto out;
98 io_addr++;
99 signature++;
100 length--;
101 } while (length);
102 retval = 1;
103 out:
104 return retval;
105 }
107 /**
108 * isa_check_signature - find BIOS signatures
109 * @io_addr: mmio address to check
110 * @signature: signature block
111 * @length: length of signature
112 *
113 * Perform a signature comparison with the ISA mmio address io_addr.
114 * Returns 1 on a match.
115 *
116 * This function is deprecated. New drivers should use ioremap and
117 * check_signature.
118 */
121 static inline int isa_check_signature(unsigned long io_addr,
122 const unsigned char *signature, int length)
123 {
124 int retval = 0;
125 do {
126 if (isa_readb(io_addr) != *signature)
127 goto out;
128 io_addr++;
129 signature++;
130 length--;
131 } while (length);
132 retval = 1;
133 out:
134 return retval;
135 }
137 #endif /* __KERNEL__ */
139 #ifdef SLOW_IO_BY_JUMPING
140 #define __SLOW_DOWN_IO "\njmp 1f\n1:\tjmp 1f\n1:"
141 #else
142 #define __SLOW_DOWN_IO "\noutb %%al,$0xed"
143 #endif
145 #ifdef REALLY_SLOW_IO
146 #define __FULL_SLOW_DOWN_IO __SLOW_DOWN_IO __SLOW_DOWN_IO __SLOW_DOWN_IO __SLOW_DOWN_IO
147 #else
148 #define __FULL_SLOW_DOWN_IO __SLOW_DOWN_IO
149 #endif
152 /*
153 * Talk about misusing macros..
154 */
155 #define __OUT1(s,x) \
156 static inline void out##s(unsigned x value, unsigned short port) {
158 #define __OUT2(s,s1,s2) \
159 __asm__ __volatile__ ("out" #s " %" s1 "0,%" s2 "1"
162 #define __OUT(s,s1,x) \
163 __OUT1(s,x) __OUT2(s,s1,"w") : : "a" (value), "Nd" (port)); } \
164 __OUT1(s##_p,x) __OUT2(s,s1,"w") __FULL_SLOW_DOWN_IO : : "a" (value), "Nd" (port));}
166 #define __IN1(s) \
167 static inline RETURN_TYPE in##s(unsigned short port) { RETURN_TYPE _v;
169 #define __IN2(s,s1,s2) \
170 __asm__ __volatile__ ("in" #s " %" s2 "1,%" s1 "0"
172 #define __IN(s,s1,i...) \
173 __IN1(s) __IN2(s,s1,"w") : "=a" (_v) : "Nd" (port) ,##i ); return _v; } \
174 __IN1(s##_p) __IN2(s,s1,"w") __FULL_SLOW_DOWN_IO : "=a" (_v) : "Nd" (port) ,##i ); return _v; }
176 #define __INS(s) \
177 static inline void ins##s(unsigned short port, void * addr, unsigned long count) \
178 { __asm__ __volatile__ ("rep ; ins" #s \
179 : "=D" (addr), "=c" (count) : "d" (port),"0" (addr),"1" (count)); }
181 #define __OUTS(s) \
182 static inline void outs##s(unsigned short port, const void * addr, unsigned long count) \
183 { __asm__ __volatile__ ("rep ; outs" #s \
184 : "=S" (addr), "=c" (count) : "d" (port),"0" (addr),"1" (count)); }
186 #define RETURN_TYPE unsigned char
187 __IN(b,"")
188 #undef RETURN_TYPE
189 #define RETURN_TYPE unsigned short
190 __IN(w,"")
191 #undef RETURN_TYPE
192 #define RETURN_TYPE unsigned int
193 __IN(l,"")
194 #undef RETURN_TYPE
196 __OUT(b,"b",char)
197 __OUT(w,"w",short)
198 __OUT(l,,int)
200 __INS(b)
201 __INS(w)
202 __INS(l)
204 __OUTS(b)
205 __OUTS(w)
206 __OUTS(l)
208 static inline void sync(void)
209 {
210 }
212 /*
213 * Given a physical address and a length, return a virtual address
214 * that can be used to access the memory range with the caching
215 * properties specified by "flags".
216 */
217 #define MAP_NOCACHE (0)
218 #define MAP_WRCOMBINE (0)
219 #define MAP_WRBACK (0)
220 #define MAP_WRTHROUGH (0)
222 static inline void *
223 map_physmem(phys_addr_t paddr, unsigned long len, unsigned long flags)
224 {
225 return (void *)(uintptr_t)paddr;
226 }
228 /*
229 * Take down a mapping set up by map_physmem().
230 */
231 static inline void unmap_physmem(void *vaddr, unsigned long flags)
232 {
234 }
236 static inline phys_addr_t virt_to_phys(void * vaddr)
237 {
238 return (phys_addr_t)(uintptr_t)(vaddr);
239 }
241 /*
242 * TODO: The kernel offers some more advanced versions of barriers, it might
243 * have some advantages to use them instead of the simple one here.
244 */
245 #define dmb() __asm__ __volatile__ ("" : : : "memory")
246 #define __iormb() dmb()
247 #define __iowmb() dmb()
249 #endif