]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - board/Marvell/sheevaplug/sheevaplug.c
Merge branch 'u-boot-imx/master' into 'u-boot-arm/master'
[glsdk/glsdk-u-boot.git] / board / Marvell / sheevaplug / sheevaplug.c
1 /*
2  * (C) Copyright 2009
3  * Marvell Semiconductor <www.marvell.com>
4  * Written-by: Prafulla Wadaskar <prafulla@marvell.com>
5  *
6  * See file CREDITS for list of people who contributed to this
7  * project.
8  *
9  * This program is free software; you can redistribute it and/or
10  * modify it under the terms of the GNU General Public License as
11  * published by the Free Software Foundation; either version 2 of
12  * the License, or (at your option) any later version.
13  *
14  * This program is distributed in the hope that it will be useful,
15  * but WITHOUT ANY WARRANTY; without even the implied warranty of
16  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17  * GNU General Public License for more details.
18  *
19  * You should have received a copy of the GNU General Public License
20  * along with this program; if not, write to the Free Software
21  * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston,
22  * MA 02110-1301 USA
23  */
25 #include <common.h>
26 #include <miiphy.h>
27 #include <asm/arch/cpu.h>
28 #include <asm/arch/kirkwood.h>
29 #include <asm/arch/mpp.h>
30 #include "sheevaplug.h"
32 DECLARE_GLOBAL_DATA_PTR;
34 int board_early_init_f(void)
35 {
36         /*
37          * default gpio configuration
38          * There are maximum 64 gpios controlled through 2 sets of registers
39          * the  below configuration configures mainly initial LED status
40          */
41         kw_config_gpio(SHEEVAPLUG_OE_VAL_LOW,
42                         SHEEVAPLUG_OE_VAL_HIGH,
43                         SHEEVAPLUG_OE_LOW, SHEEVAPLUG_OE_HIGH);
45         /* Multi-Purpose Pins Functionality configuration */
46         static const u32 kwmpp_config[] = {
47                 MPP0_NF_IO2,
48                 MPP1_NF_IO3,
49                 MPP2_NF_IO4,
50                 MPP3_NF_IO5,
51                 MPP4_NF_IO6,
52                 MPP5_NF_IO7,
53                 MPP6_SYSRST_OUTn,
54                 MPP7_GPO,
55                 MPP8_UART0_RTS,
56                 MPP9_UART0_CTS,
57                 MPP10_UART0_TXD,
58                 MPP11_UART0_RXD,
59                 MPP12_SD_CLK,
60                 MPP13_SD_CMD,
61                 MPP14_SD_D0,
62                 MPP15_SD_D1,
63                 MPP16_SD_D2,
64                 MPP17_SD_D3,
65                 MPP18_NF_IO0,
66                 MPP19_NF_IO1,
67                 MPP20_GPIO,
68                 MPP21_GPIO,
69                 MPP22_GPIO,
70                 MPP23_GPIO,
71                 MPP24_GPIO,
72                 MPP25_GPIO,
73                 MPP26_GPIO,
74                 MPP27_GPIO,
75                 MPP28_GPIO,
76                 MPP29_TSMP9,
77                 MPP30_GPIO,
78                 MPP31_GPIO,
79                 MPP32_GPIO,
80                 MPP33_GPIO,
81                 MPP34_GPIO,
82                 MPP35_GPIO,
83                 MPP36_GPIO,
84                 MPP37_GPIO,
85                 MPP38_GPIO,
86                 MPP39_GPIO,
87                 MPP40_GPIO,
88                 MPP41_GPIO,
89                 MPP42_GPIO,
90                 MPP43_GPIO,
91                 MPP44_GPIO,
92                 MPP45_GPIO,
93                 MPP46_GPIO,
94                 MPP47_GPIO,
95                 MPP48_GPIO,
96                 MPP49_GPIO,
97                 0
98         };
99         kirkwood_mpp_conf(kwmpp_config, NULL);
100         return 0;
103 int board_init(void)
105         /*
106          * arch number of board
107          */
108         gd->bd->bi_arch_number = MACH_TYPE_SHEEVAPLUG;
110         /* adress of boot parameters */
111         gd->bd->bi_boot_params = kw_sdram_bar(0) + 0x100;
113         return 0;
116 #ifdef CONFIG_RESET_PHY_R
117 /* Configure and enable MV88E1116 PHY */
118 void reset_phy(void)
120         u16 reg;
121         u16 devadr;
122         char *name = "egiga0";
124         if (miiphy_set_current_dev(name))
125                 return;
127         /* command to read PHY dev address */
128         if (miiphy_read(name, 0xEE, 0xEE, (u16 *) &devadr)) {
129                 printf("Err..%s could not read PHY dev address\n",
130                         __FUNCTION__);
131                 return;
132         }
134         /*
135          * Enable RGMII delay on Tx and Rx for CPU port
136          * Ref: sec 4.7.2 of chip datasheet
137          */
138         miiphy_write(name, devadr, MV88E1116_PGADR_REG, 2);
139         miiphy_read(name, devadr, MV88E1116_MAC_CTRL_REG, &reg);
140         reg |= (MV88E1116_RGMII_RXTM_CTRL | MV88E1116_RGMII_TXTM_CTRL);
141         miiphy_write(name, devadr, MV88E1116_MAC_CTRL_REG, reg);
142         miiphy_write(name, devadr, MV88E1116_PGADR_REG, 0);
144         /* reset the phy */
145         miiphy_reset(name, devadr);
147         printf("88E1116 Initialized on %s\n", name);
149 #endif /* CONFIG_RESET_PHY_R */