1 /*
2 * (C) Copyright 2007
3 * Stefan Roese, DENX Software Engineering, sr@denx.de.
4 *
5 * Copyright (C) 2002 Scott McNutt <smcnutt@artesyncp.com>
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
26 #include <ppc_asm.tmpl>
27 #include <config.h>
28 #include <asm/mmu.h>
30 /**************************************************************************
31 * TLB TABLE
32 *
33 * This table is used by the cpu boot code to setup the initial tlb
34 * entries. Rather than make broad assumptions in the cpu source tree,
35 * this table lets each board set things up however they like.
36 *
37 * Pointer to the table is returned in r1
38 *
39 *************************************************************************/
40 .section .bootpg,"ax"
41 .globl tlbtab
43 tlbtab:
44 tlbtab_start
46 /*
47 * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
48 * speed up boot process. It is patched after relocation to enable SA_I
49 */
50 #ifndef CONFIG_NAND_SPL
51 tlbentry(CONFIG_SYS_BOOT_BASE_ADDR, SZ_256M, CONFIG_SYS_BOOT_BASE_ADDR, 0, AC_R|AC_W|AC_X|SA_G)
52 #else
53 tlbentry(CONFIG_SYS_NAND_BOOT_SPL_SRC, SZ_4K, CONFIG_SYS_NAND_BOOT_SPL_SRC, 0, AC_R|AC_W|AC_X|SA_G)
54 tlbentry(CONFIG_SYS_SDRAM_BASE, SZ_256M, CONFIG_SYS_SDRAM_BASE, 0, AC_R|AC_W|AC_X|SA_G|SA_I)
55 #endif
57 /* TLB-entry for init-ram in dcache (SA_I must be turned off!) */
58 tlbentry(CONFIG_SYS_INIT_RAM_ADDR, SZ_4K, CONFIG_SYS_INIT_RAM_ADDR, 0, AC_R|AC_W|AC_X|SA_G)
60 /* PCI base & peripherals */
61 tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, CONFIG_SYS_PCI_BASE, 0, AC_R|AC_W|SA_G|SA_I)
63 tlbentry(CONFIG_SYS_NVRAM_BASE_ADDR, SZ_256M, CONFIG_SYS_NVRAM_BASE_ADDR, 0, AC_R|AC_W|AC_X|SA_W|SA_I)
64 tlbentry(CONFIG_SYS_NAND_ADDR, SZ_4K, CONFIG_SYS_NAND_ADDR, 0, AC_R|AC_W|AC_X|SA_W|SA_I)
66 /* PCI */
67 tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, CONFIG_SYS_PCI_MEMBASE, 0, AC_R|AC_W|SA_G|SA_I)
68 tlbentry(CONFIG_SYS_PCI_MEMBASE1, SZ_256M, CONFIG_SYS_PCI_MEMBASE1, 0, AC_R|AC_W|SA_G|SA_I)
69 tlbentry(CONFIG_SYS_PCI_MEMBASE2, SZ_256M, CONFIG_SYS_PCI_MEMBASE2, 0, AC_R|AC_W|SA_G|SA_I)
70 tlbentry(CONFIG_SYS_PCI_MEMBASE3, SZ_256M, CONFIG_SYS_PCI_MEMBASE3, 0, AC_R|AC_W|SA_G|SA_I)
72 /* USB 2.0 Device */
73 tlbentry(CONFIG_SYS_USB_DEVICE, SZ_1K, CONFIG_SYS_USB_DEVICE, 0, AC_R|AC_W|SA_G|SA_I)
75 tlbtab_end
77 #if defined(CONFIG_NAND_U_BOOT) && !defined(CONFIG_NAND_SPL)
78 /*
79 * For NAND booting the first TLB has to be reconfigured to full size
80 * and with caching disabled after running from RAM!
81 */
82 #define TLB00 TLB0(CONFIG_SYS_BOOT_BASE_ADDR, SZ_256M)
83 #define TLB01 TLB1(CONFIG_SYS_BOOT_BASE_ADDR, 0)
84 #define TLB02 TLB2(AC_R|AC_W|AC_X|SA_G|SA_I)
86 .globl reconfig_tlb0
87 reconfig_tlb0:
88 sync
89 isync
90 addi r4,r0,0x0000 /* TLB entry #0 */
91 lis r5,TLB00@h
92 ori r5,r5,TLB00@l
93 tlbwe r5,r4,0x0000 /* Save it out */
94 lis r5,TLB01@h
95 ori r5,r5,TLB01@l
96 tlbwe r5,r4,0x0001 /* Save it out */
97 lis r5,TLB02@h
98 ori r5,r5,TLB02@l
99 tlbwe r5,r4,0x0002 /* Save it out */
100 sync
101 isync
102 blr
103 #endif