Merge branch 'master' of git://git.denx.de/u-boot-microblaze
[glsdk/glsdk-u-boot.git] / board / amcc / katmai / init.S
1 /*
2  * (C) Copyright 2007
3  * Stefan Roese, DENX Software Engineering, sr@denx.de.
4  *
5  *  Copyright (C) 2002 Scott McNutt <smcnutt@artesyncp.com>
6  *
7  * See file CREDITS for list of people who contributed to this
8  * project.
9  *
10  * This program is free software; you can redistribute it and/or
11  * modify it under the terms of the GNU General Public License as
12  * published by the Free Software Foundation; either version 2 of
13  * the License, or (at your option) any later version.
14  *
15  * This program is distributed in the hope that it will be useful,
16  * but WITHOUT ANY WARRANTY; without even the implied warranty of
17  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
18  * GNU General Public License for more details.
19  *
20  * You should have received a copy of the GNU General Public License
21  * along with this program; if not, write to the Free Software
22  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23  * MA 02111-1307 USA
24  */
26 #include <ppc_asm.tmpl>
27 #include <config.h>
28 #include <asm/mmu.h>
30 /**************************************************************************
31  * TLB TABLE
32  *
33  * This table is used by the cpu boot code to setup the initial tlb
34  * entries. Rather than make broad assumptions in the cpu source tree,
35  * this table lets each board set things up however they like.
36  *
37  *  Pointer to the table is returned in r1
38  *
39  *************************************************************************/
41         .section .bootpg,"ax"
43 /**************************************************************************
44  * TLB table for revA
45  *************************************************************************/
46         .globl tlbtabA
47 tlbtabA:
48         tlbtab_start
50         /*
51          * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
52          * speed up boot process. It is patched after relocation to enable SA_I
53          */
54         tlbentry(0xff000000, SZ_16M, 0xff000000, 4, AC_R|AC_W|AC_X|SA_G)
56         /*
57          * TLB entries for SDRAM are not needed on this platform.
58          * They are dynamically generated in the SPD DDR(2) detection
59          * routine.
60          */
62         tlbentry(CONFIG_SYS_ISRAM_BASE, SZ_256K, 0x00000000, 4, AC_R|AC_W|AC_X|SA_I)
63         tlbentry(CONFIG_SYS_PERIPHERAL_BASE, SZ_4K, 0xF0000000, 4, AC_R|AC_W|SA_G|SA_I)
65         tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, 0x00000000, 0xC, AC_R|AC_W|SA_G|SA_I)
66         tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, 0x10000000, 0xC, AC_R|AC_W|SA_G|SA_I)
67         tlbentry(CONFIG_SYS_PCIE_MEMBASE, SZ_256M, 0xB0000000, 0xD, AC_R|AC_W|SA_G|SA_I)
68         tlbentry(CONFIG_SYS_PCIE_BASE, SZ_16K, 0x20000000, 0xC, AC_R|AC_W|SA_G|SA_I)
70         tlbentry(CONFIG_SYS_PCIE0_CFGBASE, SZ_16M, 0x40000000, 0xC, AC_R|AC_W|SA_G|SA_I)
71         tlbentry(CONFIG_SYS_PCIE1_CFGBASE, SZ_16M, 0x80000000, 0xC, AC_R|AC_W|SA_G|SA_I)
72         tlbentry(CONFIG_SYS_PCIE2_CFGBASE, SZ_16M, 0xC0000000, 0xC, AC_R|AC_W|SA_G|SA_I)
73         tlbentry(CONFIG_SYS_PCIE0_XCFGBASE, SZ_1K, 0x50000000, 0xC, AC_R|AC_W|SA_G|SA_I)
74         tlbentry(CONFIG_SYS_PCIE1_XCFGBASE, SZ_1K, 0x90000000, 0xC, AC_R|AC_W|SA_G|SA_I)
75         tlbentry(CONFIG_SYS_PCIE2_XCFGBASE, SZ_1K, 0xD0000000, 0xC, AC_R|AC_W|SA_G|SA_I)
76         tlbtab_end
78 /**************************************************************************
79  * TLB table for revB
80  *
81  * Notice: revB of the 440SPe chip is very strict about PLB real addresses
82  * and ranges to be mapped for config space: it seems to only work with
83  * d_nnnn_nnnn range (hangs the core upon config transaction attempts when
84  * set otherwise) while revA uses c_nnnn_nnnn.
85  *************************************************************************/
86         .globl tlbtabB
87 tlbtabB:
88         tlbtab_start
90         /*
91          * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
92          * speed up boot process. It is patched after relocation to enable SA_I
93          */
94         tlbentry(0xff000000, SZ_16M, 0xff000000, 4, AC_R|AC_W|AC_X|SA_G)
96         /*
97          * TLB entries for SDRAM are not needed on this platform.
98          * They are dynamically generated in the SPD DDR(2) detection
99          * routine.
100          */
102         tlbentry(CONFIG_SYS_ISRAM_BASE, SZ_256K, 0x00000000, 4, AC_R|AC_W|AC_X|SA_I)
104         tlbentry(CONFIG_SYS_PERIPHERAL_BASE, SZ_4K, 0xF0000000, 4, AC_R|AC_W|SA_G|SA_I)
106         tlbentry(CONFIG_SYS_ACE_BASE, SZ_1K, CONFIG_SYS_ACE_BASE, 4,AC_R|AC_W|SA_G|SA_I)
108         tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, 0x00000000, 0xC, AC_R|AC_W|SA_G|SA_I)
109         tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, 0x10000000, 0xC, AC_R|AC_W|SA_G|SA_I)
110         tlbentry(CONFIG_SYS_PCIE_MEMBASE, SZ_256M, 0xB0000000, 0xD, AC_R|AC_W|SA_G|SA_I)
112         tlbentry(CONFIG_SYS_PCIE0_CFGBASE, SZ_16M, 0x00000000, 0xD, AC_R|AC_W|SA_G|SA_I)
113         tlbentry(CONFIG_SYS_PCIE1_CFGBASE, SZ_16M, 0x20000000, 0xD, AC_R|AC_W|SA_G|SA_I)
114         tlbentry(CONFIG_SYS_PCIE2_CFGBASE, SZ_16M, 0x40000000, 0xD, AC_R|AC_W|SA_G|SA_I)
115         tlbentry(CONFIG_SYS_PCIE0_XCFGBASE, SZ_1K, 0x10000000, 0xD, AC_R|AC_W|SA_G|SA_I)
116         tlbentry(CONFIG_SYS_PCIE1_XCFGBASE, SZ_1K, 0x30000000, 0xD, AC_R|AC_W|SA_G|SA_I)
117         tlbentry(CONFIG_SYS_PCIE2_XCFGBASE, SZ_1K, 0x50000000, 0xD, AC_R|AC_W|SA_G|SA_I)
118         tlbtab_end