1 /*
2 * (C) Copyright 2007
3 * Stefan Roese, DENX Software Engineering, sr@denx.de.
4 *
5 * Copyright (C) 2002 Scott McNutt <smcnutt@artesyncp.com>
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
26 #include <ppc_asm.tmpl>
27 #include <config.h>
28 #include <asm/mmu.h>
30 /**************************************************************************
31 * TLB TABLE
32 *
33 * This table is used by the cpu boot code to setup the initial tlb
34 * entries. Rather than make broad assumptions in the cpu source tree,
35 * this table lets each board set things up however they like.
36 *
37 * Pointer to the table is returned in r1
38 *
39 *************************************************************************/
41 .section .bootpg,"ax"
42 .globl tlbtab
44 tlbtab:
45 tlbtab_start
47 /*
48 * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
49 * speed up boot process. It is patched after relocation to enable SA_I
50 */
51 tlbentry(0xfff00000, SZ_1M, 0xfff00000, 1, AC_RWX | SA_G)
53 tlbentry(0xffc00000, SZ_1M, 0xffc00000, 1, AC_RWX | SA_IG)
54 tlbentry(0xffd00000, SZ_1M, 0xffd00000, 1, AC_RWX | SA_IG)
55 tlbentry(0xffe00000, SZ_1M, 0xffe00000, 1, AC_RWX | SA_IG)
56 tlbentry(0xff900000, SZ_1M, 0xff900000, 1, AC_RWX | SA_IG)
57 tlbentry(CONFIG_SYS_EPLD_BASE, SZ_256K, 0xff000000, 1, AC_RW | SA_IG)
59 /*
60 * TLB entries for SDRAM are not needed on this platform.
61 * They are dynamically generated in the SPD DDR(2) detection
62 * routine.
63 */
65 /* internal ram (l2 cache) */
66 tlbentry(CONFIG_SYS_ISRAM_BASE, SZ_256K, 0x80000000, 0, AC_RWX | SA_I)
68 /* peripherals at f0000000 */
69 tlbentry(CONFIG_SYS_PERIPHERAL_BASE, SZ_4K, CONFIG_SYS_PERIPHERAL_BASE, 1, AC_RW | SA_IG)
71 /* PCI */
72 tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, 0x00000000, 9, AC_RW | SA_IG)
73 tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, 0x10000000, 9, AC_RW | SA_IG)
74 tlbtab_end