]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - board/amcc/sequoia/sdram.c
Move arch/ppc to arch/powerpc
[glsdk/glsdk-u-boot.git] / board / amcc / sequoia / sdram.c
1 /*
2  * (C) Copyright 2006
3  * Sylvie Gohl,             AMCC/IBM, gohl.sylvie@fr.ibm.com
4  * Jacqueline Pira-Ferriol, AMCC/IBM, jpira-ferriol@fr.ibm.com
5  * Thierry Roman,           AMCC/IBM, thierry_roman@fr.ibm.com
6  * Alain Saurel,            AMCC/IBM, alain.saurel@fr.ibm.com
7  * Robert Snyder,           AMCC/IBM, rob.snyder@fr.ibm.com
8  *
9  * (C) Copyright 2006-2007
10  * Stefan Roese, DENX Software Engineering, sr@denx.de.
11  *
12  * This program is free software; you can redistribute it and/or
13  * modify it under the terms of the GNU General Public License as
14  * published by the Free Software Foundation; either version 2 of
15  * the License, or (at your option) any later version.
16  *
17  * This program is distributed in the hope that it will be useful,
18  * but WITHOUT ANY WARRANTY; without even the implied warranty of
19  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
20  * GNU General Public License for more details.
21  *
22  * You should have received a copy of the GNU General Public License
23  * along with this program; if not, write to the Free Software
24  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
25  * MA 02111-1307 USA
26  */
28 /* define DEBUG for debug output */
29 #undef DEBUG
31 #include <common.h>
32 #include <asm/processor.h>
33 #include <asm/io.h>
34 #include <ppc440.h>
36 /*-----------------------------------------------------------------------------+
37  * Prototypes
38  *-----------------------------------------------------------------------------*/
39 extern int denali_wait_for_dlllock(void);
40 extern void denali_core_search_data_eye(void);
42 #if defined(CONFIG_NAND_SPL)
43 /* Using arch/powerpc/cpu/ppc4xx/speed.c to calculate the bus frequency is too big
44  * for the 4k NAND boot image so define bus_frequency to 133MHz here
45  * which is save for the refresh counter setup.
46  */
47 #define get_bus_freq(val)       133333333
48 #endif
50 /*************************************************************************
51  *
52  * initdram -- 440EPx's DDR controller is a DENALI Core
53  *
54  ************************************************************************/
55 phys_size_t initdram (int board_type)
56 {
57 #if !(defined(CONFIG_NAND_U_BOOT) || defined(CONFIG_SYS_RAMBOOT)) || \
58     defined(CONFIG_NAND_SPL)
59         ulong speed = get_bus_freq(0);
61         mtsdram(DDR0_02, 0x00000000);
63         mtsdram(DDR0_00, 0x0000190A);
64         mtsdram(DDR0_01, 0x01000000);
65         mtsdram(DDR0_03, 0x02030602);
66         mtsdram(DDR0_04, 0x0A020200);
67         mtsdram(DDR0_05, 0x02020308);
68         mtsdram(DDR0_06, 0x0102C812);
69         mtsdram(DDR0_07, 0x000D0100);
70         mtsdram(DDR0_08, 0x02430001);
71         mtsdram(DDR0_09, 0x00011D5F);
72         mtsdram(DDR0_10, 0x00000100);
73         mtsdram(DDR0_11, 0x0027C800);
74         mtsdram(DDR0_12, 0x00000003);
75         mtsdram(DDR0_14, 0x00000000);
76         mtsdram(DDR0_17, 0x19000000);
77         mtsdram(DDR0_18, 0x19191919);
78         mtsdram(DDR0_19, 0x19191919);
79         mtsdram(DDR0_20, 0x0B0B0B0B);
80         mtsdram(DDR0_21, 0x0B0B0B0B);
81         mtsdram(DDR0_22, 0x00267F0B);
82         mtsdram(DDR0_23, 0x00000000);
83         mtsdram(DDR0_24, 0x01010002);
84         if (speed > 133333334)
85                 mtsdram(DDR0_26, 0x5B26050C);
86         else
87                 mtsdram(DDR0_26, 0x5B260408);
88         mtsdram(DDR0_27, 0x0000682B);
89         mtsdram(DDR0_28, 0x00000000);
90         mtsdram(DDR0_31, 0x00000000);
91         mtsdram(DDR0_42, 0x01000006);
92         mtsdram(DDR0_43, 0x030A0200);
93         mtsdram(DDR0_44, 0x00000003);
94         mtsdram(DDR0_02, 0x00000001);
96         denali_wait_for_dlllock();
97 #endif /* #ifndef CONFIG_NAND_U_BOOT */
99 #ifdef CONFIG_DDR_DATA_EYE
100         /* -----------------------------------------------------------+
101          * Perform data eye search if requested.
102          * ----------------------------------------------------------*/
103         denali_core_search_data_eye();
104 #endif
106         /*
107          * Clear possible errors resulting from data-eye-search.
108          * If not done, then we could get an interrupt later on when
109          * exceptions are enabled.
110          */
111         set_mcsr(get_mcsr());
113         return (CONFIG_SYS_MBYTES_SDRAM << 20);