1 /*
2 * (C) Copyright 2007
3 * Stefan Roese, DENX Software Engineering, sr@denx.de.
4 *
5 * Copyright (C) 2002 Scott McNutt <smcnutt@artesyncp.com>
6 *
7 * See file CREDITS for list of people who contributed to this
8 * project.
9 *
10 * This program is free software; you can redistribute it and/or
11 * modify it under the terms of the GNU General Public License as
12 * published by the Free Software Foundation; either version 2 of
13 * the License, or (at your option) any later version.
14 *
15 * This program is distributed in the hope that it will be useful,
16 * but WITHOUT ANY WARRANTY; without even the implied warranty of
17 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
18 * GNU General Public License for more details.
19 *
20 * You should have received a copy of the GNU General Public License
21 * along with this program; if not, write to the Free Software
22 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
23 * MA 02111-1307 USA
24 */
26 #include <ppc_asm.tmpl>
27 #include <config.h>
28 #include <asm/mmu.h>
30 /**************************************************************************
31 * TLB TABLE
32 *
33 * This table is used by the cpu boot code to setup the initial tlb
34 * entries. Rather than make broad assumptions in the cpu source tree,
35 * this table lets each board set things up however they like.
36 *
37 * Pointer to the table is returned in r1
38 *
39 *************************************************************************/
41 .section .bootpg,"ax"
43 /**************************************************************************
44 * TLB table for revA
45 *************************************************************************/
46 .globl tlbtabA
47 tlbtabA:
48 tlbtab_start
50 /*
51 * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
52 * speed up boot process. It is patched after relocation to enable SA_I
53 */
54 tlbentry(0xff000000, SZ_16M, 0xff000000, 4, AC_RWX | SA_G)
56 /*
57 * TLB entries for SDRAM are not needed on this platform.
58 * They are dynamically generated in the SPD DDR(2) detection
59 * routine.
60 */
62 tlbentry(CONFIG_SYS_ISRAM_BASE, SZ_256K, 0x00000000, 4, AC_RWX | SA_I)
63 tlbentry(CONFIG_SYS_FPGA_BASE, SZ_1K, 0xE2000000, 4,AC_RW | SA_I)
65 tlbentry(CONFIG_SYS_OPER_FLASH, SZ_16M, 0xE7000000, 4,AC_RWX | SA_IG)
66 tlbentry(CONFIG_SYS_PERIPHERAL_BASE, SZ_4K, 0xF0000000, 4, AC_RW | SA_IG)
68 tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, 0x00000000, 0xC, AC_RW | SA_IG)
69 tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, 0x10000000, 0xC, AC_RW | SA_IG)
70 tlbentry(CONFIG_SYS_PCIE_MEMBASE, SZ_256M, 0xB0000000, 0xD, AC_RW | SA_IG)
71 tlbentry(CONFIG_SYS_PCIE_BASE, SZ_16K, 0x20000000, 0xC, AC_RW | SA_IG)
73 tlbentry(CONFIG_SYS_PCIE0_CFGBASE, SZ_16M, 0x40000000, 0xC, AC_RW | SA_IG)
74 tlbentry(CONFIG_SYS_PCIE1_CFGBASE, SZ_16M, 0x80000000, 0xC, AC_RW | SA_IG)
75 tlbentry(CONFIG_SYS_PCIE2_CFGBASE, SZ_16M, 0xC0000000, 0xC, AC_RW | SA_IG)
76 tlbentry(CONFIG_SYS_PCIE0_XCFGBASE, SZ_1K, 0x50000000, 0xC, AC_RW | SA_IG)
77 tlbentry(CONFIG_SYS_PCIE1_XCFGBASE, SZ_1K, 0x90000000, 0xC, AC_RW | SA_IG)
78 tlbentry(CONFIG_SYS_PCIE2_XCFGBASE, SZ_1K, 0xD0000000, 0xC, AC_RW | SA_IG)
79 tlbtab_end
81 /**************************************************************************
82 * TLB table for revB
83 *
84 * Notice: revB of the 440SPe chip is very strict about PLB real addresses
85 * and ranges to be mapped for config space: it seems to only work with
86 * d_nnnn_nnnn range (hangs the core upon config transaction attempts when
87 * set otherwise) while revA uses c_nnnn_nnnn.
88 *************************************************************************/
89 .globl tlbtabB
90 tlbtabB:
91 tlbtab_start
93 /*
94 * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
95 * speed up boot process. It is patched after relocation to enable SA_I
96 */
97 tlbentry(0xff000000, SZ_16M, 0xff000000, 4, AC_RWX | SA_G)
99 /*
100 * TLB entries for SDRAM are not needed on this platform.
101 * They are dynamically generated in the SPD DDR(2) detection
102 * routine.
103 */
105 tlbentry(CONFIG_SYS_ISRAM_BASE, SZ_256K, 0x00000000, 4, AC_RWX | SA_I)
106 tlbentry(CONFIG_SYS_FPGA_BASE, SZ_1K, 0xE2000000, 4,AC_RW | SA_I)
108 tlbentry(CONFIG_SYS_OPER_FLASH, SZ_16M, 0xE7000000, 4,AC_RWX | SA_IG)
109 tlbentry(CONFIG_SYS_PERIPHERAL_BASE, SZ_4K, 0xF0000000, 4, AC_RW | SA_IG)
111 tlbentry(CONFIG_SYS_PCI_BASE, SZ_256M, 0x00000000, 0xC, AC_RW | SA_IG)
112 tlbentry(CONFIG_SYS_PCI_MEMBASE, SZ_256M, 0x10000000, 0xC, AC_RW | SA_IG)
113 tlbentry(CONFIG_SYS_PCIE_MEMBASE, SZ_256M, 0xB0000000, 0xD, AC_RW | SA_IG)
115 tlbentry(CONFIG_SYS_PCIE0_CFGBASE, SZ_16M, 0x00000000, 0xD, AC_RW | SA_IG)
116 tlbentry(CONFIG_SYS_PCIE1_CFGBASE, SZ_16M, 0x20000000, 0xD, AC_RW | SA_IG)
117 tlbentry(CONFIG_SYS_PCIE2_CFGBASE, SZ_16M, 0x40000000, 0xD, AC_RW | SA_IG)
118 tlbentry(CONFIG_SYS_PCIE0_XCFGBASE, SZ_1K, 0x10000000, 0xD, AC_RW | SA_IG)
119 tlbentry(CONFIG_SYS_PCIE1_XCFGBASE, SZ_1K, 0x30000000, 0xD, AC_RW | SA_IG)
120 tlbentry(CONFIG_SYS_PCIE2_XCFGBASE, SZ_1K, 0x50000000, 0xD, AC_RW | SA_IG)
121 tlbtab_end