1 /*
2 * Copyright (C) 2011 Freescale Semiconductor, Inc.
3 * Jason Liu <r64343@freescale.com>
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not write to the Free Software
20 * Foundation Inc. 51 Franklin Street Fifth Floor Boston,
21 * MA 02110-1301 USA
22 *
23 * Refer docs/README.imxmage for more details about how-to configure
24 * and create imximage boot image
25 *
26 * The syntax is taken as close as possible with the kwbimage
27 */
29 /* image version */
30 IMAGE_VERSION 2
32 /*
33 * Boot Device : one of
34 * spi, sd (the board has no nand neither onenand)
35 */
36 BOOT_FROM sd
38 /*
39 * Device Configuration Data (DCD)
40 *
41 * Each entry must have the format:
42 * Addr-type Address Value
43 *
44 * where:
45 * Addr-type register length (1,2 or 4 bytes)
46 * Address absolute address of the register
47 * value value to be stored in the register
48 */
49 DATA 4 0x020e05a8 0x00000030
50 DATA 4 0x020e05b0 0x00000030
51 DATA 4 0x020e0524 0x00000030
52 DATA 4 0x020e051c 0x00000030
54 DATA 4 0x020e0518 0x00000030
55 DATA 4 0x020e050c 0x00000030
56 DATA 4 0x020e05b8 0x00000030
57 DATA 4 0x020e05c0 0x00000030
59 DATA 4 0x020e05ac 0x00020030
60 DATA 4 0x020e05b4 0x00020030
61 DATA 4 0x020e0528 0x00020030
62 DATA 4 0x020e0520 0x00020030
64 DATA 4 0x020e0514 0x00020030
65 DATA 4 0x020e0510 0x00020030
66 DATA 4 0x020e05bc 0x00020030
67 DATA 4 0x020e05c4 0x00020030
69 DATA 4 0x020e056c 0x00020030
70 DATA 4 0x020e0578 0x00020030
71 DATA 4 0x020e0588 0x00020030
72 DATA 4 0x020e0594 0x00020030
74 DATA 4 0x020e057c 0x00020030
75 DATA 4 0x020e0590 0x00003000
76 DATA 4 0x020e0598 0x00003000
77 DATA 4 0x020e058c 0x00000000
79 DATA 4 0x020e059c 0x00003030
80 DATA 4 0x020e05a0 0x00003030
81 DATA 4 0x020e0784 0x00000030
82 DATA 4 0x020e0788 0x00000030
84 DATA 4 0x020e0794 0x00000030
85 DATA 4 0x020e079c 0x00000030
86 DATA 4 0x020e07a0 0x00000030
87 DATA 4 0x020e07a4 0x00000030
89 DATA 4 0x020e07a8 0x00000030
90 DATA 4 0x020e0748 0x00000030
91 DATA 4 0x020e074c 0x00000030
92 DATA 4 0x020e0750 0x00020000
94 DATA 4 0x020e0758 0x00000000
95 DATA 4 0x020e0774 0x00020000
96 DATA 4 0x020e078c 0x00000030
97 DATA 4 0x020e0798 0x000C0000
99 DATA 4 0x021b081c 0x33333333
100 DATA 4 0x021b0820 0x33333333
101 DATA 4 0x021b0824 0x33333333
102 DATA 4 0x021b0828 0x33333333
104 DATA 4 0x021b481c 0x33333333
105 DATA 4 0x021b4820 0x33333333
106 DATA 4 0x021b4824 0x33333333
107 DATA 4 0x021b4828 0x33333333
109 DATA 4 0x021b0018 0x00081740
111 DATA 4 0x021b001c 0x00008000
112 DATA 4 0x021b000c 0x555A7975
113 DATA 4 0x021b0010 0xFF538E64
114 DATA 4 0x021b0014 0x01FF00DB
115 DATA 4 0x021b002c 0x000026D2
117 DATA 4 0x021b0030 0x005B0E21
118 DATA 4 0x021b0008 0x09444040
119 DATA 4 0x021b0004 0x00025576
120 DATA 4 0x021b0040 0x00000027
121 DATA 4 0x021b0000 0x831A0000
123 DATA 4 0x021b001c 0x04088032
124 DATA 4 0x021b001c 0x0408803A
125 DATA 4 0x021b001c 0x00008033
126 DATA 4 0x021b001c 0x0000803B
127 DATA 4 0x021b001c 0x00428031
128 DATA 4 0x021b001c 0x00428039
129 DATA 4 0x021b001c 0x09408030
130 DATA 4 0x021b001c 0x09408038
132 DATA 4 0x021b001c 0x04008040
133 DATA 4 0x021b001c 0x04008048
134 DATA 4 0x021b0800 0xA1380003
135 DATA 4 0x021b4800 0xA1380003
136 DATA 4 0x021b0020 0x00005800
137 DATA 4 0x021b0818 0x00022227
138 DATA 4 0x021b4818 0x00022227
140 DATA 4 0x021b083c 0x434B0350
141 DATA 4 0x021b0840 0x034C0359
142 DATA 4 0x021b483c 0x434B0350
143 DATA 4 0x021b4840 0x03650348
144 DATA 4 0x021b0848 0x4436383B
145 DATA 4 0x021b4848 0x39393341
146 DATA 4 0x021b0850 0x35373933
147 DATA 4 0x021b4850 0x48254A36
149 DATA 4 0x021b080c 0x001F001F
150 DATA 4 0x021b0810 0x001F001F
152 DATA 4 0x021b480c 0x00440044
153 DATA 4 0x021b4810 0x00440044
155 DATA 4 0x021b08b8 0x00000800
156 DATA 4 0x021b48b8 0x00000800
158 DATA 4 0x021b001c 0x00000000
159 DATA 4 0x021b0404 0x00011006
161 /* set the default clock gate to save power */
162 DATA 4 0x020c4068 0x00C03F3F
163 DATA 4 0x020c406c 0x0030FC03
164 DATA 4 0x020c4070 0x0FFFC000
165 DATA 4 0x020c4074 0x3FF00000
166 DATA 4 0x020c4078 0x00FFF300
167 DATA 4 0x020c407c 0x0F0000C3
168 DATA 4 0x020c4080 0x000003FF
170 /* enable AXI cache for VDOA/VPU/IPU */
171 DATA 4 0x020e0010 0xF00000CF
172 /* set IPU AXI-id0 Qos=0xf(bypass) AXI-id1 Qos=0x7 */
173 DATA 4 0x020e0018 0x007F007F
174 DATA 4 0x020e001c 0x007F007F