1 /*
2 * (C Copyright 2009
3 * Stefano Babic DENX Software Engineering sbabic@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not write to the Free Software
20 * Foundation Inc. 51 Franklin Street Fifth Floor Boston,
21 * MA 02110-1301 USA
22 *
23 * Refer docs/README.imxmage for more details about how-to configure
24 * and create imximage boot image
25 *
26 * The syntax is taken as close as possible with the kwbimage
27 */
29 /* image version */
30 IMAGE_VERSION 2
32 /*
33 * Boot Device : one of
34 * spi, sd (the board has no nand neither onenand)
35 */
36 BOOT_FROM sd
38 /*
39 * Device Configuration Data (DCD)
40 *
41 * Each entry must have the format:
42 * Addr-type Address Value
43 *
44 * where:
45 * Addr-type register length (1,2 or 4 bytes)
46 * Address absolute address of the register
47 * value value to be stored in the register
48 */
49 /* Setting IOMUXC */
50 DATA 4 0x53fa8554 0x00200000
51 DATA 4 0x53fa8560 0x00200000
52 DATA 4 0x53fa8594 0x00200000
53 DATA 4 0x53fa8584 0x00200000
54 DATA 4 0x53fa8558 0x00200040
55 DATA 4 0x53fa8568 0x00200040
56 DATA 4 0x53fa8590 0x00200040
57 DATA 4 0x53fa857c 0x00200040
58 DATA 4 0x53fa8564 0x00200040
59 DATA 4 0x53fa8580 0x00200040
60 DATA 4 0x53fa8570 0x00200000
61 DATA 4 0x53fa8578 0x00200000
62 DATA 4 0x53fa872c 0x00200000
63 DATA 4 0x53fa8728 0x00200000
64 DATA 4 0x53fa871c 0x00200000
65 DATA 4 0x53fa8718 0x00200000
66 DATA 4 0x53fa8574 0x00280000
67 DATA 4 0x53fa8588 0x00280000
68 DATA 4 0x53fa86f0 0x00280000
69 DATA 4 0x53fa8720 0x00280000
70 DATA 4 0x53fa86fc 0x00000000
71 DATA 4 0x53fa86f4 0x00000200
72 DATA 4 0x53fa8714 0x00000000
73 DATA 4 0x53fa8724 0x06000000
74 DATA 4 0x63fd9088 0x34333936
75 DATA 4 0x63fd9090 0x49434942
76 DATA 4 0x63fd90F8 0x00000800
77 DATA 4 0x63fd907c 0x01350138
78 DATA 4 0x63fd9080 0x01380139
79 DATA 4 0x63fd9018 0x00001710
80 DATA 4 0x63fd9000 0xc4110000
81 DATA 4 0x63fd900C 0x4d5122d2
82 DATA 4 0x63fd9010 0x92d18a22
83 DATA 4 0x63fd9014 0x00c70092
84 DATA 4 0x63fd902c 0x000026d2
85 DATA 4 0x63fd9030 0x009f000e
86 DATA 4 0x63fd9008 0x12272000
87 DATA 4 0x63fd9004 0x00030012
88 DATA 4 0x63fd901c 0x04008010
89 DATA 4 0x63fd901c 0x00008032
90 DATA 4 0x63fd901c 0x00008033
91 DATA 4 0x63fd901c 0x00008031
92 DATA 4 0x63fd901c 0x0b5280b0
93 DATA 4 0x63fd901c 0x04008010
94 DATA 4 0x63fd901c 0x00008020
95 DATA 4 0x63fd901c 0x00008020
96 DATA 4 0x63fd901c 0x0a528030
97 DATA 4 0x63fd901c 0x03c68031
98 DATA 4 0x63fd901c 0x00448031
99 DATA 4 0x63fd901c 0x04008018
100 DATA 4 0x63fd901c 0x0000803a
101 DATA 4 0x63fd901c 0x0000803b
102 DATA 4 0x63fd901c 0x00008039
103 DATA 4 0x63fd901c 0x0b528138
104 DATA 4 0x63fd901c 0x04008018
105 DATA 4 0x63fd901c 0x00008028
106 DATA 4 0x63fd901c 0x00008028
107 DATA 4 0x63fd901c 0x0a528038
108 DATA 4 0x63fd901c 0x03c68039
109 DATA 4 0x63fd901c 0x00448039
110 DATA 4 0x63fd9020 0x00005800
111 DATA 4 0x63fd9058 0x00033335
112 DATA 4 0x63fd901c 0x00000000
113 DATA 4 0x63fd9040 0x05380003
114 DATA 4 0x53fa8004 0x00194005