1 /*
2 * (C) Copyright 2009
3 * Stefano Babic DENX Software Engineering sbabic@denx.de.
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not write to the Free Software
20 * Foundation Inc. 51 Franklin Street Fifth Floor Boston,
21 * MA 02110-1301 USA
22 *
23 * Refer docs/README.imxmage for more details about how-to configure
24 * and create imximage boot image
25 *
26 * The syntax is taken as close as possible with the kwbimage
27 */
29 /* image version */
30 IMAGE_VERSION 2
32 /*
33 * Boot Device : one of
34 * spi, sd (the board has no nand neither onenand)
35 */
36 BOOT_FROM sd
38 /*
39 * Device Configuration Data (DCD)
40 *
41 * Each entry must have the format:
42 * Addr-type Address Value
43 *
44 * where:
45 * Addr-type register length (1,2 or 4 bytes)
46 * Address absolute address of the register
47 * value value to be stored in the register
48 */
49 DATA 4 0x53fa8554 0x00300000
50 DATA 4 0x53fa8558 0x00300040
51 DATA 4 0x53fa8560 0x00300000
52 DATA 4 0x53fa8564 0x00300040
53 DATA 4 0x53fa8568 0x00300040
54 DATA 4 0x53fa8570 0x00300000
55 DATA 4 0x53fa8574 0x00300000
56 DATA 4 0x53fa8578 0x00300000
57 DATA 4 0x53fa857c 0x00300040
58 DATA 4 0x53fa8580 0x00300040
59 DATA 4 0x53fa8584 0x00300000
60 DATA 4 0x53fa8588 0x00300000
61 DATA 4 0x53fa8590 0x00300040
62 DATA 4 0x53fa8594 0x00300000
63 DATA 4 0x53fa86f0 0x00300000
64 DATA 4 0x53fa86f4 0x00000000
65 DATA 4 0x53fa86fc 0x00000000
66 DATA 4 0x53fa8714 0x00000000
67 DATA 4 0x53fa8718 0x00300000
68 DATA 4 0x53fa871c 0x00300000
69 DATA 4 0x53fa8720 0x00300000
70 DATA 4 0x53fa8724 0x04000000
71 DATA 4 0x53fa8728 0x00300000
72 DATA 4 0x53fa872c 0x00300000
73 DATA 4 0x63fd9088 0x35343535
74 DATA 4 0x63fd9090 0x4d444c44
75 DATA 4 0x63fd907c 0x01370138
76 DATA 4 0x63fd9080 0x013b013c
77 DATA 4 0x63fd9018 0x00011740
78 DATA 4 0x63fd9000 0xc3190000
79 DATA 4 0x63fd900c 0x9f5152e3
80 DATA 4 0x63fd9010 0xb68e8a63
81 DATA 4 0x63fd9014 0x01ff00db
82 DATA 4 0x63fd902c 0x000026d2
83 DATA 4 0x63fd9030 0x009f0e21
84 DATA 4 0x63fd9008 0x12273030
85 DATA 4 0x63fd9004 0x0002002d
86 DATA 4 0x63fd901c 0x00008032
87 DATA 4 0x63fd901c 0x00008033
88 DATA 4 0x63fd901c 0x00028031
89 DATA 4 0x63fd901c 0x052080b0
90 DATA 4 0x63fd901c 0x04008040
91 DATA 4 0x63fd901c 0x0000803a
92 DATA 4 0x63fd901c 0x0000803b
93 DATA 4 0x63fd901c 0x00028039
94 DATA 4 0x63fd901c 0x05208138
95 DATA 4 0x63fd901c 0x04008048
96 DATA 4 0x63fd9020 0x00005800
97 DATA 4 0x63fd9040 0x05380003
98 DATA 4 0x63fd9058 0x00022227
99 DATA 4 0x63fd901C 0x00000000