1 /*
2 * (C) Copyright 2002
3 * Rich Ireland, Enterasys Networks, rireland@enterasys.com.
4 * Keith Outwater, keith_outwater@mvis.com.
5 *
6 * See file CREDITS for list of people who contributed to this
7 * project.
8 *
9 * This program is free software; you can redistribute it and/or
10 * modify it under the terms of the GNU General Public License as
11 * published by the Free Software Foundation; either version 2 of
12 * the License, or (at your option) any later version.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 *
19 * You should have received a copy of the GNU General Public License
20 * along with this program; if not, write to the Free Software
21 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
22 * MA 02111-1307 USA
23 *
24 */
26 /*
27 * Virtex2 FPGA configuration support for the GEN860T computer
28 */
30 #include <common.h>
31 #include <virtex2.h>
32 #include <command.h>
33 #include "fpga.h"
35 DECLARE_GLOBAL_DATA_PTR;
37 #if defined(CONFIG_FPGA)
39 #if 0
40 #define GEN860T_FPGA_DEBUG
41 #endif
43 #ifdef GEN860T_FPGA_DEBUG
44 #define PRINTF(fmt,args...) printf (fmt ,##args)
45 #else
46 #define PRINTF(fmt,args...)
47 #endif
49 /*
50 * Port bit numbers for the Selectmap controls
51 */
52 #define FPGA_INIT_BIT_NUM 22 /* PB22 */
53 #define FPGA_RESET_BIT_NUM 11 /* PC11 */
54 #define FPGA_DONE_BIT_NUM 16 /* PB16 */
55 #define FPGA_PROGRAM_BIT_NUM 7 /* PA7 */
57 /* Note that these are pointers to code that is in Flash. They will be
58 * relocated at runtime.
59 */
60 Xilinx_Virtex2_Slave_SelectMap_fns fpga_fns = {
61 fpga_pre_config_fn,
62 fpga_pgm_fn,
63 fpga_init_fn,
64 fpga_err_fn,
65 fpga_done_fn,
66 fpga_clk_fn,
67 fpga_cs_fn,
68 fpga_wr_fn,
69 fpga_read_data_fn,
70 fpga_write_data_fn,
71 fpga_busy_fn,
72 fpga_abort_fn,
73 fpga_post_config_fn
74 };
76 Xilinx_desc fpga[CONFIG_FPGA_COUNT] = {
77 {Xilinx_Virtex2,
78 slave_selectmap,
79 XILINX_XC2V3000_SIZE,
80 (void *) &fpga_fns,
81 0}
82 };
84 /*
85 * Display FPGA revision information
86 */
87 void print_fpga_revision (void)
88 {
89 vu_long *rev_p = (vu_long *) 0x60000008;
91 printf ("FPGA Revision 0x%.8lx"
92 " (Date %.2lx/%.2lx/%.2lx, Status \"%.1lx\", Version %.3lu)\n",
93 *rev_p,
94 ((*rev_p >> 28) & 0xf),
95 ((*rev_p >> 20) & 0xff),
96 ((*rev_p >> 12) & 0xff),
97 ((*rev_p >> 8) & 0xf), (*rev_p & 0xff));
98 }
101 /*
102 * Perform a simple test of the FPGA to processor interface using the FPGA's
103 * inverting bus test register. The great thing about doing a read/write
104 * test on a register that inverts it's contents is that you avoid any
105 * problems with bus charging.
106 * Return 0 on failure, 1 on success.
107 */
108 int test_fpga_ibtr (void)
109 {
110 vu_long *ibtr_p = (vu_long *) 0x60000010;
111 vu_long readback;
112 vu_long compare;
113 int i;
114 int j;
115 int k;
116 int pass = 1;
118 static const ulong bitpattern[] = {
119 0xdeadbeef, /* magic ID pattern for debug */
120 0x00000001, /* single bit */
121 0x00000003, /* two adjacent bits */
122 0x00000007, /* three adjacent bits */
123 0x0000000F, /* four adjacent bits */
124 0x00000005, /* two non-adjacent bits */
125 0x00000015, /* three non-adjacent bits */
126 0x00000055, /* four non-adjacent bits */
127 0xaaaaaaaa, /* alternating 1/0 */
128 };
130 for (i = 0; i < 1024; i++) {
131 for (j = 0; j < 31; j++) {
132 for (k = 0;
133 k < sizeof (bitpattern) / sizeof (bitpattern[0]);
134 k++) {
135 *ibtr_p = compare = (bitpattern[k] << j);
136 readback = *ibtr_p;
137 if (readback != ~compare) {
138 printf ("%s:%d: FPGA test fail: expected 0x%.8lx" " actual 0x%.8lx\n", __FUNCTION__, __LINE__, ~compare, readback);
139 pass = 0;
140 break;
141 }
142 }
143 if (!pass)
144 break;
145 }
146 if (!pass)
147 break;
148 }
149 if (pass) {
150 printf ("FPGA inverting bus test passed\n");
151 print_fpga_revision ();
152 } else {
153 printf ("** FPGA inverting bus test failed\n");
154 }
155 return pass;
156 }
159 /*
160 * Set the active-low FPGA reset signal.
161 */
162 void fpga_reset (int assert)
163 {
164 volatile immap_t *immap = (immap_t *) CONFIG_SYS_IMMR;
166 PRINTF ("%s:%d: RESET ", __FUNCTION__, __LINE__);
167 if (assert) {
168 immap->im_ioport.iop_pcdat &= ~(0x8000 >> FPGA_RESET_BIT_NUM);
169 PRINTF ("asserted\n");
170 } else {
171 immap->im_ioport.iop_pcdat |= (0x8000 >> FPGA_RESET_BIT_NUM);
172 PRINTF ("deasserted\n");
173 }
174 }
177 /*
178 * Initialize the SelectMap interface. We assume that the mode and the
179 * initial state of all of the port pins have already been set!
180 */
181 void fpga_selectmap_init (void)
182 {
183 PRINTF ("%s:%d: Initialize SelectMap interface\n", __FUNCTION__,
184 __LINE__);
185 fpga_pgm_fn(false, false, 0); /* make sure program pin is inactive */
186 }
189 /*
190 * Initialize the fpga. Return 1 on success, 0 on failure.
191 */
192 int gen860t_init_fpga (void)
193 {
194 int i;
196 PRINTF ("%s:%d: Initialize FPGA interface\n",
197 __FUNCTION__, __LINE__);
198 fpga_init ();
199 fpga_selectmap_init ();
201 for (i = 0; i < CONFIG_FPGA_COUNT; i++) {
202 PRINTF ("%s:%d: Adding fpga %d\n", __FUNCTION__, __LINE__, i);
203 fpga_add (fpga_xilinx, &fpga[i]);
204 }
205 return 1;
206 }
209 /*
210 * Set the FPGA's active-low SelectMap program line to the specified level
211 */
212 int fpga_pgm_fn (int assert, int flush, int cookie)
213 {
214 volatile immap_t *immap = (immap_t *) CONFIG_SYS_IMMR;
216 PRINTF ("%s:%d: FPGA PROGRAM ", __FUNCTION__, __LINE__);
218 if (assert) {
219 immap->im_ioport.iop_padat &=
220 ~(0x8000 >> FPGA_PROGRAM_BIT_NUM);
221 PRINTF ("asserted\n");
222 } else {
223 immap->im_ioport.iop_padat |=
224 (0x8000 >> FPGA_PROGRAM_BIT_NUM);
225 PRINTF ("deasserted\n");
226 }
227 return assert;
228 }
231 /*
232 * Test the state of the active-low FPGA INIT line. Return 1 on INIT
233 * asserted (low).
234 */
235 int fpga_init_fn (int cookie)
236 {
237 volatile immap_t *immap = (immap_t *) CONFIG_SYS_IMMR;
239 PRINTF ("%s:%d: INIT check... ", __FUNCTION__, __LINE__);
240 if (immap->im_cpm.cp_pbdat & (0x80000000 >> FPGA_INIT_BIT_NUM)) {
241 PRINTF ("high\n");
242 return 0;
243 } else {
244 PRINTF ("low\n");
245 return 1;
246 }
247 }
250 /*
251 * Test the state of the active-high FPGA DONE pin
252 */
253 int fpga_done_fn (int cookie)
254 {
255 volatile immap_t *immap = (immap_t *) CONFIG_SYS_IMMR;
257 PRINTF ("%s:%d: DONE check... ", __FUNCTION__, __LINE__);
258 if (immap->im_cpm.cp_pbdat & (0x80000000 >> FPGA_DONE_BIT_NUM)) {
259 PRINTF ("high\n");
260 return FPGA_SUCCESS;
261 } else {
262 PRINTF ("low\n");
263 return FPGA_FAIL;
264 }
265 }
268 /*
269 * Read FPGA SelectMap data.
270 */
271 int fpga_read_data_fn (unsigned char *data, int cookie)
272 {
273 vu_char *p = (vu_char *) SELECTMAP_BASE;
275 *data = *p;
276 #if 0
277 PRINTF ("%s: Read 0x%x into 0x%p\n", __FUNCTION__, (int) data, data);
278 #endif
279 return (int) data;
280 }
283 /*
284 * Write data to the FPGA SelectMap port
285 */
286 int fpga_write_data_fn (unsigned char data, int flush, int cookie)
287 {
288 vu_char *p = (vu_char *) SELECTMAP_BASE;
290 #if 0
291 PRINTF ("%s: Write Data 0x%x\n", __FUNCTION__, (int) data);
292 #endif
293 *p = data;
294 return (int) data;
295 }
298 /*
299 * Abort and FPGA operation
300 */
301 int fpga_abort_fn (int cookie)
302 {
303 PRINTF ("%s:%d: FPGA program sequence aborted\n",
304 __FUNCTION__, __LINE__);
305 return FPGA_FAIL;
306 }
309 /*
310 * FPGA pre-configuration function. Just make sure that
311 * FPGA reset is asserted to keep the FPGA from starting up after
312 * configuration.
313 */
314 int fpga_pre_config_fn (int cookie)
315 {
316 PRINTF ("%s:%d: FPGA pre-configuration\n", __FUNCTION__, __LINE__);
317 fpga_reset(true);
318 return 0;
319 }
322 /*
323 * FPGA post configuration function. Blip the FPGA reset line and then see if
324 * the FPGA appears to be running.
325 */
326 int fpga_post_config_fn (int cookie)
327 {
328 int rc;
330 PRINTF ("%s:%d: FPGA post configuration\n", __FUNCTION__, __LINE__);
331 fpga_reset(true);
332 udelay (1000);
333 fpga_reset(false);
334 udelay (1000);
336 /*
337 * Use the FPGA,s inverting bus test register to do a simple test of the
338 * processor interface.
339 */
340 rc = test_fpga_ibtr ();
341 return rc;
342 }
345 /*
346 * Clock, chip select and write signal assert functions and error check
347 * and busy functions. These are only stubs because the GEN860T selectmap
348 * interface handles sequencing of control signals automatically (it uses
349 * a memory-mapped interface to the FPGA SelectMap port). The design of
350 * the interface guarantees that the SelectMap port cannot be overrun so
351 * no busy check is needed. A configuration error is signalled by INIT
352 * going low during configuration, so there is no need for a separate error
353 * function.
354 */
355 int fpga_clk_fn (int assert_clk, int flush, int cookie)
356 {
357 return assert_clk;
358 }
360 int fpga_cs_fn (int assert_cs, int flush, int cookie)
361 {
362 return assert_cs;
363 }
365 int fpga_wr_fn (int assert_write, int flush, int cookie)
366 {
367 return assert_write;
368 }
370 int fpga_err_fn (int cookie)
371 {
372 return 0;
373 }
375 int fpga_busy_fn (int cookie)
376 {
377 return 0;
378 }
379 #endif