1 /*
2 *
3 * See file CREDITS for list of people who contributed to this
4 * project.
5 *
6 * This program is free software; you can redistribute it and/or
7 * modify it under the terms of the GNU General Public License as
8 * published by the Free Software Foundation; either version 2 of
9 * the License, or (at your option) any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
19 * MA 02111-1307 USA
20 */
22 #include <ppc_asm.tmpl>
23 #include <asm/mmu.h>
24 #include <config.h>
26 /**************************************************************************
27 * TLB TABLE
28 *
29 * This table is used by the cpu boot code to setup the initial tlb
30 * entries. Rather than make broad assumptions in the cpu source tree,
31 * this table lets each board set things up however they like.
32 *
33 * Pointer to the table is returned in r1
34 *
35 *************************************************************************/
36 .section .bootpg,"ax"
37 .globl tlbtab
39 tlbtab:
40 tlbtab_start
42 /*
43 * BOOT_CS (FLASH) must be first. Before relocation SA_I can be off to use the
44 * speed up boot process. It is patched after relocation to enable SA_I
45 */
46 tlbentry( 0xF0000000, SZ_256M, 0xF0000000, 1, AC_RWX | SA_G )
48 /*
49 * TLB entries for SDRAM are not needed on this platform. They are
50 * generated dynamically in the SPD DDR2 detection routine.
51 */
53 #ifdef CONFIG_SYS_INIT_RAM_DCACHE
54 /* TLB-entry for init-ram in dcache (SA_I must be turned off!) */
55 tlbentry( CONFIG_SYS_INIT_RAM_ADDR, SZ_64K, CONFIG_SYS_INIT_RAM_ADDR, 0,
56 AC_RWX | SA_G )
57 #endif
59 /* TLB-entry for PCI Memory */
60 tlbentry( CONFIG_SYS_PCI_MEMBASE + 0x00000000, SZ_256M,
61 CONFIG_SYS_PCI_MEMBASE + 0x00000000, 1, AC_RW | SA_IG )
63 tlbentry( CONFIG_SYS_PCI_MEMBASE + 0x10000000, SZ_256M,
64 CONFIG_SYS_PCI_MEMBASE + 0x10000000, 1, AC_RW | SA_IG )
66 tlbentry( CONFIG_SYS_PCI_MEMBASE + 0x20000000, SZ_256M,
67 CONFIG_SYS_PCI_MEMBASE + 0x20000000, 1, AC_RW | SA_IG )
69 tlbentry( CONFIG_SYS_PCI_MEMBASE + 0x30000000, SZ_256M,
70 CONFIG_SYS_PCI_MEMBASE + 0x30000000, 1, AC_RW | SA_IG )
72 /* TLB-entry for EBC */
73 tlbentry( CONFIG_SYS_CPLD_BASE, SZ_1K, CONFIG_SYS_CPLD_BASE, 1, AC_RW | SA_IG )
75 /* TLB-entry for Internal Registers & OCM */
76 /* I wonder why this must be executable -- lrj@acm.org 2007-10-08 */
77 tlbentry( 0xE0000000, SZ_16M, 0xE0000000, 0, AC_RWX | SA_I )
79 /*TLB-entry PCI registers*/
80 tlbentry( 0xEEC00000, SZ_1K, 0xEEC00000, 1, AC_RW | SA_IG )
82 /* TLB-entry for peripherals */
83 tlbentry( 0xEF000000, SZ_16M, 0xEF000000, 1, AC_RW | SA_IG)
85 /* TLB-entry PCI IO Space - from sr@denx.de */
86 tlbentry(0xE8000000, SZ_64K, 0xE8000000, 1, AC_RW | SA_IG)
88 tlbtab_end
90 #if defined(CONFIG_KORAT_PERMANENT)
91 .globl korat_branch_absolute
92 korat_branch_absolute:
93 mtlr r3
94 blr
95 #endif