]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - board/netstal/hcu4/hcu4.c
Move arch/ppc to arch/powerpc
[glsdk/glsdk-u-boot.git] / board / netstal / hcu4 / hcu4.c
1 /*
2  *(C) Copyright 2005-2008 Netstal Maschinen AG
3  *    Niklaus Giger (Niklaus.Giger@netstal.com)
4  *
5  *    This source code is free software; you can redistribute it
6  *    and/or modify it in source code form under the terms of the GNU
7  *    General Public License as published by the Free Software
8  *    Foundation; either version 2 of the License, or (at your option)
9  *    any later version.
10  *
11  *    This program is distributed in the hope that it will be useful,
12  *    but WITHOUT ANY WARRANTY; without even the implied warranty of
13  *    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
14  *    GNU General Public License for more details.
15  *
16  *    You should have received a copy of the GNU General Public License
17  *    along with this program; if not, write to the Free Software
18  *    Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA
19  */
21 #include  <common.h>
22 #include  <ppc4xx.h>
23 #include  <asm/processor.h>
24 #include  <asm/io.h>
25 #include  <asm/u-boot.h>
26 #include  "../common/nm.h"
28 DECLARE_GLOBAL_DATA_PTR;
30 #define HCU_MACH_VERSIONS_REGISTER      (0x7C000000 + 0xF00000)
31 #define HCU_SLOT_ADDRESS                (0x7C000000 + 0x400000)
32 #define HCU_DIGITAL_IO_REGISTER         (0x7C000000 + 0x500000)
33 #define HCU_SW_INSTALL_REQUESTED        0x10
35 /*
36  * This function is run very early, out of flash, and before devices are
37  * initialized. It is called by arch/powerpc/lib/board.c:board_init_f by virtue
38  * of being in the init_sequence array.
39  *
40  * The SDRAM has been initialized already -- start.S:start called
41  * init.S:init_sdram early on -- but it is not yet being used for
42  * anything, not even stack. So be careful.
43  */
45 /* Attention: If you want 1 microsecs times from the external oscillator
46  * 0x00004051 is okay for u-boot/linux, but different from old vxworks values
47  * 0x00804051 causes problems with u-boot and linux!
48  */
49 #define CPC0_CR0_VALUE  0x0030103c
50 #define CPC0_CR1_VALUE  0x00004051
52 int board_early_init_f (void)
53 {
54         /*
55          * Interrupt controller setup for the HCU4 board.
56          * Note: IRQ 0-15  405GP internally generated; high; level sensitive
57          *       IRQ 16    405GP internally generated; low; level sensitive
58          *      IRQ 17-24 RESERVED/UNUSED
59          *      IRQ 31 (EXT IRQ 6) (unused)
60          */
61         mtdcr(UIC0SR, 0xFFFFFFFF); /* clear all ints */
62         mtdcr(UIC0ER, 0x00000000); /* disable all ints */
63         mtdcr(UIC0CR, 0x00000000); /* set all to be non-critical */
64         mtdcr(UIC0PR, 0xFFFFE000); /* set int polarities */
65         mtdcr(UIC0TR, 0x00000000); /* set int trigger levels */
66         mtdcr(UIC0SR, 0xFFFFFFFF); /* clear all ints */
68         mtdcr(CPC0_CR1, CPC0_CR1_VALUE);
69         mtdcr(CPC0_ECR, 0x60606000);
70         mtdcr(CPC0_EIRR, 0x7C000000);
72         return 0;
73 }
75 #ifdef CONFIG_BOARD_PRE_INIT
76 int board_pre_init (void)
77 {
78         return board_early_init_f ();
79 }
80 #endif
82 int sys_install_requested(void)
83 {
84         u16 ioValue = in_be16((u16 *)HCU_DIGITAL_IO_REGISTER);
85         return (ioValue & HCU_SW_INSTALL_REQUESTED) != 0;
86 }
88 int checkboard (void)
89 {
90         u16 boardVersReg = in_be16((u16 *)HCU_MACH_VERSIONS_REGISTER);
91         u16 generation = boardVersReg & 0xf0;
92         u16 index      = boardVersReg & 0x0f;
94         /* Cannot be done in board_early_init */
95         mtdcr(CPC0_CR0,  CPC0_CR0_VALUE);
97         /* Force /RTS to active. The board it not wired quite
98          *  correctly to use cts/rtc flow control, so just force the
99          *  /RST active and forget about it.
100          */
101         writeb (readb (0xef600404) | 0x03, 0xef600404);
102         nm_show_print(generation, index, 0);
104         return 0;
107 u32 hcu_led_get(void)
109         return (~(in_be32((u32 *)GPIO0_OR)) >> 23) & 0xff;
112 /*
113  * hcu_led_set  value to be placed into the LEDs (max 6 bit)
114  */
115 void hcu_led_set(u32 value)
117         u32   tmp = ~value;
119         tmp = (tmp << 23) | 0x7FFFFF;
120         out_be32((u32 *)GPIO0_OR, tmp);
123 /*
124  * hcu_get_slot
125  */
126 u32 hcu_get_slot(void)
128         u16 slot = in_be16((u16 *)HCU_SLOT_ADDRESS);
129         return slot & 0x7f;
132 /*
133  * get_serial_number
134  */
135 u32 get_serial_number(void)
137         u32 serial = in_be32((u32 *)CONFIG_SYS_FLASH_BASE);
139         if (serial == 0xffffffff)
140                 return 0;
142         return serial;
146 /*
147  * misc_init_r.
148  */
150 int misc_init_r(void)
152         common_misc_init_r();
153         set_params_for_sw_install( sys_install_requested(), "hcu4" );
154         return 0;
157 phys_size_t initdram(int board_type)
159         long dram_size = 0;
160         u16 boardVersReg = in_be16((u16 *)HCU_MACH_VERSIONS_REGISTER);
161         u16 generation = boardVersReg & 0xf0;
162         u16 index      = boardVersReg & 0x0f;
164         if (generation == HW_GENERATION_HCU3 && index < 0xf)
165                 dram_size = 32 << 20;   /* 32 MB - RAM */
166         else
167                 dram_size = 64 << 20;   /* 64 MB - RAM */
168         init_ppc405_sdram(dram_size);
170 #ifdef DEBUG
171         show_sdram_registers();
172 #endif
174         return dram_size;
177 #if defined(CONFIG_OF_LIBFDT) && defined(CONFIG_OF_BOARD_SETUP)
178 void ft_board_setup(void *blob, bd_t *bd)
180         ft_cpu_setup(blob, bd);
183 #endif /* defined(CONFIG_OF_LIBFDT) && defined(CONFIG_OF_BOARD_SETUP) */
185 /*
186  * Hardcoded flash setup:
187  * Flash 0 is a non-CFI AMD AM29F040 flash, 8 bit flash / 8 bit bus.
188  */
189 ulong board_flash_get_legacy (ulong base, int banknum, flash_info_t * info)
191         if (banknum == 0) {     /* non-CFI boot flash */
192                 info->portwidth = 1;
193                 info->chipwidth = 1;
194                 info->interface = FLASH_CFI_X8;
195                 return 1;
196         } else
197                 return 0;