1 /*
2 *(C) Copyright 2005-2008 Netstal Maschinen AG
3 * Niklaus Giger (Niklaus.Giger@netstal.com)
4 *
5 * This source code is free software; you can redistribute it
6 * and/or modify it in source code form under the terms of the GNU
7 * General Public License as published by the Free Software
8 * Foundation; either version 2 of the License, or (at your option)
9 * any later version.
10 *
11 * This program is distributed in the hope that it will be useful,
12 * but WITHOUT ANY WARRANTY; without even the implied warranty of
13 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
14 * GNU General Public License for more details.
15 *
16 * You should have received a copy of the GNU General Public License
17 * along with this program; if not, write to the Free Software
18 * Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA
19 */
21 #include <common.h>
22 #include <asm/processor.h>
23 #include <ppc440.h>
24 #include <asm/io.h>
25 #include <asm/4xx_pci.h>
27 #include "../common/nm.h"
29 DECLARE_GLOBAL_DATA_PTR;
31 extern flash_info_t flash_info[CONFIG_SYS_MAX_FLASH_BANKS];
33 #undef BOOTSTRAP_OPTION_A_ACTIVE
35 #define SDR0_CP440 0x0180
37 #define SYSTEM_RESET 0x30000000
38 #define CHIP_RESET 0x20000000
40 #define SDR0_ECID0 0x0080
41 #define SDR0_ECID1 0x0081
42 #define SDR0_ECID2 0x0082
43 #define SDR0_ECID3 0x0083
45 #define SYS_IO_ADDRESS (CONFIG_SYS_CS_2 + 0x00e00000)
46 #define SYS_SLOT_ADDRESS (CONFIG_SYS_CPLD + 0x00400000)
47 #define HCU_DIGITAL_IO_REGISTER (CONFIG_SYS_CPLD + 0x0500000)
48 #define HCU_SW_INSTALL_REQUESTED 0x10
50 /*
51 * This function is run very early, out of flash, and before devices are
52 * initialized. It is called by arch/powerpc/lib/board.c:board_init_f by virtue
53 * of being in the init_sequence array.
54 *
55 * The SDRAM has been initialized already -- start.S:start called
56 * init.S:init_sdram early on -- but it is not yet being used for
57 * anything, not even stack. So be careful.
58 */
60 int board_early_init_f(void)
61 {
63 #ifdef BOOTSTRAP_OPTION_A_ACTIVE
64 /* Booting with Bootstrap Option A
65 * First boot, with CPR0_ICFG_RLI_MASK == 0
66 * no we setup varios boot strapping register,
67 * then we do reset the PPC440 using a chip reset
68 * Unfortunately, we cannot use this option, as Nto1 is not set
69 * with Bootstrap Option A and cannot be changed later on by SW
70 * There are no other possible boostrap options with a 8 bit ROM
71 * See Errata (Version 1.04) CHIP_9
72 */
74 u32 cpr0icfg;
75 u32 dbcr;
77 mfcpr(CPR0_ICFG, cpr0icfg);
78 if (!(cpr0icfg & CPR0_ICFG_RLI_MASK)) {
79 mtcpr(CPR0_MALD, 0x02000000);
80 mtcpr(CPR0_OPBD, 0x02000000);
81 mtcpr(CPR0_PERD, 0x05000000); /* 1:5 */
82 mtcpr(CPR0_PLLC, 0x40000238);
83 mtcpr(CPR0_PLLD, 0x01010414);
84 mtcpr(CPR0_PRIMAD, 0x01000000);
85 mtcpr(CPR0_PRIMBD, 0x01000000);
86 mtcpr(CPR0_SPCID, 0x03000000);
87 mtsdr(SDR0_PFC0, 0x00003E00); /* [CTE] = 0 */
88 mtsdr(SDR0_CP440, 0x0EAAEA02); /* [Nto1] = 1*/
89 mtcpr(CPR0_ICFG, cpr0icfg | CPR0_ICFG_RLI_MASK);
91 /*
92 * Initiate system reset in debug control register DBCR
93 */
94 dbcr = mfspr(SPRN_DBCR0);
95 mtspr(SPRN_DBCR0, dbcr | CHIP_RESET);
96 }
97 mtsdr(SDR0_CP440, 0x0EAAEA02); /* [Nto1] = 1*/
98 #endif
99 mtdcr(EBC0_CFGADDR, EBC0_CFG);
100 mtdcr(EBC0_CFGDATA, 0xb8400000);
102 /*
103 * Setup the GPIO pins
104 */
105 out32(GPIO0_OR, 0x00000000);
106 out32(GPIO0_TCR, 0x7C2FF1CF);
107 out32(GPIO0_OSRL, 0x40055000);
108 out32(GPIO0_OSRH, 0x00000000);
109 out32(GPIO0_TSRL, 0x40055000);
110 out32(GPIO0_TSRH, 0x00000400);
111 out32(GPIO0_ISR1L, 0x40000000);
112 out32(GPIO0_ISR1H, 0x00000000);
113 out32(GPIO0_ISR2L, 0x00000000);
114 out32(GPIO0_ISR2H, 0x00000000);
115 out32(GPIO0_ISR3L, 0x00000000);
116 out32(GPIO0_ISR3H, 0x00000000);
118 out32(GPIO1_OR, 0x00000000);
119 out32(GPIO1_TCR, 0xC6007FFF);
120 out32(GPIO1_OSRL, 0x00140000);
121 out32(GPIO1_OSRH, 0x00000000);
122 out32(GPIO1_TSRL, 0x00000000);
123 out32(GPIO1_TSRH, 0x00000000);
124 out32(GPIO1_ISR1L, 0x05415555);
125 out32(GPIO1_ISR1H, 0x40000000);
126 out32(GPIO1_ISR2L, 0x00000000);
127 out32(GPIO1_ISR2H, 0x00000000);
128 out32(GPIO1_ISR3L, 0x00000000);
129 out32(GPIO1_ISR3H, 0x00000000);
131 /*
132 * Setup the interrupt controller polarities, triggers, etc.
133 */
134 mtdcr(UIC0SR, 0xffffffff); /* clear all */
135 mtdcr(UIC0ER, 0x00000000); /* disable all */
136 mtdcr(UIC0CR, 0x00000005); /* ATI & UIC1 crit are critical */
137 mtdcr(UIC0PR, 0xfffff7ff); /* per ref-board manual */
138 mtdcr(UIC0TR, 0x00000000); /* per ref-board manual */
139 mtdcr(UIC0VR, 0x00000000); /* int31 highest, base=0x000 */
140 mtdcr(UIC0SR, 0xffffffff); /* clear all */
142 mtdcr(UIC1SR, 0xffffffff); /* clear all */
143 mtdcr(UIC1ER, 0x00000000); /* disable all */
144 mtdcr(UIC1CR, 0x00000000); /* all non-critical */
145 mtdcr(UIC1PR, 0xffffffff); /* per ref-board manual */
146 mtdcr(UIC1TR, 0x00000000); /* per ref-board manual */
147 mtdcr(UIC1VR, 0x00000000); /* int31 highest, base=0x000 */
148 mtdcr(UIC1SR, 0xffffffff); /* clear all */
150 mtdcr(UIC2SR, 0xffffffff); /* clear all */
151 mtdcr(UIC2ER, 0x00000000); /* disable all */
152 mtdcr(UIC2CR, 0x00000000); /* all non-critical */
153 mtdcr(UIC2PR, 0xffffffff); /* per ref-board manual */
154 mtdcr(UIC2TR, 0x00000000); /* per ref-board manual */
155 mtdcr(UIC2VR, 0x00000000); /* int31 highest, base=0x000 */
156 mtdcr(UIC2SR, 0xffffffff); /* clear all */
157 mtsdr(SDR0_PFC0, 0x00003E00); /* Pin function: */
158 mtsdr(SDR0_PFC1, 0x00848000); /* Pin function: UART0 has 4 pins */
160 /* setup BOOT FLASH */
161 mtsdr(SDR0_CUST0, 0xC0082350);
163 return 0;
164 }
166 #ifdef CONFIG_BOARD_PRE_INIT
167 int board_pre_init(void)
168 {
169 return board_early_init_f();
170 }
172 #endif
174 int sys_install_requested(void)
175 {
176 u16 *ioValuePtr = (u16 *)HCU_DIGITAL_IO_REGISTER;
177 return (in_be16(ioValuePtr) & HCU_SW_INSTALL_REQUESTED) != 0;
178 }
180 int checkboard(void)
181 {
182 u16 *hwVersReg = (u16 *) HCU_HW_VERSION_REGISTER;
183 u16 *boardVersReg = (u16 *) HCU_CPLD_VERSION_REGISTER;
184 u16 generation = in_be16(boardVersReg) & 0xf0;
185 u16 index = in_be16(boardVersReg) & 0x0f;
186 u32 ecid0, ecid1, ecid2, ecid3;
188 nm_show_print(generation, index, in_be16(hwVersReg) & 0xff);
189 mfsdr(SDR0_ECID0, ecid0);
190 mfsdr(SDR0_ECID1, ecid1);
191 mfsdr(SDR0_ECID2, ecid2);
192 mfsdr(SDR0_ECID3, ecid3);
194 printf("Chip ID 0x%x 0x%x 0x%x 0x%x\n", ecid0, ecid1, ecid2, ecid3);
196 return 0;
197 }
199 u32 hcu_led_get(void)
200 {
201 return in16(SYS_IO_ADDRESS) & 0x3f;
202 }
204 /*
205 * hcu_led_set value to be placed into the LEDs (max 6 bit)
206 */
207 void hcu_led_set(u32 value)
208 {
209 out16(SYS_IO_ADDRESS, value);
210 }
212 /*
213 * get_serial_number
214 */
215 u32 get_serial_number(void)
216 {
217 u32 *serial = (u32 *)CONFIG_SYS_FLASH_BASE;
219 if (in_be32(serial) == 0xffffffff)
220 return 0;
222 return in_be32(serial);
223 }
226 /*
227 * hcu_get_slot
228 */
229 u32 hcu_get_slot(void)
230 {
231 u16 *slot = (u16 *)SYS_SLOT_ADDRESS;
232 return in_be16(slot) & 0x7f;
233 }
236 /*
237 * misc_init_r.
238 */
239 int misc_init_r(void)
240 {
241 unsigned long usb2d0cr = 0;
242 unsigned long usb2phy0cr, usb2h0cr = 0;
243 unsigned long sdr0_pfc1;
245 #ifdef CONFIG_ENV_IS_IN_FLASH
246 /* Monitor protection ON by default */
247 (void)flash_protect(FLAG_PROTECT_SET,
248 -CONFIG_SYS_MONITOR_LEN,
249 0xffffffff,
250 &flash_info[0]);
252 #ifdef CONFIG_ENV_ADDR_REDUND
253 /* Env protection ON by default */
254 (void)flash_protect(FLAG_PROTECT_SET,
255 CONFIG_ENV_ADDR_REDUND,
256 CONFIG_ENV_ADDR_REDUND + 2*CONFIG_ENV_SECT_SIZE - 1,
257 &flash_info[0]);
258 #endif
259 #endif
261 /*
262 * USB stuff...
263 */
265 /* SDR Setting */
266 mfsdr(SDR0_PFC1, sdr0_pfc1);
267 mfsdr(SDR0_USB2D0CR, usb2d0cr);
268 mfsdr(SDR0_USB2PHY0CR, usb2phy0cr);
269 mfsdr(SDR0_USB2H0CR, usb2h0cr);
271 usb2phy0cr = usb2phy0cr &~SDR0_USB2PHY0CR_XOCLK_MASK;
272 usb2phy0cr = usb2phy0cr | SDR0_USB2PHY0CR_XOCLK_EXTERNAL; /*0*/
273 usb2phy0cr = usb2phy0cr &~SDR0_USB2PHY0CR_WDINT_MASK;
274 usb2phy0cr = usb2phy0cr | SDR0_USB2PHY0CR_WDINT_16BIT_30MHZ; /*1*/
275 usb2phy0cr = usb2phy0cr &~SDR0_USB2PHY0CR_DVBUS_MASK;
276 usb2phy0cr = usb2phy0cr | SDR0_USB2PHY0CR_DVBUS_PURDIS; /*0*/
277 usb2phy0cr = usb2phy0cr &~SDR0_USB2PHY0CR_DWNSTR_MASK;
278 usb2phy0cr = usb2phy0cr | SDR0_USB2PHY0CR_DWNSTR_HOST; /*1*/
279 usb2phy0cr = usb2phy0cr &~SDR0_USB2PHY0CR_UTMICN_MASK;
280 usb2phy0cr = usb2phy0cr | SDR0_USB2PHY0CR_UTMICN_HOST; /*1*/
282 /* An 8-bit/60MHz interface is the only possible alternative
283 * when connecting the Device to the PHY
284 */
285 usb2h0cr = usb2h0cr &~SDR0_USB2H0CR_WDINT_MASK;
286 usb2h0cr = usb2h0cr | SDR0_USB2H0CR_WDINT_16BIT_30MHZ; /*1*/
288 /* To enable the USB 2.0 Device function through the UTMI interface */
289 usb2d0cr = usb2d0cr &~SDR0_USB2D0CR_USB2DEV_EBC_SEL_MASK;
290 usb2d0cr = usb2d0cr | SDR0_USB2D0CR_USB2DEV_SELECTION; /*1*/
292 sdr0_pfc1 = sdr0_pfc1 &~SDR0_PFC1_UES_MASK;
293 sdr0_pfc1 = sdr0_pfc1 | SDR0_PFC1_UES_USB2D_SEL; /*0*/
295 mtsdr(SDR0_PFC1, sdr0_pfc1);
296 mtsdr(SDR0_USB2D0CR, usb2d0cr);
297 mtsdr(SDR0_USB2PHY0CR, usb2phy0cr);
298 mtsdr(SDR0_USB2H0CR, usb2h0cr);
300 /*clear resets*/
301 udelay(1000);
302 mtsdr(SDR0_SRST1, 0x00000000);
303 udelay(1000);
304 mtsdr(SDR0_SRST0, 0x00000000);
305 printf("USB: Host(int phy) Device(ext phy)\n");
307 common_misc_init_r();
308 set_params_for_sw_install( sys_install_requested(), "hcu5" );
309 /* We cannot easily enable trace before, as there are other
310 * routines messing around with sdr0_pfc1. And I do not need it.
311 */
312 if (mfspr(SPRN_DBCR0) & 0x80000000) {
313 /* External debugger alive
314 * enable trace facilty for Lauterbach
315 * CCR0[DTB]=0 Enable broadcast of trace information
316 * SDR0_PFC0[TRE] Trace signals are enabled instead of
317 * GPIO49-63
318 */
319 mtspr(SPRN_CCR0, mfspr(SPRN_CCR0) &~ (CCR0_DTB));
320 mtsdr(SDR0_PFC0, sdr0_pfc1 | SDR0_PFC0_TRE_ENABLE);
321 }
322 return 0;
323 }
324 #ifdef CONFIG_PCI
325 int board_with_pci(void)
326 {
327 u32 reg;
329 mfsdr(SDR0_PCI0, reg);
330 return (reg & SDR0_XCR_PAE_MASK);
331 }
333 /*
334 * pci_pre_init
335 *
336 * This routine is called just prior to registering the hose and gives
337 * the board the opportunity to check things. Returning a value of zero
338 * indicates that things are bad & PCI initialization should be aborted.
339 *
340 * Different boards may wish to customize the pci controller structure
341 * (add regions, override default access routines, etc) or perform
342 * certain pre-initialization actions.
343 *
344 */
345 int pci_pre_init(struct pci_controller *hose)
346 {
347 unsigned long addr;
349 if (!board_with_pci()) { return 0; }
351 /*
352 * Set priority for all PLB3 devices to 0.
353 * Set PLB3 arbiter to fair mode.
354 */
355 mfsdr(SD0_AMP1, addr);
356 mtsdr(SD0_AMP1, (addr & 0x000000FF) | 0x0000FF00);
357 addr = mfdcr(PLB3_ACR);
358 mtdcr(PLB3_ACR, addr | 0x80000000); /* Sequoia */
360 /*
361 * Set priority for all PLB4 devices to 0.
362 */
363 mfsdr(SD0_AMP0, addr);
364 mtsdr(SD0_AMP0, (addr & 0x000000FF) | 0x0000FF00);
365 addr = mfdcr(PLB4_ACR) | 0xa0000000; /* Was 0x8---- */
366 mtdcr(PLB4_ACR, addr); /* Sequoia */
368 /*
369 * As of errata version 0.4, CHIP_8: Incorrect Write to DDR SDRAM.
370 * Workaround: Disable write pipelining to DDR SDRAM by setting
371 * PLB0_ACR[WRP] = 0.
372 */
373 mtdcr(PLB0_ACR, 0); /* PATCH HAB: WRITE PIPELINING OFF */
375 /* Segment1 */
376 mtdcr(PLB1_ACR, 0); /* PATCH HAB: WRITE PIPELINING OFF */
378 return board_with_pci();
379 }
381 /*
382 * Override weak default pci_master_init()
383 */
384 void pci_master_init(struct pci_controller *hose)
385 {
386 if (!board_with_pci())
387 return;
389 __pci_master_init(hose);
390 }
391 #endif /* defined(CONFIG_PCI) */
393 #if defined(CONFIG_OF_LIBFDT) && defined(CONFIG_OF_BOARD_SETUP)
394 void ft_board_setup(void *blob, bd_t *bd)
395 {
396 ft_cpu_setup(blob, bd);
398 }
399 #endif /* defined(CONFIG_OF_LIBFDT) && defined(CONFIG_OF_BOARD_SETUP) */
401 /*
402 * Hardcoded flash setup:
403 * Flash 0 is a non-CFI AMD AM29F040 flash, 8 bit flash / 8 bit bus.
404 */
405 ulong board_flash_get_legacy (ulong base, int banknum, flash_info_t * info)
406 {
407 if (banknum == 0) { /* non-CFI boot flash */
408 info->portwidth = 1;
409 info->chipwidth = 1;
410 info->interface = FLASH_CFI_X8;
411 return 1;
412 } else
413 return 0;
414 }