1 /*
2 * (C) Copyright 2010,2011
3 * NVIDIA Corporation <www.nvidia.com>
4 *
5 * See file CREDITS for list of people who contributed to this
6 * project.
7 *
8 * This program is free software; you can redistribute it and/or
9 * modify it under the terms of the GNU General Public License as
10 * published by the Free Software Foundation; either version 2 of
11 * the License, or (at your option) any later version.
12 *
13 * This program is distributed in the hope that it will be useful,
14 * but WITHOUT ANY WARRANTY; without even the implied warranty of
15 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
16 * GNU General Public License for more details.
17 *
18 * You should have received a copy of the GNU General Public License
19 * along with this program; if not, write to the Free Software
20 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21 * MA 02111-1307 USA
22 */
24 #include <common.h>
25 #include <asm/io.h>
26 #include <asm/arch/clock.h>
27 #include <asm/arch/funcmux.h>
28 #include <asm/arch/pinmux.h>
29 #include <asm/arch/tegra.h>
30 #include <asm/arch-tegra/mmc.h>
31 #include <asm/gpio.h>
32 #ifdef CONFIG_TEGRA_MMC
33 #include <mmc.h>
34 #endif
37 #ifdef CONFIG_TEGRA_MMC
38 /*
39 * Routine: pin_mux_mmc
40 * Description: setup the pin muxes/tristate values for the SDMMC(s)
41 */
42 static void pin_mux_mmc(void)
43 {
44 funcmux_select(PERIPH_ID_SDMMC4, FUNCMUX_SDMMC4_ATB_GMA_GME_8_BIT);
45 funcmux_select(PERIPH_ID_SDMMC2, FUNCMUX_SDMMC2_DTA_DTD_8BIT);
47 /* For power GPIO PI6 */
48 pinmux_tristate_disable(PINGRP_ATA);
49 /* For CD GPIO PH2 */
50 pinmux_tristate_disable(PINGRP_ATD);
52 /* For power GPIO PT3 */
53 pinmux_tristate_disable(PINGRP_DTB);
54 /* For CD GPIO PI5 */
55 pinmux_tristate_disable(PINGRP_ATC);
56 }
58 /* this is a weak define that we are overriding */
59 int board_mmc_init(bd_t *bd)
60 {
61 debug("board_mmc_init called\n");
63 /* Enable muxes, etc. for SDMMC controllers */
64 pin_mux_mmc();
66 debug("board_mmc_init: init SD slot J26\n");
67 /* init dev 0, SD slot J26, with 4-bit bus */
68 /* The board has an 8-bit bus, but 8-bit doesn't work yet */
69 tegra_mmc_init(0, 4, GPIO_PI6, GPIO_PH2);
71 debug("board_mmc_init: init SD slot J5\n");
72 /* init dev 2, SD slot J5, with 4-bit bus */
73 tegra_mmc_init(2, 4, GPIO_PT3, GPIO_PI5);
75 return 0;
76 }
77 #endif
79 void pin_mux_usb(void)
80 {
81 funcmux_select(PERIPH_ID_USB2, FUNCMUX_USB2_ULPI);
82 pinmux_set_func(PINGRP_CDEV2, PMUX_FUNC_PLLP_OUT4);
83 pinmux_tristate_disable(PINGRP_CDEV2);
84 /* USB2 PHY reset GPIO */
85 pinmux_tristate_disable(PINGRP_UAC);
86 }