]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - glsdk/glsdk-u-boot.git/blob - board/nvidia/seaboard/seaboard.c
Merge remote-tracking branch 'u-boot-ti/master'
[glsdk/glsdk-u-boot.git] / board / nvidia / seaboard / seaboard.c
1 /*
2  *  (C) Copyright 2010,2011
3  *  NVIDIA Corporation <www.nvidia.com>
4  *
5  * See file CREDITS for list of people who contributed to this
6  * project.
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
16  * GNU General Public License for more details.
17  *
18  * You should have received a copy of the GNU General Public License
19  * along with this program; if not, write to the Free Software
20  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
21  * MA 02111-1307 USA
22  */
24 #include <common.h>
25 #include <asm/io.h>
26 #include <asm/arch/tegra.h>
27 #include <asm/arch/clock.h>
28 #include <asm/arch/funcmux.h>
29 #include <asm/arch/gpio.h>
30 #include <asm/arch/pinmux.h>
31 #include <asm/arch-tegra/mmc.h>
32 #include <asm/gpio.h>
33 #ifdef CONFIG_TEGRA_MMC
34 #include <mmc.h>
35 #endif
37 /* TODO: Remove this code when the SPI switch is working */
38 #if !defined(CONFIG_SPI_UART_SWITCH) && (CONFIG_MACH_TYPE != MACH_TYPE_VENTANA)
39 void gpio_early_init_uart(void)
40 {
41         /* Enable UART via GPIO_PI3 (port 8, bit 3) so serial console works */
42 #ifndef CONFIG_SPL_BUILD
43         gpio_request(GPIO_PI3, NULL);
44 #endif
45         gpio_direction_output(GPIO_PI3, 0);
46 }
47 #endif
49 #ifdef CONFIG_TEGRA_MMC
50 /*
51  * Routine: pin_mux_mmc
52  * Description: setup the pin muxes/tristate values for the SDMMC(s)
53  */
54 static void pin_mux_mmc(void)
55 {
56         funcmux_select(PERIPH_ID_SDMMC4, FUNCMUX_SDMMC4_ATB_GMA_GME_8_BIT);
57         funcmux_select(PERIPH_ID_SDMMC3, FUNCMUX_SDMMC3_SDB_4BIT);
59         /* For power GPIO PI6 */
60         pinmux_tristate_disable(PINGRP_ATA);
61         /* For CD GPIO PI5 */
62         pinmux_tristate_disable(PINGRP_ATC);
63 }
65 /* this is a weak define that we are overriding */
66 int board_mmc_init(bd_t *bd)
67 {
68         debug("board_mmc_init called\n");
70         /* Enable muxes, etc. for SDMMC controllers */
71         pin_mux_mmc();
73         debug("board_mmc_init: init eMMC\n");
74         /* init dev 0, eMMC chip, with 4-bit bus */
75         /* The board has an 8-bit bus, but 8-bit doesn't work yet */
76         tegra_mmc_init(0, 4, -1, -1);
78         debug("board_mmc_init: init SD slot\n");
79         /* init dev 1, SD slot, with 4-bit bus */
80         tegra_mmc_init(1, 4, GPIO_PI6, GPIO_PI5);
82         return 0;
83 }
84 #endif
86 void pin_mux_usb(void)
87 {
88         /* For USB's GPIO PD0. For now, since we have no pinmux in fdt */
89         pinmux_tristate_disable(PINGRP_SLXK);
90 }