7adb52405c13ab41391b97ab5ce612bffe5b96c3
[glsdk/glsdk-u-boot.git] / board / ti / ti814x / evm.c
1 /*
2  * evm.c
3  *
4  * Board functions for TI814x EVM
5  *
6  * Copyright (C) 2011, Texas Instruments, Incorporated - http://www.ti.com/
7  *
8  * This program is free software; you can redistribute it and/or
9  * modify it under the terms of the GNU General Public License as
10  * published by the Free Software Foundation; either version 2 of
11  * the License, or (at your option) any later version.
12  *
13  * This program is distributed in the hope that it will be useful,
14  * but WITHOUT ANY WARRANTY; without even the implied warranty of
15  * MERCHANTABILITY or FITNESS FOR A PARTICULAR /PURPOSE.  See the
16  * GNU General Public License for more details.
17  */
19 #include <common.h>
20 #include <cpsw.h>
21 #include <errno.h>
22 #include <spl.h>
23 #include <asm/arch/cpu.h>
24 #include <asm/arch/hardware.h>
25 #include <asm/arch/omap.h>
26 #include <asm/arch/ddr_defs.h>
27 #include <asm/arch/clock.h>
28 #include <asm/arch/gpio.h>
29 #include <asm/arch/mmc_host_def.h>
30 #include <asm/arch/sys_proto.h>
31 #include <asm/io.h>
32 #include <asm/emif.h>
33 #include <asm/gpio.h>
34 #include "evm.h"
36 DECLARE_GLOBAL_DATA_PTR;
38 #ifdef CONFIG_SPL_BUILD
39 static struct wd_timer *wdtimer = (struct wd_timer *)WDT_BASE;
40 static struct uart_sys *uart_base = (struct uart_sys *)DEFAULT_UART_BASE;
41 #endif
43 static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE;
45 /* UART Defines */
46 #ifdef CONFIG_SPL_BUILD
47 #define UART_RESET              (0x1 << 1)
48 #define UART_CLK_RUNNING_MASK   0x1
49 #define UART_SMART_IDLE_EN      (0x1 << 0x3)
51 static void rtc32k_enable(void)
52 {
53         struct rtc_regs *rtc = (struct rtc_regs *)RTC_BASE;
55         /*
56          * Unlock the RTC's registers.  For more details please see the
57          * RTC_SS section of the TRM.  In order to unlock we need to
58          * write these specific values (keys) in this order.
59          */
60         writel(0x83e70b13, &rtc->kick0r);
61         writel(0x95a4f1e0, &rtc->kick1r);
63         /* Enable the RTC 32K OSC by setting bits 3 and 6. */
64         writel((1 << 3) | (1 << 6), &rtc->osc);
65 }
67 static void uart_enable(void)
68 {
69         u32 regVal;
71         /* UART softreset */
72         regVal = readl(&uart_base->uartsyscfg);
73         regVal |= UART_RESET;
74         writel(regVal, &uart_base->uartsyscfg);
75         while ((readl(&uart_base->uartsyssts) &
76                 UART_CLK_RUNNING_MASK) != UART_CLK_RUNNING_MASK)
77                 ;
79         /* Disable smart idle */
80         regVal = readl(&uart_base->uartsyscfg);
81         regVal |= UART_SMART_IDLE_EN;
82         writel(regVal, &uart_base->uartsyscfg);
83 }
85 static void wdt_disable(void)
86 {
87         writel(0xAAAA, &wdtimer->wdtwspr);
88         while (readl(&wdtimer->wdtwwps) != 0x0)
89                 ;
90         writel(0x5555, &wdtimer->wdtwspr);
91         while (readl(&wdtimer->wdtwwps) != 0x0)
92                 ;
93 }
95 static const struct cmd_control evm_ddr2_cctrl_data = {
96         .cmd0csratio    = 0x80,
97         .cmd0dldiff     = 0x04,
98         .cmd0iclkout    = 0x00,
100         .cmd1csratio    = 0x80,
101         .cmd1dldiff     = 0x04,
102         .cmd1iclkout    = 0x00,
104         .cmd2csratio    = 0x80,
105         .cmd2dldiff     = 0x04,
106         .cmd2iclkout    = 0x00,
107 };
109 static const struct emif_regs evm_ddr2_emif0_regs = {
110         .sdram_config                   = 0x40801ab2,
111         .ref_ctrl                       = 0x10000c30,
112         .sdram_tim1                     = 0x0aaaf552,
113         .sdram_tim2                     = 0x043631d2,
114         .sdram_tim3                     = 0x00000327,
115         .emif_ddr_phy_ctlr_1            = 0x00000007
116 };
118 static const struct emif_regs evm_ddr2_emif1_regs = {
119         .sdram_config                   = 0x40801ab2,
120         .ref_ctrl                       = 0x10000c30,
121         .sdram_tim1                     = 0x0aaaf552,
122         .sdram_tim2                     = 0x043631d2,
123         .sdram_tim3                     = 0x00000327,
124         .emif_ddr_phy_ctlr_1            = 0x00000007
125 };
127 const struct dmm_lisa_map_regs evm_lisa_map_regs = {
128         .dmm_lisa_map_0                 = 0x00000000,
129         .dmm_lisa_map_1                 = 0x00000000,
130         .dmm_lisa_map_2                 = 0x806c0300,
131         .dmm_lisa_map_3                 = 0x806c0300,
132 };
134 static const struct ddr_data evm_ddr2_data = {
135         .datardsratio0          = ((0x35<<10) | (0x35<<0)),
136         .datawdsratio0          = ((0x20<<10) | (0x20<<0)),
137         .datawiratio0           = ((0<<10) | (0<<0)),
138         .datagiratio0           = ((0<<10) | (0<<0)),
139         .datafwsratio0          = ((0x90<<10) | (0x90<<0)),
140         .datawrsratio0          = ((0x50<<10) | (0x50<<0)),
141         .datauserank0delay      = 1,
142         .datadldiff0            = 0x4,
143 };
144 #endif
146 /*
147  * early system init of muxing and clocks.
148  */
149 void s_init(void)
151 #ifdef CONFIG_SPL_BUILD
152         /* WDT1 is already running when the bootloader gets control
153          * Disable it to avoid "random" resets
154          */
155         wdt_disable();
157         /* Enable timer */
158         timer_init();
160         /* Setup the PLLs and the clocks for the peripherals */
161         pll_init();
163         /* Enable RTC32K clock */
164         rtc32k_enable();
166         /* Set UART pins */
167         enable_uart0_pin_mux();
169         /* Set MMC pins */
170         enable_mmc1_pin_mux();
172         /* Set Ethernet pins */
173         enable_enet_pin_mux();
175         /* Enable UART */
176         uart_enable();
178         gd = &gdata;
180         preloader_console_init();
182         config_dmm(&evm_lisa_map_regs);
184         config_ddr(0, 0, &evm_ddr2_data, &evm_ddr2_cctrl_data,
185                    &evm_ddr2_emif0_regs, 0);
186         config_ddr(0, 0, &evm_ddr2_data, &evm_ddr2_cctrl_data,
187                    &evm_ddr2_emif1_regs, 1);
188 #endif
191 /*
192  * Basic board specific setup.  Pinmux has been handled already.
193  */
194 int board_init(void)
196         gd->bd->bi_boot_params = PHYS_DRAM_1 + 0x100;
197         return 0;
200 #if !defined(CONFIG_SPL_BUILD) && defined(CONFIG_GENERIC_MMC)
201 int board_mmc_init(bd_t *bis)
203         omap_mmc_init(1, 0, 0, -1, -1);
205         return 0;
207 #endif
209 #ifdef CONFIG_DRIVER_TI_CPSW
210 static void cpsw_control(int enabled)
212         /* VTP can be added here */
214         return;
217 static struct cpsw_slave_data cpsw_slaves[] = {
218         {
219                 .slave_reg_ofs  = 0x50,
220                 .sliver_reg_ofs = 0x700,
221                 .phy_id         = 1,
222         },
223         {
224                 .slave_reg_ofs  = 0x90,
225                 .sliver_reg_ofs = 0x740,
226                 .phy_id         = 0,
227         },
228 };
230 static struct cpsw_platform_data cpsw_data = {
231         .mdio_base              = CPSW_MDIO_BASE,
232         .cpsw_base              = CPSW_BASE,
233         .mdio_div               = 0xff,
234         .channels               = 8,
235         .cpdma_reg_ofs          = 0x100,
236         .slaves                 = 1,
237         .slave_data             = cpsw_slaves,
238         .ale_reg_ofs            = 0x600,
239         .ale_entries            = 1024,
240         .host_port_reg_ofs      = 0x28,
241         .hw_stats_reg_ofs       = 0x400,
242         .mac_control            = (1 << 5),
243         .control                = cpsw_control,
244         .host_port_num          = 0,
245         .version                = CPSW_CTRL_VERSION_1,
246 };
247 #endif
249 int board_eth_init(bd_t *bis)
251         uint8_t mac_addr[6];
252         uint32_t mac_hi, mac_lo;
254         if (!eth_getenv_enetaddr("ethaddr", mac_addr)) {
255                 printf("<ethaddr> not set. Reading from E-fuse\n");
256                 /* try reading mac address from efuse */
257                 mac_lo = readl(&cdev->macid0l);
258                 mac_hi = readl(&cdev->macid0h);
259                 mac_addr[0] = mac_hi & 0xFF;
260                 mac_addr[1] = (mac_hi & 0xFF00) >> 8;
261                 mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
262                 mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
263                 mac_addr[4] = mac_lo & 0xFF;
264                 mac_addr[5] = (mac_lo & 0xFF00) >> 8;
266                 if (is_valid_ether_addr(mac_addr))
267                         eth_setenv_enetaddr("ethaddr", mac_addr);
268                 else
269                         printf("Unable to read MAC address. Set <ethaddr>\n");
270         }
272         return cpsw_register(&cpsw_data);