Merge u-boot/master into u-boot-ti/master
[glsdk/glsdk-u-boot.git] / board / timll / devkit8000 / devkit8000.c
1 /*
2  * (C) Copyright 2004-2008
3  * Texas Instruments, <www.ti.com>
4  *
5  * Author :
6  *      Sunil Kumar <sunilsaini05@gmail.com>
7  *      Shashi Ranjan <shashiranjanmca05@gmail.com>
8  *
9  * (C) Copyright 2009
10  * Frederik Kriewitz <frederik@kriewitz.eu>
11  *
12  * Derived from Beagle Board and 3430 SDP code by
13  *      Richard Woodruff <r-woodruff2@ti.com>
14  *      Syed Mohammed Khasim <khasim@ti.com>
15  *
16  *
17  * See file CREDITS for list of people who contributed to this
18  * project.
19  *
20  * This program is free software; you can redistribute it and/or
21  * modify it under the terms of the GNU General Public License as
22  * published by the Free Software Foundation; either version 2 of
23  * the License, or (at your option) any later version.
24  *
25  * This program is distributed in the hope that it will be useful,
26  * but WITHOUT ANY WARRANTY; without even the implied warranty of
27  * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
28  * GNU General Public License for more details.
29  *
30  * You should have received a copy of the GNU General Public License
31  * along with this program; if not, write to the Free Software
32  * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
33  * MA 02111-1307 USA
34  */
35 #include <common.h>
36 #include <twl4030.h>
37 #include <asm/io.h>
38 #include <asm/arch/mmc_host_def.h>
39 #include <asm/arch/mux.h>
40 #include <asm/arch/sys_proto.h>
41 #include <asm/arch/mem.h>
42 #include <asm/mach-types.h>
43 #include "devkit8000.h"
44 #include <asm/gpio.h>
45 #ifdef CONFIG_DRIVER_DM9000
46 #include <net.h>
47 #include <netdev.h>
48 #endif
50 DECLARE_GLOBAL_DATA_PTR;
52 static u32 gpmc_net_config[GPMC_MAX_REG] = {
53         NET_GPMC_CONFIG1,
54         NET_GPMC_CONFIG2,
55         NET_GPMC_CONFIG3,
56         NET_GPMC_CONFIG4,
57         NET_GPMC_CONFIG5,
58         NET_GPMC_CONFIG6,
59         0
60 };
62 /*
63  * Routine: board_init
64  * Description: Early hardware init.
65  */
66 int board_init(void)
67 {
68         gpmc_init(); /* in SRAM or SDRAM, finish GPMC */
69         /* board id for Linux */
70         gd->bd->bi_arch_number = MACH_TYPE_DEVKIT8000;
71         /* boot param addr */
72         gd->bd->bi_boot_params = (OMAP34XX_SDRC_CS0 + 0x100);
74         return 0;
75 }
77 /* Configure GPMC registers for DM9000 */
78 static void gpmc_dm9000_config(void)
79 {
80         enable_gpmc_cs_config(gpmc_net_config, &gpmc_cfg->cs[6],
81                 CONFIG_DM9000_BASE, GPMC_SIZE_16M);
82 }
84 /*
85  * Routine: misc_init_r
86  * Description: Configure board specific parts
87  */
88 int misc_init_r(void)
89 {
90         struct ctrl_id *id_base = (struct ctrl_id *)OMAP34XX_ID_L4_IO_BASE;
91 #ifdef CONFIG_DRIVER_DM9000
92         uchar enetaddr[6];
93         u32 die_id_0;
94 #endif
96         twl4030_power_init();
97 #ifdef CONFIG_TWL4030_LED
98         twl4030_led_init(TWL4030_LED_LEDEN_LEDAON | TWL4030_LED_LEDEN_LEDBON);
99 #endif
101 #ifdef CONFIG_DRIVER_DM9000
102         /* Configure GPMC registers for DM9000 */
103         enable_gpmc_cs_config(gpmc_net_config, &gpmc_cfg->cs[6],
104                         CONFIG_DM9000_BASE, GPMC_SIZE_16M);
106         /* Use OMAP DIE_ID as MAC address */
107         if (!eth_getenv_enetaddr("ethaddr", enetaddr)) {
108                 printf("ethaddr not set, using Die ID\n");
109                 die_id_0 = readl(&id_base->die_id_0);
110                 enetaddr[0] = 0x02; /* locally administered */
111                 enetaddr[1] = readl(&id_base->die_id_1) & 0xff;
112                 enetaddr[2] = (die_id_0 & 0xff000000) >> 24;
113                 enetaddr[3] = (die_id_0 & 0x00ff0000) >> 16;
114                 enetaddr[4] = (die_id_0 & 0x0000ff00) >> 8;
115                 enetaddr[5] = (die_id_0 & 0x000000ff);
116                 eth_setenv_enetaddr("ethaddr", enetaddr);
117         }
118 #endif
120         dieid_num_r();
122         return 0;
125 /*
126  * Routine: set_muxconf_regs
127  * Description: Setting up the configuration Mux registers specific to the
128  *              hardware. Many pins need to be moved from protect to primary
129  *              mode.
130  */
131 void set_muxconf_regs(void)
133         MUX_DEVKIT8000();
136 #if defined(CONFIG_GENERIC_MMC) && !defined(CONFIG_SPL_BUILD)
137 int board_mmc_init(bd_t *bis)
139         return omap_mmc_init(0, 0, 0, -1, -1);
141 #endif
143 #if defined(CONFIG_DRIVER_DM9000) & !defined(CONFIG_SPL_BUILD)
144 /*
145  * Routine: board_eth_init
146  * Description: Setting up the Ethernet hardware.
147  */
148 int board_eth_init(bd_t *bis)
150         return dm9000_initialize(bis);
152 #endif
154 #ifdef CONFIG_SPL_OS_BOOT
155 /*
156  * Do board specific preperation before SPL
157  * Linux boot
158  */
159 void spl_board_prepare_for_linux(void)
161         gpmc_dm9000_config();
164 /*
165  * devkit8000 specific implementation of spl_start_uboot()
166  *
167  * RETURN
168  * 0 if the button is not pressed
169  * 1 if the button is pressed
170  */
171 int spl_start_uboot(void)
173         int val = 0;
174         if (!gpio_request(SPL_OS_BOOT_KEY, "U-Boot key")) {
175                 gpio_direction_input(SPL_OS_BOOT_KEY);
176                 val = gpio_get_value(SPL_OS_BOOT_KEY);
177                 gpio_free(SPL_OS_BOOT_KEY);
178         }
179         return !val;
181 #endif
183 /*
184  * Routine: get_board_mem_timings
185  * Description: If we use SPL then there is no x-loader nor config header
186  * so we have to setup the DDR timings ourself on the first bank.  This
187  * provides the timing values back to the function that configures
188  * the memory.  We have either one or two banks of 128MB DDR.
189  */
190 void get_board_mem_timings(struct board_sdrc_timings *timings)
192         /* General SDRC config */
193         timings->mcfg = MICRON_V_MCFG_165(128 << 20);
194         timings->rfr_ctrl = SDP_3430_SDRC_RFR_CTRL_165MHz;
196         /* AC timings */
197         timings->ctrla = MICRON_V_ACTIMA_165;
198         timings->ctrlb = MICRON_V_ACTIMB_165;
200         timings->mr = MICRON_V_MR_165;