1 /*
2 * Copyright (c) 2011 The Chromium OS Authors.
3 * (C) Copyright 2002-2006
4 * Wolfgang Denk, DENX Software Engineering, wd@denx.de.
5 *
6 * (C) Copyright 2002
7 * Sysgo Real-Time Solutions, GmbH <www.elinos.com>
8 * Marius Groeger <mgroeger@sysgo.de>
9 *
10 * See file CREDITS for list of people who contributed to this
11 * project.
12 *
13 * This program is free software; you can redistribute it and/or
14 * modify it under the terms of the GNU General Public License as
15 * published by the Free Software Foundation; either version 2 of
16 * the License, or (at your option) any later version.
17 *
18 * This program is distributed in the hope that it will be useful,
19 * but WITHOUT ANY WARRANTY; without even the implied warranty of
20 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
21 * GNU General Public License for more details.
22 *
23 * You should have received a copy of the GNU General Public License
24 * along with this program; if not, write to the Free Software
25 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
26 * MA 02111-1307 USA
27 */
29 #include <common.h>
30 #include <linux/compiler.h>
31 #include <version.h>
32 #include <environment.h>
33 #include <fdtdec.h>
34 #if defined(CONFIG_CMD_IDE)
35 #include <ide.h>
36 #endif
37 #include <i2c.h>
38 #include <initcall.h>
39 #include <logbuff.h>
41 /* TODO: Can we move these into arch/ headers? */
42 #ifdef CONFIG_8xx
43 #include <mpc8xx.h>
44 #endif
45 #ifdef CONFIG_5xx
46 #include <mpc5xx.h>
47 #endif
48 #ifdef CONFIG_MPC5xxx
49 #include <mpc5xxx.h>
50 #endif
52 #include <post.h>
53 #include <spi.h>
54 #include <watchdog.h>
55 #include <asm/io.h>
56 #ifdef CONFIG_MP
57 #include <asm/mp.h>
58 #endif
59 #include <asm/sections.h>
60 #ifdef CONFIG_X86
61 #include <asm/init_helpers.h>
62 #include <asm/relocate.h>
63 #endif
64 #include <linux/compiler.h>
66 /*
67 * Pointer to initial global data area
68 *
69 * Here we initialize it if needed.
70 */
71 #ifdef XTRN_DECLARE_GLOBAL_DATA_PTR
72 #undef XTRN_DECLARE_GLOBAL_DATA_PTR
73 #define XTRN_DECLARE_GLOBAL_DATA_PTR /* empty = allocate here */
74 DECLARE_GLOBAL_DATA_PTR = (gd_t *) (CONFIG_SYS_INIT_GD_ADDR);
75 #else
76 DECLARE_GLOBAL_DATA_PTR;
77 #endif
79 /*
80 * sjg: IMO this code should be
81 * refactored to a single function, something like:
82 *
83 * void led_set_state(enum led_colour_t colour, int on);
84 */
85 /************************************************************************
86 * Coloured LED functionality
87 ************************************************************************
88 * May be supplied by boards if desired
89 */
90 inline void __coloured_LED_init(void) {}
91 void coloured_LED_init(void)
92 __attribute__((weak, alias("__coloured_LED_init")));
93 inline void __red_led_on(void) {}
94 void red_led_on(void) __attribute__((weak, alias("__red_led_on")));
95 inline void __red_led_off(void) {}
96 void red_led_off(void) __attribute__((weak, alias("__red_led_off")));
97 inline void __green_led_on(void) {}
98 void green_led_on(void) __attribute__((weak, alias("__green_led_on")));
99 inline void __green_led_off(void) {}
100 void green_led_off(void) __attribute__((weak, alias("__green_led_off")));
101 inline void __yellow_led_on(void) {}
102 void yellow_led_on(void) __attribute__((weak, alias("__yellow_led_on")));
103 inline void __yellow_led_off(void) {}
104 void yellow_led_off(void) __attribute__((weak, alias("__yellow_led_off")));
105 inline void __blue_led_on(void) {}
106 void blue_led_on(void) __attribute__((weak, alias("__blue_led_on")));
107 inline void __blue_led_off(void) {}
108 void blue_led_off(void) __attribute__((weak, alias("__blue_led_off")));
110 /*
111 * Why is gd allocated a register? Prior to reloc it might be better to
112 * just pass it around to each function in this file?
113 *
114 * After reloc one could argue that it is hardly used and doesn't need
115 * to be in a register. Or if it is it should perhaps hold pointers to all
116 * global data for all modules, so that post-reloc we can avoid the massive
117 * literal pool we get on ARM. Or perhaps just encourage each module to use
118 * a structure...
119 */
121 /*
122 * Could the CONFIG_SPL_BUILD infection become a flag in gd?
123 */
125 #if defined(CONFIG_WATCHDOG)
126 static int init_func_watchdog_init(void)
127 {
128 puts(" Watchdog enabled\n");
129 WATCHDOG_RESET();
131 return 0;
132 }
134 int init_func_watchdog_reset(void)
135 {
136 WATCHDOG_RESET();
138 return 0;
139 }
140 #endif /* CONFIG_WATCHDOG */
142 void __board_add_ram_info(int use_default)
143 {
144 /* please define platform specific board_add_ram_info() */
145 }
147 void board_add_ram_info(int)
148 __attribute__ ((weak, alias("__board_add_ram_info")));
150 static int init_baud_rate(void)
151 {
152 gd->baudrate = getenv_ulong("baudrate", 10, CONFIG_BAUDRATE);
153 return 0;
154 }
156 static int display_text_info(void)
157 {
158 ulong bss_start, bss_end;
160 #ifdef CONFIG_SYS_SYM_OFFSETS
161 bss_start = _bss_start_ofs + _TEXT_BASE;
162 bss_end = _bss_end_ofs + _TEXT_BASE;
163 #else
164 bss_start = (ulong)&__bss_start;
165 bss_end = (ulong)&__bss_end;
166 #endif
167 debug("U-Boot code: %08X -> %08lX BSS: -> %08lX\n",
168 CONFIG_SYS_TEXT_BASE, bss_start, bss_end);
170 #ifdef CONFIG_MODEM_SUPPORT
171 debug("Modem Support enabled\n");
172 #endif
173 #ifdef CONFIG_USE_IRQ
174 debug("IRQ Stack: %08lx\n", IRQ_STACK_START);
175 debug("FIQ Stack: %08lx\n", FIQ_STACK_START);
176 #endif
178 return 0;
179 }
181 static int announce_dram_init(void)
182 {
183 puts("DRAM: ");
184 return 0;
185 }
187 #ifdef CONFIG_PPC
188 static int init_func_ram(void)
189 {
190 #ifdef CONFIG_BOARD_TYPES
191 int board_type = gd->board_type;
192 #else
193 int board_type = 0; /* use dummy arg */
194 #endif
196 gd->ram_size = initdram(board_type);
198 if (gd->ram_size > 0)
199 return 0;
201 puts("*** failed ***\n");
202 return 1;
203 }
204 #endif
206 static int show_dram_config(void)
207 {
208 ulong size;
210 #ifdef CONFIG_NR_DRAM_BANKS
211 int i;
213 debug("\nRAM Configuration:\n");
214 for (i = size = 0; i < CONFIG_NR_DRAM_BANKS; i++) {
215 size += gd->bd->bi_dram[i].size;
216 debug("Bank #%d: %08lx ", i, gd->bd->bi_dram[i].start);
217 #ifdef DEBUG
218 print_size(gd->bd->bi_dram[i].size, "\n");
219 #endif
220 }
221 debug("\nDRAM: ");
222 #else
223 size = gd->ram_size;
224 #endif
226 print_size(size, "");
227 board_add_ram_info(0);
228 putc('\n');
230 return 0;
231 }
233 ulong get_effective_memsize(void)
234 {
235 #ifndef CONFIG_VERY_BIG_RAM
236 return gd->ram_size;
237 #else
238 /* limit stack to what we can reasonable map */
239 return ((gd->ram_size > CONFIG_MAX_MEM_MAPPED) ?
240 CONFIG_MAX_MEM_MAPPED : gd->ram_size);
241 #endif
242 }
244 void __dram_init_banksize(void)
245 {
246 #if defined(CONFIG_NR_DRAM_BANKS) && defined(CONFIG_SYS_SDRAM_BASE)
247 gd->bd->bi_dram[0].start = CONFIG_SYS_SDRAM_BASE;
248 gd->bd->bi_dram[0].size = get_effective_memsize();
249 #endif
250 }
252 void dram_init_banksize(void)
253 __attribute__((weak, alias("__dram_init_banksize")));
255 #if defined(CONFIG_HARD_I2C) || defined(CONFIG_SOFT_I2C)
256 static int init_func_i2c(void)
257 {
258 puts("I2C: ");
259 i2c_init(CONFIG_SYS_I2C_SPEED, CONFIG_SYS_I2C_SLAVE);
260 puts("ready\n");
261 return 0;
262 }
263 #endif
265 #if defined(CONFIG_HARD_SPI)
266 static int init_func_spi(void)
267 {
268 puts("SPI: ");
269 spi_init();
270 puts("ready\n");
271 return 0;
272 }
273 #endif
275 __maybe_unused
276 static int zero_global_data(void)
277 {
278 memset((void *)gd, '\0', sizeof(gd_t));
280 return 0;
281 }
283 static int setup_mon_len(void)
284 {
285 #ifdef CONFIG_SYS_SYM_OFFSETS
286 gd->mon_len = _bss_end_ofs;
287 #else
288 /* TODO: use (ulong)&__bss_end - (ulong)&__text_start; ? */
289 gd->mon_len = (ulong)&__bss_end - CONFIG_SYS_MONITOR_BASE;
290 #endif
291 return 0;
292 }
294 __weak int arch_cpu_init(void)
295 {
296 return 0;
297 }
299 static int setup_fdt(void)
300 {
301 #ifdef CONFIG_OF_EMBED
302 /* Get a pointer to the FDT */
303 gd->fdt_blob = _binary_dt_dtb_start;
304 #elif defined CONFIG_OF_SEPARATE
305 /* FDT is at end of image */
306 # ifdef CONFIG_SYS_SYM_OFFSETS
307 gd->fdt_blob = (void *)(_end_ofs + CONFIG_SYS_TEXT_BASE);
308 # else
309 gd->fdt_blob = (ulong *)&_end;
310 # endif
311 #endif
312 /* Allow the early environment to override the fdt address */
313 gd->fdt_blob = (void *)getenv_ulong("fdtcontroladdr", 16,
314 (uintptr_t)gd->fdt_blob);
315 return 0;
316 }
318 /* Get the top of usable RAM */
319 __weak ulong board_get_usable_ram_top(ulong total_size)
320 {
321 return gd->ram_top;
322 }
324 static int setup_dest_addr(void)
325 {
326 debug("Monitor len: %08lX\n", gd->mon_len);
327 /*
328 * Ram is setup, size stored in gd !!
329 */
330 debug("Ram size: %08lX\n", (ulong)gd->ram_size);
331 #if defined(CONFIG_SYS_MEM_TOP_HIDE)
332 /*
333 * Subtract specified amount of memory to hide so that it won't
334 * get "touched" at all by U-Boot. By fixing up gd->ram_size
335 * the Linux kernel should now get passed the now "corrected"
336 * memory size and won't touch it either. This should work
337 * for arch/ppc and arch/powerpc. Only Linux board ports in
338 * arch/powerpc with bootwrapper support, that recalculate the
339 * memory size from the SDRAM controller setup will have to
340 * get fixed.
341 */
342 gd->ram_size -= CONFIG_SYS_MEM_TOP_HIDE;
343 #endif
344 #ifdef CONFIG_SYS_SDRAM_BASE
345 gd->ram_top = CONFIG_SYS_SDRAM_BASE;
346 #endif
347 gd->ram_top += get_effective_memsize();
348 gd->ram_top = board_get_usable_ram_top(gd->mon_len);
349 gd->dest_addr = gd->ram_top;
350 debug("Ram top: %08lX\n", (ulong)gd->ram_top);
351 #if defined(CONFIG_MP) && (defined(CONFIG_MPC86xx) || defined(CONFIG_E500))
352 /*
353 * We need to make sure the location we intend to put secondary core
354 * boot code is reserved and not used by any part of u-boot
355 */
356 if (gd->dest_addr > determine_mp_bootpg(NULL)) {
357 gd->dest_addr = determine_mp_bootpg(NULL);
358 debug("Reserving MP boot page to %08lx\n", gd->dest_addr);
359 }
360 #endif
361 gd->dest_addr_sp = gd->dest_addr;
362 return 0;
363 }
365 #if defined(CONFIG_LOGBUFFER) && !defined(CONFIG_ALT_LB_ADDR)
366 static int reserve_logbuffer(void)
367 {
368 /* reserve kernel log buffer */
369 gd->dest_addr -= LOGBUFF_RESERVE;
370 debug("Reserving %dk for kernel logbuffer at %08lx\n", LOGBUFF_LEN,
371 gd->dest_addr);
372 return 0;
373 }
374 #endif
376 #ifdef CONFIG_PRAM
377 /* reserve protected RAM */
378 static int reserve_pram(void)
379 {
380 ulong reg;
382 reg = getenv_ulong("pram", 10, CONFIG_PRAM);
383 gd->dest_addr -= (reg << 10); /* size is in kB */
384 debug("Reserving %ldk for protected RAM at %08lx\n", reg,
385 gd->dest_addr);
386 return 0;
387 }
388 #endif /* CONFIG_PRAM */
390 /* Round memory pointer down to next 4 kB limit */
391 static int reserve_round_4k(void)
392 {
393 gd->dest_addr &= ~(4096 - 1);
394 return 0;
395 }
397 #if !(defined(CONFIG_SYS_ICACHE_OFF) && defined(CONFIG_SYS_DCACHE_OFF)) && \
398 defined(CONFIG_ARM)
399 static int reserve_mmu(void)
400 {
401 /* reserve TLB table */
402 gd->arch.tlb_size = 4096 * 4;
403 gd->dest_addr -= gd->arch.tlb_size;
405 /* round down to next 64 kB limit */
406 gd->dest_addr &= ~(0x10000 - 1);
408 gd->arch.tlb_addr = gd->dest_addr;
409 debug("TLB table from %08lx to %08lx\n", gd->arch.tlb_addr,
410 gd->arch.tlb_addr + gd->arch.tlb_size);
411 return 0;
412 }
413 #endif
415 #ifdef CONFIG_LCD
416 static int reserve_lcd(void)
417 {
418 #ifdef CONFIG_FB_ADDR
419 gd->fb_base = CONFIG_FB_ADDR;
420 #else
421 /* reserve memory for LCD display (always full pages) */
422 gd->dest_addr = lcd_setmem(gd->dest_addr);
423 gd->fb_base = gd->dest_addr;
424 #endif /* CONFIG_FB_ADDR */
425 return 0;
426 }
427 #endif /* CONFIG_LCD */
429 #if defined(CONFIG_VIDEO) && (!defined(CONFIG_PPC) || defined(CONFIG_8xx)) \
430 && !defined(CONFIG_ARM) && !defined(CONFIG_X86)
431 static int reserve_video(void)
432 {
433 /* reserve memory for video display (always full pages) */
434 gd->dest_addr = video_setmem(gd->dest_addr);
435 gd->fb_base = gd->dest_addr;
437 return 0;
438 }
439 #endif
441 static int reserve_uboot(void)
442 {
443 /*
444 * reserve memory for U-Boot code, data & bss
445 * round down to next 4 kB limit
446 */
447 gd->dest_addr -= gd->mon_len;
448 gd->dest_addr &= ~(4096 - 1);
449 #ifdef CONFIG_E500
450 /* round down to next 64 kB limit so that IVPR stays aligned */
451 gd->dest_addr &= ~(65536 - 1);
452 #endif
454 debug("Reserving %ldk for U-Boot at: %08lx\n", gd->mon_len >> 10,
455 gd->dest_addr);
456 return 0;
457 }
459 #ifndef CONFIG_SPL_BUILD
460 /* reserve memory for malloc() area */
461 static int reserve_malloc(void)
462 {
463 gd->dest_addr_sp = gd->dest_addr - TOTAL_MALLOC_LEN;
464 debug("Reserving %dk for malloc() at: %08lx\n",
465 TOTAL_MALLOC_LEN >> 10, gd->dest_addr_sp);
466 return 0;
467 }
469 /* (permanently) allocate a Board Info struct */
470 static int reserve_board(void)
471 {
472 gd->dest_addr_sp -= sizeof(bd_t);
473 gd->bd = (bd_t *)gd->dest_addr_sp;
474 memset(gd->bd, '\0', sizeof(bd_t));
475 debug("Reserving %zu Bytes for Board Info at: %08lx\n",
476 sizeof(bd_t), gd->dest_addr_sp);
477 return 0;
478 }
479 #endif
481 static int setup_machine(void)
482 {
483 #ifdef CONFIG_MACH_TYPE
484 gd->bd->bi_arch_number = CONFIG_MACH_TYPE; /* board id for Linux */
485 #endif
486 return 0;
487 }
489 static int reserve_global_data(void)
490 {
491 gd->dest_addr_sp -= sizeof(gd_t);
492 gd->new_gd = (gd_t *)gd->dest_addr_sp;
493 debug("Reserving %zu Bytes for Global Data at: %08lx\n",
494 sizeof(gd_t), gd->dest_addr_sp);
495 return 0;
496 }
498 static int reserve_fdt(void)
499 {
500 /*
501 * If the device tree is sitting immediate above our image then we
502 * must relocate it. If it is embedded in the data section, then it
503 * will be relocated with other data.
504 */
505 if (gd->fdt_blob) {
506 gd->fdt_size = ALIGN(fdt_totalsize(gd->fdt_blob) + 0x1000, 32);
508 gd->dest_addr_sp -= gd->fdt_size;
509 gd->new_fdt = (void *)gd->dest_addr_sp;
510 debug("Reserving %lu Bytes for FDT at: %p\n",
511 gd->fdt_size, gd->new_fdt);
512 }
514 return 0;
515 }
517 static int reserve_stacks(void)
518 {
519 #ifdef CONFIG_SPL_BUILD
520 # ifdef CONFIG_ARM
521 gd->dest_addr_sp -= 128; /* leave 32 words for abort-stack */
522 gd->irq_sp = gd->dest_addr_sp;
523 # endif
524 #else
525 # ifdef CONFIG_PPC
526 ulong *s;
527 # endif
529 /* setup stack pointer for exceptions */
530 gd->dest_addr_sp -= 16;
531 gd->dest_addr_sp &= ~0xf;
532 gd->irq_sp = gd->dest_addr_sp;
534 /*
535 * Handle architecture-specific things here
536 * TODO(sjg@chromium.org): Perhaps create arch_reserve_stack()
537 * to handle this and put in arch/xxx/lib/stack.c
538 */
539 # ifdef CONFIG_ARM
540 # ifdef CONFIG_USE_IRQ
541 gd->dest_addr_sp -= (CONFIG_STACKSIZE_IRQ + CONFIG_STACKSIZE_FIQ);
542 debug("Reserving %zu Bytes for IRQ stack at: %08lx\n",
543 CONFIG_STACKSIZE_IRQ + CONFIG_STACKSIZE_FIQ, gd->dest_addr_sp);
545 /* 8-byte alignment for ARM ABI compliance */
546 gd->dest_addr_sp &= ~0x07;
547 # endif
548 /* leave 3 words for abort-stack, plus 1 for alignment */
549 gd->dest_addr_sp -= 16;
550 # elif defined(CONFIG_PPC)
551 /* Clear initial stack frame */
552 s = (ulong *) gd->dest_addr_sp;
553 *s = 0; /* Terminate back chain */
554 *++s = 0; /* NULL return address */
555 # endif /* Architecture specific code */
557 return 0;
558 #endif
559 }
561 static int display_new_sp(void)
562 {
563 debug("New Stack Pointer is: %08lx\n", gd->dest_addr_sp);
565 return 0;
566 }
568 #ifdef CONFIG_PPC
569 static int setup_board_part1(void)
570 {
571 bd_t *bd = gd->bd;
573 /*
574 * Save local variables to board info struct
575 */
577 bd->bi_memstart = CONFIG_SYS_SDRAM_BASE; /* start of memory */
578 bd->bi_memsize = gd->ram_size; /* size in bytes */
580 #ifdef CONFIG_SYS_SRAM_BASE
581 bd->bi_sramstart = CONFIG_SYS_SRAM_BASE; /* start of SRAM */
582 bd->bi_sramsize = CONFIG_SYS_SRAM_SIZE; /* size of SRAM */
583 #endif
585 #if defined(CONFIG_8xx) || defined(CONFIG_8260) || defined(CONFIG_5xx) || \
586 defined(CONFIG_E500) || defined(CONFIG_MPC86xx)
587 bd->bi_immr_base = CONFIG_SYS_IMMR; /* base of IMMR register */
588 #endif
589 #if defined(CONFIG_MPC5xxx)
590 bd->bi_mbar_base = CONFIG_SYS_MBAR; /* base of internal registers */
591 #endif
592 #if defined(CONFIG_MPC83xx)
593 bd->bi_immrbar = CONFIG_SYS_IMMR;
594 #endif
595 #if defined(CONFIG_MPC8220)
596 bd->bi_mbar_base = CONFIG_SYS_MBAR; /* base of internal registers */
597 bd->bi_inpfreq = gd->arch.inp_clk;
598 bd->bi_pcifreq = gd->pci_clk;
599 bd->bi_vcofreq = gd->arch.vco_clk;
600 bd->bi_pevfreq = gd->arch.pev_clk;
601 bd->bi_flbfreq = gd->arch.flb_clk;
603 /* store bootparam to sram (backward compatible), here? */
604 {
605 u32 *sram = (u32 *) CONFIG_SYS_SRAM_BASE;
607 *sram++ = gd->ram_size;
608 *sram++ = gd->bus_clk;
609 *sram++ = gd->arch.inp_clk;
610 *sram++ = gd->cpu_clk;
611 *sram++ = gd->arch.vco_clk;
612 *sram++ = gd->arch.flb_clk;
613 *sram++ = 0xb8c3ba11; /* boot signature */
614 }
615 #endif
617 return 0;
618 }
620 static int setup_board_part2(void)
621 {
622 bd_t *bd = gd->bd;
624 bd->bi_intfreq = gd->cpu_clk; /* Internal Freq, in Hz */
625 bd->bi_busfreq = gd->bus_clk; /* Bus Freq, in Hz */
626 #if defined(CONFIG_CPM2)
627 bd->bi_cpmfreq = gd->arch.cpm_clk;
628 bd->bi_brgfreq = gd->arch.brg_clk;
629 bd->bi_sccfreq = gd->arch.scc_clk;
630 bd->bi_vco = gd->arch.vco_out;
631 #endif /* CONFIG_CPM2 */
632 #if defined(CONFIG_MPC512X)
633 bd->bi_ipsfreq = gd->arch.ips_clk;
634 #endif /* CONFIG_MPC512X */
635 #if defined(CONFIG_MPC5xxx)
636 bd->bi_ipbfreq = gd->arch.ipb_clk;
637 bd->bi_pcifreq = gd->pci_clk;
638 #endif /* CONFIG_MPC5xxx */
640 return 0;
641 }
642 #endif
644 #ifdef CONFIG_SYS_EXTBDINFO
645 static int setup_board_extra(void)
646 {
647 bd_t *bd = gd->bd;
649 strncpy((char *) bd->bi_s_version, "1.2", sizeof(bd->bi_s_version));
650 strncpy((char *) bd->bi_r_version, U_BOOT_VERSION,
651 sizeof(bd->bi_r_version));
653 bd->bi_procfreq = gd->cpu_clk; /* Processor Speed, In Hz */
654 bd->bi_plb_busfreq = gd->bus_clk;
655 #if defined(CONFIG_405GP) || defined(CONFIG_405EP) || \
656 defined(CONFIG_440EP) || defined(CONFIG_440GR) || \
657 defined(CONFIG_440EPX) || defined(CONFIG_440GRX)
658 bd->bi_pci_busfreq = get_PCI_freq();
659 bd->bi_opbfreq = get_OPB_freq();
660 #elif defined(CONFIG_XILINX_405)
661 bd->bi_pci_busfreq = get_PCI_freq();
662 #endif
664 return 0;
665 }
666 #endif
668 #ifdef CONFIG_POST
669 static int init_post(void)
670 {
671 post_bootmode_init();
672 post_run(NULL, POST_ROM | post_bootmode_get(0));
674 return 0;
675 }
676 #endif
678 static int setup_baud_rate(void)
679 {
680 /* Ick, can we get rid of this line? */
681 gd->bd->bi_baudrate = gd->baudrate;
683 return 0;
684 }
686 static int setup_dram_config(void)
687 {
688 /* Ram is board specific, so move it to board code ... */
689 dram_init_banksize();
691 return 0;
692 }
694 static int reloc_fdt(void)
695 {
696 if (gd->new_fdt) {
697 memcpy(gd->new_fdt, gd->fdt_blob, gd->fdt_size);
698 gd->fdt_blob = gd->new_fdt;
699 }
701 return 0;
702 }
704 static int setup_reloc(void)
705 {
706 gd->relocaddr = gd->dest_addr;
707 gd->start_addr_sp = gd->dest_addr_sp;
708 gd->reloc_off = gd->dest_addr - CONFIG_SYS_TEXT_BASE;
709 memcpy(gd->new_gd, (char *)gd, sizeof(gd_t));
711 debug("Relocation Offset is: %08lx\n", gd->reloc_off);
712 debug("Relocating to %08lx, new gd at %p, sp at %08lx\n",
713 gd->dest_addr, gd->new_gd, gd->dest_addr_sp);
715 return 0;
716 }
718 /* ARM calls relocate_code from its crt0.S */
719 #if !defined(CONFIG_ARM)
721 static int jump_to_copy(void)
722 {
723 /*
724 * x86 is special, but in a nice way. It uses a trampoline which
725 * enables the dcache if possible.
726 *
727 * For now, other archs use relocate_code(), which is implemented
728 * similarly for all archs. When we do generic relocation, hopefully
729 * we can make all archs enable the dcache prior to relocation.
730 */
731 #ifdef CONFIG_X86
732 /*
733 * SDRAM and console are now initialised. The final stack can now
734 * be setup in SDRAM. Code execution will continue in Flash, but
735 * with the stack in SDRAM and Global Data in temporary memory
736 * (CPU cache)
737 */
738 board_init_f_r_trampoline(gd->start_addr_sp);
739 #else
740 relocate_code(gd->dest_addr_sp, gd->new_gd, gd->dest_addr);
741 #endif
743 return 0;
744 }
745 #endif
747 /* Record the board_init_f() bootstage (after arch_cpu_init()) */
748 static int mark_bootstage(void)
749 {
750 bootstage_mark_name(BOOTSTAGE_ID_START_UBOOT_F, "board_init_f");
752 return 0;
753 }
755 static init_fnc_t init_sequence_f[] = {
756 #if !defined(CONFIG_CPM2) && !defined(CONFIG_MPC512X) && \
757 !defined(CONFIG_MPC83xx) && !defined(CONFIG_MPC85xx) && \
758 !defined(CONFIG_MPC86xx)
759 zero_global_data,
760 #endif
761 setup_fdt,
762 setup_mon_len,
763 #if defined(CONFIG_MPC85xx) || defined(CONFIG_MPC86xx)
764 /* TODO: can this go into arch_cpu_init()? */
765 probecpu,
766 #endif
767 arch_cpu_init, /* basic arch cpu dependent setup */
768 #ifdef CONFIG_X86
769 cpu_init_f, /* TODO(sjg@chromium.org): remove */
770 # ifdef CONFIG_OF_CONTROL
771 find_fdt, /* TODO(sjg@chromium.org): remove */
772 # endif
773 #endif
774 mark_bootstage,
775 #ifdef CONFIG_OF_CONTROL
776 fdtdec_check_fdt,
777 #endif
778 #if defined(CONFIG_BOARD_EARLY_INIT_F)
779 board_early_init_f,
780 #endif
781 /* TODO: can any of this go into arch_cpu_init()? */
782 #if defined(CONFIG_PPC) && !defined(CONFIG_8xx_CPUCLK_DEFAULT)
783 get_clocks, /* get CPU and bus clocks (etc.) */
784 #if defined(CONFIG_TQM8xxL) && !defined(CONFIG_TQM866M) \
785 && !defined(CONFIG_TQM885D)
786 adjust_sdram_tbs_8xx,
787 #endif
788 /* TODO: can we rename this to timer_init()? */
789 init_timebase,
790 #endif
791 #if defined(CONFIG_BOARD_EARLY_INIT_F)
792 board_early_init_f,
793 #endif
794 #ifdef CONFIG_ARM
795 timer_init, /* initialize timer */
796 #endif
797 #ifdef CONFIG_BOARD_POSTCLK_INIT
798 board_postclk_init,
799 #endif
800 #ifdef CONFIG_FSL_ESDHC
801 get_clocks,
802 #endif
803 #ifdef CONFIG_SYS_ALLOC_DPRAM
804 #if !defined(CONFIG_CPM2)
805 dpram_init,
806 #endif
807 #endif
808 #if defined(CONFIG_BOARD_POSTCLK_INIT)
809 board_postclk_init,
810 #endif
811 env_init, /* initialize environment */
812 #if defined(CONFIG_8xx_CPUCLK_DEFAULT)
813 /* get CPU and bus clocks according to the environment variable */
814 get_clocks_866,
815 /* adjust sdram refresh rate according to the new clock */
816 sdram_adjust_866,
817 init_timebase,
818 #endif
819 init_baud_rate, /* initialze baudrate settings */
820 serial_init, /* serial communications setup */
821 console_init_f, /* stage 1 init of console */
822 #if defined(CONFIG_X86) && defined(CONFIG_OF_CONTROL)
823 prepare_fdt, /* TODO(sjg@chromium.org): remove */
824 #endif
825 display_options, /* say that we are here */
826 display_text_info, /* show debugging info if required */
827 #if defined(CONFIG_8260)
828 prt_8260_rsr,
829 prt_8260_clks,
830 #endif /* CONFIG_8260 */
831 #if defined(CONFIG_MPC83xx)
832 prt_83xx_rsr,
833 #endif
834 #ifdef CONFIG_PPC
835 checkcpu,
836 #endif
837 #if defined(CONFIG_DISPLAY_CPUINFO)
838 print_cpuinfo, /* display cpu info (and speed) */
839 #endif
840 #if defined(CONFIG_MPC5xxx)
841 prt_mpc5xxx_clks,
842 #endif /* CONFIG_MPC5xxx */
843 #if defined(CONFIG_MPC8220)
844 prt_mpc8220_clks,
845 #endif
846 #if defined(CONFIG_DISPLAY_BOARDINFO)
847 checkboard, /* display board info */
848 #endif
849 INIT_FUNC_WATCHDOG_INIT
850 #if defined(CONFIG_MISC_INIT_F)
851 misc_init_f,
852 #endif
853 INIT_FUNC_WATCHDOG_RESET
854 #if defined(CONFIG_HARD_I2C) || defined(CONFIG_SOFT_I2C)
855 init_func_i2c,
856 #endif
857 #if defined(CONFIG_HARD_SPI)
858 init_func_spi,
859 #endif
860 #ifdef CONFIG_X86
861 dram_init_f, /* configure available RAM banks */
862 /* x86 would prefer that this happens after relocation */
863 dram_init,
864 #endif
865 announce_dram_init,
866 /* TODO: unify all these dram functions? */
867 #ifdef CONFIG_ARM
868 dram_init, /* configure available RAM banks */
869 #endif
870 #ifdef CONFIG_PPC
871 init_func_ram,
872 #endif
873 #ifdef CONFIG_POST
874 post_init_f,
875 #endif
876 INIT_FUNC_WATCHDOG_RESET
877 #if defined(CONFIG_SYS_DRAM_TEST)
878 testdram,
879 #endif /* CONFIG_SYS_DRAM_TEST */
880 INIT_FUNC_WATCHDOG_RESET
882 #ifdef CONFIG_POST
883 init_post,
884 #endif
885 INIT_FUNC_WATCHDOG_RESET
886 /*
887 * Now that we have DRAM mapped and working, we can
888 * relocate the code and continue running from DRAM.
889 *
890 * Reserve memory at end of RAM for (top down in that order):
891 * - area that won't get touched by U-Boot and Linux (optional)
892 * - kernel log buffer
893 * - protected RAM
894 * - LCD framebuffer
895 * - monitor code
896 * - board info struct
897 */
898 setup_dest_addr,
899 #if defined(CONFIG_LOGBUFFER) && !defined(CONFIG_ALT_LB_ADDR)
900 reserve_logbuffer,
901 #endif
902 #ifdef CONFIG_PRAM
903 reserve_pram,
904 #endif
905 reserve_round_4k,
906 #if !(defined(CONFIG_SYS_ICACHE_OFF) && defined(CONFIG_SYS_DCACHE_OFF)) && \
907 defined(CONFIG_ARM)
908 reserve_mmu,
909 #endif
910 #ifdef CONFIG_LCD
911 reserve_lcd,
912 #endif
913 /* TODO: Why the dependency on CONFIG_8xx? */
914 #if defined(CONFIG_VIDEO) && (!defined(CONFIG_PPC) || defined(CONFIG_8xx)) \
915 && !defined(CONFIG_ARM) && !defined(CONFIG_X86)
916 reserve_video,
917 #endif
918 reserve_uboot,
919 #ifndef CONFIG_SPL_BUILD
920 reserve_malloc,
921 reserve_board,
922 #endif
923 setup_machine,
924 reserve_global_data,
925 reserve_fdt,
926 reserve_stacks,
927 setup_dram_config,
928 show_dram_config,
929 #ifdef CONFIG_PPC
930 setup_board_part1,
931 INIT_FUNC_WATCHDOG_RESET
932 setup_board_part2,
933 #endif
934 setup_baud_rate,
935 display_new_sp,
936 #ifdef CONFIG_SYS_EXTBDINFO
937 setup_board_extra,
938 #endif
939 INIT_FUNC_WATCHDOG_RESET
940 reloc_fdt,
941 setup_reloc,
942 #ifndef CONFIG_ARM
943 jump_to_copy,
944 #endif
945 NULL,
946 };
948 void board_init_f(ulong boot_flags)
949 {
950 #ifndef CONFIG_X86
951 gd_t data;
953 gd = &data;
954 #endif
956 gd->flags = boot_flags;
958 if (initcall_run_list(init_sequence_f))
959 hang();
961 #ifndef CONFIG_ARM
962 /* NOTREACHED - jump_to_copy() does not return */
963 hang();
964 #endif
965 }
967 #ifdef CONFIG_X86
968 /*
969 * For now this code is only used on x86.
970 *
971 * init_sequence_f_r is the list of init functions which are run when
972 * U-Boot is executing from Flash with a semi-limited 'C' environment.
973 * The following limitations must be considered when implementing an
974 * '_f_r' function:
975 * - 'static' variables are read-only
976 * - Global Data (gd->xxx) is read/write
977 *
978 * The '_f_r' sequence must, as a minimum, copy U-Boot to RAM (if
979 * supported). It _should_, if possible, copy global data to RAM and
980 * initialise the CPU caches (to speed up the relocation process)
981 *
982 * NOTE: At present only x86 uses this route, but it is intended that
983 * all archs will move to this when generic relocation is implemented.
984 */
985 static init_fnc_t init_sequence_f_r[] = {
986 init_cache_f_r,
987 copy_uboot_to_ram,
988 clear_bss,
989 do_elf_reloc_fixups,
991 NULL,
992 };
994 void board_init_f_r(void)
995 {
996 if (initcall_run_list(init_sequence_f_r))
997 hang();
999 /*
1000 * U-Boot has been copied into SDRAM, the BSS has been cleared etc.
1001 * Transfer execution from Flash to RAM by calculating the address
1002 * of the in-RAM copy of board_init_r() and calling it
1003 */
1004 (board_init_r + gd->reloc_off)(gd, gd->relocaddr);
1006 /* NOTREACHED - board_init_r() does not return */
1007 hang();
1008 }
1009 #endif /* CONFIG_X86 */
1011 void hang(void)
1012 {
1013 puts("### ERROR ### Please RESET the board ###\n");
1014 for (;;);
1015 }