1 /*
2 * (C) Copyright 2007
3 * Gerald Van Baren, Custom IDEAS, vanbaren@cideas.com
4 * Based on code written by:
5 * Pantelis Antoniou <pantelis.antoniou@gmail.com> and
6 * Matthew McClintock <msm@freescale.com>
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 #include <common.h>
28 #include <command.h>
29 #include <linux/ctype.h>
30 #include <linux/types.h>
31 #include <asm/global_data.h>
32 #include <fdt.h>
33 #include <libfdt.h>
34 #include <fdt_support.h>
36 #define MAX_LEVEL 32 /* how deeply nested we will go */
37 #define SCRATCHPAD 1024 /* bytes of scratchpad memory */
38 #ifndef CONFIG_CMD_FDT_MAX_DUMP
39 #define CONFIG_CMD_FDT_MAX_DUMP 64
40 #endif
42 /*
43 * Global data (for the gd->bd)
44 */
45 DECLARE_GLOBAL_DATA_PTR;
47 static int fdt_valid(void);
48 static int fdt_parse_prop(char *const*newval, int count, char *data, int *len);
49 static int fdt_print(const char *pathp, char *prop, int depth);
50 static int is_printable_string(const void *data, int len);
52 /*
53 * The working_fdt points to our working flattened device tree.
54 */
55 struct fdt_header *working_fdt;
57 void set_working_fdt_addr(void *addr)
58 {
59 char buf[17];
61 working_fdt = addr;
63 sprintf(buf, "%lx", (unsigned long)addr);
64 setenv("fdtaddr", buf);
65 }
67 /*
68 * Get a value from the fdt and format it to be set in the environment
69 */
70 static int fdt_value_setenv(const void *nodep, int len, const char *var)
71 {
72 if (is_printable_string(nodep, len))
73 setenv(var, (void *)nodep);
74 else if (len == 4) {
75 char buf[11];
77 sprintf(buf, "0x%08X", *(uint32_t *)nodep);
78 setenv(var, buf);
79 } else if (len%4 == 0 && len <= 20) {
80 /* Needed to print things like sha1 hashes. */
81 char buf[41];
82 int i;
84 for (i = 0; i < len; i += sizeof(unsigned int))
85 sprintf(buf + (i * 2), "%08x",
86 *(unsigned int *)(nodep + i));
87 setenv(var, buf);
88 } else {
89 printf("error: unprintable value\n");
90 return 1;
91 }
92 return 0;
93 }
95 /*
96 * Flattened Device Tree command, see the help for parameter definitions.
97 */
98 int do_fdt (cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[])
99 {
100 if (argc < 2)
101 return CMD_RET_USAGE;
103 /*
104 * Set the address of the fdt
105 */
106 if (argv[1][0] == 'a') {
107 unsigned long addr;
108 /*
109 * Set the address [and length] of the fdt.
110 */
111 if (argc == 2) {
112 if (!fdt_valid()) {
113 return 1;
114 }
115 printf("The address of the fdt is %p\n", working_fdt);
116 return 0;
117 }
119 addr = simple_strtoul(argv[2], NULL, 16);
120 set_working_fdt_addr((void *)addr);
122 if (!fdt_valid()) {
123 return 1;
124 }
126 if (argc >= 4) {
127 int len;
128 int err;
129 /*
130 * Optional new length
131 */
132 len = simple_strtoul(argv[3], NULL, 16);
133 if (len < fdt_totalsize(working_fdt)) {
134 printf ("New length %d < existing length %d, "
135 "ignoring.\n",
136 len, fdt_totalsize(working_fdt));
137 } else {
138 /*
139 * Open in place with a new length.
140 */
141 err = fdt_open_into(working_fdt, working_fdt, len);
142 if (err != 0) {
143 printf ("libfdt fdt_open_into(): %s\n",
144 fdt_strerror(err));
145 }
146 }
147 }
149 return CMD_RET_SUCCESS;
150 }
152 if (!working_fdt) {
153 puts(
154 "No FDT memory address configured. Please configure\n"
155 "the FDT address via \"fdt addr <address>\" command.\n"
156 "Aborting!\n");
157 return CMD_RET_FAILURE;
158 }
160 /*
161 * Move the working_fdt
162 */
163 if (strncmp(argv[1], "mo", 2) == 0) {
164 struct fdt_header *newaddr;
165 int len;
166 int err;
168 if (argc < 4)
169 return CMD_RET_USAGE;
171 /*
172 * Set the address and length of the fdt.
173 */
174 working_fdt = (struct fdt_header *)simple_strtoul(argv[2], NULL, 16);
175 if (!fdt_valid()) {
176 return 1;
177 }
179 newaddr = (struct fdt_header *)simple_strtoul(argv[3],NULL,16);
181 /*
182 * If the user specifies a length, use that. Otherwise use the
183 * current length.
184 */
185 if (argc <= 4) {
186 len = fdt_totalsize(working_fdt);
187 } else {
188 len = simple_strtoul(argv[4], NULL, 16);
189 if (len < fdt_totalsize(working_fdt)) {
190 printf ("New length 0x%X < existing length "
191 "0x%X, aborting.\n",
192 len, fdt_totalsize(working_fdt));
193 return 1;
194 }
195 }
197 /*
198 * Copy to the new location.
199 */
200 err = fdt_open_into(working_fdt, newaddr, len);
201 if (err != 0) {
202 printf ("libfdt fdt_open_into(): %s\n",
203 fdt_strerror(err));
204 return 1;
205 }
206 working_fdt = newaddr;
208 /*
209 * Make a new node
210 */
211 } else if (strncmp(argv[1], "mk", 2) == 0) {
212 char *pathp; /* path */
213 char *nodep; /* new node to add */
214 int nodeoffset; /* node offset from libfdt */
215 int err;
217 /*
218 * Parameters: Node path, new node to be appended to the path.
219 */
220 if (argc < 4)
221 return CMD_RET_USAGE;
223 pathp = argv[2];
224 nodep = argv[3];
226 nodeoffset = fdt_path_offset (working_fdt, pathp);
227 if (nodeoffset < 0) {
228 /*
229 * Not found or something else bad happened.
230 */
231 printf ("libfdt fdt_path_offset() returned %s\n",
232 fdt_strerror(nodeoffset));
233 return 1;
234 }
235 err = fdt_add_subnode(working_fdt, nodeoffset, nodep);
236 if (err < 0) {
237 printf ("libfdt fdt_add_subnode(): %s\n",
238 fdt_strerror(err));
239 return 1;
240 }
242 /*
243 * Set the value of a property in the working_fdt.
244 */
245 } else if (argv[1][0] == 's') {
246 char *pathp; /* path */
247 char *prop; /* property */
248 int nodeoffset; /* node offset from libfdt */
249 static char data[SCRATCHPAD]; /* storage for the property */
250 int len; /* new length of the property */
251 int ret; /* return value */
253 /*
254 * Parameters: Node path, property, optional value.
255 */
256 if (argc < 4)
257 return CMD_RET_USAGE;
259 pathp = argv[2];
260 prop = argv[3];
261 if (argc == 4) {
262 len = 0;
263 } else {
264 ret = fdt_parse_prop(&argv[4], argc - 4, data, &len);
265 if (ret != 0)
266 return ret;
267 }
269 nodeoffset = fdt_path_offset (working_fdt, pathp);
270 if (nodeoffset < 0) {
271 /*
272 * Not found or something else bad happened.
273 */
274 printf ("libfdt fdt_path_offset() returned %s\n",
275 fdt_strerror(nodeoffset));
276 return 1;
277 }
279 ret = fdt_setprop(working_fdt, nodeoffset, prop, data, len);
280 if (ret < 0) {
281 printf ("libfdt fdt_setprop(): %s\n", fdt_strerror(ret));
282 return 1;
283 }
285 /********************************************************************
286 * Get the value of a property in the working_fdt.
287 ********************************************************************/
288 } else if (argv[1][0] == 'g') {
289 char *subcmd; /* sub-command */
290 char *pathp; /* path */
291 char *prop; /* property */
292 char *var; /* variable to store result */
293 int nodeoffset; /* node offset from libfdt */
294 const void *nodep; /* property node pointer */
295 int len = 0; /* new length of the property */
297 /*
298 * Parameters: Node path, property, optional value.
299 */
300 if (argc < 5)
301 return CMD_RET_USAGE;
303 subcmd = argv[2];
305 if (argc < 6 && subcmd[0] != 's')
306 return CMD_RET_USAGE;
308 var = argv[3];
309 pathp = argv[4];
310 prop = argv[5];
312 nodeoffset = fdt_path_offset(working_fdt, pathp);
313 if (nodeoffset < 0) {
314 /*
315 * Not found or something else bad happened.
316 */
317 printf("libfdt fdt_path_offset() returned %s\n",
318 fdt_strerror(nodeoffset));
319 return 1;
320 }
322 if (subcmd[0] == 'n' || (subcmd[0] == 's' && argc == 5)) {
323 int reqIndex = -1;
324 int startDepth = fdt_node_depth(
325 working_fdt, nodeoffset);
326 int curDepth = startDepth;
327 int curIndex = -1;
328 int nextNodeOffset = fdt_next_node(
329 working_fdt, nodeoffset, &curDepth);
331 if (subcmd[0] == 'n')
332 reqIndex = simple_strtoul(argv[5], NULL, 16);
334 while (curDepth > startDepth) {
335 if (curDepth == startDepth + 1)
336 curIndex++;
337 if (subcmd[0] == 'n' && curIndex == reqIndex) {
338 const char *nodeName = fdt_get_name(
339 working_fdt, nextNodeOffset, NULL);
341 setenv(var, (char *)nodeName);
342 return 0;
343 }
344 nextNodeOffset = fdt_next_node(
345 working_fdt, nextNodeOffset, &curDepth);
346 if (nextNodeOffset < 0)
347 break;
348 }
349 if (subcmd[0] == 's') {
350 /* get the num nodes at this level */
351 char buf[11];
353 sprintf(buf, "%d", curIndex + 1);
354 setenv(var, buf);
355 } else {
356 /* node index not found */
357 printf("libfdt node not found\n");
358 return 1;
359 }
360 } else {
361 nodep = fdt_getprop(
362 working_fdt, nodeoffset, prop, &len);
363 if (len == 0) {
364 /* no property value */
365 setenv(var, "");
366 return 0;
367 } else if (len > 0) {
368 if (subcmd[0] == 'v') {
369 int ret;
371 ret = fdt_value_setenv(nodep, len, var);
372 if (ret != 0)
373 return ret;
374 } else if (subcmd[0] == 'a') {
375 /* Get address */
376 char buf[11];
378 sprintf(buf, "0x%08X", (uint32_t)nodep);
379 setenv(var, buf);
380 } else if (subcmd[0] == 's') {
381 /* Get size */
382 char buf[11];
384 sprintf(buf, "0x%08X", len);
385 setenv(var, buf);
386 } else
387 return CMD_RET_USAGE;
388 return 0;
389 } else {
390 printf("libfdt fdt_getprop(): %s\n",
391 fdt_strerror(len));
392 return 1;
393 }
394 }
396 /*
397 * Print (recursive) / List (single level)
398 */
399 } else if ((argv[1][0] == 'p') || (argv[1][0] == 'l')) {
400 int depth = MAX_LEVEL; /* how deep to print */
401 char *pathp; /* path */
402 char *prop; /* property */
403 int ret; /* return value */
404 static char root[2] = "/";
406 /*
407 * list is an alias for print, but limited to 1 level
408 */
409 if (argv[1][0] == 'l') {
410 depth = 1;
411 }
413 /*
414 * Get the starting path. The root node is an oddball,
415 * the offset is zero and has no name.
416 */
417 if (argc == 2)
418 pathp = root;
419 else
420 pathp = argv[2];
421 if (argc > 3)
422 prop = argv[3];
423 else
424 prop = NULL;
426 ret = fdt_print(pathp, prop, depth);
427 if (ret != 0)
428 return ret;
430 /*
431 * Remove a property/node
432 */
433 } else if (strncmp(argv[1], "rm", 2) == 0) {
434 int nodeoffset; /* node offset from libfdt */
435 int err;
437 /*
438 * Get the path. The root node is an oddball, the offset
439 * is zero and has no name.
440 */
441 nodeoffset = fdt_path_offset (working_fdt, argv[2]);
442 if (nodeoffset < 0) {
443 /*
444 * Not found or something else bad happened.
445 */
446 printf ("libfdt fdt_path_offset() returned %s\n",
447 fdt_strerror(nodeoffset));
448 return 1;
449 }
450 /*
451 * Do the delete. A fourth parameter means delete a property,
452 * otherwise delete the node.
453 */
454 if (argc > 3) {
455 err = fdt_delprop(working_fdt, nodeoffset, argv[3]);
456 if (err < 0) {
457 printf("libfdt fdt_delprop(): %s\n",
458 fdt_strerror(err));
459 return err;
460 }
461 } else {
462 err = fdt_del_node(working_fdt, nodeoffset);
463 if (err < 0) {
464 printf("libfdt fdt_del_node(): %s\n",
465 fdt_strerror(err));
466 return err;
467 }
468 }
470 /*
471 * Display header info
472 */
473 } else if (argv[1][0] == 'h') {
474 u32 version = fdt_version(working_fdt);
475 printf("magic:\t\t\t0x%x\n", fdt_magic(working_fdt));
476 printf("totalsize:\t\t0x%x (%d)\n", fdt_totalsize(working_fdt),
477 fdt_totalsize(working_fdt));
478 printf("off_dt_struct:\t\t0x%x\n",
479 fdt_off_dt_struct(working_fdt));
480 printf("off_dt_strings:\t\t0x%x\n",
481 fdt_off_dt_strings(working_fdt));
482 printf("off_mem_rsvmap:\t\t0x%x\n",
483 fdt_off_mem_rsvmap(working_fdt));
484 printf("version:\t\t%d\n", version);
485 printf("last_comp_version:\t%d\n",
486 fdt_last_comp_version(working_fdt));
487 if (version >= 2)
488 printf("boot_cpuid_phys:\t0x%x\n",
489 fdt_boot_cpuid_phys(working_fdt));
490 if (version >= 3)
491 printf("size_dt_strings:\t0x%x\n",
492 fdt_size_dt_strings(working_fdt));
493 if (version >= 17)
494 printf("size_dt_struct:\t\t0x%x\n",
495 fdt_size_dt_struct(working_fdt));
496 printf("number mem_rsv:\t\t0x%x\n",
497 fdt_num_mem_rsv(working_fdt));
498 printf("\n");
500 /*
501 * Set boot cpu id
502 */
503 } else if (strncmp(argv[1], "boo", 3) == 0) {
504 unsigned long tmp = simple_strtoul(argv[2], NULL, 16);
505 fdt_set_boot_cpuid_phys(working_fdt, tmp);
507 /*
508 * memory command
509 */
510 } else if (strncmp(argv[1], "me", 2) == 0) {
511 uint64_t addr, size;
512 int err;
513 addr = simple_strtoull(argv[2], NULL, 16);
514 size = simple_strtoull(argv[3], NULL, 16);
515 err = fdt_fixup_memory(working_fdt, addr, size);
516 if (err < 0)
517 return err;
519 /*
520 * mem reserve commands
521 */
522 } else if (strncmp(argv[1], "rs", 2) == 0) {
523 if (argv[2][0] == 'p') {
524 uint64_t addr, size;
525 int total = fdt_num_mem_rsv(working_fdt);
526 int j, err;
527 printf("index\t\t start\t\t size\n");
528 printf("-------------------------------"
529 "-----------------\n");
530 for (j = 0; j < total; j++) {
531 err = fdt_get_mem_rsv(working_fdt, j, &addr, &size);
532 if (err < 0) {
533 printf("libfdt fdt_get_mem_rsv(): %s\n",
534 fdt_strerror(err));
535 return err;
536 }
537 printf(" %x\t%08x%08x\t%08x%08x\n", j,
538 (u32)(addr >> 32),
539 (u32)(addr & 0xffffffff),
540 (u32)(size >> 32),
541 (u32)(size & 0xffffffff));
542 }
543 } else if (argv[2][0] == 'a') {
544 uint64_t addr, size;
545 int err;
546 addr = simple_strtoull(argv[3], NULL, 16);
547 size = simple_strtoull(argv[4], NULL, 16);
548 err = fdt_add_mem_rsv(working_fdt, addr, size);
550 if (err < 0) {
551 printf("libfdt fdt_add_mem_rsv(): %s\n",
552 fdt_strerror(err));
553 return err;
554 }
555 } else if (argv[2][0] == 'd') {
556 unsigned long idx = simple_strtoul(argv[3], NULL, 16);
557 int err = fdt_del_mem_rsv(working_fdt, idx);
559 if (err < 0) {
560 printf("libfdt fdt_del_mem_rsv(): %s\n",
561 fdt_strerror(err));
562 return err;
563 }
564 } else {
565 /* Unrecognized command */
566 return CMD_RET_USAGE;
567 }
568 }
569 #ifdef CONFIG_OF_BOARD_SETUP
570 /* Call the board-specific fixup routine */
571 else if (strncmp(argv[1], "boa", 3) == 0)
572 ft_board_setup(working_fdt, gd->bd);
573 #endif
574 /* Create a chosen node */
575 else if (argv[1][0] == 'c') {
576 unsigned long initrd_start = 0, initrd_end = 0;
578 if ((argc != 2) && (argc != 4))
579 return CMD_RET_USAGE;
581 if (argc == 4) {
582 initrd_start = simple_strtoul(argv[2], NULL, 16);
583 initrd_end = simple_strtoul(argv[3], NULL, 16);
584 }
586 fdt_chosen(working_fdt, 1);
587 fdt_initrd(working_fdt, initrd_start, initrd_end, 1);
588 }
589 /* resize the fdt */
590 else if (strncmp(argv[1], "re", 2) == 0) {
591 fdt_resize(working_fdt);
592 }
593 else {
594 /* Unrecognized command */
595 return CMD_RET_USAGE;
596 }
598 return 0;
599 }
601 /****************************************************************************/
603 static int fdt_valid(void)
604 {
605 int err;
607 if (working_fdt == NULL) {
608 printf ("The address of the fdt is invalid (NULL).\n");
609 return 0;
610 }
612 err = fdt_check_header(working_fdt);
613 if (err == 0)
614 return 1; /* valid */
616 if (err < 0) {
617 printf("libfdt fdt_check_header(): %s", fdt_strerror(err));
618 /*
619 * Be more informative on bad version.
620 */
621 if (err == -FDT_ERR_BADVERSION) {
622 if (fdt_version(working_fdt) <
623 FDT_FIRST_SUPPORTED_VERSION) {
624 printf (" - too old, fdt %d < %d",
625 fdt_version(working_fdt),
626 FDT_FIRST_SUPPORTED_VERSION);
627 working_fdt = NULL;
628 }
629 if (fdt_last_comp_version(working_fdt) >
630 FDT_LAST_SUPPORTED_VERSION) {
631 printf (" - too new, fdt %d > %d",
632 fdt_version(working_fdt),
633 FDT_LAST_SUPPORTED_VERSION);
634 working_fdt = NULL;
635 }
636 return 0;
637 }
638 printf("\n");
639 return 0;
640 }
641 return 1;
642 }
644 /****************************************************************************/
646 /*
647 * Parse the user's input, partially heuristic. Valid formats:
648 * <0x00112233 4 05> - an array of cells. Numbers follow standard
649 * C conventions.
650 * [00 11 22 .. nn] - byte stream
651 * "string" - If the the value doesn't start with "<" or "[", it is
652 * treated as a string. Note that the quotes are
653 * stripped by the parser before we get the string.
654 * newval: An array of strings containing the new property as specified
655 * on the command line
656 * count: The number of strings in the array
657 * data: A bytestream to be placed in the property
658 * len: The length of the resulting bytestream
659 */
660 static int fdt_parse_prop(char * const *newval, int count, char *data, int *len)
661 {
662 char *cp; /* temporary char pointer */
663 char *newp; /* temporary newval char pointer */
664 unsigned long tmp; /* holds converted values */
665 int stridx = 0;
667 *len = 0;
668 newp = newval[0];
670 /* An array of cells */
671 if (*newp == '<') {
672 newp++;
673 while ((*newp != '>') && (stridx < count)) {
674 /*
675 * Keep searching until we find that last ">"
676 * That way users don't have to escape the spaces
677 */
678 if (*newp == '\0') {
679 newp = newval[++stridx];
680 continue;
681 }
683 cp = newp;
684 tmp = simple_strtoul(cp, &newp, 0);
685 *(uint32_t *)data = __cpu_to_be32(tmp);
686 data += 4;
687 *len += 4;
689 /* If the ptr didn't advance, something went wrong */
690 if ((newp - cp) <= 0) {
691 printf("Sorry, I could not convert \"%s\"\n",
692 cp);
693 return 1;
694 }
696 while (*newp == ' ')
697 newp++;
698 }
700 if (*newp != '>') {
701 printf("Unexpected character '%c'\n", *newp);
702 return 1;
703 }
704 } else if (*newp == '[') {
705 /*
706 * Byte stream. Convert the values.
707 */
708 newp++;
709 while ((stridx < count) && (*newp != ']')) {
710 while (*newp == ' ')
711 newp++;
712 if (*newp == '\0') {
713 newp = newval[++stridx];
714 continue;
715 }
716 if (!isxdigit(*newp))
717 break;
718 tmp = simple_strtoul(newp, &newp, 16);
719 *data++ = tmp & 0xFF;
720 *len = *len + 1;
721 }
722 if (*newp != ']') {
723 printf("Unexpected character '%c'\n", *newp);
724 return 1;
725 }
726 } else {
727 /*
728 * Assume it is one or more strings. Copy it into our
729 * data area for convenience (including the
730 * terminating '\0's).
731 */
732 while (stridx < count) {
733 size_t length = strlen(newp) + 1;
734 strcpy(data, newp);
735 data += length;
736 *len += length;
737 newp = newval[++stridx];
738 }
739 }
740 return 0;
741 }
743 /****************************************************************************/
745 /*
746 * Heuristic to guess if this is a string or concatenated strings.
747 */
749 static int is_printable_string(const void *data, int len)
750 {
751 const char *s = data;
753 /* zero length is not */
754 if (len == 0)
755 return 0;
757 /* must terminate with zero or '\n' */
758 if (s[len - 1] != '\0' && s[len - 1] != '\n')
759 return 0;
761 /* printable or a null byte (concatenated strings) */
762 while (((*s == '\0') || isprint(*s) || isspace(*s)) && (len > 0)) {
763 /*
764 * If we see a null, there are three possibilities:
765 * 1) If len == 1, it is the end of the string, printable
766 * 2) Next character also a null, not printable.
767 * 3) Next character not a null, continue to check.
768 */
769 if (s[0] == '\0') {
770 if (len == 1)
771 return 1;
772 if (s[1] == '\0')
773 return 0;
774 }
775 s++;
776 len--;
777 }
779 /* Not the null termination, or not done yet: not printable */
780 if (*s != '\0' || (len != 0))
781 return 0;
783 return 1;
784 }
787 /*
788 * Print the property in the best format, a heuristic guess. Print as
789 * a string, concatenated strings, a byte, word, double word, or (if all
790 * else fails) it is printed as a stream of bytes.
791 */
792 static void print_data(const void *data, int len)
793 {
794 int j;
796 /* no data, don't print */
797 if (len == 0)
798 return;
800 /*
801 * It is a string, but it may have multiple strings (embedded '\0's).
802 */
803 if (is_printable_string(data, len)) {
804 puts("\"");
805 j = 0;
806 while (j < len) {
807 if (j > 0)
808 puts("\", \"");
809 puts(data);
810 j += strlen(data) + 1;
811 data += strlen(data) + 1;
812 }
813 puts("\"");
814 return;
815 }
817 if ((len %4) == 0) {
818 if (len > CONFIG_CMD_FDT_MAX_DUMP)
819 printf("* 0x%08x [0x%08x]", (unsigned int)data, len);
820 else {
821 const u32 *p;
823 printf("<");
824 for (j = 0, p = data; j < len/4; j++)
825 printf("0x%08x%s", fdt32_to_cpu(p[j]),
826 j < (len/4 - 1) ? " " : "");
827 printf(">");
828 }
829 } else { /* anything else... hexdump */
830 if (len > CONFIG_CMD_FDT_MAX_DUMP)
831 printf("* 0x%08x [0x%08x]", (unsigned int)data, len);
832 else {
833 const u8 *s;
835 printf("[");
836 for (j = 0, s = data; j < len; j++)
837 printf("%02x%s", s[j], j < len - 1 ? " " : "");
838 printf("]");
839 }
840 }
841 }
843 /****************************************************************************/
845 /*
846 * Recursively print (a portion of) the working_fdt. The depth parameter
847 * determines how deeply nested the fdt is printed.
848 */
849 static int fdt_print(const char *pathp, char *prop, int depth)
850 {
851 static char tabs[MAX_LEVEL+1] =
852 "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t"
853 "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t";
854 const void *nodep; /* property node pointer */
855 int nodeoffset; /* node offset from libfdt */
856 int nextoffset; /* next node offset from libfdt */
857 uint32_t tag; /* tag */
858 int len; /* length of the property */
859 int level = 0; /* keep track of nesting level */
860 const struct fdt_property *fdt_prop;
862 nodeoffset = fdt_path_offset (working_fdt, pathp);
863 if (nodeoffset < 0) {
864 /*
865 * Not found or something else bad happened.
866 */
867 printf ("libfdt fdt_path_offset() returned %s\n",
868 fdt_strerror(nodeoffset));
869 return 1;
870 }
871 /*
872 * The user passed in a property as well as node path.
873 * Print only the given property and then return.
874 */
875 if (prop) {
876 nodep = fdt_getprop (working_fdt, nodeoffset, prop, &len);
877 if (len == 0) {
878 /* no property value */
879 printf("%s %s\n", pathp, prop);
880 return 0;
881 } else if (len > 0) {
882 printf("%s = ", prop);
883 print_data (nodep, len);
884 printf("\n");
885 return 0;
886 } else {
887 printf ("libfdt fdt_getprop(): %s\n",
888 fdt_strerror(len));
889 return 1;
890 }
891 }
893 /*
894 * The user passed in a node path and no property,
895 * print the node and all subnodes.
896 */
897 while(level >= 0) {
898 tag = fdt_next_tag(working_fdt, nodeoffset, &nextoffset);
899 switch(tag) {
900 case FDT_BEGIN_NODE:
901 pathp = fdt_get_name(working_fdt, nodeoffset, NULL);
902 if (level <= depth) {
903 if (pathp == NULL)
904 pathp = "/* NULL pointer error */";
905 if (*pathp == '\0')
906 pathp = "/"; /* root is nameless */
907 printf("%s%s {\n",
908 &tabs[MAX_LEVEL - level], pathp);
909 }
910 level++;
911 if (level >= MAX_LEVEL) {
912 printf("Nested too deep, aborting.\n");
913 return 1;
914 }
915 break;
916 case FDT_END_NODE:
917 level--;
918 if (level <= depth)
919 printf("%s};\n", &tabs[MAX_LEVEL - level]);
920 if (level == 0) {
921 level = -1; /* exit the loop */
922 }
923 break;
924 case FDT_PROP:
925 fdt_prop = fdt_offset_ptr(working_fdt, nodeoffset,
926 sizeof(*fdt_prop));
927 pathp = fdt_string(working_fdt,
928 fdt32_to_cpu(fdt_prop->nameoff));
929 len = fdt32_to_cpu(fdt_prop->len);
930 nodep = fdt_prop->data;
931 if (len < 0) {
932 printf ("libfdt fdt_getprop(): %s\n",
933 fdt_strerror(len));
934 return 1;
935 } else if (len == 0) {
936 /* the property has no value */
937 if (level <= depth)
938 printf("%s%s;\n",
939 &tabs[MAX_LEVEL - level],
940 pathp);
941 } else {
942 if (level <= depth) {
943 printf("%s%s = ",
944 &tabs[MAX_LEVEL - level],
945 pathp);
946 print_data (nodep, len);
947 printf(";\n");
948 }
949 }
950 break;
951 case FDT_NOP:
952 printf("%s/* NOP */\n", &tabs[MAX_LEVEL - level]);
953 break;
954 case FDT_END:
955 return 1;
956 default:
957 if (level <= depth)
958 printf("Unknown tag 0x%08X\n", tag);
959 return 1;
960 }
961 nodeoffset = nextoffset;
962 }
963 return 0;
964 }
966 /********************************************************************/
968 U_BOOT_CMD(
969 fdt, 255, 0, do_fdt,
970 "flattened device tree utility commands",
971 "addr <addr> [<length>] - Set the fdt location to <addr>\n"
972 #ifdef CONFIG_OF_BOARD_SETUP
973 "fdt boardsetup - Do board-specific set up\n"
974 #endif
975 "fdt move <fdt> <newaddr> <length> - Copy the fdt to <addr> and make it active\n"
976 "fdt resize - Resize fdt to size + padding to 4k addr\n"
977 "fdt print <path> [<prop>] - Recursive print starting at <path>\n"
978 "fdt list <path> [<prop>] - Print one level starting at <path>\n"
979 "fdt get value <var> <path> <prop> - Get <property> and store in <var>\n"
980 "fdt get name <var> <path> <index> - Get name of node <index> and store in <var>\n"
981 "fdt get addr <var> <path> <prop> - Get start address of <property> and store in <var>\n"
982 "fdt get size <var> <path> [<prop>] - Get size of [<property>] or num nodes and store in <var>\n"
983 "fdt set <path> <prop> [<val>] - Set <property> [to <val>]\n"
984 "fdt mknode <path> <node> - Create a new node after <path>\n"
985 "fdt rm <path> [<prop>] - Delete the node or <property>\n"
986 "fdt header - Display header info\n"
987 "fdt bootcpu <id> - Set boot cpuid\n"
988 "fdt memory <addr> <size> - Add/Update memory node\n"
989 "fdt rsvmem print - Show current mem reserves\n"
990 "fdt rsvmem add <addr> <size> - Add a mem reserve\n"
991 "fdt rsvmem delete <index> - Delete a mem reserves\n"
992 "fdt chosen [<start> <end>] - Add/update the /chosen branch in the tree\n"
993 " <start>/<end> - initrd start/end addr\n"
994 "NOTE: Dereference aliases by omiting the leading '/', "
995 "e.g. fdt print ethernet0."
996 );