1 /*
2 * (C) Copyright 2007
3 * Gerald Van Baren, Custom IDEAS, vanbaren@cideas.com
4 * Based on code written by:
5 * Pantelis Antoniou <pantelis.antoniou@gmail.com> and
6 * Matthew McClintock <msm@freescale.com>
7 *
8 * See file CREDITS for list of people who contributed to this
9 * project.
10 *
11 * This program is free software; you can redistribute it and/or
12 * modify it under the terms of the GNU General Public License as
13 * published by the Free Software Foundation; either version 2 of
14 * the License, or (at your option) any later version.
15 *
16 * This program is distributed in the hope that it will be useful,
17 * but WITHOUT ANY WARRANTY; without even the implied warranty of
18 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
19 * GNU General Public License for more details.
20 *
21 * You should have received a copy of the GNU General Public License
22 * along with this program; if not, write to the Free Software
23 * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
24 * MA 02111-1307 USA
25 */
27 #include <common.h>
28 #include <command.h>
29 #include <linux/ctype.h>
30 #include <linux/types.h>
31 #include <asm/global_data.h>
32 #include <fdt.h>
33 #include <libfdt.h>
34 #include <fdt_support.h>
36 #define MAX_LEVEL 32 /* how deeply nested we will go */
37 #define SCRATCHPAD 1024 /* bytes of scratchpad memory */
39 /*
40 * Global data (for the gd->bd)
41 */
42 DECLARE_GLOBAL_DATA_PTR;
44 static int fdt_valid(void);
45 static int fdt_parse_prop(char *const*newval, int count, char *data, int *len);
46 static int fdt_print(const char *pathp, char *prop, int depth);
48 /*
49 * The working_fdt points to our working flattened device tree.
50 */
51 struct fdt_header *working_fdt;
53 void set_working_fdt_addr(void *addr)
54 {
55 char buf[17];
57 working_fdt = addr;
59 sprintf(buf, "%lx", (unsigned long)addr);
60 setenv("fdtaddr", buf);
61 }
63 /*
64 * Flattened Device Tree command, see the help for parameter definitions.
65 */
66 int do_fdt (cmd_tbl_t * cmdtp, int flag, int argc, char * const argv[])
67 {
68 if (argc < 2)
69 return CMD_RET_USAGE;
71 /*
72 * Set the address of the fdt
73 */
74 if (argv[1][0] == 'a') {
75 unsigned long addr;
76 /*
77 * Set the address [and length] of the fdt.
78 */
79 if (argc == 2) {
80 if (!fdt_valid()) {
81 return 1;
82 }
83 printf("The address of the fdt is %p\n", working_fdt);
84 return 0;
85 }
87 addr = simple_strtoul(argv[2], NULL, 16);
88 set_working_fdt_addr((void *)addr);
90 if (!fdt_valid()) {
91 return 1;
92 }
94 if (argc >= 4) {
95 int len;
96 int err;
97 /*
98 * Optional new length
99 */
100 len = simple_strtoul(argv[3], NULL, 16);
101 if (len < fdt_totalsize(working_fdt)) {
102 printf ("New length %d < existing length %d, "
103 "ignoring.\n",
104 len, fdt_totalsize(working_fdt));
105 } else {
106 /*
107 * Open in place with a new length.
108 */
109 err = fdt_open_into(working_fdt, working_fdt, len);
110 if (err != 0) {
111 printf ("libfdt fdt_open_into(): %s\n",
112 fdt_strerror(err));
113 }
114 }
115 }
117 return CMD_RET_SUCCESS;
118 }
120 if (!working_fdt) {
121 puts(
122 "No FDT memory address configured. Please configure\n"
123 "the FDT address via \"fdt addr <address>\" command.\n"
124 "Aborting!\n");
125 return CMD_RET_FAILURE;
126 }
128 /*
129 * Move the working_fdt
130 */
131 if (strncmp(argv[1], "mo", 2) == 0) {
132 struct fdt_header *newaddr;
133 int len;
134 int err;
136 if (argc < 4)
137 return CMD_RET_USAGE;
139 /*
140 * Set the address and length of the fdt.
141 */
142 working_fdt = (struct fdt_header *)simple_strtoul(argv[2], NULL, 16);
143 if (!fdt_valid()) {
144 return 1;
145 }
147 newaddr = (struct fdt_header *)simple_strtoul(argv[3],NULL,16);
149 /*
150 * If the user specifies a length, use that. Otherwise use the
151 * current length.
152 */
153 if (argc <= 4) {
154 len = fdt_totalsize(working_fdt);
155 } else {
156 len = simple_strtoul(argv[4], NULL, 16);
157 if (len < fdt_totalsize(working_fdt)) {
158 printf ("New length 0x%X < existing length "
159 "0x%X, aborting.\n",
160 len, fdt_totalsize(working_fdt));
161 return 1;
162 }
163 }
165 /*
166 * Copy to the new location.
167 */
168 err = fdt_open_into(working_fdt, newaddr, len);
169 if (err != 0) {
170 printf ("libfdt fdt_open_into(): %s\n",
171 fdt_strerror(err));
172 return 1;
173 }
174 working_fdt = newaddr;
176 /*
177 * Make a new node
178 */
179 } else if (strncmp(argv[1], "mk", 2) == 0) {
180 char *pathp; /* path */
181 char *nodep; /* new node to add */
182 int nodeoffset; /* node offset from libfdt */
183 int err;
185 /*
186 * Parameters: Node path, new node to be appended to the path.
187 */
188 if (argc < 4)
189 return CMD_RET_USAGE;
191 pathp = argv[2];
192 nodep = argv[3];
194 nodeoffset = fdt_path_offset (working_fdt, pathp);
195 if (nodeoffset < 0) {
196 /*
197 * Not found or something else bad happened.
198 */
199 printf ("libfdt fdt_path_offset() returned %s\n",
200 fdt_strerror(nodeoffset));
201 return 1;
202 }
203 err = fdt_add_subnode(working_fdt, nodeoffset, nodep);
204 if (err < 0) {
205 printf ("libfdt fdt_add_subnode(): %s\n",
206 fdt_strerror(err));
207 return 1;
208 }
210 /*
211 * Set the value of a property in the working_fdt.
212 */
213 } else if (argv[1][0] == 's') {
214 char *pathp; /* path */
215 char *prop; /* property */
216 int nodeoffset; /* node offset from libfdt */
217 static char data[SCRATCHPAD]; /* storage for the property */
218 int len; /* new length of the property */
219 int ret; /* return value */
221 /*
222 * Parameters: Node path, property, optional value.
223 */
224 if (argc < 4)
225 return CMD_RET_USAGE;
227 pathp = argv[2];
228 prop = argv[3];
229 if (argc == 4) {
230 len = 0;
231 } else {
232 ret = fdt_parse_prop(&argv[4], argc - 4, data, &len);
233 if (ret != 0)
234 return ret;
235 }
237 nodeoffset = fdt_path_offset (working_fdt, pathp);
238 if (nodeoffset < 0) {
239 /*
240 * Not found or something else bad happened.
241 */
242 printf ("libfdt fdt_path_offset() returned %s\n",
243 fdt_strerror(nodeoffset));
244 return 1;
245 }
247 ret = fdt_setprop(working_fdt, nodeoffset, prop, data, len);
248 if (ret < 0) {
249 printf ("libfdt fdt_setprop(): %s\n", fdt_strerror(ret));
250 return 1;
251 }
253 /*
254 * Print (recursive) / List (single level)
255 */
256 } else if ((argv[1][0] == 'p') || (argv[1][0] == 'l')) {
257 int depth = MAX_LEVEL; /* how deep to print */
258 char *pathp; /* path */
259 char *prop; /* property */
260 int ret; /* return value */
261 static char root[2] = "/";
263 /*
264 * list is an alias for print, but limited to 1 level
265 */
266 if (argv[1][0] == 'l') {
267 depth = 1;
268 }
270 /*
271 * Get the starting path. The root node is an oddball,
272 * the offset is zero and has no name.
273 */
274 if (argc == 2)
275 pathp = root;
276 else
277 pathp = argv[2];
278 if (argc > 3)
279 prop = argv[3];
280 else
281 prop = NULL;
283 ret = fdt_print(pathp, prop, depth);
284 if (ret != 0)
285 return ret;
287 /*
288 * Remove a property/node
289 */
290 } else if (strncmp(argv[1], "rm", 2) == 0) {
291 int nodeoffset; /* node offset from libfdt */
292 int err;
294 /*
295 * Get the path. The root node is an oddball, the offset
296 * is zero and has no name.
297 */
298 nodeoffset = fdt_path_offset (working_fdt, argv[2]);
299 if (nodeoffset < 0) {
300 /*
301 * Not found or something else bad happened.
302 */
303 printf ("libfdt fdt_path_offset() returned %s\n",
304 fdt_strerror(nodeoffset));
305 return 1;
306 }
307 /*
308 * Do the delete. A fourth parameter means delete a property,
309 * otherwise delete the node.
310 */
311 if (argc > 3) {
312 err = fdt_delprop(working_fdt, nodeoffset, argv[3]);
313 if (err < 0) {
314 printf("libfdt fdt_delprop(): %s\n",
315 fdt_strerror(err));
316 return err;
317 }
318 } else {
319 err = fdt_del_node(working_fdt, nodeoffset);
320 if (err < 0) {
321 printf("libfdt fdt_del_node(): %s\n",
322 fdt_strerror(err));
323 return err;
324 }
325 }
327 /*
328 * Display header info
329 */
330 } else if (argv[1][0] == 'h') {
331 u32 version = fdt_version(working_fdt);
332 printf("magic:\t\t\t0x%x\n", fdt_magic(working_fdt));
333 printf("totalsize:\t\t0x%x (%d)\n", fdt_totalsize(working_fdt),
334 fdt_totalsize(working_fdt));
335 printf("off_dt_struct:\t\t0x%x\n",
336 fdt_off_dt_struct(working_fdt));
337 printf("off_dt_strings:\t\t0x%x\n",
338 fdt_off_dt_strings(working_fdt));
339 printf("off_mem_rsvmap:\t\t0x%x\n",
340 fdt_off_mem_rsvmap(working_fdt));
341 printf("version:\t\t%d\n", version);
342 printf("last_comp_version:\t%d\n",
343 fdt_last_comp_version(working_fdt));
344 if (version >= 2)
345 printf("boot_cpuid_phys:\t0x%x\n",
346 fdt_boot_cpuid_phys(working_fdt));
347 if (version >= 3)
348 printf("size_dt_strings:\t0x%x\n",
349 fdt_size_dt_strings(working_fdt));
350 if (version >= 17)
351 printf("size_dt_struct:\t\t0x%x\n",
352 fdt_size_dt_struct(working_fdt));
353 printf("number mem_rsv:\t\t0x%x\n",
354 fdt_num_mem_rsv(working_fdt));
355 printf("\n");
357 /*
358 * Set boot cpu id
359 */
360 } else if (strncmp(argv[1], "boo", 3) == 0) {
361 unsigned long tmp = simple_strtoul(argv[2], NULL, 16);
362 fdt_set_boot_cpuid_phys(working_fdt, tmp);
364 /*
365 * memory command
366 */
367 } else if (strncmp(argv[1], "me", 2) == 0) {
368 uint64_t addr, size;
369 int err;
370 addr = simple_strtoull(argv[2], NULL, 16);
371 size = simple_strtoull(argv[3], NULL, 16);
372 err = fdt_fixup_memory(working_fdt, addr, size);
373 if (err < 0)
374 return err;
376 /*
377 * mem reserve commands
378 */
379 } else if (strncmp(argv[1], "rs", 2) == 0) {
380 if (argv[2][0] == 'p') {
381 uint64_t addr, size;
382 int total = fdt_num_mem_rsv(working_fdt);
383 int j, err;
384 printf("index\t\t start\t\t size\n");
385 printf("-------------------------------"
386 "-----------------\n");
387 for (j = 0; j < total; j++) {
388 err = fdt_get_mem_rsv(working_fdt, j, &addr, &size);
389 if (err < 0) {
390 printf("libfdt fdt_get_mem_rsv(): %s\n",
391 fdt_strerror(err));
392 return err;
393 }
394 printf(" %x\t%08x%08x\t%08x%08x\n", j,
395 (u32)(addr >> 32),
396 (u32)(addr & 0xffffffff),
397 (u32)(size >> 32),
398 (u32)(size & 0xffffffff));
399 }
400 } else if (argv[2][0] == 'a') {
401 uint64_t addr, size;
402 int err;
403 addr = simple_strtoull(argv[3], NULL, 16);
404 size = simple_strtoull(argv[4], NULL, 16);
405 err = fdt_add_mem_rsv(working_fdt, addr, size);
407 if (err < 0) {
408 printf("libfdt fdt_add_mem_rsv(): %s\n",
409 fdt_strerror(err));
410 return err;
411 }
412 } else if (argv[2][0] == 'd') {
413 unsigned long idx = simple_strtoul(argv[3], NULL, 16);
414 int err = fdt_del_mem_rsv(working_fdt, idx);
416 if (err < 0) {
417 printf("libfdt fdt_del_mem_rsv(): %s\n",
418 fdt_strerror(err));
419 return err;
420 }
421 } else {
422 /* Unrecognized command */
423 return CMD_RET_USAGE;
424 }
425 }
426 #ifdef CONFIG_OF_BOARD_SETUP
427 /* Call the board-specific fixup routine */
428 else if (strncmp(argv[1], "boa", 3) == 0)
429 ft_board_setup(working_fdt, gd->bd);
430 #endif
431 /* Create a chosen node */
432 else if (argv[1][0] == 'c') {
433 unsigned long initrd_start = 0, initrd_end = 0;
435 if ((argc != 2) && (argc != 4))
436 return CMD_RET_USAGE;
438 if (argc == 4) {
439 initrd_start = simple_strtoul(argv[2], NULL, 16);
440 initrd_end = simple_strtoul(argv[3], NULL, 16);
441 }
443 fdt_chosen(working_fdt, 1);
444 fdt_initrd(working_fdt, initrd_start, initrd_end, 1);
445 }
446 /* resize the fdt */
447 else if (strncmp(argv[1], "re", 2) == 0) {
448 fdt_resize(working_fdt);
449 }
450 else {
451 /* Unrecognized command */
452 return CMD_RET_USAGE;
453 }
455 return 0;
456 }
458 /****************************************************************************/
460 static int fdt_valid(void)
461 {
462 int err;
464 if (working_fdt == NULL) {
465 printf ("The address of the fdt is invalid (NULL).\n");
466 return 0;
467 }
469 err = fdt_check_header(working_fdt);
470 if (err == 0)
471 return 1; /* valid */
473 if (err < 0) {
474 printf("libfdt fdt_check_header(): %s", fdt_strerror(err));
475 /*
476 * Be more informative on bad version.
477 */
478 if (err == -FDT_ERR_BADVERSION) {
479 if (fdt_version(working_fdt) <
480 FDT_FIRST_SUPPORTED_VERSION) {
481 printf (" - too old, fdt %d < %d",
482 fdt_version(working_fdt),
483 FDT_FIRST_SUPPORTED_VERSION);
484 working_fdt = NULL;
485 }
486 if (fdt_last_comp_version(working_fdt) >
487 FDT_LAST_SUPPORTED_VERSION) {
488 printf (" - too new, fdt %d > %d",
489 fdt_version(working_fdt),
490 FDT_LAST_SUPPORTED_VERSION);
491 working_fdt = NULL;
492 }
493 return 0;
494 }
495 printf("\n");
496 return 0;
497 }
498 return 1;
499 }
501 /****************************************************************************/
503 /*
504 * Parse the user's input, partially heuristic. Valid formats:
505 * <0x00112233 4 05> - an array of cells. Numbers follow standard
506 * C conventions.
507 * [00 11 22 .. nn] - byte stream
508 * "string" - If the the value doesn't start with "<" or "[", it is
509 * treated as a string. Note that the quotes are
510 * stripped by the parser before we get the string.
511 * newval: An array of strings containing the new property as specified
512 * on the command line
513 * count: The number of strings in the array
514 * data: A bytestream to be placed in the property
515 * len: The length of the resulting bytestream
516 */
517 static int fdt_parse_prop(char * const *newval, int count, char *data, int *len)
518 {
519 char *cp; /* temporary char pointer */
520 char *newp; /* temporary newval char pointer */
521 unsigned long tmp; /* holds converted values */
522 int stridx = 0;
524 *len = 0;
525 newp = newval[0];
527 /* An array of cells */
528 if (*newp == '<') {
529 newp++;
530 while ((*newp != '>') && (stridx < count)) {
531 /*
532 * Keep searching until we find that last ">"
533 * That way users don't have to escape the spaces
534 */
535 if (*newp == '\0') {
536 newp = newval[++stridx];
537 continue;
538 }
540 cp = newp;
541 tmp = simple_strtoul(cp, &newp, 0);
542 *(uint32_t *)data = __cpu_to_be32(tmp);
543 data += 4;
544 *len += 4;
546 /* If the ptr didn't advance, something went wrong */
547 if ((newp - cp) <= 0) {
548 printf("Sorry, I could not convert \"%s\"\n",
549 cp);
550 return 1;
551 }
553 while (*newp == ' ')
554 newp++;
555 }
557 if (*newp != '>') {
558 printf("Unexpected character '%c'\n", *newp);
559 return 1;
560 }
561 } else if (*newp == '[') {
562 /*
563 * Byte stream. Convert the values.
564 */
565 newp++;
566 while ((stridx < count) && (*newp != ']')) {
567 while (*newp == ' ')
568 newp++;
569 if (*newp == '\0') {
570 newp = newval[++stridx];
571 continue;
572 }
573 if (!isxdigit(*newp))
574 break;
575 tmp = simple_strtoul(newp, &newp, 16);
576 *data++ = tmp & 0xFF;
577 *len = *len + 1;
578 }
579 if (*newp != ']') {
580 printf("Unexpected character '%c'\n", *newp);
581 return 1;
582 }
583 } else {
584 /*
585 * Assume it is one or more strings. Copy it into our
586 * data area for convenience (including the
587 * terminating '\0's).
588 */
589 while (stridx < count) {
590 size_t length = strlen(newp) + 1;
591 strcpy(data, newp);
592 data += length;
593 *len += length;
594 newp = newval[++stridx];
595 }
596 }
597 return 0;
598 }
600 /****************************************************************************/
602 /*
603 * Heuristic to guess if this is a string or concatenated strings.
604 */
606 static int is_printable_string(const void *data, int len)
607 {
608 const char *s = data;
610 /* zero length is not */
611 if (len == 0)
612 return 0;
614 /* must terminate with zero */
615 if (s[len - 1] != '\0')
616 return 0;
618 /* printable or a null byte (concatenated strings) */
619 while (((*s == '\0') || isprint(*s)) && (len > 0)) {
620 /*
621 * If we see a null, there are three possibilities:
622 * 1) If len == 1, it is the end of the string, printable
623 * 2) Next character also a null, not printable.
624 * 3) Next character not a null, continue to check.
625 */
626 if (s[0] == '\0') {
627 if (len == 1)
628 return 1;
629 if (s[1] == '\0')
630 return 0;
631 }
632 s++;
633 len--;
634 }
636 /* Not the null termination, or not done yet: not printable */
637 if (*s != '\0' || (len != 0))
638 return 0;
640 return 1;
641 }
644 /*
645 * Print the property in the best format, a heuristic guess. Print as
646 * a string, concatenated strings, a byte, word, double word, or (if all
647 * else fails) it is printed as a stream of bytes.
648 */
649 static void print_data(const void *data, int len)
650 {
651 int j;
653 /* no data, don't print */
654 if (len == 0)
655 return;
657 /*
658 * It is a string, but it may have multiple strings (embedded '\0's).
659 */
660 if (is_printable_string(data, len)) {
661 puts("\"");
662 j = 0;
663 while (j < len) {
664 if (j > 0)
665 puts("\", \"");
666 puts(data);
667 j += strlen(data) + 1;
668 data += strlen(data) + 1;
669 }
670 puts("\"");
671 return;
672 }
674 if ((len %4) == 0) {
675 const u32 *p;
677 printf("<");
678 for (j = 0, p = data; j < len/4; j ++)
679 printf("0x%x%s", fdt32_to_cpu(p[j]), j < (len/4 - 1) ? " " : "");
680 printf(">");
681 } else { /* anything else... hexdump */
682 const u8 *s;
684 printf("[");
685 for (j = 0, s = data; j < len; j++)
686 printf("%02x%s", s[j], j < len - 1 ? " " : "");
687 printf("]");
688 }
689 }
691 /****************************************************************************/
693 /*
694 * Recursively print (a portion of) the working_fdt. The depth parameter
695 * determines how deeply nested the fdt is printed.
696 */
697 static int fdt_print(const char *pathp, char *prop, int depth)
698 {
699 static char tabs[MAX_LEVEL+1] =
700 "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t"
701 "\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t\t";
702 const void *nodep; /* property node pointer */
703 int nodeoffset; /* node offset from libfdt */
704 int nextoffset; /* next node offset from libfdt */
705 uint32_t tag; /* tag */
706 int len; /* length of the property */
707 int level = 0; /* keep track of nesting level */
708 const struct fdt_property *fdt_prop;
710 nodeoffset = fdt_path_offset (working_fdt, pathp);
711 if (nodeoffset < 0) {
712 /*
713 * Not found or something else bad happened.
714 */
715 printf ("libfdt fdt_path_offset() returned %s\n",
716 fdt_strerror(nodeoffset));
717 return 1;
718 }
719 /*
720 * The user passed in a property as well as node path.
721 * Print only the given property and then return.
722 */
723 if (prop) {
724 nodep = fdt_getprop (working_fdt, nodeoffset, prop, &len);
725 if (len == 0) {
726 /* no property value */
727 printf("%s %s\n", pathp, prop);
728 return 0;
729 } else if (len > 0) {
730 printf("%s = ", prop);
731 print_data (nodep, len);
732 printf("\n");
733 return 0;
734 } else {
735 printf ("libfdt fdt_getprop(): %s\n",
736 fdt_strerror(len));
737 return 1;
738 }
739 }
741 /*
742 * The user passed in a node path and no property,
743 * print the node and all subnodes.
744 */
745 while(level >= 0) {
746 tag = fdt_next_tag(working_fdt, nodeoffset, &nextoffset);
747 switch(tag) {
748 case FDT_BEGIN_NODE:
749 pathp = fdt_get_name(working_fdt, nodeoffset, NULL);
750 if (level <= depth) {
751 if (pathp == NULL)
752 pathp = "/* NULL pointer error */";
753 if (*pathp == '\0')
754 pathp = "/"; /* root is nameless */
755 printf("%s%s {\n",
756 &tabs[MAX_LEVEL - level], pathp);
757 }
758 level++;
759 if (level >= MAX_LEVEL) {
760 printf("Nested too deep, aborting.\n");
761 return 1;
762 }
763 break;
764 case FDT_END_NODE:
765 level--;
766 if (level <= depth)
767 printf("%s};\n", &tabs[MAX_LEVEL - level]);
768 if (level == 0) {
769 level = -1; /* exit the loop */
770 }
771 break;
772 case FDT_PROP:
773 fdt_prop = fdt_offset_ptr(working_fdt, nodeoffset,
774 sizeof(*fdt_prop));
775 pathp = fdt_string(working_fdt,
776 fdt32_to_cpu(fdt_prop->nameoff));
777 len = fdt32_to_cpu(fdt_prop->len);
778 nodep = fdt_prop->data;
779 if (len < 0) {
780 printf ("libfdt fdt_getprop(): %s\n",
781 fdt_strerror(len));
782 return 1;
783 } else if (len == 0) {
784 /* the property has no value */
785 if (level <= depth)
786 printf("%s%s;\n",
787 &tabs[MAX_LEVEL - level],
788 pathp);
789 } else {
790 if (level <= depth) {
791 printf("%s%s = ",
792 &tabs[MAX_LEVEL - level],
793 pathp);
794 print_data (nodep, len);
795 printf(";\n");
796 }
797 }
798 break;
799 case FDT_NOP:
800 printf("%s/* NOP */\n", &tabs[MAX_LEVEL - level]);
801 break;
802 case FDT_END:
803 return 1;
804 default:
805 if (level <= depth)
806 printf("Unknown tag 0x%08X\n", tag);
807 return 1;
808 }
809 nodeoffset = nextoffset;
810 }
811 return 0;
812 }
814 /********************************************************************/
816 U_BOOT_CMD(
817 fdt, 255, 0, do_fdt,
818 "flattened device tree utility commands",
819 "addr <addr> [<length>] - Set the fdt location to <addr>\n"
820 #ifdef CONFIG_OF_BOARD_SETUP
821 "fdt boardsetup - Do board-specific set up\n"
822 #endif
823 "fdt move <fdt> <newaddr> <length> - Copy the fdt to <addr> and make it active\n"
824 "fdt resize - Resize fdt to size + padding to 4k addr\n"
825 "fdt print <path> [<prop>] - Recursive print starting at <path>\n"
826 "fdt list <path> [<prop>] - Print one level starting at <path>\n"
827 "fdt set <path> <prop> [<val>] - Set <property> [to <val>]\n"
828 "fdt mknode <path> <node> - Create a new node after <path>\n"
829 "fdt rm <path> [<prop>] - Delete the node or <property>\n"
830 "fdt header - Display header info\n"
831 "fdt bootcpu <id> - Set boot cpuid\n"
832 "fdt memory <addr> <size> - Add/Update memory node\n"
833 "fdt rsvmem print - Show current mem reserves\n"
834 "fdt rsvmem add <addr> <size> - Add a mem reserve\n"
835 "fdt rsvmem delete <index> - Delete a mem reserves\n"
836 "fdt chosen [<start> <end>] - Add/update the /chosen branch in the tree\n"
837 " <start>/<end> - initrd start/end addr\n"
838 "NOTE: Dereference aliases by omiting the leading '/', "
839 "e.g. fdt print ethernet0."
840 );